LPC微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Microcontrollers Knowledge Base

讨论

排序依据:
LPC4088 Closed Payment Loop Demo - Compiling the software & flashing the board After connecting the three boards together, it's time to compile the software and flash it onto the board. To do so, please follow below steps. Download the software.​​ Unzip the software. Open the Keil Multi-Project workspace by opening the file .\LPC4088 POS Demo\Project_BlueboardPOS_Workspace.uvmpw. Note: Keil version V.4.54 or higher is required to open the workspace correctly. If you do not meet this requirement, an error will be shown when opening the workspace. Compile project "CDL" by right-clicking on the CDL project and selecting option "Set as Active Project" (1). Next, click on the "Rebuild" button (2) Repeat Step 4) for the 4 remaining projects (BSP, emWinlib, NxpRdLib_PublicRelease, Project_BlueboardPOS). Connect the Keil ULINK2 debugger to the baseboard (J8). If any other debugger than the Keil ULINK2 is used, the Keil project should be changed to use this other debugger. Power-up the board. Although the Embedded Artists base-board can be powered by a USB connection, it is advisable to use the power-jack because of the high-power consumption of the 7" LCD. Powering the board by USB may result in incorrect behavior. With project "Project_BlueboardPOS" set as active project, click on the "Load" button ( ). This will load the compiled POS demo to the FLASH. Proceed to "Running the demo"​
查看全文
#emc‌ #读缓冲‌ #清洗‌
查看全文
LPC4088 Closed Payment Loop Demo - Running the demo Directly after programming the FLASH has finished, or after power-up, the demo is ready to use. The following screen will be presented: In order to use the demo, first the Mifare Classic card must be initialized. This can be done by holding the card in-range of the RFID antenna and pushing the center button of the Embedded Artists base-board. If successful, a confirmation message is shown for half a second. Next, credit must be added to the card. This is done by again holding the card in-range of the RFID antenna, but now pushing the joystick to the top-position (towards the edge of the board). Every time the joystick is pushed to the top-position, $10 will be added to the card. If successful, a confirmation message is shown for half a second after pressing the joystick. The credit can be queried by pressing the "Query Card" button. Now that the card is initialized and charged, products can be purchased. By pushing the product-buttons in the 3x3 grid, products can be selected. Every time a product is selected, it is added to the listbox and the total cost is updated. Upon pressing "Checkout", the credit available on the card is read-in, the total cost is subtracted and the new credit is written back to the card. A confirmation of this action will be shown.
查看全文
Demo demonstrate how to use EMC to connect with external SDRAM.
查看全文
LPC4088 Closed Payment Loop Demo - Connecting the boards together In order to use the demo, the three boards (Embedded Artists Base Board, LPC4088 OEM module, CLRC663 Blueboard) must be connected together. Please follow below steps to accomplish this. 1) Place the LPC4088 OEM module in the baseboard. 2) Secure the 7" LCD board ontop of the baseboard using the supplied plastic spacers. Connect the two boards electrically together by using the supplied flatcable. 3) Connect the Blueboard to the base board. This is done by 8 wires and a USB-A to USB Mini-B cable. The USB connecting is only used for +5V and GND, not for data. For the 8 wire conenctions, please refer to the table below. EA Baseboard Blueboard Function USB UBS 5V supply / GND +3V3, [J4] 2 3V3 3.3V supply GPIO37, [J5] 23 P2.4 CLRC663 Interface Select0 GPIO40, [J3] 28 P2.5 CLRC663 Interface Select1 GPIO38, [J3] 27 P0.3 CLRC663 Reset I2C-SDA, [J5] 25 SDA SDA I2C-SCL, [J5] 26 SCL SCL - P2.0 CLRC663 I 2 C address, connect to GND - P2.1 CLRC663 I 2 C address, connect to GND Proceed to "Compiling the software & flashing the board".
查看全文
lpcopen. uart  #ring_buffer
查看全文
AN12037 is a commonly adopted solution among LPC users when USB DFU Secondary Bootloader. However when customers run the demo code, they would find their PCs has problem of recognizing LpcDevice. Scenario 1: “ LpcDevice flashes in Device Manager in a very short time then disappear for ever… “ Scenario 2: “ Device Manager can’t recognize LpcDevice…”     This is because the default demo code set DFU device only exist in 5 seconds. User must type dfu command ( dfu-util.exe -l ) very fast before de-initialize USB     So we suggest modify the code to increase the DFU device existence time. Change if ( dwSysTicks > 5 )‍ to if ( dwSysTicks > 30 )‍   Theoretically, the DFU existance time increases to 30 seconds. Thus we can have enough time slot to type DFU command.
查看全文
https://community.nxp.com/community/general-purpose-mcus/lpc/blog/2020/06/15/lpc55s69-powerquad-part-1-a-great-solution-for-the-industrial-iot-and-smart-metering 
查看全文
LPCXpresso54608 development board up and running out of the box with our unified software development kit (SDK)!
查看全文
#ISP‌ #bootrom‌ memremap‌
查看全文