LPC Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Microcontrollers Knowledge Base

Discussions

Sort by:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2019/02/26/lpc55xx-multicore-applications-with-mcuxpresso-ide
View full article
#emc‌ #读缓冲‌ #清洗‌
View full article
Demo demonstrate how to use EMC to connect with external SDRAM.
View full article
LPC4088 Closed Payment Loop Demo - Connecting the boards together In order to use the demo, the three boards (Embedded Artists Base Board, LPC4088 OEM module, CLRC663 Blueboard) must be connected together. Please follow below steps to accomplish this. 1) Place the LPC4088 OEM module in the baseboard. 2) Secure the 7" LCD board ontop of the baseboard using the supplied plastic spacers. Connect the two boards electrically together by using the supplied flatcable. 3) Connect the Blueboard to the base board. This is done by 8 wires and a USB-A to USB Mini-B cable. The USB connecting is only used for +5V and GND, not for data. For the 8 wire conenctions, please refer to the table below. EA Baseboard Blueboard Function USB UBS 5V supply / GND +3V3, [J4] 2 3V3 3.3V supply GPIO37, [J5] 23 P2.4 CLRC663 Interface Select0 GPIO40, [J3] 28 P2.5 CLRC663 Interface Select1 GPIO38, [J3] 27 P0.3 CLRC663 Reset I2C-SDA, [J5] 25 SDA SDA I2C-SCL, [J5] 26 SCL SCL - P2.0 CLRC663 I 2 C address, connect to GND - P2.1 CLRC663 I 2 C address, connect to GND Proceed to "Compiling the software & flashing the board".
View full article
AN12037 is a commonly adopted solution among LPC users when USB DFU Secondary Bootloader. However when customers run the demo code, they would find their PCs has problem of recognizing LpcDevice. Scenario 1: “ LpcDevice flashes in Device Manager in a very short time then disappear for ever… “ Scenario 2: “ Device Manager can’t recognize LpcDevice…”     This is because the default demo code set DFU device only exist in 5 seconds. User must type dfu command ( dfu-util.exe -l ) very fast before de-initialize USB     So we suggest modify the code to increase the DFU device existence time. Change if ( dwSysTicks > 5 )‍ to if ( dwSysTicks > 30 )‍   Theoretically, the DFU existance time increases to 30 seconds. Thus we can have enough time slot to type DFU command.
View full article
lpcopen. uart  #ring_buffer
View full article
LPC4088 Closed Payment Loop Demo - Running the demo Directly after programming the FLASH has finished, or after power-up, the demo is ready to use. The following screen will be presented: In order to use the demo, first the Mifare Classic card must be initialized. This can be done by holding the card in-range of the RFID antenna and pushing the center button of the Embedded Artists base-board. If successful, a confirmation message is shown for half a second. Next, credit must be added to the card. This is done by again holding the card in-range of the RFID antenna, but now pushing the joystick to the top-position (towards the edge of the board). Every time the joystick is pushed to the top-position, $10 will be added to the card. If successful, a confirmation message is shown for half a second after pressing the joystick. The credit can be queried by pressing the "Query Card" button. Now that the card is initialized and charged, products can be purchased. By pushing the product-buttons in the 3x3 grid, products can be selected. Every time a product is selected, it is added to the listbox and the total cost is updated. Upon pressing "Checkout", the credit available on the card is read-in, the total cost is subtracted and the new credit is written back to the card. A confirmation of this action will be shown.
View full article
https://community.nxp.com/community/general-purpose-mcus/lpc/blog/2020/06/15/lpc55s69-powerquad-part-1-a-great-solution-for-the-industrial-iot-and-smart-metering 
View full article
LPCXpresso54608 development board up and running out of the box with our unified software development kit (SDK)!
View full article