Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
The SAI of Kinetis supports 4 modes:normal mode, network mode, I2S mode, AC97 mode, the documentation give the brief introduction about the 4 modes, give the waveform of the 4 modes.
View full article
I need to connect multi phy device with a single cpu. I want realize a follow hardware (see picture MultiPhys.jpg ). My dubt is if this schematic is correct. I need to send frame either PHY1 or PHY2. My application is like a gateway, it sends messages to network in selective way ( and it receives from every PHYs device ). Is it possible connect many PHY device with one RMII bus? what is the correct way to connect many PHY device on RMII bus? Anyone knowns documents that describe multi Phy configurations ?
View full article
As most of people familiar with FRDM-K64F which is a bit old but it is still a hot device in the market. This document focused on the ADC measurement to verify the deviation. In general, the sample code were modified /come with MCUXpresso SDK, which is an ADC polling example. ADC reading was done by two ways: 1) Polling the status register of ADC conversion complete flag until ADC conversion is done. 2) CPU core is in sleep right after ADC conversion is started by software trigger. Interrupt is generated when ADC conversion is done and CPU core wakes up by this interrupt. The value of ADC reading is measured 5000 times. And, it is averaged, also calculate max/min value. Finally, the standard deviation is calculated based on the 5000 measured value. PRINTF is a terminal console and print out by semi-hosting. Interrupt method or polling method can been selected by the define of INTERRUPT or POLLING. #define INTERRUPT 0   //ADC conversion wait for “INTERRUPT” should be defined to 1 #define POLLING 1   //ADC conversion wait for “POLLING” should be defined to 1
View full article
Hi: Kinetis's ADC have no multi channels sequence sampling function, compared with LPC's ADC. But we could use DMA for such case, attached are two demos: 1.multi_channels_edma_ADC_DMA_SW_TRIG Description: use SW trigger DMA transfer for 6 ADC channels, DMA ch0 is for ADC channels transfer, DMA ch1 is for ADC sample result transfer in DMA ch1 ISR, report ADC sample are done; 2.multi_channels_edma_ADC_DMA_LPIT_HW_TRIG Description: use LPIT timely trigger DMA transfer for 6 ADC channels, DMA ch0 is for ADC channels transfer, DMA ch1 is for ADC sample result transfer in DMA ch1 ISR, report ADC sample are done; but LPIT could trigger continuously without SW engage.
View full article
This document introduces basic usage of NVIC based on Freescale Kinetis. please see the attached document for details.
View full article
MAPS-KS22 Board Introduction: MAPS boards are localization evaluation boards for Chinese customers. The MAPS boards are suitable for NXP MCU product, with low coat, more flexibility and easy-copy features, which matching with local customer requirements and better for learning and product evaluation. MAPS board includes four parts board, which are MCU Board, Peripheral Board, Application Board & Socket Board. The naming of MAPS are using the four-part board initial letter. MCU board is NXP Kinetis MCU based evaluation main board with chip related special module interface/device, such as graphic LCD/ENET interface and etc. The MCU board fan out all MCU pins as test points for measuring. The MCU board also provide two 32-pin socket to connect external peripheral board or application board. Peripheral Board collects more general device into one board and using two 32-pin socket connects with MCU board. The MAPS-Dock is the first peripheral board, which with below configuration: Micor-SD card slot; six touch pads; USB FS interface; IrDA transceiver; one SPI Interface (SPI-Flash); two UART interface; four buttons; one I2S interface (audio codec); one CAN interface; two potentionmeter; one DAC output interface; 128x64 monochrome LCD; one 5-way button. It also with SWD debugger on board and USB CDC virtual COM. Application Board designed for special applications, such as motor control, IOT, Smart Home, Wireless Charger and etc. Socket Board provides interface for FreeDOM boards/Arduino boards/Customer defined boards. MAPS-KS22 board MCU board for KS22 chip evaluation. KS22 MCU is based on the ARM® Cortex®-M4 core with 120MHz MCUs with FPU, offering full-speed USB 2.0 OTG, in addition to other features like USB crystal-less functionality. MAPS-KS22 oobe demo porting process MAPS-KS22 oobe demo is based KSDK V1.0, which will show Freescale LOGO on the SPI color LCD and meanwhile use FlexIO I2S to play an audio on microphone. Step1: visit Kinetis Expert website (http://kex.nxp.com/en/welcome) to download MAPS-KS22 KSDK V2.0 software: Step2: download [Kinetis SDK Project Generator Tool] from below link and generate oobe demo project based on MAPS-KS22 SDK V2.0 software: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=KSDK-PROJECT-GENERATOR-TOOL&appType=file1&location=null&DOWNLOAD_ID=null Step 3: After that, open the oobe project, which located at default path: C:\Freescale\SDK_2.0_MAPS-KS22\boards\mapsks22\user_apps\oobe\iar The default project is based on <hello-world> demo, it need to add LED control code. Those part of code could be found at <main.c> file and related pin muxing code at <pin_mux.c> file. Step 4: Modify ili9341 related driver: For the oobe project with two major functions, the first one is to display Freescale LOGO at LCD. The MAPS-KS22 board graphic LCD is using ili9341 TFT LCD driver with SPI interface with KS22 chip. The previous oobe project is using GPIO pins emulate SPI communication, we will make the similar application with KSDK V2.0 driver. Most modification based on the GPIO pins control. Please check below code at <ili9341.h> file, which call KSDK V2.0 GPIO driver: #define ILI9341_CS_HIGH()       GPIO_SetPinsOutput(BOARD_LCD_CS_GPIO, 1U << BOARD_LCD_CS_PIN) #define ILI9341_CS_LOW()        GPIO_ClearPinsOutput(BOARD_LCD_CS_GPIO, 1U << BOARD_LCD_CS_PIN) #define ILI9341_CLK_HIGH()      GPIO_SetPinsOutput(BOARD_LCD_CLK_GPIO, 1U << BOARD_LCD_CLK_PIN)  #define ILI9341_CLK_LOW()       GPIO_ClearPinsOutput(BOARD_LCD_CLK_GPIO, 1U << BOARD_LCD_CLK_PIN) #define ILI9341_MOSI_HIGH()     GPIO_SetPinsOutput(BOARD_LCD_MOSI_GPIO, 1U << BOARD_LCD_MOSI_PIN) #define ILI9341_MOSI_LOW()      GPIO_ClearPinsOutput(BOARD_LCD_MOSI_GPIO, 1U << BOARD_LCD_MOSI_PIN)      #define ILI9341_MISO_HIGH()     GPIO_SetPinsOutput(BOARD_LCD_MISO_GPIO, 1U << BOARD_LCD_MISO_PIN) #define ILI9341_MISO_LOW()      GPIO_ClearPinsOutput(BOARD_LCD_MISO_GPIO, 1U << BOARD_LCD_MISO_PIN) And it also need to add ili9341 control pin muxing initialization code at <pin_mux.c> file. Step 5: We could modify the Freescale logo with new NXP logo, which could using [Embedded GUI Conversion Utility3.0] tool. This tool could be downloaded from below link:  http://tinyurl.com/eGUI-Convert  The conversion result of the graphic data is 16-bit array, which need be transfer to 8-bit array. After that, compile and download the image to the board, it with below result: Step 6: The oobe demo provide another function to play music with MAPS-DOCK board WM8960 codec chip, then using headphone will hear the sound. For the KS22 with FlexIO module, the demo will use FlexIO emulating I2S bus to transfer data to WM8960 codec chip. About I2S bus MCLK clock source, the MAPS-KS22 provide two selection, one is using TPM1_CH1 pin, the other one is using I2S0_MCLK pin with JP5 jumper selection. In oobe demo, we use TPM1_CH1 pin to generate 12MHz MCLK clock with TPM module output compare mode. Related code, please refer below tpm_init_output_compare() function at <main.c> file: //enable clock gating of tpm1 CLOCK_EnableClock(kCLOCK_Tpm1); //set TMP output compare mode TPM_SetupOutputCompare(BOARD_TPM_BASEADDR, BOARD_TPM_CHANNEL, kTPM_ToggleOnMatch, 1U); BOARD_TPM_BASEADDR->MOD = 0x1; TPM_StartTimer(BOARD_TPM_BASEADDR, kTPM_SystemClock);   //TPM counter increments on every TPM counter clock Step 7: WM8960 is a stereo CODEC chip provide I2C port for chip configuration. There need to initialization the WM8960 chip before using it with related driver <wm8960.c> & <wm8960.h> files. The MAPS-KS22 board using LPI2C0 module connects with WM8960 chip, so there need to port using LPI2C driver of KSDK V2.0 and modify the WM8960 driver related. The LPI2C module initialization code located at <main.c> with lpi2c_master_init() function. The WM8960 driver major modification with WOLFSON_WriteReg() function at <wm8960.c> file, calling the LPI2C driver of KSDK V2.0 with below code:  wolfson_status_t WOLFSON_WriteReg(uint8_t reg, uint16_t val) {       uint8_t cmd,buff;        status_t ret;        cmd = (reg << 1) | ((val >> 😎 & 0x0001);    // register address        buff = val & 0xFF;     //data        reg_cache[reg] = val;      // copy data to cache         uint8_t data[2];         data[0] = cmd;         data[1] = buff;         //start lpi2c tx operation                   ret = LPI2C_MasterStart(LPI2C0, WM8960_I2C_ADDR, kLPI2C_Write);           // send two data with register address and related value          ret = LPI2C_MasterSend(LPI2C0, data, 2);                //stop lpi2c tx operation                  ret = LPI2C_MasterStop(LPI2C0);               if(ret != kStatus_Success)          {  return kStatus_WOLFSON_I2CFail;  }          return kStatus_WOLFSON_Success; } After WM8960 chip driver modification, there could call related driver to initialize WM8960 chip and configure the communication interface with I2S bus. Following steps focus on how to transfer data to WM8960 codec with I2S bus. Step 8:  The FlexIO modul will simulate I2S bus call FlexIO_I2S_MasterInit() function in <main.c> file to initialize FlexIO module as I2S master. There using FXIO0_D4 pin as I2S bit clock pin, using FXIO0_D5 pin as I2S Transmit pin and using FXIO0_D6 pin as I2S Transmit Frame Sync pin. KSDK V2.0 provide FlexIO for I2S driver located at <fsl_flexio_i2s.h> file. Step 9: There will call eDMA with FlexIO module to reduce the core work load during the I2S data transfer. It will initialize the eDMA & DMAMUX modules for FlexIO. Related code located at <main.c> file with ConfigDMAforFlexIOI2STX() function: void ConfigDMAforFlexIOI2STX(void) { EDMA_GetDefaultConfig(&dmaConfig); EDMA_Init(EXAMPLE_DMA, &dmaConfig); EDMA_CreateHandle(&dmaHandle, EXAMPLE_DMA, EXAMPLE_CHANNEL); DMAMUX_Init(DMAMUX0); DMAMUX_SetSource(DMAMUX0, EXAMPLE_CHANNEL, EXAMPLE_DMA_SOURCE); DMAMUX_EnableChannel(DMAMUX0, EXAMPLE_CHANNEL); }    Step 10: KSDK V2.0 software provides FlexIO I2S eDMA driver located at <fsl_flexio_i2s_edma.c> file, with below codes to initialize FlexIO I2S master DMA handler and to configure the sample rate & audio data format to be transferred: FLEXIO_I2S_TransferTxCreateHandleEDMA(&base, &txHandle, callback, NULL, &dmaHandle); FLEXIO_I2S_TransferSetFormatEDMA(&base, &txHandle, &format, 48000000); Step 11: After above preparation, following action will start to transfer music data to WM8960 codec with below code. When the music data transfer finished, the callback function will be called to start next round data transferred. Then we could hear the sound with endless loop. static void callback(FLEXIO_I2S_Type *i2sBase, flexio_i2s_edma_handle_t *handle, status_t status, void *userData) {   // Initiate FlexIO I2S transfer again after previous transfer finished  FLEXIO_I2S_TransferSendEDMA(&base, &txHandle, &xfer); } About more detailed oobe demo software info, please check attached file. The default oobe demo located path is: C:\Freescale\SDK_2.0_MAPS-KS22\boards\mapsks22\user_apps\oobe
View full article
       FreeRTOS is a high quality, risk free, supported, free RTOS, and now it is already successful to porting more 35 architectures. As a popular RTOS, more and more embedded engineers considering it for their next project.        Next, I’m going to show you the steps of creating a MAPS-K22 FreeRTOS demo by IAR and I’ve also attached a template demo and FreeRTOS source code (Fig 1). Fig 1 FreeRTOS source code directories and files     1. Copy the FreeRTOS source code to ~\MAPSK22_SC\Libraries     2. Create FreeRTOS_Source group in the workspace, then add the source code (Fig 2) Fig 2 3. Add an application code in the main.c This is a very simple configuration. It creates two tasks, one software timer, and also uses a button interrupt. The two tasks communicate via a queue. The receiving task toggles the LED3 each time a value is received. Pressing user button K5 generates an interrupt. The interrupt service routine for which resets a software timer, then turn the LED1 on. The software timer has a five second period. The timer will expire when K5 has not been pressed again for a full five seconds. The callback function that executes when the timer expires simply turn the LED1 on again. Therefore, pressing K5 will turn the LED1 on, and the LED1 will remain on until a full five seconds pass without the button being pressed again. 4. Modify the Include Directories 5. Run the FreeRTOS demo After build the modified application code, then run it on MAPS-K22 board (Fig 3) Fig 3 IMPORTANT! Cortex-M FreeRTOS port specific configuration Configuration items specific to this demo are contained in ~\MAPSK22_SC\Libraries\RTOS\config\K22F51212\iar. The constants defined in this file can be edited to suit your application. In particular configTICK_RATE_HZ This sets the frequency of the RTOS tick interrupt. The supplied value of 1000Hz is useful for testing the RTOS kernel functionality but is faster than most applications require. Lowering this value will improve efficiency. configKERNEL_INTERRUPT_PRIORITY and configMAX_SYSCALL_INTERRUPT_PRIORITY See the RTOS kernel configuration documentation for full information on these configuration constants. configLIBRARY_LOWEST_INTERRUPT_PRIORITY and configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY These are equivalents to configKERNEL_INTERRUPT_PRIORITY and configMAX_SYSCALL_INTERRUPT_PRIORITY, but presented in a form suitable for passing into the Freescale NVIC_SetPriority() library function. The NVIC_SetPriority() function expects priorities to be in the range of 0 to 15 - 0 being the highest priority and 15 being the lowest priority.
View full article
Basic explanation of the ADC module. Explicación básica del modulo de ADC.
View full article
    MMA9553L是飞思卡尔的一款计步传感器,本文就如何快速使用该传感器做一个简单介绍。    你可能还见到过MMA955xL, 它与MMA9553L是什么关系呢?简单的来说MMA955xL是一个统称,它包括MMA9550L、MMA9551L、MMA9553L和MMA9559L这几个具体型号,其实这四种传感器在硬件上都是一样的。其内部主要由ColdFire 内核、模拟前端、Flash、IIC和SPI接口等部分组成,原理框图如下图所示:    它们的不同之处在于内部的Firmware不同,Firmware在芯片出厂时就已经固化在芯片里面了,不同的Firmware对于不同的功能。这里介绍的MMA9553L主要就用作计步器功能。        MMA9553L和MCU之间可以通过IIC接口或者SPI接口通讯,所以使用MMA9553L的首要前提是把MCU的IIC或者SPI调通。接口调通之后就可以来操作此传感器了。这里以IIC为例来说明。附件为参考代码。 测试平台:IAR7.2 + FRDM_KL25Z+FRDM-FXS-MULTI FRDM-FXS-MULTI开发板上带有MMA9553L,将FRDM-FXS-MULTI开发板和FRDM_KL25Z连接在一起就可以使用了。     下面分析一下源代码:        首先是调用初始化函数pedometer_init(),此函数主要调用以下几个函数:      pedometer_write_config();       // config     pedometer_enable();         // enable pedometer     pedometer_int0_enable();    // enable INT_O pin     pedometer_active();         // active MMA9553 pedometer_wakeup();   // wakeup 在此重点分析前两个函数。第一个函数 pedometer_write_config(),该函数的具体实现如下: void pedometer_write_config(void) {     unsigned char Buf[]={0x15,0x20,0x00,0x10,                            0x0C,0xE0,                            0x13,0x20,                            0x00,0x96,                            0x60,0x50,                            0xAF,0x50,                            0x04,0x03,                            0x05,0x01,                            0x00,0x00};     dvMMA9553_Write(MMA9553_Slave_Addr, MMA9553_Sub_Addr, Buf, 20); } 此函数很简单,就是通过IIC给9553发送一条命令,命令的内容Buf数组中的20个字节    的数据。 dvMMA9553_Write()函数的第一个参数代表MMA9553L的地址,为0x4C。datasheet中有说明。 #define MMA9553_Slave_Addr  0x4C dvMMA9553_Write()函数的第二个参数代表寄存器地址,为0x00。 #define MMA9553_Sub_Addr    0x00 发送的这一串命令:0x15,0x20,0x00,0x10,0x0C,0xE0,0x13,0x20,0x00,0x96,0x60,0x50,0xAF,0x50,0x04,0x03,0x05,0x01,0x00,0x00 具体是什么含义呢? 0x15:表示Application ID,计步器的Application ID就是0x15 0x20:表示这条命令是Write Config command,即这条命令是用来写Configuration 寄存器的。 0x00:表示配置寄存器的偏移地址。 0x10:表示要写16字节的内容。 0x0C,0xE0,0x13,0x20,0x00,0x96,0x60,0x50,0xAF,0x50,0x04,0x03,0x05,0x01,0x00,0x00 这16字节就是写入配置寄存器中的具体内容。 配置寄存器共用8个,分别是Sleep Minimum register,Sleep Maximum register,Sleep Count Threshold register,Configuration/Step Length register,Height/Weight register,Filter register,Speed Period/Step Coalesce register,Activity Count Threshold register,每个寄存器为16 bit(2 字节),所以总共16字节。 第二个函数 pedometer_enable(),该函数的具体实现如下: void pedometer_enable(void) {     unsigned char Buf[]={0x17,0x20,0x05,0x01,0x00};     dvMMA9553_Write(MMA9553_Slave_Addr, MMA9553_Sub_Addr, Buf, 5); } 这次写入的命令是0x17,0x20,0x05,0x01,0x00 0x17:表示Application ID 0x20:表示这条命令是Write Config command 0x05,0x01,0x00 这三个表示在偏移地址0x5处,写入一个字节的数据0x00 其他几个函数也类似,都是写入一条命令,对某种Application的配置寄存进行设置。 初始化完了,现在就可以读取步数了。 通过调用pedometer_main() 函数就可以读取到步数。 该函数的实现如下: void pedometer_main(void) {     unsigned char Buf[20];     pedometer_cmd_readstatus(); // read  status      while(1)         {            dvMMA9553_Read(MMA9553_Slave_Addr, MMA9553_Sub_Addr, Buf, 2);            if(Buf[1]==0x80)            {               dvMMA9553_Read(MMA9553_Slave_Addr, MMA9553_Sub_Addr, Buf, 16);               break;             }         }         m_status.StepCount = Buf[6] * 256 + Buf[7];         m_status.Distance  = Buf[8] * 256 + Buf[9];         m_status.Calories  = Buf[12] * 256 + Buf[13]; } 主要调用了两个函数,一是pedometer_cmd_readstatus(),这个函数的实现如下: void pedometer_cmd_readstatus(void) {     unsigned char Buf[]={0x15,0x30,0x00,0x0C};     dvMMA9553_Write(MMA9553_Slave_Addr, MMA9553_Sub_Addr, Buf, 4 ); } 它是发送了0x15,0x30,0x00,0x0C这条命令 0x15:表示Application ID 0x30:表示Read Status command 0x00:表示偏移地址 0x0C:表示需要读的字节数为12 之后调用dvMMA9553_Read()函数,通过IIC读取16字节的数据(4字节起始信息+12字节status register内容),读到的16字节数据如下: Step count register寄存器如下,通过其值可以算出步数来。    另外还可以读取三轴加速度的值,过程与读取步数是类似的,也是先写配置寄存器,然后再读取状态寄存器。   总的来说操作MMA955L的关键搞清楚有两个重要的寄存器:配置寄存器和状态寄存器。配置寄存器可读可写,状态寄存器只可读。 写配置寄存器,格式是: APP_ID+0x20+offset+number+number字节的内容 读配置寄存器,格式为: 先发送:APP_ID+0x10+offset+number, 再通过IIC读number+4字节的内容,前4字节为起始信息。 读状态寄存器,格式为: 先发送:APP_ID+0x30+offset+number,再通过IIC读number+4字节的内容,前4字节为起始信息。 读Command 回的内容如下:
View full article
From K61/K64/K66 reference manual/ datasheet, it is mentioned that the SDHC clock can be set up to 50MHz. But from the SDHC timing spec, SDHC output timing violate SD specification if SDHC clock is 50MHz, because output delay (SD6 tOD) is max 6.5ns.  SD specification require setup time at SD card 6ns, then output delay should less than 4 ns if SDHC clock is 50MHz. In other word, according to the SD card specification, input set-up time is minimum 6ns, then maximum of SD6 should be 4ns in order to support 50 MHz clock frequency. So we recommend customer to drop the SDHC clock frequency to 40MHz, then the 6.5ns output valid time will allow them to meet the 6ns setup requirement for the card.
View full article
My customer wanted to use K60 in his design but he only has the Keil IDE, so I helped to port some examples in KINETIS_SC for him as a starting point. The attachment is my porting work, which also includes a exe file to create new keil project. You may refer to "keil\build\uv4\make_new_project_keil.exe" for details. Hope that helps, B.R Kan
View full article
Hi,, Can anyone please post the code for SPI (Serial peripheral interface) using MK22D5.h....I tried doing using processor expert but im getting errors in the main program..please post the code for SPI Thank you
View full article
       RSA is a major cryptosystem in the public key cryptography. It is wildly used nowadays.  But why are we interested in elliptic    curve cryptography?   1. The smaller parameters can be used in elliptic curve cryptography (ECC) than with  RSA systems at a given security level.       2. In particular, private-key operations (such as signature generation and decryption) for ECC are many times more efficient        than RSA private-key operations.     3. Public-key operations (such as signature verification and encryption) for ECC are more efficient than RSA if a  bigger       encryption exponent e is selected for RSA.           The advantages offered by ECC can be important in environments where processing     power, storage, bandwidth, or power consumption is constrained.              KL26Z MCU is 48 MHz ARM Cortex-M0+ core, there are only 128K ROM and 16K RAM on chip. When you want to use the    public key cryptography, the elliptic curve cryptography may be a good choice for this low cost MCU.        This example implements a simple ECC certification from PC to USB.  After certification,     USB can get encrypted data from PC and decrypt these data to plain text.   KL26-Freedom : 1.   Open the porject file at folder kecc/build/cw/KECC/kl26_ecc/test   2.  Build the image and flush it with OpenSDA.   3. Open the Tera Term and start running image on KL26Z     PC running environment:     1. Install  these packets on PC:         python-2.7.3.msi, pycrypto-2.6.win32-py2.7.exe, pyserial-2.7.win32.exe and pywin32-219.win32-py2.7         2. Connect USB cable to KL26Z Freedom and install the CDC driver with       Freescale_CDC_Driver_Kinetis.inf driver     3. Open the application folder and run the usbkey.py.                 4. If USB admits  PC certification message, then PC can put encrypted data to USB.               This  demo only tested on WIN7 64bit. IF you can't open the CDC port, you need reset the KL26Z freedom board and restart the usbkey.py.     This ECC demo uses a library including some security toolkits for ECC certification.     1. Signature and verify : ECDSA     2. Key exchanging         :ECCRYPT    3.  Digest                         : SHA1    4. Symmetric   cipher     : AES and base64      All tools and codes are in following KECC.zip. Original Attachment has been moved to: kecc.zip
View full article
The Technical University in Brasov (Romania) has set up a Medical Teaching lab featuring the Freescale Tower Kit K53 with Oximeter MED-SPO2 and 2 electrode system EKG MED-EKG. Find below the material associated to this lab led by Prof. Sorin-Aurel Moraru from the Faculty of Engineering. He can be contacted at [email protected] The course is in Romanian and include an overview of the hardware and exercises
View full article
The Kinetis family has abundant low power mode. Customers may confused to figure out the different way to wake up from the low power mode. 1)  In VLPR, VLPW:  the NVIC remains sensitive to interrupts, so any interrupt will be serviced. 2)  In Stop, VLPS:  the device can be waked up by USB wake up interrupt only. 3)  In LLS, VLLSx:  the device won't be able to wake up from any USB source. 4)  LLWU is used to wake up, so customer would able to wake up from any of the available LLWU wake up sources. As for the USB module, there has two different interrupts for a USB resume event. One asynchronous to be able to wake from a low power mode, which is triggered by change in the state of the USB lines. The other is synchronous and is triggered only after 2.5 us of detecting a K state (D+ = 0, D- = 1, for Full Speed). The application is responsible to transition to the low power mode whenever it requires it, and for this purpose it must check the device state as reported by the USB stack. When a suspend condition is detected in the bus, the SLEEP interrupt triggers and the stack changes its state to suspend; then the application will transition to the low power mode. When this SLEEP interrupt occurs, the asynchronous wake interrupt is enabled, and is disabled when it is triggered (this is required by the module to clear the interrupt). In normal conditions, the synchronous resume interrupt or the reset interrupt will be triggered afterwards, causing the stack to transition its state to other than suspend. The application can then know that communication is active again and will avoid entering the low power mode again.
View full article
Hello,      Is your clock correctly configured, what is its frequency?   You can monitor some of clocks in K0 MCU by routing it to  PTC3/CLKOUT pin. you can get it easily by selecting desired clock on  SIM_SOPT2[CLKOUTSEL] register and configuring PTC3 for CLKOUT function.   For example to monitor  1 KHz 1 low power osillator   LPO, ---------------------------------------------------------------------------------------------------------------------------- /*  ClockOutput options */ #define CLOCKOUT_FLASH_CLOCK    2 #define CLOCKOUT_LPO                       3 #define CLOCKOUT_MCGIRC                4 #define CLOCKOUT_RTC32KHZ            5 #define CLOCKOUT_OSCERCLK0       6 /* Configure clock output option according to  */               SIM_SOPT2 = SIM_SOPT2_CLKOUTSEL(CLOCKOUT_LPO); /* Configure PTC3 as clock output) */              PORTC_PCR3 = PORT_PCR_MUX(5);   //CLKOUT function selected on PTC3 ------------------------------------------------------------------------------------------------------------------------------------                 In attached document you can find captures of all clock options,  and notes on what need to be configured to get the clock output.                        Note:       Please note that Clock out (CLKOUT) on PTC3 is not currently shown in Signal Multiplexing and Signal Descriptions of RM.  It is already reported and will be fixed on next release of Reference Manual/Data sheet.
View full article
This is a presentation used to explain the Low Power Timer adapted by Vicente Gómez, Freescale TIC. LPTMR Module Explanation. Connection Diagram. Operation Modes Hands-On Configure a timer so that it generates an interruption every x time.  Explicación del Low Power Timer presentado por Vicente Gómez, Freescale TIC.- Explicación de los Modulos LPTMR . Diagrama de conexiones. Modos de operación Hands-on Configurar un timer para que genere una interrupción cada X tiempo.
View full article
Kinetis KV10 chip is the entry point of the V Series product, which are designed for a wide range of BLDC, PMSM and ACIM motor control and digital power conversion applications. KV10 is using ARM Cortex-M0+ core, the core frequency could up to 75MHz. And KV10 provides various feature powerful modules, such as ADC modules (2x 16-bit ADCs with two capture and hold circuits and up to 1.2 MS/s samples rate in 12-bit mode — simultaneous measurement of current and voltage phase, reduced jitter on input values improving system accuracy 12-bit mode) and DMA modules (4-channel DMA — reduced CPU loading for improved application performance). The demo is using PDB hardware trigger two ADC modules conversion (12-bit single-ended mode) at the same time; the two ADC modules will trigger each related DMA channels to transfer ADC result to ADC buffer located at SRAM (start from 0x2000_0000) when finish each conversion. The ADC DMA channel 0 will link to trigger DMA channel 2 to transfer ADC result from ADC result buffer to SPI FIFO. When DMA channel 2 transfer done, in related interrupt service routine will software trigger PDB to start the next round of ADC conversion. Below is the processing chart: For the customer requires to transfer 9 ADC conversion results out (5 of ADC0 and 4 of ADC1) , the ADC buffer need interleaved storage result from two ADC modules. Below diagram shows the detailed info: Below is the test result and test environment. It will take almost 15.4us to get and transfer all 9 12-bit ADC conversion results. The demo code is attached. The project is based on TWR-KV10Z32 Sample Code Package could be downloaded from here. Wish it helps.
View full article
The DOC focuses on how to access SDRAM based on K65 SDRAM controller, it describes the hardware connection especially the address connection, the SDRAM controller initialization,the code to access SDRAM.
View full article