Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
Recently I did a porting based on AN4370SW for a customer to support TWR-K20D72M, and with some modification in source code, header file and link file as well, it works well as expected. The following simple describes what I have done: 1.Copy the project file folder for K20D50M "AN4370SW\Source\Device\app\dfu_bootloader\iar_ew\kinetis_k20" and rename is as "kinetis_k20d70m" 2.Change the target settings as well as the flash loader. 3. Replace the header file for K20D50M and include it in derivative.h. The header file for K20D72M can be found from KINETIS_72MHz_SRC(http://cache.freescale.com/files/32bit/software/KINETIS_72MHz_SRC.zip?fpsp=1&WT_TYPE=Lab%20and%20Test%20Software&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=zip&WT_ASSET=Downloads&sr=9) 4.Modify the interrupt table in cstartup_M.s, which is more likely a K60's vertor table. 5.Search the code related with the macro "MCU_MK20D5", and add similar code snippet for K20D72M , You may easily find them by search the keyword "MCU_MK20D7". That code parts include initialization for MCG, and PIT0 and USB interrupt enablements, some definition in bootloader.h . 6. Copy the link file from K20D50M, and modify the PFLASH size,SRAM size and DFLASH size as shown below: Perform MassErase before programming . and then you may press the SW1 on TWR-K20D72M to select which mode to enter after download the application firmware: pressing SW1 to enter bootloader mode and releasing it to enter application mode. 7. Build image for this DFU bootloader. Actually the bareboard projects in KINETIS_72MHz_SRC can be used for that purpose, and only link file needs some modification to put the image starting from 0xA000, since exception table redirection has already been done in these projects. after that, user needs change some settings in the CW projects to use the new link file: and generate S19 file as the output as well as the map file: after compiling , you will have a xxx.afx.s19 file, but that is not the final format, we still need to transform it to bin format, and it can be done by a small tool in "C:\Program Files\Freescale\CW MCU v10.3\MCU\prog" There are some settings for this tool to transform the S19 file, by clicking Burner->Burner Dialog, you will see some option views, please set them as below: Referring to the above figure, maybe you would wonder how to set up the Origin and Length field, actually Origin is the value where the image starts from just as the link file specified , and Length is calculated by the results from the map file. Please refer to the following figure for details. 0x3550 = 0x1c90 + 0x18c0. I also attached the burner's configuration file and image link file as well as the image for reference. Please copy the link file in "KINETIS_72MHz_SRC\build\cw\linker_files". Please kindly refer to the attachment for more details. Hope that helps, B.R Kan
記事全体を表示
The installation file containing MKM34Z256 training examples programmed using Kinetis-M bare metal drivers and compiled using IAR EWARM 7.40.1. These examples explain programming steps for GPIO, Low Power Timer, Sigma Delta ADC, Memory Math Arithmetic Unit, and LCD on-chip peripherals. In addition, you will learn how to create simple FreeRTOS and 1-phase power meter applications. All examples including their handouts will be installed on your PC in c:\Freescale\KM34Z75_EXAMPLES subfolder. For more information about each example, please refer to its handout.
記事全体を表示
1. Overview BLE beacon is a common use of low power Bluetooth and it broadcasts advertisement at some interval. Freescale BLE beacon demo use Freescale Kinetis KL16 low power MCU and EMC EM9301 Bluetooth controller to implement a beacon reference design. Freescale BLE beacon features low power consumption of an average cost of 50uA with 600ms interval. Freescale Kinetis KL16 coordinates with EM9301 through SPI interface. View attachment to learn more
記事全体を表示
Archive file of the Kinetis-M bare-metal drivers and software examples REV 4.1.5 - this version is not yet available @ nxp.com. Release notes 4.1.5 (Apr.22,2016): Added configuration structures for watchdog timer operating in debug mode. Included IAR EWARM 7.60.1 project templates. Modified LLWU Pin Falling Edge Wakeup example. Please refer to How to download and install KM Bare-metal divers
記事全体を表示
Hi Community members! Here you can find the source code of the MSD Host Bootloader implemented on the AN4368 document using the TWR-K70F120M and CodeWarrior 10.6 and a document that describes the migration process of the original source code for the TWR-K60N512 to a TWR-K70F120M and the steps to use the application. Attached you will find a image.s19 file created to be used with the bootloader application as an example. :smileyinfo: This document and code are intended to demonstrate the use of the AN4368 source code on a 120 MHz device and CodeWarrior 10.6 but is not replacing the work done on the application note. I hope this can be helpful for you! Best Regards, Adrian :smileyplus: If it was useful for you do not forget to click on the Like button. It would be nice!
記事全体を表示
Dear all :      I would like to share an IoT application note to you. The note will help us to setup a FRDM-K64F to connect to Microsoft Azure and get alarm message from Azure. Detail please refer to attachment. Demonstration : IoT client (FRDM-K64F) report data to Cloud (Microsoft Azure) IoT client receive data from Cloud Could computing IoT client data and take action Tools : FRDM-K64F ( http://www.freescale.com/FRDM-K64F ) Device Explorer ( http://aka.ms/iot-hub-how-to-use-device-explorer ) Visual Studio 2015 SSH client ( PuTTY  or Tera Term ) mbed  ( http://www.mbed.com ) Microsoft Azure ( https://azure.microsoft.com )
記事全体を表示
Summary:   This tool is based upon the Audio BiQuad Cookbook Here:   http://www.musicdsp.org/files/Audio-EQ-Cookbook.txt   Very useful for configuring the FRDM-JAM and the MonkeyJam software!     Requirements:   You need a machine with the .net 4.0 Framework (or greater) Installed (Windows 7 or Greater).    If you have issues go here:   Download Microsoft .NET Framework 4 (Standalone Installer) from Official Microsoft Download Center   Instructions:   Just unzip and run the .exe   Please report any problems in the comments section Original Attachment has been moved to: BiQuadFilterView---1.0.0.zip
記事全体を表示
Here you will find both the code and project files for the ADC project. This project configures the ADC to perform single conversions, by default this is performed using a 16 bit configuration. The code uses ADC0, channel 12, once the conversion is finished it is displayed at the serial terminal. Code: #include "mbed.h" AnalogIn AnIn(A0); DigitalOut led(LED1); Serial pc(USBTX,USBRX); float x; int main() {     pc.printf(" ADC demo code\r\n");     while (1)     {     x=AnIn.read();     pc.printf("ADC0_Ch12=(%d)\r\n", x);     wait(.2);     } }
記事全体を表示
        在我们嵌入式工程应用中,中断作为最常用的异步手段是必不可少的,而且在一个应用程序中,一个中断往往是不够用的,多个中断混合使用甚至多级中断嵌套也经常会使用到,而这样就涉及到一个中断优先级的问题。         以我们最熟悉的Cortex-M系列为例,我们知道ARM从Cortex-M系列开始引入了NVIC的概念(Nested Vectors Interrupts Controller),即嵌套向量中断控制器,以它为核心通过一张中断向量表来控制系统中断功能,NVIC可以提供以下几个功能: 1)可嵌套中断支持; 2)向量中断支持; 3)动态优先级调整支持; 4)中断可屏蔽。         抛开其他不谈,这里我们只说说中断优先级的问题。我们知道NVIC的核心工作原理即是对一张中断向量表的维护上,其中M4最多支持240+16个中断向量,M0+则最多支持32+16个中断向量,而这些中断向量默认的优先级则是向量号越小的优先级越高,即从小到大,优先级是递减的。但是我们肯定不会满足于默认的状态(人往往不满足于约束,换句俗话说就是不喜欢按套路出牌,呵呵),而NVIC则恰恰提供了这种灵活性,即支持动态优先级调整,无论是M0+还是M4除了3个中断向量之外(复位、NMI和HardFault,他们的中断优先级为负数,它们3个的优先级是最高的且不可更改),其他中断向量都是可以动态调整的。         不过需要注意的是,中断向量表的前16个为内核级中断,之后的为外部中断,而内核级中断和外部中断的优先级则是由两套不同的寄存器组来控制的,其中内核级中断由SCB_SHPRx寄存器来控制(M0+为SCB_SHPR[2:3],M4为SCB_SHPR[1:3]),外部中断则由NVIC_IPRx来控制(M0+为NVIC_IPR[0:7],M4为NVIC_IPR[0:59]),如下图所示: M0+中断优先级寄存器: M4中断优先级寄存器:         其中M4所支持的动态优先级范围为0~15(8位中只有高四位[7:4]才有效),而M0+所支持的动态优先级范围则为0~3(8位中只有高两位[7:6]才有效),而且秉承着号越小优先级越高的原则(0最高,15或3为最小),同时也间接解释了为什么复位(-3)、NMI(-2)和HardFault(-1)优先级最高的原因,很简单,人家都是负的了,谁还能比他们高,呵呵,而且这三位中复位优先级最高,NMI其次,HardFault最低(这个最低仅限于这三者)。 下面给出个ARM CMSIS库中关于M0+和M4中断优先级设置的API函数NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority)实现供大家来参考: M0+: NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority) {   if(IRQn < 0) {     SCB->SHP[_SHP_IDX(IRQn)] = (SCB->SHP[_SHP_IDX(IRQn)] & ~(0xFF << _BIT_SHIFT(IRQn))) |         (((priority << (8 - __NVIC_PRIO_BITS)) & 0xFF) << _BIT_SHIFT(IRQn)); }  /* set Priority for Cortex-M  System Interrupts */   else {     NVIC->IP[_IP_IDX(IRQn)] = (NVIC->IP[_IP_IDX(IRQn)] & ~(0xFF << _BIT_SHIFT(IRQn))) |         (((priority << (8 - __NVIC_PRIO_BITS)) & 0xFF) << _BIT_SHIFT(IRQn)); }   /* set Priority for device specific Interrupts  */ } M4: void NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority) {   if(IRQn < 0) {     SCB->SHP[((uint32_t)(IRQn) & 0xF)-4] = ((priority << (8 - __NVIC_PRIO_BITS)) & 0xff); } /* set Priority for Cortex-M  System Interrupts */   else {     NVIC->IP[(uint32_t)(IRQn)] = ((priority << (8 - __NVIC_PRIO_BITS)) & 0xff);    }        /* set Priority for device specific Interrupts  */ }
記事全体を表示
The Real Time Clock (RTC) module is the right tool when we want to keep tracking the current time for our applications. For the Freedom Platform (KL25Z) the RTC module features include: 32-bit seconds counter with roll-over protection and 32-bit alarm 16-bit prescaler with compensation that can correct errors between 0.12 ppm and 3906 ppm. Register write protection. Lock register requires POR or software reset to enable write access. 1 Hz square wave output. This document describes how to implement the module configuration. Also, how to modify the hardware in order feed a 32 KHz frequency to RTC module (it is just a simple wire link).     Hardware. The RTC module needs a source clock of 32 KHz. This source is not wired on the board; hence we need to wire it. Do not be afraid of this, it is just a simple wire between PTC3 and PTC1 and the good news are that these pins are external.   PTC1 is configured as the RTC_CLKIN it means that this is the input of source clock.     PTC3 is configured as CLKOUT (several options of clock frequency can be selected in SIM_SOPT2[CLKOUTSEL] register). For this application we need to select the 32 Khz clock frequency.                         RTC configuration using Processor Expert. First of all we need to set the configurations above-mentioned in Component Inspector of CPU component. Enable RTC clock input and select PTC1 in Pin Name field. This selects PTC1 as RTC clock input. MCGIRCLK source as slow in Clock Source Settings > Clock Source Setting 0 > Internal reference clock > MCGIRCLK source. This selects the 32 KHz clock frequency. Set ERCLK32K Clock Source to RTC Clock Input in Clock Source Settings > Clock Source Setting 0 > External reference clock > ERCLK32K Clock Source. This sets the RTC_CLKIN as the 32 KHz input for RTC module. Select PTC3 as the CLKOUT pin and the CLKOUT pin output as MCGIRCLK in Internal peripherals > System Integration Module > CLKOUT pin control. With this procedure we have a frequency of 32 KHz on PTC3 and PTC1 configured as RTC clock-in source. The MCG mode configurations in this case is PEE mode: 96 MHz PLL clock, 48 MHz Core Clock and 24 MHz Bus clock.   For the RTC_LDD component the only important thing is to select the ERCKL32K as the Clock Source. The image below shows the RTC_LDD component configuration for this application.   After this you only need to Generate Processor Expert Code and write your application.  The code of this example application can be found in the attachments of the post. The application prints every second the current time.     RTC bare-metal configuration. For a non-PEx application we need to do the same configurations above. Enable the internal reference clock. MCGIRCLK is active.          MCG_C1 |= MCG_C1_IRCLKEN_MASK; Select the slow internal reference clock source.          MCG_C2 &= ~(MCG_C2_IRCS_MASK); Set PTC1 as RTC_CLKIN and select 32 KHz clock source for the RTC module.          PORTC_PCR1 |= (PORT_PCR_MUX(0x1));              SIM_SOPT1 |= SIM_SOPT1_OSC32KSEL(0b10); Set PTC3 as CLKOUT pin and selects the MCGIRCLK clock to output on the CLKOUT pin.     SIM_SOPT2 |= SIM_SOPT2_CLKOUTSEL(0b100);     PORTC_PCR3 |= (PORT_PCR_MUX(0x5));   And the RTC module configuration could be as follows (this is the basic configuration just with seconds interrupt): Enable software access and interrupts to the RTC module.     SIM_SCGC6 |= SIM_SCGC6_RTC_MASK; Clear all RTC registers.   RTC_CR = RTC_CR_SWR_MASK; RTC_CR &= ~RTC_CR_SWR_MASK;   if (RTC_SR & RTC_SR_TIF_MASK){      RTC_TSR = 0x00000000; } Set time compensation parameters. (These parameters can be different for each application) RTC_TCR = RTC_TCR_CIR(1) | RTC_TCR_TCR(0xFF); Enable time seconds interrupt for the module and enable its irq. enable_irq(INT_RTC_Seconds - 16); RTC_IER |= RTC_IER_TSIE_MASK; Enable time counter. RTC_SR |= RTC_SR_TCE_MASK; Write to Time Seconds Register. RTC_TSR = 0xFF;   After this configurations you can write your application, do not forget to add you Interrupt Service Routine to the vector table and implement an ISR code.   In the attachments you can find two zip files: PEx application and non-PEx application.   I hope this could be useful for you,   Adrián Sánchez Cano. Original Attachment has been moved to: FRDM-KL25Z-RTC-TEST.zip Original Attachment has been moved to: FRDM-KL25Z-PEx-RTC.zip
記事全体を表示
Kinetis Programming using PE multilink Connect All the VDD to +3.3V and all VSS to GND. Connect 10K pullup resistor to RESET_b pin of the controller. If the controller have the option of JTAG/SWD/EZport make sure to connect 10K pullup resistor to NMI_b or EZP_CS_b pin. NMI_b pins selects the interrupt to highest priority so the controller won't enter into programming mode and EZP_CS_b pin is used for selecting Ezport programming method.   At factory reset condition, all the controller is in the continuous watchdog enabled mode and constantly resetting and the voltage level on the reset pin will be approx 1.64V after adding the pullup resistor as mentioned in point 2. Do not add any filter capacitor on the reset pin while programming the controller for the first time. As it will not let the logic level go low while programming. Which is essential. On probing the reset pin to the oscilloscope the following will be the pattern Before programming we need to mass erase the controller otherwise it will be in continuous reset mode. And to do that we need to configure SWD/JTAG mode. The following configurations for K20P48 LQFP in SWD mode. For mass erase following steps we need to follow. Search for thunderbolt icon in code warrior ie flash programmer and click on the drop-down menu on the icon.     Click on edit then      After configuring the above settings then click on the erase whole device option shown on step 9. If the microcontroller have JTAG/SWD and EZPORT then connect the microcontroller to JTAG port using PORT B of multilink with 20 pin headder. Try avoiding jumpers instead connect the 20 pin cable provided with PE multilink programmer. As all GND pins need to be connected on board's GND.   If the problem still persist then refer to this link Freescale community programmer
記事全体を表示
The following file contains example code for usage of ADC, UART, DAC, GPIO, I2C, interrupts, MCG and timers for the k53 platform. Regards.
記事全体を表示
Here you will find the code and project files corresponding to the I2C-Accelerometer project. The accelerometer/magnetometer is connected to the I2C port, although bot the accelerometer and magnetometer are contained within a single package, they must be initialized individually. In this example the measurements from both devices (X,Y and Z axis) is performed and displayed at the serial terminal. In order to compile the project, the following library must be imported: FXOS8700Q.h Code: #include "mbed.h" #include "FXOS8700Q.h" //I2C lines for FXOS8700Q accelerometer/magnetometer FXOS8700Q_acc acc( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); FXOS8700Q_mag mag( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); //Temrinal enable Serial pc(USBTX, USBRX); MotionSensorDataUnits mag_data; MotionSensorDataUnits acc_data; int main() {     float faX, faY, faZ;     float fmX, fmY, fmZ;     acc.enable();     printf("\r\n\nFXOS8700Q Who Am I= %X\r\n", acc.whoAmI());     while (true)     {         acc.getAxis(acc_data);         mag.getAxis(mag_data);         printf("FXOS8700Q ACC: X=%1.4f Y=%1.4f Z=%1.4f  ", acc_data.x, acc_data.y, acc_data.z);         printf("    MAG: X=%4.1f Y=%4.1f Z=%4.1f\r\n", mag_data.x, mag_data.y, mag_data.z);         acc.getX(&faX);         acc.getY(&faY);         acc.getZ(&faZ);         mag.getX(&fmX);         mag.getY(&fmY);         mag.getZ(&fmZ);         printf("FXOS8700Q ACC: X=%1.4f Y=%1.4f Z=%1.4f  ", faX, faY, faZ);         printf("    MAG: X=%4.1f Y=%4.1f Z=%4.1f\r\n", fmX, fmY, fmZ);                 wait(1.0);     } }
記事全体を表示
The ARM Cortex-M4 Kinetis K50 MCU integrates an analog measurement engine consisting of integrated operational and transimpedance amplifiers and high-resolution ADC and DAC modules that make it ideal for portable healthcare and medical applications. For more information visit www.freescale.com/kinetis
記事全体を表示
Introduction The K32L3A60VPJ1AT MCU is a next generation Kinetis dual core device.  This device brings processing and multi-tasking capabilities that legacy Kinetis devices did not support.  In addition, the K32L3A60VPJ1AT offers improved power consumption and security features.   Some important aspects of these security features lie in a nonvolatile information register (IFR) memory region and how this region is programmed.  The IFR memory region is a memory space with restricted access separate from the main array and is comprised of an erasable IFR region and a non-erasable IFR region.  The non-erasable IFR region contains the program once identifier and the version identifier.  The erasable IFR region holds the flash security, flash options, mass erase enable, and other such features that governs how the device behaves.  In legacy Kinetis devices, certain fields of the main flash array (flash addresses 0x400 - 0x40F) configured the IFR at boot time.  In the K32L3A60VPJ1AT however, the IFR memory region is no longer controlled in this manner.  This presents challenges when trying to configure these settings.  The purpose of this document is to explain how these settings can be changed and provide some options of how to make these changes.   IFR Field Programming Process The first step in configuring the IFR fields is understanding how the these fields are programmed via the hardware. IFR fields are programmed using a special flash command called the Program Index Command. Once programmed, the flash configuration values cannot be reprogrammed without first erasing these fields.  The only way to erase these values is via a mass erase.  This provides security in that the IFR values cannot be changed without erasing the user code as well.  In addition, changes to the user code image cannot affect the bootloader operation, ensuring that a secure boot function can be executed.  The procedure for writing the erasable IFR values is described here:   Write FCCOB0 with the Program Index command (0x43). Write FCCOB1 with the Index to be programmed. The possible Indexes are listed in Erasable IFR Map table (table 16.4.1.2 in the K32L3A6 reference manual). Write FCCOB2 and FCCOB3 with 0x00 as they are not used with this command.  Write FCCOB4 - FCCOBB with the desired value.  (Note that not all of the indexes use all of the FCCOB fields.  Be sure to consult the Erasable IFR Map table for which FCCOB fields are used for the index you are programming). NOTE:  For 2 byte IFR fields that map to 2 bit wide register bit fields (i.e., SEC0, FSLACC, MEEN, and KEYEN fields which map to the FSEC register bit fields), the lower FCCOB register maps to the LSB of the bit field and the upper FCCOB register maps to the MSB of the bit field.  For example, to write 0b'10 to the FSEC field, FCCOB6 should be written to 0xFF and FCCOB7 should be written to 0x00 before executing the Flash command.  Write 0x70 to the Flash status register (FSTAT) to clear any errors that might have been present from the last flash command. (Note that this command MUST be a byte write.) Write 0x80 to the Flash status register (FSTAT) to initiate the programmed flash command. Poll the FSTAT register until the CCIF bit field (bit field 7) is one ('1').  (Note that it may not be possible in your scripting language to do this, or it may just be easier to simply wait for the flash command to finish executing. In these cases, wait significantly longer than the typical Program Index command completion time of 110us.)   After the IFR has been programmed, the IFR should be read back to verify that it completed correctly.  The process for this is as follows:   Write FCCOB0 with the Read Index command (0x41). Write FCCOB1 with the Index to be read.  The possible Indexes are listed in Erasable IFR Map table (table 16.4.1.2 in the K32L3A6 reference manual). Write FCCOB2 - FCCOBB with 0. The results will be stored in FCCOB4 - FCCOBB so, these should be cleared to ensure correct results are received. Write 0x70 to the Flash status register (FSTAT) to clear any errors that might have been present from the last flash command. Note that this command MUST be a byte write. Write 0x80 to the Flash status register (FSTAT) to initiate the programmed flash command. Poll the FSTAT register until the CCIF bit field (bit field 7) is one ('1').  (Note that it may not be possible in your scripting language to do this, or it may just be easier to simply wait for the flash command to finish executing. In these cases, wait significantly longer than the maximum Read Index command completion time of 35us.)   When using the Program Index Command, you must know which index you want to modify to create the correct flash commands.  The index list can be found in the IFR descriptions section of the Flash chapter in the K32L3A60VPJ1AT reference manual.     There are several different options for programming the FOPT fields. These options are: Using the Kinetis Flash Tool  Using blhost Debugger script Subroutine in user software   Option #1: Kinetis Flash Tool Using the Kinetis Flash Tool is likely the most convenient method to change the IFR values.  The Kinetis Flash Tool uses either the UART or USB protocol to interface with the K32L3A6 bootloader and write the IFR fields desired. One of the biggest advantages for the Kinetis Flash Tool is that it provides a graphical interface for users to easily program the IFR fields. The following figure is a picture of the Kinetis Flash Tool and highlights the important input controls and tabs to be used when programming the IFR fields:     This field is the Port set box.  It selects the interface (UART or USB) to be used when communicating to the bootloader.  This box also allows for configuration of the interface.  Consult the K32L3A6 reference manual for default configurations.   This is the Flash Utilities tab.  Select this tab to see the controls shown in this image.  This is the Index input field.  The Index of the IFR to program should be entered here.  This is the Hex digits field.  This value will be programmed at the IFR Index indicated in the Index field. The value here should be in hex format WITHOUT the preceding "0x".  Note that this will write to the FCCOBs in descending order.  For example, to write 0b'10 to the KEYEN field, FFFFFF00 should be written to the Hex digits field. Refer to the programming process outlined in the IFR Field Programming Process in this document for more information.    This is the Byte Count field.  This tells the utility how many bytes to program and must be the byte count of that IFR field.  Consult the Erasable IFR Map table in the reference manual for the value of the specific IFR index to be programmed.   This is the Program button.  After all of the fields have been filled out, click this button to program the desired IFR location.    Option #2: BLHOST The MCUBoot package also includes a command line executable to interface with the bootloader.  This tool, blhost, can be used to program the IFR fields as well.  The "flash-program-once" command should be used to program the desired IFR location.  The syntax of this command is as follows:   flash-program-once <index> <byteCount> <data>   So for example, if you want to program the FOPT IFR field (record index 0x84) with 0xFFFFF3FF, the correct syntax using this command would be   flash-program-once 0x84 4 FFFFF3FF   After programming, the "flash-read-once" command can be used to read back and verify the programmed IFR field(s).  Below is an example using the previous IFR locations   flash-read-once 0x84 4   Below is a full example of erasing the device, programming the FOPT IFR, and reading the FOPT IFR back from the command line using blhost.     When Programming two byte fields, blhost orders the bytes in descending FCCOBx order (just like the Kinetis Flash Tool).  The blhost utility also requires the input to be 4 or 8 byte aligned, but the flash-program-once command only uses the last 2 bytes.  The upper 4 bytes can be padded with 0's or F's. For example, to write the KEYEN field such that the KEYEN bit field is 0b'10, the command would be as follows: flash-program-once 0x83 4 FFFFFF00 Below is a full example of using the blhost command line to erase the device, program the KEYEN IFR, read the KEYEN IFR back, and evaluate the FSEC bit field using the Attach to Running Target function in a debugger.     After executing a pin reset and attaching to the running target:     Option #3: Debugger Script A simple debugger script is another convenient way to write the IFR values.  Debugger scripts are executed in the background of the debug session initiation process (therefore are hidden operations from the user) and typically can be edited easily using any text editor.  However, it can be cumbersome to change the value because this generally must done manually with each programming by the user. With that in mind, it is a good idea to have different connect scripts for different configurations   The first step in using a debugger script is writing a debugger script.  The capabilities and syntax of a debugger script are dependent on your toolchain. For the purposes of this document, we will focus on MCUXpresso IDE.  MCUXpresso IDE uses the PokeXX and PeekXX (where XX is 8, 16, or 32 depending on whether you want to byte access, half-word or word access to the desired register) commands, which are debugger agnostic. So the same commands that work on a device will continue to work whether you are debugging with a JLink or CMSIS-DAP, or whatever other debugger you are using. Below is an example of a MCUXpresso connect script which writes the FOPT register and then reads it back for printing to the debug log.    5140 REM ====================Program FOPT=================================== 5150 Poke32 this 0x40023004 0x43840000 5160 REM Stuff FCCOB registers with desired FOPT value 5170 Poke32 this 0x40023008 v% 5171 s% = Peek32 this 0x40023008 5172 Print "New Val ";~s% 5180 Poke32 this 0x4002300c 0x00000000 5180 Poke8 this 0x40023000 0x70 5190 Poke8 this 0x40023000 0x80 5200 wait 1000 6000 REM ================== Read FOPT ===================================== 6001 REM Now read the FOPT back 6010 Poke32 this 0x40023004 0x41840000 6020 Poke32 this 0x40023008 0x00000000 6030 Poke32 this 0x4002300c 0x00000000 6040 Poke8 this 0x40023000 0x70 6050 Poke8 this 0x40023000 0x80 6060 wait 1000 6070 s% = Peek32 this 0x40023008 6080 Print "New FOPT Val ";~s%   Note in the above script that v% is the desired FOPT value and it has been defined in sections of the script not shown (at line 164).    162 REM This is the value to be written to the FOPT 164 v% = 0xfffff3ff   After the script is written, MCUXpresso must be told to use the connect script.  This is done in the Debug Configurations window.  Assuming a debug configuration has already been created, click on the arrow next to the green bug icon and select Debug Configurations.       In the resulting dialog box, select the debug configuration you want to use, and select the Linkserver Debug tab.  In the Connect Script field, point MCUXpresso to the location of your connect script.       That's all that needs to be done in the IDE. The selected debug configuration should now be using the script which was written.     Some debuggers will allow standalone command line running of a script, such as a JLink debugger.  As the JLink is one of the more popular external debuggers that we encounter, an example of programming using this script has been provided below.     // Now Program the FOPT w4 0x40023004, 0x43840000 // The 43 selects the Program Index command. The 84 selects the FOPT IFR field. // Stuff the FCCOB registers (4-7) with the FOPT value we want to write. // ** (Boot Settings) ** w4 0x40023008, 0xfffff3ff // Write 0xFFFF_1FFF to boot the M4 from internal Flash. Asserting the NMI pin will force booting from the ROM. // Write FCCOB registers 8-B with dummy values. w4 0x4002300c, 0x00000000 // Write the FSTAT register to clear any errors that could have been present. w1 0x40023000, 0x70 // Launch the flash command. w1 0x40023000, 0x80 // Wait for the flash command to finish. Sleep 1 // Now Read the FOPT back w4 0x40023004, 0x41840000 // The 43 selects the Program Index command. The 84 selects the FOPT IFR field. // Stuff the FCCOB registers (4-7) with the FOPT value we want to write. // ** (Boot Settings) ** w4 0x40023008, 0x00000000 // Write 0xFFFF_F1FF to boot the M0+ from internal Flash. Asserting the NMI pin will force booting from the ROM. // Write FCCOB registers 8-B with dummy values. w4 0x4002300c, 0x00000000 // Write the FSTAT register to clear any errors that could have been present. w1 0x40023000, 0x70 // Launch the flash command. w1 0x40023000, 0x80 // Wait for the flash command to finish. Sleep 1 // Read the memory back to verify the FOPT settings that should be present after reset. mem32 40023000,4     Option #4: Subroutine in User Software Occasionally the requirements of your system will prevent implementation of any of the above methods to program the IFR values.  In these cases, you may need to implement your own subroutine to program the IFR.  The procedure to do this is essentially the same as in the debugger script methods, just written in code instead of an external script.  The flash drivers provided in the SDK aid in this process.  One key to remember is that you likely will need to erase the entire flash.  So this subroutine and flash drivers should be placed in RAM memory.  The SDK flash drivers also operate a little differently from the Kinetis flash tool and blhost.  The FCCOB registers will be loaded in ascending order.  For example, to write 0b'10 to the SEC0 bit field in the FSEC register, the command would be: result = FLASH_ProgramOnce(&s_flashDriver, 0x80, ifr2write, 0x2); where ifr2write is an array defined as uint8_t ifr2write[2] = {0x00, 0xFF}; The above will result in 0x00 being loaded to FCCOB6 and 0xFF being loaded to FCCOB7 and SEC0 will then be 0b'10 on the reset after the command is successfully executed.   Conclusion In summary, the IFR registers are nonvolatile information registers that govern certain behaviors of the K32L3A MCU.  The IFR is dividing into an erasable IFR space and non-erasable IFR space, both of which are not a part of the main flash array.  Programming these values requires the use of special flash commands and requires that these values haven't been previously written since the last mass erase.  There are, in general, four different methods of programming the FOPT register settings.  The four methods are:   Kinetis Flash Tool BLhost command line interface Debugger script  User software subroutine   Each method has its advantages, therefore, you should pick the one that meets your needs and is most convenient. However with any of the methods chosen, the IFR values must not have been programmed before writing erasable IFR fields. It is best to perform a mass erase (which can be done using any of the methods presented in this document) before attempting to program any IFR fields.     
記事全体を表示
Trimming internal reference clock of ICS (internal clock source) module using OSDA connection Pavel Šádek, Rožnov, Czech Republic   Simple apps does not require crystal driven clock precision. Internal reference clock based timing of MCU can be used instead.   Manufacturing process yealds to frequency deviation, that is why all MCU devices are factory programmed with a trim value in a reserved memory location. This value is uploaded to the ICS_C3 register and ICS_C4[SCFTRIM] during any reset initialization. For finer precision, trim the internal oscillator in the application and set ICS_C4[SCFTRIM] accordingly.   The TRIM bits effect the ICSOUT frequency if the ICS is in FLL engaged internal (FEI), FLL bypassed internal (FBI), or FLL bypassed internal low power (FBILP) mode.   The internal reference clock can be trimmed also in program time of the device to any value between 31.25 and 39.062kHz, this allows also achieving exotic bus frequencies.  The value applied in Processor Expert does not propagate into Pemicro connection manager. No matter if Processor expert is used or not , we need to configure it it by ourselves in connection of OSDA (same for debugging or programming). So this is a guide how to do so.   In the program initialization we need to initialize the ICS_C3 register and ICS_C4[SCFTRIM]. It can be done siply this way:   /* System clock initialization */   if ( *((uint8_t*) 0x03FFU) != 0xFFU) {     ICS_C3 = *((uint8_t*) 0x03FFU);     ICS_C4 = (ICS_C4 & 0xFEU) | ((*((uint8_t*) 0x03FEU)) & 0x01U);   }   Then hit   flag, choose debug configuration and you will see configuration of your connectons, I have here only OSDA for my Kinetis E Freedom board (it is similar across families of Kinetis, ColdFire or S08 just connection would be SWD, Jtag or BDM) You will get new window   Choose „Advanced Programming Options“ button     Enable calculating of Trim value and programming into Flash location. If the TRIM frequency is different from default, check the box to use custom one in valid range – the one you(or Processor Expert) have used for your timing calculations. Hit DONE and your effort is done!   Next, when you will launch debugging session by hitting bug on button these values will be applied.   My RESULT:   ICS_C3 was trimmed to value of 0x57 for 39.062kHz and 0x9B for 31.250kHz for my Kinetis E Freedom board. Precision is better then 1% in room temp. This is ok for serial comunication without need of crystal for example. Note: Values out from my discovered range of 0x57 – 0x9B leads to frequencies that are out of specification of ICS and should not be used for this exact device.  The limits will be slightly different for every single device.
記事全体を表示
Encrypted QuadSPI image Implementation       The Kinetis family of MCU includes the system security and flash protection features that can be used to protect code and data from unauthorized access or modification. This application note discusses the usage of encrypted boot with the KBOOT and experiment with the FRDM-K82 board. FRDM-K82 board
記事全体を表示
作者 Shaozhong Liang         MQX4.0支持长文件名(Long FileName),但不支持中文长文件名。在MQX创建长文件名的文件时,只是简单地将文件名对应的字符串由转换为UNICODE编码。         如果使用的是拉丁字母,其编码将会被补全为2个字节,前面一个字节为0x00,例如字符“A”的编码是0x0041,是0x00接上字符对应的ASCII码。这个编码方式在英文字符串上编解码不成问题。         但是中文的表示方式是以GB2312编码方式,用2个字节来表示一个中文字。         例如中文字“啊”,对应的GB2312码为0xB0A1,MQX会将这2个字节拆分为0xB0和0xA1,然后分别进行UNICODE编码,这时候“啊”的编码将是0x00B0,0x00A1,变成4个字节的UNICODE编码。         最终将导致错误乱码,“啊”因此会被译码显示成  °  和  ¡         而实际上“啊”在UNICODE编码为0x554A,为了MQX能够支持中文长文件名,此时我们需要对GB2312和UNICODE进行转换。         我们需要对MFS源代码进行修改。现在修改后的代码只支持创建文件,暂时不支持修改已经存在的中文长文件名文件。         将附件中的文件替换原有的文件,重新编译MFS库和应用程序即可。         按照这种方法修改后,对中文字对应的GB2312编码范围进行UNICODE的转换,处理后文件名将支持中文,同时也可以实现中英文文件名的混用。 mfs\source\generic\mfs_entry.c 修改了函数MFS_create_directory_entry mfs\source\generic\mfs_lfn.c 增加了长文件名保存函数MFS_lfn_save 增加了oem字符集到unicode字符集的转换函数MFS_oem2unicode,用户层的代码直接使用中文文件名,有转换函数转换为对应的UNICODE编码。 由于GB2312全集占用空间太大,用户可以将gb2unicode.c的字符集表oem2unicode_table中数据进行精简。 mfs\source\include\mfs_prv.h 增加了上述函数声明。 Original Attachment has been moved to: lfn_mfs.rar
記事全体を表示
The following file contains codewarrior code that was migrated from the IAR example code in the sample code package at the freescale webpage. It contains the following examples: adc_demo freedom_greem_led freedom_red_led lcd_rtc_lowpower PIT_basic sLCD_freedom uart_low_power_wu_dut Regards
記事全体を表示