Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
1. Introduction MCUboot is a common used bootloader for most of Kinetis and i.mx RT devices. It can support download application via UART/USB/CAN/I2C/SPI. It enables quick and easy programming of Kinetis MCUs and i.mx RT MPU through the entire product life cycle, including application development, final product manufacturing, and beyond. K64 is a very popular device in Kinetis family. It has a M4 core, 512k and above flash, 120M main frequency and plenty of interface, such as I2C/SPI/UART/CAN/USB/ENET. But it is a bit awkward that the MCUboot demo of K64 is not include CAN. Does K64’s CAN can’t support bootloader application? No, of course not. Here we are going to port CAN function to K64 bootloader. There are two kind of CAN peripheral in Kinetis family, FlexCAN and MSCAN. FlexCAN is more complex than MSCAN. K64 has a FlexCAN. To speed up our work, we can port FlexCAN driver and related code from TWR-KV46 bootloader. Hardware: two TWR-SER board two sets of TWR-ELEV TWR-K65F150M TWR-K64F120M   Software: MCUXpresso 11.0 MCUBoot 2.0.0 package SDK_2.6.0_TWR-K64F120M 2. Software porting Step 1, copy below files to twrk64f120m_tower_bootloader project. \drivers\fsl_flexcan.c \drivers\fsl_flexcan.h        \source\bootloader\src\flexcan_peripheral_interface.c   Step 2, modify the project to enable the FlexCAN.       In bootloader_config.h, change BL_CONFIG_CAN definition to 1.        In peripherals_MK64F12.c, add #if BL_CONFIG_CAN     // CAN0     {.typeMask = kPeripheralType_CAN,      .instance = 0,      .pinmuxConfig = can_pinmux_config,      .controlInterface = &g_flexcanControlInterface,      .byteInterface = &g_flexcanByteInterface,      .packetInterface = &g_framingPacketInterface }, #endif    // BL_CONFIG_CAN       Pin mux setting. In peripherals_pinmux.h, add #define BL_ENABLE_PINMUX_CAN0 (BL_CONFIG_CAN) //! CAN pinmux configurations #define CAN0_RX_PORT_BASE PORTB #define CAN0_RX_GPIO_PIN_NUM 18             // PIN 13 in the PTA group #define CAN0_RX_FUNC_ALT_MODE kPORT_MuxAlt2 // ALT mode for CAN0 RX functionality for pin 13 #define CAN0_TX_PORT_BASE PORTB #define CAN0_TX_GPIO_PIN_NUM 19             // PIN 12 in the PTA group #define CAN0_TX_FUNC_ALT_MODE kPORT_MuxAlt2 // ALT mode for CAN0 TX functionality for pin 12       Set clock. FlexCAN clock source can be OSCERCLK or bus clock. Here we use bus clock run at 48Mhz. In flexcan_peripheral.c, add these code. const flexcan_timing_config_t bit_rate_table48m[] = {     { 23, 3, 4, 4, 4 }, /* 125 kHz */     { 11, 3, 4, 4, 4 }, /* 250 kHz */     { 5, 3, 4, 4, 4 },  /* 500 kHz */     { 3, 3, 4, 4, 4 },  /* 750 kHz */     { 2, 3, 4, 4, 4 }   /* 1   MHz */ }; change line 621 FLEXCAN_SetTimingConfig((CAN_Type *)baseAddr, &bit_rate_table48m[s_flexcanInfo.baudrate]); Step 3, compile the project.   3. Function test Software preparation To connect bootloader via CAN bus, NXP has TWR-K65 as bridge. But its source code is not in K64 SDK. It is in MCUBoot2.0.0 package. User can download the package from https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools/mcuboot-mcu-bootloader-for-nxp-microcontrollers:MCUBOOT The bridge project is called buspal which can be found in NXP_Kinetis_Bootloader_2_0_0\apps\bus_pal\MK65F18. BusPal is an embedded software tool that is available as a companion to blhost. The tool acts as a bus translator with an established connection with blhost over UART and with the target device over I2C, SPI, or CAN, and assists blhost in carrying out commands and responses from the USB target device. The BusPal is available for selected platforms. The source code for BusPal is provided with the Kinetis bootloader release, it support FRDM-KL25, TWR-KV46F150M and TWR-K65F180M and can be customized to run on other platforms. More detail of buspal is in Kinetis blhost User's Guide appendix C.   Hardware connection TWR-SER has TJA1050 as transceiver. We can connect J7 on both boards. When construct the Tower system, user should take care the power. The power tree is very flexible. Improper setting may cause TJA1050 can’t work.   The Buspal project on TWR-K65F180M use UART1 to connect with computer. The port is on TWR-SER. To make the connection simple, we can share the openSDA UART port. The openSDA UART use UART2, we can jump UART1 signal to J33 and J34 on K65 tower board.     Testing: Open a command window, type >blhost -p com4,57600 –buspal can,0,321,123 – get-property 10 This command can check if the whole system work properly. Then, you can download the code to K64 now. Please type >blhost -p com4,57600 –buspal can,0,321,123 – flash-image xxxxxx.s19 erase
View full article
El programador USBDM es una interfaz de programación y depuración para los microcontroladores Freescale, existen varias versiones de esta herramienta, el programador MantaRay USBDM está basada en la versión para los microcontroladores HCS08(BDM) y Kinetis (SWDIO). Toda la información acerca de este proyecto puedes encontrarlo en http://usbdm.sourceforge.net/index.html BDM (Background debug mode) El puerto de programación BDM es una interfaz de programación desarrollada por Freescale para los microcontroladores HCS08 (8 bits) y Coldfire V1 (32 bits). Las características más sobresalientes sobre este puerto de programación es que solo utiliza un pin de programación (BKGD). Además de permitir la programación de la memoria flash, también permite el "debug in circuit" esto quiere decir que podemos depurar nuestro codigo en tiempo real a través del software Codewarrior. SWDIO Es la versión minima del JTAG para los microcontroladores Kinetis (Cortex ARM 32 bits) en la cual solo utiliza una linea de comunicación (SWDIO) y una señal de reloj (SWCLK). Este puerto esta en los Cortex M0 como son KL01, KL02, KL03, KL1x,KL2x,KE02,KE04 y KE06. El programador MantaRay USBDM permite la programación y la depuración de los microcontroladores de Freescale de la gama de 8 bits y 32 bits. Shrimp El complemento perfecto para el programador MantaRay USBDM es Shrimp, una pequeña tarjeta que tiene el tamaño exacta de un integrado con montaje DIP28 600mil, la cual, la hace una herramienta flexible, al hacer prototipos en una protoboard, y después en un prototipo final. La tarjeta Shrimp es compatible con los microcontroladores de 8 bits MC9S08PA16 y de 32 bits MKE02Z16, los dos totalmente compatibles en pines y periféricos. MC9S08PA16 8-Bit S08 central processor unit (CPU) – Up to 20 MHz bus at 2.7 V to 5.5 V across temperature range of -40 °C to 105 °C – Supporting up to 40 interrupt/reset sources – Supporting up to four-level nested interrupt – On-chip memory – Up to 16 KB flash read/program/erase over full operating voltage and temperature – Up to 256 byte EEPROM; 2-byte erase sector; program and erase while executing flash – Up to 2048 byte random-access memory (RAM) – Flash and RAM access protection MKE02Z16 • Operating characteristics – Voltage range: 2.7 to 5.5 V – Flash write voltage range: 2.7 to 5.5 V – Temperature range (ambient): -40 to 105°C • Performance – Up to 40 MHz ARM® Cortex-M0+ core and up to 20 MHz bus clock – Single cycle 32-bit x 32-bit multiplier – Single cycle I/O access port • Memories and memory interfaces – Up to 16 KB flash – Up to 256 B EEPROM – Up to 2 KB RAM Más información técnica la puedes encontrar en el siguiente link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KE02&nodeId=01624698C90DE4 http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S08P&nodeId=01624684491437EDDD Muy pronto mas adelantos de este proyecto
View full article
The 5V Kinetis E series MCUs are designed to maintain high robustness for complex electrical noise environments and high-reliability applications. Kinetis EA series MCUs using the same architecture with automotive level operation temperature range, are various used for auto body electrical application. There was a reality customer requirement to let KEA core running the application (light a LED) within 20ms from power up. It need to know the whole startup processing for KE/KEA product. Please check below picture to get more info about boot sequence: During the power up phase, after VDD rising to VPOR voltage threshold, there with about 15us delay before internal IRC start oscillating. T2 interval is FLL acquisition time to make FLL generating clock. The Reset_b pin is released and then the system is released from reset. After that, the NVM starts internal initialization. Flash Controller is released from reset and begins initialization operations while the core is still halted before the flash initialization completes. When the flash Initialization completes (16 μs) , the core sets up the stack, program counter (PC), and link register (LR). The processor reads the start SP (SP_main) from vector-table offset 0. The core reads the start PC from vector-table offset 4. LR is set to 0xFFFF_FFFF. The CPU begin to execute the first instruction. Overview the whole power up processing, FLL acquisition time is the longest time interval almost 1ms, then following power up time about 0.1ms (using 17KV/sec VDD ramp-up slew rate). There seems a lot of time left to run the chip initialization code and application code. Customer requirement (power up to light a led within 20ms) should be matched without any problem. While, during customer test, there seems it need to take more than 30ms to find the LED be lighten after power up. In order to check the issue, we get the customer test code and find there with below clock initialization code: void Clk_Init() {                 ICS_C1|=ICS_C1_IRCLKEN_MASK; /* Enable the internal reference clock*/                 ICS_C3= 0x90;                                    /* Reference clock frequency = 31.25 KHz*/                       while(!(ICS_S & ICS_S_LOCK_MASK));  /* Wait for FLL lock, now running at 40 MHz (1280 * 31.25Khz) */                                               ICS_C2|=ICS_C2_BDIV(1)  ;                    /*BDIV=2, Bus clock = 20 MHz*/                 ICS_S |= ICS_S_LOCK_MASK ;              /* Clear Loss of lock sticky bit */      } We do a test to check the Clk_init() function execution time and find it will take almost 25ms. We toggle a GPIO pin and almost 25ms for checking ICS status register [LOCK] be asserted. KE/KEA product using ICS module as clock source, which default mode is FEI. In general, during the chip initialization, using ICS status register [LOCK] bit to check if the FLL cock is stable or not. From KE/KEA product datasheet, the Max. FLL acquisition time is 2ms. Why the ICS_S[LOCK] bit be asserted need take more than 25ms? After double check with ICS IP owner, we get below info: The FLL_S[LOCK] bit act as “LOCK detection”, the LOCK bit will be set if FLL clock frequency stays within the tolerance 6% for 20ms~30ms. After acquisition time (max. 2ms) FLL achieved clock accuracy as same as LOCK bit be asserted. After ICS configuration modified, customer can call a 2ms delay routine to make sure FLL acquisition clock successfully before executing the application code. 
View full article
Hi All: when someone program FSL MCU  by theirself program tool, and the flash size is over 64KByte , please reference the document. the document is chinese version Br Felix
View full article
I need to connect multi phy device with a single cpu. I want realize a follow hardware (see picture MultiPhys.jpg ). My dubt is if this schematic is correct. I need to send frame either PHY1 or PHY2. My application is like a gateway, it sends messages to network in selective way ( and it receives from every PHYs device ). Is it possible connect many PHY device with one RMII bus? what is the correct way to connect many PHY device on RMII bus? Anyone knowns documents that describe multi Phy configurations ?
View full article
I recently developed a Visual Studio .NET application that uses an OpenSDA virtual serial port to communicate with a FRDM-K64F. My serial protocol is a binary command-response protocol, which means that every time the .NET application sends a command packet to the serial port, it should always receive a response packet back. You can find more details about the protocol in the Freescale Intelligent Sensing Framework, but for the purposes of this document, all that matters is that every command should receive a response. My Visual Studio .NET application uses the SerialPort class, and worked beautifully...until I changed the OpenSDA firmware. Originally I used OpenSDA firmware from P&E; this time I had tried out Segger. In theory, this change should not have made a difference, however with the Segger firmware my .NET application never received response packets. I knew that the command packets were transmitting correctly from PC to board because they would turn a board LED on and off as expected. I tried using a binary terminal, RealTerm, to send commands to see if it would receive responses, and it did. So the problem had to be in my .NET application. After a lot of googling and some trial-and-error, I ultimately found that enabling the Data Terminal Ready (DTR) signal did the trick. Strangely, I didn't need to enable DTR in RealTerm. The moral of the story is that if you want to use Segger OpenSDA with a .NET SerialPort, then you must enable DTR. Fortunately this configuration also works with P&E and mbed OpenSDA.
View full article
Some of our customers encountered clock stretching issue when using the I2C. Actually the first should been in mind is the clock stretching is usually done by the slave, not the master.  In the case for the Kinetis as master to connect with I2C device, the clock stretching should been done by the slave device. In this case the slave device should hold the clock signal low until it has data available. There isn’t anything that needs to be done to enable clock stretching on the master side. So how the code do with the clock stretching? The slave should toggling read_start high first and reading the data register to actually start the transfer. Be remember that the read from the data register is what actually triggers the transfer. Customer always missed this point.
View full article
MAPS-KS22 Board Introduction: MAPS boards are localization evaluation boards for Chinese customers. The MAPS boards are suitable for NXP MCU product, with low coat, more flexibility and easy-copy features, which matching with local customer requirements and better for learning and product evaluation. MAPS board includes four parts board, which are MCU Board, Peripheral Board, Application Board & Socket Board. The naming of MAPS are using the four-part board initial letter. MCU board is NXP Kinetis MCU based evaluation main board with chip related special module interface/device, such as graphic LCD/ENET interface and etc. The MCU board fan out all MCU pins as test points for measuring. The MCU board also provide two 32-pin socket to connect external peripheral board or application board. Peripheral Board collects more general device into one board and using two 32-pin socket connects with MCU board. The MAPS-Dock is the first peripheral board, which with below configuration: Micor-SD card slot; six touch pads; USB FS interface; IrDA transceiver; one SPI Interface (SPI-Flash); two UART interface; four buttons; one I2S interface (audio codec); one CAN interface; two potentionmeter; one DAC output interface; 128x64 monochrome LCD; one 5-way button. It also with SWD debugger on board and USB CDC virtual COM. Application Board designed for special applications, such as motor control, IOT, Smart Home, Wireless Charger and etc. Socket Board provides interface for FreeDOM boards/Arduino boards/Customer defined boards. MAPS-KS22 board MCU board for KS22 chip evaluation. KS22 MCU is based on the ARM® Cortex®-M4 core with 120MHz MCUs with FPU, offering full-speed USB 2.0 OTG, in addition to other features like USB crystal-less functionality. MAPS-KS22 oobe demo porting process MAPS-KS22 oobe demo is based KSDK V1.0, which will show Freescale LOGO on the SPI color LCD and meanwhile use FlexIO I2S to play an audio on microphone. Step1: visit Kinetis Expert website (http://kex.nxp.com/en/welcome) to download MAPS-KS22 KSDK V2.0 software: Step2: download [Kinetis SDK Project Generator Tool] from below link and generate oobe demo project based on MAPS-KS22 SDK V2.0 software: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=KSDK-PROJECT-GENERATOR-TOOL&appType=file1&location=null&DOWNLOAD_ID=null Step 3: After that, open the oobe project, which located at default path: C:\Freescale\SDK_2.0_MAPS-KS22\boards\mapsks22\user_apps\oobe\iar The default project is based on <hello-world> demo, it need to add LED control code. Those part of code could be found at <main.c> file and related pin muxing code at <pin_mux.c> file. Step 4: Modify ili9341 related driver: For the oobe project with two major functions, the first one is to display Freescale LOGO at LCD. The MAPS-KS22 board graphic LCD is using ili9341 TFT LCD driver with SPI interface with KS22 chip. The previous oobe project is using GPIO pins emulate SPI communication, we will make the similar application with KSDK V2.0 driver. Most modification based on the GPIO pins control. Please check below code at <ili9341.h> file, which call KSDK V2.0 GPIO driver: #define ILI9341_CS_HIGH()       GPIO_SetPinsOutput(BOARD_LCD_CS_GPIO, 1U << BOARD_LCD_CS_PIN) #define ILI9341_CS_LOW()        GPIO_ClearPinsOutput(BOARD_LCD_CS_GPIO, 1U << BOARD_LCD_CS_PIN) #define ILI9341_CLK_HIGH()      GPIO_SetPinsOutput(BOARD_LCD_CLK_GPIO, 1U << BOARD_LCD_CLK_PIN)  #define ILI9341_CLK_LOW()       GPIO_ClearPinsOutput(BOARD_LCD_CLK_GPIO, 1U << BOARD_LCD_CLK_PIN) #define ILI9341_MOSI_HIGH()     GPIO_SetPinsOutput(BOARD_LCD_MOSI_GPIO, 1U << BOARD_LCD_MOSI_PIN) #define ILI9341_MOSI_LOW()      GPIO_ClearPinsOutput(BOARD_LCD_MOSI_GPIO, 1U << BOARD_LCD_MOSI_PIN)      #define ILI9341_MISO_HIGH()     GPIO_SetPinsOutput(BOARD_LCD_MISO_GPIO, 1U << BOARD_LCD_MISO_PIN) #define ILI9341_MISO_LOW()      GPIO_ClearPinsOutput(BOARD_LCD_MISO_GPIO, 1U << BOARD_LCD_MISO_PIN) And it also need to add ili9341 control pin muxing initialization code at <pin_mux.c> file. Step 5: We could modify the Freescale logo with new NXP logo, which could using [Embedded GUI Conversion Utility3.0] tool. This tool could be downloaded from below link:  http://tinyurl.com/eGUI-Convert  The conversion result of the graphic data is 16-bit array, which need be transfer to 8-bit array. After that, compile and download the image to the board, it with below result: Step 6: The oobe demo provide another function to play music with MAPS-DOCK board WM8960 codec chip, then using headphone will hear the sound. For the KS22 with FlexIO module, the demo will use FlexIO emulating I2S bus to transfer data to WM8960 codec chip. About I2S bus MCLK clock source, the MAPS-KS22 provide two selection, one is using TPM1_CH1 pin, the other one is using I2S0_MCLK pin with JP5 jumper selection. In oobe demo, we use TPM1_CH1 pin to generate 12MHz MCLK clock with TPM module output compare mode. Related code, please refer below tpm_init_output_compare() function at <main.c> file: //enable clock gating of tpm1 CLOCK_EnableClock(kCLOCK_Tpm1); //set TMP output compare mode TPM_SetupOutputCompare(BOARD_TPM_BASEADDR, BOARD_TPM_CHANNEL, kTPM_ToggleOnMatch, 1U); BOARD_TPM_BASEADDR->MOD = 0x1; TPM_StartTimer(BOARD_TPM_BASEADDR, kTPM_SystemClock);   //TPM counter increments on every TPM counter clock Step 7: WM8960 is a stereo CODEC chip provide I2C port for chip configuration. There need to initialization the WM8960 chip before using it with related driver <wm8960.c> & <wm8960.h> files. The MAPS-KS22 board using LPI2C0 module connects with WM8960 chip, so there need to port using LPI2C driver of KSDK V2.0 and modify the WM8960 driver related. The LPI2C module initialization code located at <main.c> with lpi2c_master_init() function. The WM8960 driver major modification with WOLFSON_WriteReg() function at <wm8960.c> file, calling the LPI2C driver of KSDK V2.0 with below code:  wolfson_status_t WOLFSON_WriteReg(uint8_t reg, uint16_t val) {       uint8_t cmd,buff;        status_t ret;        cmd = (reg << 1) | ((val >> 😎 & 0x0001);    // register address        buff = val & 0xFF;     //data        reg_cache[reg] = val;      // copy data to cache         uint8_t data[2];         data[0] = cmd;         data[1] = buff;         //start lpi2c tx operation                   ret = LPI2C_MasterStart(LPI2C0, WM8960_I2C_ADDR, kLPI2C_Write);           // send two data with register address and related value          ret = LPI2C_MasterSend(LPI2C0, data, 2);                //stop lpi2c tx operation                  ret = LPI2C_MasterStop(LPI2C0);               if(ret != kStatus_Success)          {  return kStatus_WOLFSON_I2CFail;  }          return kStatus_WOLFSON_Success; } After WM8960 chip driver modification, there could call related driver to initialize WM8960 chip and configure the communication interface with I2S bus. Following steps focus on how to transfer data to WM8960 codec with I2S bus. Step 8:  The FlexIO modul will simulate I2S bus call FlexIO_I2S_MasterInit() function in <main.c> file to initialize FlexIO module as I2S master. There using FXIO0_D4 pin as I2S bit clock pin, using FXIO0_D5 pin as I2S Transmit pin and using FXIO0_D6 pin as I2S Transmit Frame Sync pin. KSDK V2.0 provide FlexIO for I2S driver located at <fsl_flexio_i2s.h> file. Step 9: There will call eDMA with FlexIO module to reduce the core work load during the I2S data transfer. It will initialize the eDMA & DMAMUX modules for FlexIO. Related code located at <main.c> file with ConfigDMAforFlexIOI2STX() function: void ConfigDMAforFlexIOI2STX(void) { EDMA_GetDefaultConfig(&dmaConfig); EDMA_Init(EXAMPLE_DMA, &dmaConfig); EDMA_CreateHandle(&dmaHandle, EXAMPLE_DMA, EXAMPLE_CHANNEL); DMAMUX_Init(DMAMUX0); DMAMUX_SetSource(DMAMUX0, EXAMPLE_CHANNEL, EXAMPLE_DMA_SOURCE); DMAMUX_EnableChannel(DMAMUX0, EXAMPLE_CHANNEL); }    Step 10: KSDK V2.0 software provides FlexIO I2S eDMA driver located at <fsl_flexio_i2s_edma.c> file, with below codes to initialize FlexIO I2S master DMA handler and to configure the sample rate & audio data format to be transferred: FLEXIO_I2S_TransferTxCreateHandleEDMA(&base, &txHandle, callback, NULL, &dmaHandle); FLEXIO_I2S_TransferSetFormatEDMA(&base, &txHandle, &format, 48000000); Step 11: After above preparation, following action will start to transfer music data to WM8960 codec with below code. When the music data transfer finished, the callback function will be called to start next round data transferred. Then we could hear the sound with endless loop. static void callback(FLEXIO_I2S_Type *i2sBase, flexio_i2s_edma_handle_t *handle, status_t status, void *userData) {   // Initiate FlexIO I2S transfer again after previous transfer finished  FLEXIO_I2S_TransferSendEDMA(&base, &txHandle, &xfer); } About more detailed oobe demo software info, please check attached file. The default oobe demo located path is: C:\Freescale\SDK_2.0_MAPS-KS22\boards\mapsks22\user_apps\oobe
View full article
Fat File System for SD card using SPI for Kinetis-K60, K22 and K20
View full article
在工业热电偶数据采集与处理方面,ADI,MAXIM的模拟芯片几乎占据了90%以上的市场,尽管他们的单片售价高的吓人。1片16位的AD芯片没有个2个美金是买不到的,24位的更不用多说。现在他们的竞争对手来了,飞思卡尔针对表计市场推出的基于M0+内核的KM1x,KM3x,片上集成24位的Σ-Δ模拟前端, 其中2路带有独立的可编程最高32倍PGA,无论是市场上应用最多的K型热电偶、还是专注于低温测量的T型热电偶,通过合理的配置都可以满足他们极宽范围的量程。确切的讲,KMxx和这两种产品根本不能算是一个数量级的PK对手,无论从资源上还是从价格上。但是尽管这样,就一定能打败竞争对手吗?首先得有的说服力的参考设计吧,不着急,已经开始设计了。 处理器:MKM33Z128CLH5 暂定功能: 1. K型热电偶+T型热电偶兼容采集处理,板上预留2种热电偶接口,带冷端温度补偿功能 2. 按键切换热电偶类型 3. 段码式LCD显示采集的实时温度,状态显示 4. 低功耗演示,面向手持式设备市场 5. 音乐变调蜂鸣器 主要针对竞争目标:Maxin的 MAX31855KASA (T型热电偶) 关于精度嘛,等参考设计完成了测试一下就知道了。 以上参考设计敬请等待,也欢迎多提宝贵建议。
View full article
This is a port of the TWR_K60N512 "Audio" Demo into Kinetis Design Studio and into eGUI 3.0 (from 2.1). The original demo is from Petr Gargulak and was under "Freescale_embedded_GUI_SW.zip\_Official_Demos\EGUI_D4D_Demo\TWR_K60N512\BareMetal\CW_10_1" avaiable on the freescale website. Some of the major porting differnces (this may help others porting similar projects): KDS: KDS by default does not define 'asm()', switch these to '__asm()' or change compiler settings (see: Sorting out asm(); in KDS: How to change your compiler language to GNU ISO90) eGUI 2.1 -> 3.0: Autosize feature has gone, all object sizes now need to be declared Objects seem to add padding of some sort: even with objects where size was previously declared, these had to be increased by ~3px in each direction, else text/images would not render. 'D4D_OBJECT_SYS_FUNCTION' structure no longer contains 'type'. It suggests using strName instead to identifier object. D4D_TEXTBOX no longer has title or icon functionality. When building this project there will be ~7 warnings from the compiler, including 2 of my own. The code should function fine. note: TWR_LCD settings for this project, switches are set up with in following sequence: "01111110". regards, Rael S-R
View full article
The FlexIO module was first introduced in the Freescale Kinetis KL43 family. It is capable of emulating various serial communication protocols including: UART, SPI and I2C. The FlexIO module is very flexible and you can configure it according to your communication needs. The main components of the FlexIO module are the shifters, timers, and pins. Data is loaded onto a shifter and a timer is assigned to generate the shifter clock and use a pin to output the data from the shifter. The KL43 FlexIO module has 4 32-bit shifters, 4 16-bit timers and 8 bidirectional I/O pins. Each shifter and timer has its own configuration registers. The most important registers that configure the whole FlexIO behavior are the SHIFTCFG, SHIFTCTL, TIMCFG, TIMCTL and TIMCMP registers. There are other registers that contain status flags, interrupt enabling bits and the buffers for the shifters. Shifters have a timer assigned to them to generate the shift clock and it can be configured to shift data in or out. When the shifter is configured to transmit mode, the data from the SHIFTBUF register will be loaded to the shifter and the shifter status flag will be set meaning that the shifter is ready to start the transmission. In receive mode, the shifter status flag is set when SHIFTBUF has been loaded with the data from the shifter, and the status flag is cleared when the SHITBUF register is read. The timers are highly configurable, they can use external or internal triggers to generate certain conditions to reset, enable and disable the timer. The triggers can be a timer output, shifter status flag, pin input or an external trigger input. They can be configured to enable in response to a trigger, pin or shifter condition. Each shifter or timer can be configured to use any FlexIO pin with either polarity. The pins can be used as an input or output. A pin configured as an input for a timer can be used to receive a clock and use it as the shifter clock that is assigned to this timer. Once everything is configured you need to read/write the shifter buffers and the shifter and timer status flags to start a transmission or to read the contents of the shifter buffer when receiving data. The following diagram gives a high-level overview of the configuration of FlexIO timers and shifters. Figure 1. FlexIO block diagram In the following example configuration, the FlexIO module will be configured as a transmitter. It will use one shifter, two timers, and three pins. The pins will be used for the outputs of the shifter and the two timers. One timer will be used as the shifter clock and the other timer will be used as a chip select to show when a transmission is being made. The FlexIO will be configured to have a baud rate of FlexIO clock/4 and will do an 8-bit transmission. Figure 2. Example transmission Timer 0 Timer Configuration 0 Register (FLEXIO_TIMCFG0) = 0x00002200 TIMOUT = 0    Timer output is logic one when enabled and is not affected by timer reset. TIMDEC = 0    Decrement counter on FlexIO clock, Shift clock equals Timer output. TIMRST = 0    Timer never reset. TIMDIS = 2    Timer disabled on Timer compare. TIMENA = 2    Timer enabled on Trigger high. TSTOP  = 0    Stop bit is disabled. TSTART = 0    Start bit disabled. Timer Control 0 Register (FLEXIO_TIMCTL0) = 0x01C30101 TRGSEL = 1    Trigger select. Shifter 0 status flag. TRGPOL = 1    Trigger active low. TRGSRC = 1    Internal trigger selected. PINCFG = 3    Timer pin output. PINSEL = 1    Timer pin 1 select. PINPOL = 0    Pin is active high. TIMOD  = 1    Dual 8-bit counters baud/bit mode. Timer Compare 0 Register (FLEXIO_TIMCMP0) = 0x00000F01 TIMCMP = 0x00000F01        Configure 8-bit transfer with a baud rate of FlexIO clock/4. Set TIMCMP[15:8] = (number of bits x 2) - 1. Set TIMCMP[7:0] = (baud rate divider / 2) - 1. In our case we want an 8-bit transfer so TIMCMP[15:8] = 0xF and a baud rate divider of 4 so TIMCMP[7:0] = 0x1. Timer 1 Timer Configuration 1 Register (FLEXIO_TIMCFG1) = 0x00001100 TIMOUT = 0    Timer output is logic one when enabled and is not affected by timer reset. TIMDEC = 0    Decrement counter on FlexIO clock, Shift clock equals Timer output. TIMRST = 0    Timer never reset. TIMDIS = 1    Timer disabled on Timer N-1 disable. TIMENA = 1    Timer enabled on Timer N-1 enable. TSTOP  = 0    Stop bit is disabled. TSTART = 0    Start bit disabled. Timer Control 1 Register (FLEXIO_TIMCTL1) = 0x00030283 TRGSEL = 0    Trigger select. Doesn’t matter because we won’t use a trigger. TRGPOL = 0    Trigger active high. TRGSRC = 0    External trigger selected. PINCFG = 3    Timer pin output. PINSEL = 2    Timer pin 2 select. PINPOL = 1    Pin is active low. TIMOD  = 3    Single 16-bit counter mode. Timer Compare 1 Register (FLEXIO_TIMCMP1) = 0x0000FFFF TIMCMP = 0x0000FFFF Never compare. Shifter 0 Shifter Control 0 Register (FLEXIO_SHIFTCTL0) TIMSEL = 0    Timer 0 select. TIMPOL = 0    Shift on posedge of Shift clock. PINCFG = 3    Shifter pin output. PINSEL = 0    Shifter pin 0 select. PINPOL = 0    Pin is active high. SMOD   = 2    Transmit mode. Load SHIFTBUF contents into the Shifter on expiration of the Timer. Shifter Configuration 0 Register (FLEXIO_SHIFTCFG0) INSRC  = 0    The input source of the shifter is from a pin. In our cause this doesn’t matter because our shifter is set as transmit mode. SSTOP  = 0    Stop bit disabled. SSTART = 0    Start bit disabled. Once all the FlexIO components are configured you have to enable the FlexIO instance by setting the FLEXEN bit in the FLEX_CTRL register. Initially, the shifter status flag is set and is cleared each time the SHIFTBUF register is written. This flag is set each time the SHIFTBUF data has been transferred to the Shifter (SHIFTBUF is empty).  The shifter status flag 0 is configured to be the trigger of the timer 0, so as soon as the status flag is cleared, the timer 0 will be enabled because TIMENA = 2 (Timer enabled on Trigger high)and TRGPOL = 1 (Trigger active low). The shifter will begin to shift out the data on the positive edge of the clock (TIMPOL = 0) until the timer is disabled. The timer will disable when the timer counter reaches 0 (TIMDIS = 2). The timer 1 is configured to be active (low) when the timer 0 is enabled. This is because TIMDIS = 1 and TIMENA = 1. The compare register is configured to 16-bit counter and set to 0xFFFF. With this value the timer will never compare and always be active when the timer is enabled. To send data, you have to make sure that the previous transaction was completed and you can check this by reading the TIMSTAT flag. This flag sets each time the timer counter reaches 0. Once the TIMSTAT flag is set, you clear it and write your new data to the SHITBUF register to start the transaction. The KSDK 1.2.0 has drivers and a HAL to facilitate the configuration of the FlexIO module. Some of the important functions are: FLEXIO_DRV_Init(uint32_t instance, const flexio_user_config_t *userConfigPtr); Use this function to initialize the FlexIO module before using it. In this configuration you can change the settings in the FLEXIO_CTRL register such as: Doze Enable, Debug Enable, Fast Access and software reset. FLEXIO_HAL_ConfigureTimer(FLEXIO_Type * base, uint32_t timerIdx, const flexio_timer_config_t *timerConfigPtr); Use this function to configure a timer in the FlexIO. This function uses a configuration structure that can change the TIMCFG, TIMCTL and TIMCPM registers. FLEXIO_HAL_ConfigureShifter(FLEXIO_Type * base, uint32_t shifterIdx, const flexio_shifter_config_t *shifterConfigPtr); Use this function to configure a shifter in the FlexIO. This function uses a configuration structure that can change the SHIFTCFG and SHIFTCTL registers. FLEXIO_HAL_SetShifterBuffer(FLEXIO_Type * base, uint32_t shifterIdx, uint32_t value); Use this function to start a transmission. When writing to the SHIFTBUF register, the Shifter Status Flag is cleared. FLEXIO_DRV_Start(uint32_t instance); Use this function to enable the FlexIO module by setting the FLEXEN bit in the FLEX_CTRL register. FLEXIO_HAL_GetTimerStatusFlags(FLEXIO_Type * base); This function returns the contents of the TIMSTAT register. You can use this function to check when a transmission is finished. FLEXIO_HAL_ClearTimerStatusFlags(FLEXIO_Type * base, uint32_t mask); This function clears a specific Timer Status Flag. You can use this function to clear a flag after you read that the flag was set. To change the frequency of the transmission you have to change the value of the TIMCMP register. In dual 8-bit counters baud/bit mode, the lower 8-bits configures the baud rate divider equal to (CMP[7:0] + 1) * 2 and the upper 8-bits configure the number of bits in each word equal to (CMP[15:8] + 1) / 2. In our example the baud rate divider is set to 4, this means CMP[7:0] has the value 1. The number of bits transmitted is set to 8, this means CMP[15:8] has the value 0xF. Let’s change the baud rate divider to 32. To obtain the CMP[7:0] value, we will have to solve the simple equation: 32 = (CMP[7:0]+1)*2 CMP[7:0] = 15=0xF Now let’s change the number of bits to 16. The CMP[15:8] value is defined by: 16 = ((CMP[15:8]+1))/2 CMP[15:8] = 31=0x1F The value for the TIMCMP for the timer 0 has to be 0x00001F0F to get a baud rate divider of 32 and a word length of 16 bits. The waveform will look as follows. Figure 3. 16-bit transmission By default the shifter in the FlexIO transmits the LSB first. To change the transmission order, you have to write to the SHIFTBUFBIS (Bit swapped) register instead of the SHIFTBUF register. There are also other buffer registers: SHIFTBUFBYS and SHIFTBUFBBS. The first register swaps the bytes and the second register swaps the bytes and bits at the same time. When using one of these registers you have to be careful to consider that the length of the SHIFTBUF registers is of 32 bits, so if you choose to use the SHIFTBUFBIS for a transmission and your transmission length is not of 32 bits, you have to start writing your data starting from the most significant bit. The following image shows a MSB transmission. The value 0x6AED0000 was written to the SHIFTBUFBIS register. Figure 4. MSB 16-bit transmission The FlexIO module supports automatic start and stop bit handling. All you have to do is change the SHIFTCFG and the TIMCFG configuration bits. In the SHIFTCFG register set SSTOP to 11 if you want the stop bit to have the value 1, and set the SSTART to 10 if you want the stop bit to have the value 0. In the TIMCFG register set the TSART to 1 and the TSOP to 10. The transmission will look as the following image. Data transmitted 0x0F. Figure 5. Transmission with start and stop bit Changing the phase of the clock is very easy, you just have to set the TIMPOL bit to 1 in the SHIFTCTL register. Figure 6. Shift on negedge of Shift clock The conditions to disable and enable the timers can be configured by changing the TIMENA and TIMDIS values in the TIMCFG register. In our example the timer is enabled by the trigger high. The trigger can be set to be an external pin, a shifter status flag, or a timer output. In our case the trigger was set to the shifter status flag, but you can change this configuration to your communication needs. The timer can also be enabled when the previous timer is enabled, on a certain pin edge, or with a combination of pins and triggers. The timer in the example above disables on the timer compare. This means that when the timer counter reaches zero, the timer will disable automatically. The timer counter is loaded with the timer compare value every time it reaches zero or when it is first enabled.  The timer can also be disabled by other conditions such as: when the previous timer is disabled, on a trigger falling edge, on a pin edge, or on a combination of these. Each pin can be configured to be active high or low. When a pin polarity is changed it only affects the output of the pin, for example, if a timer is set to be the shifter clock and you change the pin polarity, the shifter clock will not change its polarity, only the output to the pin from the timer will change. The configuration for the polarity of the pins is located in the TIMCTL and SHIFTCTL. When the PINPOL value is changed to 1, the pin is active low. In the following image the polarity of the timer pin and the shifter pin was changed to 1, so they are active low. Figure 7. Timer and Shifter active low The FlexIO module can generate an interrupt from 3 sources: Shifter error, Shifter status flag and Timer status flag. To enable the interrupts you need to set the bits in the SHIFTSIEN,SHIFTEIEN and TIMIEN. If you are using KSDK you can enable the interrupt in NVIC by setting true .useInt in the FlexIO user config that the function FLEXIO_DRV_Init utilizes. The default handler for the interruption is named UART2_FLEXIO_IRQHandler. The following example configuration will configure the FlexIO module as a receiver. This configuration works with the first example configuration shown. Both tower boards (TWR-KL43Z48M) have to be connected as shown further below in the Table 1 Hardware connnections. The FlexIO module will use one Shifter, one timer, and three pins. The pins will be used for the input of the shifter, the input clock for the timer and the trigger for the timer. The timer will use pin 1 as an input and its output will be the same as the input clock. The trigger for the timer will be the transmitter chip select pin and it will be used to enable or disable the timer. The FlexIO will be configured to do an 8-bit transmission. Shifter 0 Shifter Control 0 Register (FLEXIO_SHIFTCTL0) = 0x00800001 TIMSEL = 0    Timer 0 select. TIMPOL = 1    Shift on negedge of Shift clock. PINCFG = 0    Shifter pin output disabled. PINSEL = 0    Shifter pin 0 select. PINPOL = 0    Pin is active high. SMOD   = 1    Receive mode. Captures the current Shifter content into the SHIFTBUF on expiration of the Timer. Shifter Configuration 0 Register (FLEXIO_SHIFTCFG0) = 0x00000000 INSRC  = 0    The input source of the shifter is from a pin. In our cause this doesn’t matter because our shifter is set as transmit mode. SSTOP  = 0    Stop bit disabled. SSTART = 0    Start bit disabled. Timer 0 Timer Configuration 0 Register (FLEXIO_TIMCFG0) = 0x01206602 TIMOUT = 1    Timer output is logic zero when enabled and is not affected by timer reset. TIMDEC = 2    Decrement counter on Pin input (both edges), Shift clock equals Pin input. TIMRST = 0    Timer never reset. TIMDIS = 6    Timer disabled on Trigger rising edge. TIMENA = 6    Timer enabled on Trigger falling edge. TSTOP  = 0    Stop bit is disabled. TSTART = 1    Start bit enabled. Timer Control 0 Register (FLEXIO_TIMCTL0) = 0x04C00103 TRGSEL = 4    Trigger select. Pin 2 input. TRGPOL = 1    Trigger active low. TRGSRC = 1    Internal trigger selected. PINCFG = 0    Timer pin output disabled. PINSEL = 1    Timer pin 1 select. PINPOL = 0    Pin is active high. TIMOD  = 3    Single 16-bit counter mode. Timer Compare 0 Register (FLEXIO_TIMCMP0) = 0x0000000F TIMCMP = 0x0000000F Configure 8-bit transfer. Set TIMCMP = (number of bits x 2) - 1. The shifter status flag is set every time the SHIFTBUF register has been loaded with data from the shifter. This occurs every time that the transmitter sends 8 bits of data. You can read the shifter status flag by polling or by enabling an interrupt based on your needs. This flag clears automatically when you read the SHITBUF register. During the transmission, the first thing that happens is that timer from the receiver will be enabled because the chip select signal from the transmitter is configured as a trigger. Once the timer is enabled, the timer will begin to decrement on the pin input, this means that the shifter clock of the receiver will be equal to the pin input. The transmitter shifter is configured to shift data out on the positive edge of the clock and the receiver shifter is configured to shift data in on the negative edge of the clock. After 8 bits have been transmitted, the compare register from the receiver will reach 0 and this generates an event to store the data from the shifter to the SHITBUF register and the Shifter Status Flag will be set. Finally the timer will be disabled by the chip select signal and keep waiting for another transaction. The hardware connections are shown in the following table. Signal name TWR-KL43Z48M transmitter TWR-KL43Z48M receiver Pin name Board Location Pin name Board Location Serial Data PTD0/FXIO0_D0 B46 PTD0/FXIO0_D0 B46 Clock PTD1/FXIO0_D1 B48 PTD1/FXIO0_D1 B48 Chip Select PTD2/FXIO0_D2 B45 PTD2/FXIO0_D2 B45 GND GND B2 GND B2 Table 1. Hardware connections Figure 8. Hardware connections The example projects for the FlexIO transmitter and receiver are developed in KDS 3.0.0 with KSDK 1.2.0. The application lets the user communicate with the transmitter via a serial terminal and the transmitter sends each character to the receiver via FlexIO and the receiver displays the received character on another serial terminal. To be able to compile the project, first you need to compile the library located in C:\Freescale\KSDK_1.2.0\lib\ksdk_platform_lib\kds\KL43Z4. Once the two TWR-KL43Z48M are connected as described above, import both projects into KDS, compile the platform library, and both projects. Open two serial terminals configured to 115200 bauds and run each project on a different tower. On the transmitter terminal you can write anything and it will be displayed and transmitted to the receiver tower via FlexIO and will be shown on the other terminal. Figure 9. FlexIO example application. Transmitter (left terminal). Receiver (Right terminal). The FlexIO module is also capable of generating a PWM signal by configuring one of its timers to the Dual 8-bit counters PWM mode. This mode is configured by writing 01 to TIMOD in the TIMCTL register. In this mode, the lower 8-bits of the counter and compare register are used to configure the high period of the timer output and the upper 8-bits are used to configure the low period of the timer output. The shifter bit count is configured using another timer or external signal. To calculate the frequency of the PWM signal you have to add the lower 8-bits of the counter and the upper 8-bits and divide it by the FlexIO clock*2 (Only if the timer is configured to decrement on the FlexIO clock.) The frequency of the PWM signal is given by: f = (FlexIO clock)/(TIMCMP[15:8]+TIMCPM[7:0]+2) To calculate the TIMCMP values to get a certain frequency you can solve the equation for TIMCMP TIMCMP[15:8]+TIMCPM[7:0] = (FlexIO clock)/f-2 For example, let’s say we want a 200kHz PWM signal, by using the formula above and using the FlexIO clock of 48MHz, we get that the sum of the TIMCMP values must be 238. If we want a 50% duty cycle we need to write the value 238/2 to the lower and upper 8 bits of the TIMCMP register. The waveform generated by these settings is shown in the figure below. Figure 10. 200kHz 50% duty cycle PWM signal To change the duty cycle you need to change the values of TIMCPM[15:8] and TIMCPM[7:0] but without changing the sum of both values, otherwise the frequency will also be altered. For example, if we need a 20% duty cycle we multiply 0.20*238 and 0.8*238. We round up the results and get TIMCPM[7:0] = 48 and TIMCPM[15:8] = 190. The waveform generated will look as shown in the figure below. Figure 11. 200kHz 20% duty cycle PWM signal
View full article
Producto dirigido para terapias visuales y motrices. Consiste en una matriz de 6x3 LEDs, una columna verde, una amarilla y una roja. Aleatoria mente, se encenderá un LED que se encuentra hasta arriba, y ese irá bajando por la columna de su color hasta llegar al ultimo. Cuando eso suceda, se deberá presionar el botón del color correspondiente. Si esto se realiza correctamente, se suma un punto, de lo contrario se restan tres y suena un buzzer. Los puntos se despliegan en pantalla. La velocidad del juego se puede controlar con un potenciometro y un motor Servo se mueve dependiendo del puntaje.
View full article
Hi All, NXP provide a software driver library for Kinetis M devices, the KM bare-metal drivers. It includes support for peripherals and FreeRTOS. :smileyalert:NOTE: Before creating a new FreeRTOS project for KM devices you need to download the KM driver support package and install it. You can find the instructions HERE​. FreeRTOS new project creation The following instructions will guide you to generate a new project for Kinetis M devices with all the bare-metal drivers’ support. You can either select create a new project without FreeRTOS support or with it. In this case the instructions show how to create a FreeRTOS project for IAR 7.5. Go to template folder in the KM drivers package installation folder Run the make_project by Double clicking on it The make-project application guide the user to select the appropriate application. Select the IDE for new project support according to the application requirements. NOTE: The IDEs showed are only the IDEs that its support package is installed. The new project creation also manages the debug options for the project. Select the specific debug option for your new project. Select the KM variant you are using. NOTE: For KM34Z256 devices the default option is MKMxxZ256 and is selected automatically. The creation of the project supports creating linked or standalone projects: o   Create projects in driver’s subfolder: The project will be created in the path KMxxxSWDRV_Rx_x_x\build\supported_ide\projects and all the folders and files inside the project will be linked to the real location setting virtual folders in the workspace. In this case it will not be possible to move the project from that location, doing it will cause building problems. o   Create Standalone project: The standalone project option will let us select the new project location and will link the files to the actual project location. In this case the necessary source code will be copied to a new location. This options is recommended for versions control If option 1 is selected the project will be generated, you can check the project in the mentioned folder. If option 2 is selected following instructions need to be followed. Type the path that will contain the new project. In this path project files will be installed. Type project name and press enter. Project will be created and make_project window will self-close. Project folder structure looks like next: Open the IAR project by double clicking in the .eww file of the new project. FreeRTOS project structure This section will discuss the FreeRTOS default project and main.c file structure. Here a project created for IAR 7.5 is presented as an example. There are two main folders in a FreeRTOS application. The rest of the folders and files are the same for non-RTOS applications. freertos > contains all the FreeRTOS Kernel source code project > Contains files to configure definitions, FreeMaster usage and the main function. NOTE: The main function will be always contained in a file named project_name.c This is the structure of the project_name.c file: By default the main function contains the code to create and start two different tasks. Also, in the same file, the two tasks are defined. The main function initializes the application peripherals and create task A and task B. The xTaskCreate() function creates a new task and adds it to the list of tasks that are ready to run. The functions is defined as: pvTaskCode. Pointer to the task entry function. Tasks must be implemented to never return. pcName. A descriptive name for the task. This is mainly used to ease debugging. Max length defined by configMAX_TASK_NAME_LEN. usStackDepth. The size of the task stack specified as the number of variables the stack can hold - not the number of bytes. For example, if the stack is 16 bits wide and usStackDepth is defined as 100, 200 bytes will be allocated for stack storage. The stack depth multiplied by the stack width must not exceed the maximum value that can be contained in a variable of type size_t. pvParameters. Pointer that will be used as the parameter for the task being created. uxPriority. The priority at which the task should run. pvCreatedTask. Used to pass back a handle by which the created task can be referenced. After creating the two tasks the main functions calls vTaskStartScheduler() that starts the real time kernel. After calling the kernel has control over which tasks are executed and when. The task source code looks like the following: Tasks receive pvParameters parameter, this is the one that this passed when Task is created (refer to the pvPrameters in cTaskCreate function). Each task has an infinite loop, this means the task will run continuously but the RTOS schedules will the one deciding when each task will run according to priority. Default project can be modified by user adding tasks and using RTOS services to create application. If support for a different IDE is needed you just need to change follow the instructions decribed in FreeRTOS project creation and select the IDEs required by your application. References: FreeRTOS manual from THE TOOLCHAIN​ Hope information helps! Happy FreeRTOS coding! Regards, Adrian Cano NXP FAE
View full article
As most of people familiar with FRDM-K64F which is a bit old but it is still a hot device in the market. This document focused on the ADC measurement to verify the deviation. In general, the sample code were modified /come with MCUXpresso SDK, which is an ADC polling example. ADC reading was done by two ways: 1) Polling the status register of ADC conversion complete flag until ADC conversion is done. 2) CPU core is in sleep right after ADC conversion is started by software trigger. Interrupt is generated when ADC conversion is done and CPU core wakes up by this interrupt. The value of ADC reading is measured 5000 times. And, it is averaged, also calculate max/min value. Finally, the standard deviation is calculated based on the 5000 measured value. PRINTF is a terminal console and print out by semi-hosting. Interrupt method or polling method can been selected by the define of INTERRUPT or POLLING. #define INTERRUPT 0   //ADC conversion wait for “INTERRUPT” should be defined to 1 #define POLLING 1   //ADC conversion wait for “POLLING” should be defined to 1
View full article
      Kinetis SDK是针对于Kinetis系列MCU所做的软件开发套件,又称为KSDK。它由强大的外设驱动代码库,协议栈库与示例代码库等部分组成,能够简化和加快对于Kinetis 系列MCU的应用开发。另外,Kinetis SDK是免费的工具,而且所有的硬件抽象和外设驱动软件均开放完整源代码。目前最新版本为2.0,支持 Kinetis 主流MCU,随后会不断更新完善。对于SDK支持MCU的更新情况,可登陆以下KSDK的下载页面了解。       有关KSDK的更多信息可以从网址www.nxp.com/ksdk 获得。
View full article
Hi All, This Kinetis Design Tips and Tricks document is used for those needing to have a checklist or troubleshooting document for their Kinetis hardware designs.  This will be a living document that is updated as needed. Enjoy all! Please give any and all feedback on this forum. Mike Steffen
View full article
FFT presentation for metering customers, targeted especially for KM3x / KM3x_256 devices. It briefly describes: How to Use it, and Why to Use it.
View full article
Kinetis E series MCUs target to applications where require high performance on EMC/ESD. With 5V power supply and robust IO design, Kinetis E series MCUs can help customer for a robust design. Here take a Microwave Oven demo as example, shares how to make a robust design with Kinetis E Series MCU, from hardware, software perspective.
View full article
最近,有客户反映在IAR6.6 环境中,即便在程序中配置了Kinetis的加密字段“0x40C -0x40F”,但在实际程序运行中发现这些加密位并没有被真正的写进去。现根据Colleagues的分析,结合个人的理解总结如下,描述不清楚之处希望能提出宝贵意见。 原因:新版本的IAR 6.6 为了防止用户在使用Kinetis过程中误操作导致芯片被锁死,默认将加密位Disable了,在烧录Flash的时候设了最后一道闸门,将0x40C -0x40F的值统一成0xFFFFFFFE (解密模式)。 如果要完成加密, 可以修改其Flash Loader配置。 证据:在C:\Program Files\IAR Systems\Embedded Workbench 6.5_2\arm\config\flashloader\Freescale文件夹中,查看FlashK60Dxxx128K.board文件可以看到如下描述,其中<args_doc>与</args_doc>可以理解为一些注释,需要按解决方法的步骤设置。 <args_doc>.....--enable_config_write - allow programming of 0x40C - 0x40F with user supplied data, in other case flashloader after erase of block 0 will write 0xFFFFFFFE (unsecure state).</args_doc> 解决方法: 1) 打开IAR的Options配置框,选择Debuger的Download 标签,勾选如下图所示的选项,可以看到此项目中对应的.board文件; 2) 点击edit按钮, 显示如下对话框,两处分别对应着包含不同Flash Memory的器件设备; 3) 对于不包含FlexNVM的器件,选择0x0-0xfffffff对应的条目,然后选择Edit; 4) 在下面的对话框中的extra edit 项目中填写 “--enable_config_write” , 它意味着打开了在烧录Flash的时候设置的最后一道闸门,使能了用户对加密字段“0x40C -0x40F”的配置。关于此参数选项含义,可以查看下面框中parameters description的描述。 5) 选择OK , 回到上级对话框,如下图可以看到“--enable_config_write”作为一个Extra Parameters显示出来; 6)再次选择OK,回到上层对话框。 此处不用担心OK后修改的配置会替换Flash Loader中的默认配置,因为系统会自动保存刚才的修改到一个新的board文件,并存储到当前工程的文件目录中; 7) 选择“save ”,保存; 8) 选择"OK”,然后开始下载。 9) 如果以后需要加密的时候, 可以使用新的board文件, 不需要加密的时候,选择使用IAR下面的board文件。      至此,完成整个配置过程。 关于在J_flash中选择使用加密: 1)在Jflash中选择project settings; 2)在Project settings栏选择CPU标签,勾选Device选项,并点击Freescale MKL25Z128xxx4后面的方框; 3)在如下窗口Manufacturer中选择Freescale,找到对应的Device,选择带有"allow security"的选项,就可以支持加密了。否则即便在程序中Kinetis的加密字节设置了加密,代码也不会实     际的运行。
View full article