Kinetis微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Microcontrollers Knowledge Base

讨论

排序依据:
Kinetis KV10 chip is the entry point of the V Series product, which are designed for a wide range of BLDC, PMSM and ACIM motor control and digital power conversion applications. KV10 is using ARM Cortex-M0+ core, the core frequency could up to 75MHz. And KV10 provides various feature powerful modules, such as ADC modules (2x 16-bit ADCs with two capture and hold circuits and up to 1.2 MS/s samples rate in 12-bit mode — simultaneous measurement of current and voltage phase, reduced jitter on input values improving system accuracy 12-bit mode) and DMA modules (4-channel DMA — reduced CPU loading for improved application performance). The demo is using PDB hardware trigger two ADC modules conversion (12-bit single-ended mode) at the same time; the two ADC modules will trigger each related DMA channels to transfer ADC result to ADC buffer located at SRAM (start from 0x2000_0000) when finish each conversion. The ADC DMA channel 0 will link to trigger DMA channel 2 to transfer ADC result from ADC result buffer to SPI FIFO. When DMA channel 2 transfer done, in related interrupt service routine will software trigger PDB to start the next round of ADC conversion. Below is the processing chart: For the customer requires to transfer 9 ADC conversion results out (5 of ADC0 and 4 of ADC1) , the ADC buffer need interleaved storage result from two ADC modules. Below diagram shows the detailed info: Below is the test result and test environment. It will take almost 15.4us to get and transfer all 9 12-bit ADC conversion results. The demo code is attached. The project is based on TWR-KV10Z32 Sample Code Package could be downloaded from here. Wish it helps.
查看全文
   1.  K60 eDMA 16-channel implementation Local memory containing transfer control descriptors for each of the 16 channels 32-byte TCD stored in local memory for each channel    2.  DMA memory to memory performance In the traditional M2M data movement, performance is best expressed as the peak data transfer rates In most implementations, this transfer rate is limited by the speed of the source and destination address spaces.     3.  eDMA peak transfer rate   4. Performance test         With K60 100MHz (TWR-K60D100M), implement internal SRAM-SRAM eDMA data transfer. If  transfer size setting as 32-bit in TCD Transfer Attributes (DMA_TCD_ATTR), there will has one wait state during each read/write. That's why the DMA performance doesn't up to 200MB/s as the manual stated.       We highly recommend setting DMA transfer size to 16-byte at DMA_TCD_ATTR register, it will much increase the DMA performance.(Get 162MB/s transfer rate with TWR-K60D100M board.) 5.  Testing code attached.
查看全文
ButtonRace O ∆ []   ButtonRace es un juguete simple, un pequeño invento, que permitirá cambiar la vida de los niños que sufren alguna discapacidad. Nuestra creación está diseñada de una manera muy simple que, a su vez, permite a los niños con capacidades diferentes tener el máximo aprovechamiento. En general, nuestro objetivo era desarrollar los reflejos ojo-mano y estimular el aprendizaje de los niños. Esto, sin caer en las terapias actuales, que al ser tan habituales, pueden volverse menos efectivas. En resumen, el juego consiste en que el niño debe presionar el botón correspondiente a la figura que le es mostrada, lo que permitirá que un pequeña estrella avance a través de una pista de forma determinada. El mecanismo funciona a través del uso de una tarjeta Freedom de Freescale. Además, del uso de una serie de LEDS, un servomotor y algunos sensores infrarrojos y de presión. El sistema está diseñado para darle una retroalimentación al infante, para ver si su respuesta fue correcta. Las figuras encienden en color azul en el momento en que el niño debe presionar algún botón. Dependiendo de si la respuesta fue acertada, la misma figura cambia de color a verde o rojo. Dependiendo de si la figura y el botón corresponden, además, un servomotor moverá la estrella por la pista. Después de varias respuestas correctas, la estrella llegará a una meta, donde el sistema se reiniciará automáticamente. Nuestra intención es que este sistema tan simple de aprendizaje para niños, puede ser utilizado para enseñar otras cosas, además de cumplir nuestro objetivo principal.   Original Attachment has been moved to: Buttonrace.odt
查看全文
Example of integrating CMSIS3.20 into MQX4.0.x on the TWR-K70F120M (with floating point unit) using CW10.4 using the MQX4.0.2\mqx\examples\hello2 project. In the attached ZIP file (hello2twrk70f120m_CMSIS_FPU.zip) is a MSWord document detailing the steps used.  That document name is TWR-K70F120M_CMSIS_CW10.4_MQX4.0.x.docx. Regards, David
查看全文
Printer extruders and recyclers use Motors that benefit from torque control that can be obtained by using Kinetis V, a BLDC motor  and the Freescale Motor control algorithms. A plastic waste extruder for RepRap 3D printer filament.  Image: RepRapWiki See this link for more details: How recycled plastic for 3D printing will drive sustainability and improve social consciousness - TechRepublic "Durable, shiny, new plastic -- it's what makes most 3D printers run. And as 3D printing grows in popularity and we begin to scale projects in every industry, the world is going to use a lot more of it. If the industry goal is to have 3D printers in most homes and businesses with lots of other 3D printers running constantly in manufacturing centers, we'll naturally add even more to the 33.6 million tons of plastic Americans toss each year, only 6.5% of which is recycled. It's estimated that 100 million tons of plastic is floating in the world's oceans. Each piece can take anywhere from 500 to 1,000 years to decompose."
查看全文
Simple guide to setting up a PIT to create a 1 second reccuring interrupt that toggles an LED without the use of processor expert.
查看全文
Hi All, Embedded systems industry are tending to optimized their products to offers a better performance in power management, aiming for longer battery life, using low-power modes in the application without reducing functionality. With this in mind, it arises a requirement in these compact devices, power supply monitor. This document will include a brief description of some features available in different power modes of the Kinetis family and it will focus on how we can implement these features, using KSDK 2.0, to monitor power supply voltage and detect when this voltage has fallen at determined value. This document is based MCU K21 but the same principles can be applied to any Kinetis K and L family. It will use KDS 3.2 as IDE and TWR-K21F120M evaluation board as target.   Hope you can find it useful Best Regards Jorge Alcala
查看全文
Hello,      Is your clock correctly configured, what is its frequency?   You can monitor some of clocks in K0 MCU by routing it to  PTC3/CLKOUT pin. you can get it easily by selecting desired clock on  SIM_SOPT2[CLKOUTSEL] register and configuring PTC3 for CLKOUT function.   For example to monitor  1 KHz 1 low power osillator   LPO, ---------------------------------------------------------------------------------------------------------------------------- /*  ClockOutput options */ #define CLOCKOUT_FLASH_CLOCK    2 #define CLOCKOUT_LPO                       3 #define CLOCKOUT_MCGIRC                4 #define CLOCKOUT_RTC32KHZ            5 #define CLOCKOUT_OSCERCLK0       6 /* Configure clock output option according to  */               SIM_SOPT2 = SIM_SOPT2_CLKOUTSEL(CLOCKOUT_LPO); /* Configure PTC3 as clock output) */              PORTC_PCR3 = PORT_PCR_MUX(5);   //CLKOUT function selected on PTC3 ------------------------------------------------------------------------------------------------------------------------------------                 In attached document you can find captures of all clock options,  and notes on what need to be configured to get the clock output.                        Note:       Please note that Clock out (CLKOUT) on PTC3 is not currently shown in Signal Multiplexing and Signal Descriptions of RM.  It is already reported and will be fixed on next release of Reference Manual/Data sheet.
查看全文
The KL TSI Library provides the following benefits: • Reduces time to market and development costs. Already available turn-key TSI Library for IH cooker, remote controller applications, etc. • KL TSI is a hardware touch sensing solution, without any additional peripherals, e.g. Timers, GPIO, CPU execution, as a result reduces overall system cost and size. • Enhances reliability by enabling environment adaptive algorithm, eliminating water droplet and stream influence, and filtering electromagnetic interference. • Easy to use, simplifies user interface design. Flexible TSI software library enabling customers to develop an application • FreeMaster1.4 visualizes TSI signal on screen, thus customer can debug and tune touch software simply.
查看全文
Hello Community fellows! This time I would like to thank BlackNight for giving us great material to work on. There have been several posts inquiring the uses of USB stack and Processor Expert. The examples he has worked on and now shares with all of us, include this and many more useful concepts that you'll find interesting with the use of boards. For this issue he turns his FRDM-KL25Z into a generic USB keyboard device. With a simple button press he is able to send any keyboard actions to his laptop, making such as ‘print screen’ a single button press...isn't that amazing? :smileygrin: Well, I'll say no more, you better check it out yourself!  MCU on Eclipse by Erich Styger
查看全文
1. Kinetis L系列将NMI和Reset管脚复用成GPIO需要注意的问题 2. 如何在IAR、Keil和Codewarrior中禁止掉Kinetis的NMI脚 3. Kinetis Reset管脚与外部看门狗/复位芯片接法 4. Kinetis L系列外部IO中断分配问题 5. KL2x/KL4x使用USB模块时需要注意VOUT33管脚的接法 6. Kinetis K系列SPI接口设计注意事项 7. Kinetis芯片Reset管脚出现方波的原因及解决办法
查看全文
作者 Sam Wang & River Liang    说明,本文对比8位MCU的位操作在系统升级到M0+内核的MCU后所带来的影响,可以作为客户对升级MCU时,对代码及RAM上资源的评估使用. 一)简单的I/O翻转对比.对比条件:MCU为MC9S08PT与KE02,开发平台CW10.3                   1.使用PT的代码如下:          if (!PORT_PTAD_PTAD0){             PORT_PTAD_PTAD0=1;         }else{             PORT_PTAD_PTAD0=0;}       PT的代码编译后占用9个Byte。                000002D4 000004   BRSET  0,PORT_PTAD,PORT_PTAD                000002D7 1000     BSET   0,PORT_PTAD                000002D9 202E     BRA    *+48       ;abs = 0x0309                000002DB 1100     BCLR   0,PORT_PTAD       2.KE是基于ARM的M0+内核,使用的代码如下                  if(GPIOA_PDOR & 0x1)                     { GPIOA_PCOR = 0x1;}                  else                     { GPIOA_PSOR = 0X1;}       编译后结果为                00000706:   ldr r3,[pc,#24]                00000708:   ldr r2,[r3,#0]                0000070a:   movs r3,#1                0000070c:   ands r3,r2                0000070e:   beq main+0x6c (0x718)       ; 0x00000718                00000710:   ldr r3,[pc,#12]                00000712:   movs r2,#1                00000714:   str r2,[r3,#8]                00000716:   b main+0x20 (0x6cc)       ; 0x000006cc                00000718:   ldr r3,[pc,#4]                0000071a:   movs r2,#1                0000071c:   str r2,[r3,#4]       这段M0+内核的代码编译后占用24个Byte       3.KE系列是Freescale在M0+的基础上加入了位操作引擎BME,用以优化ARM内核的位操作性能,使用BME功能的代码如下                     #define PTA0_SET   (void) (*((volatile unsigned char *)(0x4C000000+(0<<21)+0xF004))) //?==0                                                       //LAS1      第0位       GPIOA_PSOR地址的A0-A19                     #define PTA0_CLR   (void)(*((volatile unsigned char *)(0x4C000000+(0<<21)+0xFF008)))                                                      //LAS1      第0位       GPIOA_PCOR地址的A0-A19                     #define PTA0                *((volatile unsigned char *)(0x50000000+(0<<23)+(0<<19)+0xF000))                                                     //UBFX           第0位     1位           GPIOA_PDOR 地址的A0-A18                if (!(PTA0))                     {PTA0_SET; }                else                     {PTA0_CLR;}           KE的BME代码编译结果如下:                    165                if (!(PTA0)){                 00000998:   ldr r3,[pc,#24]                0000099a:   ldrb r3,[r3,#0]                0000099c:   uxtb r3,r3                0000099e:   cmp r3,#0                000009a0:   bne RTC_IRQHandler+0x18 (0x9a8); 0x000009a8                  166                PTA0_SET;                                             //Using BME                000009a2:   ldr r3,[pc,#20]                000009a4:   ldrb r3,[r3,#0]                000009a6:   b RTC_IRQHandler+0x1c (0x9ac); 0x000009ac                  168                PTA0_CLR;      //Using FASTER GPIO                000009a8:   ldr r3,[pc,#16]                000009aa:   ldrb r3,[r3,#0]       代码编译后占用20个Byte         4, CW里面有设置可以优化C编译器,具体路径在Project->Proteries->C/C++ Build->Setting->GCC C Complier->Optimization           优化后共用16个Byte                  165         if (!(PTA0)){                 0000091e:   ldr r3,[pc,#20]                00000920:   ldrb r3,[r3,#0]                00000922:   cmp r3,#0                00000924:   bne RTC_IRQHandler+0x12 (0x92a); 0x0000092a                  166                         PTA0_SET;                                             //Using BME                00000926:   ldr r3,[pc,#16]                00000928:   b RTC_IRQHandler+0x12 (0x92c); 0x0000092c                  168                         PTA0_CLR;      //Using FASTER GPIO                0000092a:   ldr r3,[pc,#16]                0000092c:   ldrb r3,[r3,#0]       5, 结果     如果单纯靠M0+内核访问寄存器,KE代码的占用空间与PT的比为24:9        如果使用KE的BME功能,代码与PT的比为16:9(使用了BME)        在判断Bit时, KE使用代码与PT的比为8:3        单单设置一个Bit时KE与PT代码占比为4:2 因此在M0+等ARM核上进行位操作,其效率比8位单片机低,使用了BME功能后,可以有效提高位操作的性能。 二)典型变量的位操作. 对比条件:MCU为MC9S08PT与KE02,开发平台CW10.3                测试代码:if (xx&1){              xx&=0xFE;       }else{             xx|=1;}       1,设置XX在0 page时,其与上面的I/O翻转结果一样,代码为9个BYTES    2,在KE中,编译结果如下,设置优化前,需要52个Bytes的代码量,26个执行周期.                                                     if (xx&1){                00000a52:   ldr r3,[pc,#64]                00000a54:   ldrb r3,[r3,#0]                00000a56:   uxtb r3,r3                00000a58:   mov r2,r3                00000a5a:   movs r3,#1                00000a5c:   ands r3,r2                00000a5e:   uxtb r3,r3                00000a60:   cmp r3,#0                00000a62:   beq main+0x5a (0xa76)       ; 0x00000a76                     200                         xx&=0xFe;                00000a64:   ldr r3,[pc,#44]                00000a66:   ldrb r3,[r3,#0]                00000a68:   uxtb r3,r3                00000a6a:   movs r2,#1                00000a6c:   bics r3,r2                00000a6e:   uxtb r2,r3                00000a70:   ldr r3,[pc,#32]                00000a72:   strb r2,[r3,#0]                     203         }}                00000a74:   b main+0x28 (0xa44)       ; 0x00000a44                     202                         xx|=1;                00000a76:   ldr r3,[pc,#28]                00000a78:   ldrb r3,[r3,#0]                00000a7a:   uxtb r3,r3                00000a7c:   movs r2,#1                00000a7e:   orrs r3,r2                00000a80:   uxtb r2,r3                00000a82:   ldr r3,[pc,#16]                00000a84:   strb r2,[r3,#0]                     203         }}       3, 设置优化后,需要22/20个Bytes的代码量,11/10个执行周期.                ldr r3,[pc,#40]                     199         if (xx&1){                0000095e:   movs r2,#1                     197         xx++;                00000960:   ldrb r1,[r3,#0]                00000962:   adds r1,#1                00000964:   uxtb r1,r1                00000966:   strb r1,[r3,#0]                     199         if (xx&1){                00000968:   ldrb r1,[r3,#0]                0000096a:   tst r1,r2                0000096c:   beq main+0x34 (0x974)       ; 0x00000974                     200                         xx&=0xFe;                0000096e:   ldrb r1,[r3,#0]                00000970:   bics r1,r2                00000972:   b main+0x34 (0x978)       ; 0x00000978                     202                         xx|=1;                00000974:   ldrb r1,[r3,#0]                00000976:   orrs r1,r2                00000978:   strb r1,[r3,#0]                0000097a:   b main+0x20 (0x960)       ; 0x00000960 如果采用以空间换时间的话,其参考代码如下.                 if (xx==0){                                 xx=1;                 }else{                                 xx=0;  }       4, 如考虑中断嵌套的话,还令需要4个Byte代码。       5, 结果 KE使用代码与PT的比为至少为20:9。      在判断Bit时, KE使用代码与PT的比为8:3.       6,使用BYTE替换Bit, 编译结果,设置优化前,需要22个BYTES.                     197         if (xx==0){                000009e8:   ldr r3,[pc,#44]                000009ea:   ldrb r3,[r3,#0]                000009ec:   cmp r3,#0                000009ee:   bne main+0x38 (0x9f8)       ; 0x000009f8                     198                         xx=1;                000009f0:   ldr r3,[pc,#36]                000009f2:   movs r2,#1                000009f4:   strb r2,[r3,#0]                000009f6:   b main+0x3e (0x9fe)       ; 0x000009fe                     200                         xx=0;                000009f8:   ldr r3,[pc,#28]                000009fa:   movs r2,#0                000009fc:   strb r2,[r3,#0]    7,设置优化后,需要16/14个BYTES的代码量.                     197         xx++;                0000095c:   ldr r3,[pc,#36]                     202                         xx=1;                0000095e:   movs r1,#1                     197         xx++;                00000960:   ldrb r0,[r3,#0]                00000962:   adds r0,#1                00000964:   uxtb r0,r0                00000966:   strb r0,[r3,#0]                     199         if (xx){                00000968:   ldrb r0,[r3,#0]                0000096a:   cmp r0,#0                0000096c:   beq main+0x32 (0x972)       ; 0x00000972                     200                         xx=0;                0000096e:   strb r2,[r3,#0]                00000970:   b main+0x20 (0x960)       ; 0x00000960                     202                         xx=1;                00000972:   strb r1,[r3,#0]                00000974:   b main+0x20 (0x960)       ; 0x00000960       8, 结果 ,在RAM的空间允许的情况下,KE使用代码与PT的比为至少为12:9. 三) 8 bit变量加1       1,在PT中对8 bit变量加1,只需要4个BYTES.    24:                 XX++; 00000014 450000   LDHX   #XX       00000017 7C       INC    ,X       2,M0+的8 bit变量加1,设置优化前,需要14个BYTES                     197         xx++;                00000a44:   ldr r3,[pc,#48]                00000a46:   ldrb r3,[r3,#0]                00000a48:   uxtb r3,r3                00000a4a:   adds r3,#1                00000a4c:   uxtb r2,r3                00000a4e:   ldr r3,[pc,#40]                00000a50:   strb r2,[r3,#0]       3,而如果使用优化设置,那么要12个BYTES                     197         xx++;                0000095c:   ldr r3,[pc,#36]                     202                         xx=1;                0000095e:   movs r1,#1                     197         xx++;                00000960:   ldrb r0,[r3,#0]                00000962:   adds r0,#1                00000964:   uxtb r0,r0                00000966:   strb r0,[r3,#0]       4, 结果 , 在8 bit变量加1时,KE使用代码与PT的比为至少为12:4,但这是32bitARM内核操作8bit变量都普遍存在效率变低的现象。 四) 16位+8位加法       1, 8 bit 编译结果,需要8个BYTES.                0000008 320000    LDHX   xx                0000000B AF01     AIX    #1                0000000D 960000   STHX   xx       2, M0+ 编译结果,设置优化前,需要10个BYTES.                00000a44:   ldr r3,[pc,#44]                00000a46:   ldr r3,[r3,#0]                00000a48:   adds r2,r3,#1                00000a4a:   ldr r3,[pc,#40]                00000a4c:   str r2,[r3,#0].       3, M0+ 编译结果,设置优化后,需要8个BYTES.                0000095c:   ldr r3,[pc,#20]                0000095c:   ldr r3,[pc,#20]                0000095e:   ldr r2,[r3,#0]                00000960:   adds r2,#1                00000962:   str r2,[r3,#0]       4,结果,M0+在16位加法时能够达到8bit单片机的效率,结果相同. 五)结论     因此用户在移植PT(或其它8 bit MCU)代码到KE02时,要选型时需要充分考虑客户原先代码具体运算情况,理论上存在使用KE后代码变大的情况.   但是使用KE等32bitM0+内核时可以在16bit或以上的乘、加运算时获得更好的效率,占用更小的代码空间和运算时间。   另外KE对GPIO的控制寄存器比PT多了一些功能,可以一次操作多个I/O,是不错的功能.
查看全文
The following document contains a list of documents , questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in Kinetis processors or MCUXpresso, you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table FAQ: MCUXpresso Software and Tools  Getting Started with MCUXpresso and FRDM-K64F  Generating a downloadable MCUXpresso SDK v.2 package  Quick Start Guide – Using MCUXpresso SDK with PINs&amp;CLOCKs Config Tools  Moving to MCUXpresso IDE from Kinetis Design Studio Kinetis Microcontrollers Guides and examples Using RTC module on FRDM-KL25Z  Baremetal code examples using FRDM-K64F Using IAR EWARM to program flash configuration field Understanding FlexIO  Kinetis K80 FAQ How To: Secure e-mail client (SMTP + SSL) with KSDK1.3 + WolfSSL for FRDM-K64F  Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+  PIT- ADC- DMA Example for FRDM-KL25z, FRDM-K64F, TWR-K60D100 and TWR-K70  USB tethering host (RNDIS protocol) implementation for Kinetis - How to use your cellphone to provide internet connectivity for your Freedom Board using KSDK Write / read the internal flash Tracking down Hard Faults  How to create chain of pbuf's to be sent? Send data using UDP.  Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading  USB VID/PID numbers for small manufacturers and such like  Open SDA and FreeMaster OpenSDAv2  Freedom OpenSDA Firmware Issues Reported on Windows 10 Let´s start with FreeMASTER!  The Kinetis Design Studio IDE (KDS IDE) is no longer being actively developed and is not recommended for new designs. The MCUXpresso IDE has now replaced the Kinetis Design Studio IDE as the recommended software development toolchain for NXP’s Kinetis, LPC and i.MX RT Cortex-M based devices. However, this documents continue to receive considerable amount of views in 2019 which means it could be useful to some people. Kinetis Design Studio New Kinetis Design Studio v3.2.0 available Using Kinetis Design Studio v3.x with Kinetis SDK v2.0  GDB Debugging with Kinetis Design Studio  KDS Debug Configurations (OpenOCD, P&amp;E, Segger) How to use printf() to print string to Console and UART in KDS2.0  Kinetis Design Studio - enabling C++ in KSDK projects  Using MK20DX256xxx7 with KDS and KSDK  Kinetis SDK Kinetis SDK FAQ  Introducing Kinetis SDK v2  How to: install KSDK 2.0  Writing my first KSDK1.2 Application in KDS3.0 - Hello World and Toggle LED with GPIO Interrupt 
查看全文
Freedog KL25Z | Linino The Freedog is a MIPS board based on the Atheros AR9331 and the Kinetis L Series KL25Z  MCUs built on ARM® Cortex™-M0+ processor. The Atheros processor supports Linino, a Linux distribution based on OpenWRT. The board has built-in Ethernet and WiFi support, a USB-A port, micro-SD card slot, 20 digital input/output pins (of which 7 can be used as PWM outputs and 12 as analog inputs), a 8 MHz crystal oscillator, a micro USB connection, an SWD header, and 3 reset buttons. The external row of the pin-header is Arduino compatible.
查看全文
This document covers some of the more common questions about the new Kinetis K8x family. Any new specific issues or questions should be posted into it's own thread, and will be added to this document as appropriate. Kinetis K80 Basics What is the K8x family? It is a new Kinetis family of Cortex-M4F devices, running up to 150MHz, that include 256K of Flash and 256K of SRAM. It features FS USB, SDRAM, QuadSPI, SPI, I2C, LPUART, and much much more. How does the Kinetis K8x family differ from other Kinetis K families? The K8x family offers the same advantages and compatibility as other Kinetis K families, but also offers several new features not found on other Kinetis K families: QuadSPI Support Dual Voltage Domains (independent VDDIO domain down to 1.8V for QuadSPI or other interfaces) EMVSIM (Euro, MasterCard, Visa Serial Interface Module) FlexIO Additionally the K81 and K82 families offer the following new security modules: LTC (Low Power Trusted Cryptography) Encryption / Decryption algorithms in hardware (as opposed to using mmCAU s/w libs) OTFAD (On The Fly AES Decryption) Zero latency decryption when executing encrypted code from QuadSPI Secure RAM 2KB of Secure Session RAM Because of the addition of a second voltage domain and QuadSPI, there is no hardware pin compatibility with previous Kinetis derivatives. However there is significant module and enablement re-use, so if you’re familiar with other Kinetis devices, it will be easy to get started with the K80. Where can I find reference manuals, datasheets, and errata? These can be found on the K8x documentation pages. Detailed information on the K81 is under NDA, so please contact your NXP sales representative for those documents. What’s the difference between the different K8x devices? K80 is the base version, which includes QuadSPI controller, SDRAM controller, FS USB, and much more. K81 adds DryIce Tamper Detect and the LTC/OTFAD modules K82 adds just the LTC/OTFAD modules K80 and K82 families have the same pin out for their respective packages. The pinout for K81 is slightly different but can still be compatible. What boards are available to evaluate the K80 family? FRDM-K82F: A Freedom board with a 100LQFP K82 device. Also includes dual QuadSPI, touch pad, Arduino compatible footprint, and FlexIO header compatible with OV7670 camera. TWR-K80F150M: A Tower board with 121XFBGA K80 device. Includes dual QuadSPI, SDRAM, EVMSIM, SDCard holder, touch pads, and more. TWR-POS-K81: A Point of Sale reference design board in tower form factor. This board is only available via your NXP sales representative. The K8x MCU Family Hardware Tools selection guide has more details on board differences. What packages are available? The 100 LQFP and 121 XFBGA packages are lead packages available today. The 144 LQFP package and the WLCSP are part of the Package Your Way (PYW) program, and you should contact your NXP sales representative if interested in those packages. What is the difference between K8x and KL8x families? The KL8x family shares many of the same features as the K8x family. The biggest differences are that the KL8x family uses the Cortex-M0+ core (instead of Cortex-M4F), has a lower max clock speed, and has less internal Flash and RAM. It also reduces the instances of peripherals available, but still includes QuadSPI, FlexIO, LTC, and BootROM peripherals like on the K80. See the KL8x Fact Sheet for more details. KL8x devices will be available in the first quarter of 2016. Software/Tools Where can I find instructions and details on the hardware used to evaluate the K8x family? FRDM-K82F: http://nxp.com/frdm-k82f/startnow​ TWR-K80F150M: http://nxp.com/twr-k80f150m/startnow ​ Which version of Kinetis SDK supports the K8x family? Kinetis Software Development Kit (KSDK) support is split depending on the evaluation platform. For TWR-K80F150M, support can be found in the Kinetis SDK 1.3 Mainline Release. For FRDM-K82F, support can be found in the Kinetis SDK FRDM-K82F Stand-alone release. Note that the FRDM-K82 standalone release is truly standalone, and does not require the mainline release to be installed. How do I run the FRDM-K82F OV7670 camera demo? See this Community post: https://community.freescale.com/docs/DOC-329438 How can I use the micro SD card reader on the TWR-K80F150M? Because the SD card signals are shared with the QuadSPI signals, the SD card slot is not connected by default. See section 3.14 of the TWR-K80F150M User Guide for details on how to connect it, with the understanding that QuadSPI will not be available on the board while using SDHC. How do I use the SDRAM on the TWR-K80F150M? See section 3.9 of the TWR-K80F150M User Guide. Due to the layout of the board, the OpenSDA UART feature cannot be used while running the SDRAM as jumpers J6 and J8 need to be removed. QuadSPI What is QuadSPI Flash? Why should I use it? QuadSPI is a name for a popular type of serial NOR flash memory that is SPI compatible, but also allows for multiple data lines (up to 4 per device, or 8 if done in parallel) with bi-directional data for increased memory bandwidth. The QuadSPI controller on the K8x also allows for Execute-In-Place (XIP) mode so that code can be executed out of this external memory. QuadSPI memory can be used for either extra memory storage or for extra code space, or a combination of both. After initialization, it appears as a readable area of memory starting at 0x6800_0000 (as well as at the alias regions). How can I program the QuadSPI? There is an example application in Kinetis SDK that shows how to program the QuadSPI at C:\Freescale\KSDK_1.3.0\examples\twrk80f150m\driver_examples\qspi For programming an entire application, the ROM bootloader can be used. Details are in the K80 Bootloader Tools Package. The Kinetis Bootloader QuadSPI User's Guide that comes as part of that package describes all the steps needed to get up and running with QuadSPI. There is also an example Kinetis SDK application that runs out of QuadSPI at C:\Freescale\KSDK_1.3.0\examples\twrk80f150m\demo_apps\hello_world_qspi_alias What performance tips are there if doing QuadSPI XIP? A few key performance factors: Ensure both the data and instruction cache is enabled Use as many data lines as possible (4, or 8 if available in dual/octal modes) Use DDR mode Any critical code should be placed in Flash/RAM for fastest performance If using XIP, code should be executed out of the QuadSPI aliased address space which starts at 0x0400_0000. A more detailed app note is under development. How do I debug code located in QuadSPI? You must make use of the aliased QuadSPI address space at 0x0400_0000. There is an example of this in the hello_world_qspi_alias example in Kinetis SDK. Due to the architecture of the M4 core on Kinetis, breakpoints cannot be set in the 6800_0000 address space, which is why the alias address space is provided. What app notes are available for the QuadSPI? Because the QuadSPI module found on the K8x family has also been used on other NXP devices, there are some app notes available that can be useful for QuadSPI development. Note that some of the implementation details and features as described in the app notes will be different for K8x, so please use the K8x reference manual for full details. AN4186​ AN4512​ AN4777​ ROM Bootloader Where can I find more information on the bootloader that comes built into the silicon of the K8x family? Download the K80 Bootloader Tools package. If interested in QuadSPI, the Kinetis Bootloader QuadSPI User's Guide that comes as part of that package describes all the steps needed to get up and running with QuadSPI. The other information found on the Kinetis Bootloader website is also useful as this is what the ROM Bootloader is based off of. What interfaces does the ROM Bootloader support? The ROM Bootloader on the K8x family can interface via LPUART, I2C, SPI, or USB HID (via BLHost) to erase and program both the internal flash and/or QuadSPI flash. This is the same bootloader found on other Kinetis devices, but also includes some more advanced features to support QuadSPI. How can I enter bootloader mode? By default, when using a Kinetis SDK project, the bootloader is disabled and the code immediately jumps to the address in Flash pointed at location 0x4. By asserting the NMI pin at reset though, the part can be forced to enter bootloader mode. This is useful for programming the QuadSPI or interfacing with the bootloader in other ways. This feature is controlled via the FOPT[BOOTPIN_OPT] bit, which the Kinetis SDK code sets to '0' to enable the NMI pin to enter bootloader mode. The NMI button on each board is: FRDM-K82F: SW2 TWR-K80F150M: SW2 The FOPT register (at 0x40C) can be modified to always go into Bootloader mode if desired. Details are in boot chapter of the K80 reference manual. Where is the bootloader configuration data found in Kinetis SDK? The Bootloader Configuration Area (BCA), which begins at address 0x3C0, is defined in C:\Freescale\KSDK_1.3.0\platform\devices\MK80F25615\startup\system_MK80F25615.c starting on line 133. You must also add the define BOOTLOADER_CONFIG in the project settings to let the linker files know to program this BCA area. The FOPT configuration register (at 0x40D) is defined in C:\Freescale\KSDK_1.3.0_K82\platform\devices\MK82F25615\startup\<compiler>\startup_MK80F25615.s and by default is set to 0x3D which disables the bootloader, but does enable the option to enter bootloader via the NMI pin at reset (see previous question) How can I use the UART port on the FRDM-K82F with the BootROM? The OpenSDA/UART lines on the FRDM-K82F use LPUART4, which is not used by the BootROM. If you would like to use the serial UART lines to interact with the BootROM, you can blue wire a connection from either J24 or J1, and connect to R32 (RX) and R36 (TX). This was due to muxing trade-offs. The OpenSDA/UART lines on the TWR-K80F150M are connected to UART1 and thus no modification is necessary for that board. Also keep in mind that you can use the USB interface with the BLHost tool on both boards with no modification. The examples in Kinetis SDK setup the QuadSPI Configuration Block (QCB) data using a qspi_config.bin file. How can I generate my own custom QCB file? There is a C file that come as part of Kinetis SDK (C:\Freescale\KSDK_1.3.0\examples\twrk80f150m\demo_apps\hello_world_qspi\qspi_config_block_generator.c) or in the KBoot zip file, that can be compiled with various toolchains on a host computer, that will then produce a .bin file. You could import this file, and then after compilation, run it, and it will write out the new .bin to your hard drive. There is a tool under development that simplifies this process by reading in that example .bin file and then you can modify the fields in the app, and then it will write out the modified .bin file. Can I jump directly to QuadSPI for Execute in Place (XiP) after booting? Yes. However note that you must still put the Bootloader Configuration Area (BCA) into internal flash. And you also may want to put the QuadSPI Configuration Block (QCB) in flash as well since it needs to be read before the QuadSPI is setup. Thus even if all your code is in QuadSPI address space, the internal flash must also be written at least once to put in the configuration data. Once you have that set though, then you can develop code by only programming the QuadSPI address space. Troubleshooting I’m having debugger connection issues when using an external debugger, like a Segger JLink. Why? It’s likely that the OpenSDA circuit is interfering, and thus needs to be isolated via jumpers on the board. For TWR-K80F150M: Pull J16 and J17 For FRDM-K82F: Pull J6 and J7 Also make sure you are using the correct debug header for the K8x device on the board: For TWR-K80F150M: J11 For FRDM-K82F: J19 Where is the CMSIS-DAP/OpenOCD debug configuration for the K8x family in Kinetis Design Studio? KDS 3.0 does not support programming the K8x family via the CMSIS-DAP interface. You will need to change the OpenSDA app on the board to either J-Link or P&E as described in the K8x Getting Started guides (Part 3). I can't get OpenSDA on the FRDM-K82F into bootloader mode. Make sure jumper J23 is on pins 1-2 to connect the reset signal to the OpenSDA circuit. On some early versions of the board this was incorrectly installed on pins 2-3 instead. When using IAR with the default CMSIS-DAP debug interface, I sometimes get the error: “Fatal error: CPU did not power up” This is an issue in some older versions of IAR. Upgrade to at least version 7.40.5 which fixes this. When using KDS with the JLink interface with the FRDM-K82F board, I get an error. If you see the error "The selected device 'MK82FN256XXX15' is unknown to this version of the J-Link software." it's because the J-Link driver that comes with KDS 3.0.0 does not know about the K82 family. You can either select a MK80FN256XXX15 device (which is compatible with the K82 on the board) or update the JLink software by downloading and installing the latest JLink Software and documentation pack. At the end of the installation process it will ask to update the DLLs used by the IDEs installed on your computer, so make sure to check the KDS checkbox on that screen. I’m using the P&E OpenSDA App and debugging is not working. I get either "Error reading data from OpenSDA hardware. E17925" or “The system tried to join a drive to a directory on a joined drive” in KDS If using IAR, make sure you have the latest version (7.40.7 or later) If using KDS, you need to update the P&E plugin in KDS. Go to Help->Check for Updates, and select the P&E debug update. Make sure not to select the other debugger updates as it will break it in KDS 3.0.0 (see this thread)
查看全文
当芯片被加密后,在Keil或IAR中下载或者调试时,会弹出以下提示信息: 这时如果点击Yes,那么将会对Flash进行一次mass erase,这样就可以重新下载或者调试程序了。 如果把Do not show this message again复选框勾选上的话,那么以后将不再弹出此提示框,并且会自动进行一次mass erase。 实际使用中,不建议勾选Do not show this message again这一复选框,因为勾上之后就无法直观的看到芯片被锁的提示了。 如果不小心把这一复选框勾上了的话,想要恢复到原来的设置,只能通过修改注册表的方法来实现,具体步骤如下 1) 在CMD窗口下,输入regedit,打开注册表    2)设置 HKEY_CURRENT_USER => Software => SEGGER => J-Link => DontShowAgainUnlockKinetis 为0   
查看全文
¡EL GRAN DÍA HA LLEGADO, PARTICIPA Y ELIGE AL MEJOR! Te esperamos en el Centro de Congresos del Tecnológico de Monterrey Campus Guadalajara, la exhibición de los proyectos estará disponible a partir de las 09:00 hrs. Se nombrará al ganador a las 13:00 hrs. En seguida de la premiación de The Freescale Cup. La votación se abrirá a las 9:00hrs. Y se cerrará a las 12:30hrs, se tomarán en cuenta solo las interacciones realizadas dentro de este horario. Vota y califica tu proyecto favorito, sigue 2 pasos: 1. VOTA Elige solo UNA de estas 2 opciones. Ingresa a tu cuenta Twitter Publica el hashtag del proyecto #KinetisChallenge Ingresa al Facebook de Freescale University Programs Encuentra la liga y contesta la encuesta, o si lo prefieres puedes hacerlo desde el siguiente acceso.: https://es.surveymonkey.com/s/JQY76J9 2. CALIFICA Califica cada uno de los proyectos de acuerdo a los criterios de selección. Ingresa a https://apps.facebook.com/ranktab/rt.php?l=1452 Califica cada proyecto con los 3 criterios. Observa la matriz de burbujas para ver la opinión de los participantes. Comparte tu calificación en tu muro. Se tomarán en cuenta la sumatoria de votos en Twitter y Survey Monkey; así como la calificación en RankTab. ¡LA ELECCIÓN ESTÁ EN TUS MANOS!
查看全文
This file describes how to install KSDK, is easy and simple with images and descriptions step by step, so you wont have problems with the installation.
查看全文
Este teclado interactivo, esta hecho para ayudar a discapacitados en su desarrollo motriz. El teclado contara con cuatro botones, los cuales tienen un led en la parte superior y un sensor piezoelectrico. El LED superior se enciende, avisando al paciente que debe presionar el boton. El boton al ser presionado, activa al sensor, el cual manda una señal a la tarjeta freedom y prende un LED verde si activo el boton indicado o rojo si se equivoco. Finalmente el resultado de los botones activa un servomotor.   Ficha técnica del proyecto, indicando una descripción breve de su funcionamiento y especificaciones técnicas. Requerimientos técnicos para la exhibición del demo, como conexiones para lap top o conexión de internet.   Ficha tecnica Teclado interactivo para discapacitados Descripcion Este teclado se controla con la computadora. Tiene 4 botones y cada uno tiene un LED en la parte superior. El terapeuta elije que LED prender y el paciente debe presionar el botón correspondiente. Si presiona el botón debido, se prendera un LED verde y girara un servomotor, si se presiona cualquiera de los otros botones, se encenderá un LED rojo y el servomotor no reaccionara. Especificaciones de construcción Construcción: madera, MDF. Microcontrolador: Tarjeta Freedom Servomotor (x1) Capacitores cerámicos: microfaradios (x4) Sensores Piezoelectricos (x4) Leds (x6) Resistencias: 10K (x10) Requerimientos tecnicos Conexión USB a una computadora con programa Realterm para la comunicación serial.           Video final Tapete interactivo video final - YouTube Original Attachment has been moved to: codigo-teclado.txt.zip
查看全文