Kinetis微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Microcontrollers Knowledge Base

讨论

排序依据:
As we know, uC/OS –II is a scalable, ROMable, preemptive real-time kernel that manages multiple tasks and it has been ported to more than 45 CPU architectures.  In this article, you can learn the steps of porting uC/OS –II to MAPS-22. Downloading uC/OS-II source code and application project To obtain the μC/OS-II source code and projects, simply point your favorite browser to: www.Micrium.com/Books/Micrium-uCOS-II. You will be required to register. This means that you’ll have to provide information about yourself. Download and execute the following file: Micrium-Book-uCOS-II-TWR-K53N512.exe. Fig 1 shows the directory structure created by this executable. All files are placed under the \Micrium directory. There are two main sub-directories: \Examples and \Software and they are described below. Fig 1 Directories and Files μC/OS-II is fairly easy to use once it is understood exactly which source files are needed to make up a μC/OS-II-based application. Fig 2 shows the μC/OS-II architecture and its relationship with hardware. Of course, in addition to the timer and interrupt controller, hardware would most likely contain such other devices as Universal Asynchronous Receiver Transmitters (UARTs), Analog to Digital Converters (ADCs), Ethernet controller(s) and more. Fig 2 F2-(1) The application code consists of project or product files. For convenience, these are simply called app.c and app.h, however an application can contain any number of files that do not have to be called app.*. The application code is typically where one would find the main(). F2-(2) The Board Support Package (BSP) code needed by μC/OS-II is typically quite simple and generally, μC/OS-II only requires that you initialize a periodic interrupt source which is used for time delays and timeouts. This functionality can be placed in a file called bsp.c along with its corresponding header file, bsp.h. Semiconductor manufacturers often provide library functions in source form for accessing the peripherals on their CPU or MCU. These libraries are also part of the BSP. F2-(3) This is the μC/OS-II processor-independent code. This code is written in highly portable ANSI C. F2-(4) This is the μC/OS-II code that is adapted to a specific CPU architecture and is called a port. F2-(5) Configuration files are used to define μC/OS-II features (os_cfg.h) to include in the application, specify the size of certain variables and data structures expected by μC/OS-II, such as idle task stack size and tick rate among others. Below is a summary of all directories and files involved in a μC/OS-II-based project (Fig 3). The“<-Cfg” on the far right indicates that these files are typically copied into the application directory and edited based on the project requirements. Fig 3 Porting Steps 1. Copy uC/OS-II source code to ~\MAPSK22_SC\Libraries which includes peripheral driver files, startup code and devices header 2. Copy os_cfg.h, app_cfg.h which reside in ~\Micrium-Book-uCOS-II-TWR-K53N512\Micrium\Examples\Freescale\TWR-K53N512\(project name) to ~\MAPSK22_SC\Project\MAPSK22\1-Template\src Summary: configuration files os_cfg.h, app_cfg.h should be adapt to the specific requirements of the application code 3. Copy lib_def.h which resides in ~\Micrium\Software\uC-LIB to ~\MAPSK22_SC\Libraries\drivers\K\inc 4. Adds systick timer initialization function in system_MK22F51212.c void SystemTickInit (void) {   uint32_t cpu_clk_freq;   uint32_t cnts;   cpu_clk_freq = SystemCoreClock;    cnts  = cpu_clk_freq / (uint32_t)OS_TICKS_PER_SEC;            OS_CPU_SysTickInit(cnts);     5. Modify the interrupt vector 6. Create uC/OS-II group in the workspace, then add the uC/OS-II source code and os_cfg.h, app_cfg.h 7. Add application code in the main.c and please check the attachment. 8. Modify the Include Directories    Run the uC/OS-II application After build the modified application code, then run it on MAPS-K22 board(Fig 4). Fig 4 You can find the LED3 and LED4 flash every 2s, however for the LED1 and LED2, it’s 1s. And some informations’re illustrated in the Hyper Terminal (Fig 5)
查看全文
Update of FreeMASTER component for PE
查看全文
To do: Same as exercise 5 but now with interrupts.   In this exercise, you realize a windscreen wiper with the Tower. The LEDs simulate the moving wiper by running from left to right and back again. The user interface is simple: With pushbutton1, the time delay interval is increased in steps of 1 second starting from 5 seconds delay down to 1 second and further to continuous wiping. With pushbutton2 the delay is decreased in the same way. If the delay is decreased, the wiper should start immediately, because right now there is a need for wiping. This is not true for increasing the delay. In this case, wait till the current delay time is over, set the new delay. In technical terms: Use asynchronous interval reset for decrease and synchronous reset for increase.   Use the timer and the port interrupts for the pushbuttons in this Kinetis exercise.   Result: TWR_K60_wiper_int.zip Original Attachment has been moved to: TWR_K60_wiper_int.zip
查看全文
General Purpose Input/Output module presented by Jose Maria Casillas, Freescale TIC. Module explanation and alternative pin´s functions. Short explanation on the Bit Manipulation Engine (BME). Hands-On: LED RGB. Push Button. Módulo GPIO (General Purpose I/O) presentado por Jose María Casillas, Freescale TIC. Explicar el modulo y las funciones alternativas de los pines. Breve descripción del Bit Manipulation Engine (BME). Hands-On: LED RGB. Push Button.
查看全文
This document introduces basic usage of NVIC based on Freescale Kinetis. please see the attached document for details.
查看全文
The NXP VID/PID program (Vendor ID and Product ID program) is available for major NXP MCU families such as LPC, Kinetis, MCX, i.MX RT series and the i.MX series of MPUs. The USB VID/PID Program enables NXP customers without USB-IF membership to obtain free USB Product IDs (PIDs) under the NXP Vendor ID (VID).   What is USB VID/PID Program? The NXP USB VID program will allow users to apply for the NXP VID and get up to 3 FREE PIDs. For more details, please create a support ticket and associated FAQ below.   Steps to apply for the NXP USB VID/PID Program Step 1: Create a support ticket with relevant details for instance company name, PIDs, purpose. Step 2: NXP will review the request and if approved, will issue you the PIDs. Note: The moment we receive a customer's request to the time they obtain a free VID/PID, there may be a delay of a month. FAQ for the USB VID/PID Program Can I use this VID for any microcontroller in the NXP portfolio? >> No. This program is intended to cover the major MCU and MPU families listed at the top of this page.   What are the benefits of using the NXP VID/PID Program? >> USB-IF membership not required >> Useful for low volume production runs that do not exceed 10,000 units >> Quick time to market   Can I use the NXP VID and issued PID/s for USB certification? >> You may submit a product using the NXP VID and issued PID/s for compliance testing to qualify to use the Certified USB logo in conjunction with the product, but you must provide written authorization to use the VID from NXP at the time of registration of your product for USB certification. Additionally, subject to prior approval by USB-IF, you can use the NXP VID and assigned PID/s for the purpose of verifying or enabling interoperability.   What are the drawbacks of using the NXP VID/PID program? >> Production run cannot exceed 10,000 units. See NXP VID application for more details. >> Up to 3 PIDs can be issued from NXP per customer. If more than 3 PIDs are needed, you have to get your own VID from usb.org: http://www.usb.org/developers/vendor/ >> The USB integrators list is only visible to people who are members of USB-IF. NXP has full control on selecting which products will be visible on the USB integrators list.   How do I get the VID if I don't use NXP’s VID? >> You can get your own VID from usb.org. Please visit http://www.usb.org/developers/vendor/   Do I also get the license to use the USB-IF’s trademarked and licensed logo if I use the NXP VID? >> No. No other privileges are provided other than those listed in the NXP legal agreement. If you wish to use USB-IF’s trademarked and licensed USB logo, please follow the below steps:                 1. The company must be a USB vendor (i.e. obtain a USB vendor ID).                 2. The company must execute the USB-IF Trademark License Agreement.                 3. The product bearing the logo must successfully pass USB-IF Compliance Testing and appear on the Integrators List under that company’s name.   Can I submit my product for compliance testing using the NXP VID and assigned PIDs? >> Yes, you would be able to submit your products for USB-IF certification by using the NXP VID and assigned PID. However, if the product passes the compliance test and gets certified, it will be listed under “NXP Semiconductors” in the Integrators list. Also, you will not have access to use any of the USB-IF trademarked and licensed USB logos. How long does it take to obtain the PID from NXP? >> It can take up to 4 weeks to get the PIDs from NXP once the application is submitted.   Are there any restrictions on the types of devices that can be developed using the NXP issued PIDs? >> This service requireds the USB microcontroller to be NXP products.   Can I choose/request for a specific PID for my application? >> No. NXP will not be able to accommodate such requests.
查看全文
unexplained secured, unexplained locked and unexplained link error.
查看全文
Share some information on how to use micro-trace buffer.
查看全文
What is it KSDK? = Kinetis Software Development Kit Kinetis SDK v2 is a collection of comprehensive software enablement for NXP Kinetis Microcontrollers that includes: •system startup •peripheral drivers •USB and connectivity stacks •Middleware •Real-time operating system (RTOS) kernels. Documents – Release Note, API Reference Manual, Getting Started with KSDK, for USB – User Guide, USB Composite Device Guide, USB Device Reference Manual and USB Host Reference Manual. All these documents is possible to find at Software Development Kit for Kinetis MCUs|NXP or <ksdk_path>\SDK_2.0_selected_device\docs KSDK Structure Diagram KSDK Features •ARM® and DSP standard libraries, and CMSIS-compliant device header files which provide direct access to the peripheral registers •Open-source peripheral drivers •Open-source RTOS wrapper driver •Real time operation systems (RTOS) including FreeRTOS OS, μC/OS-II, and μC/OS-III •Stacks and middleware in source or object formats including: − CMSIS-DSP -  a suite of common signal processing functions − FatFs - a FatFile System for small embedded systems − mmCAU - Memory-Mapped Cryptographic Acceleration Unit − SDMMC - software component supporting SD Cards and eMMC − DMA Manager - software component used for managing on-chip DMA channel resources − mbedTLS and WolfSSL - cryptographic SSL/TLS libraries − lwIP and USB Stack - a light-weight TCP/IP stack KSDK Evolution KSDK v1/v2 – what new features KSDK 2.0 brings •MQX Kernel removed from KSDK -> focus on FreeRTOS •MQX RTCS Ethernet and MFS File System Stacks -> lwIP and FatFS •OSA, Power Manager and Clock Manager -> no longer required by the drivers •USB Stack re-write -> BSD licensed solution •No platform library -> single project with all needed files •Mbed TLS now included as part of the accelerated cryptography drivers •Eliminates separate HAL and Peripheral Driver -> single driver for each peripheral •Processor Expert -> Kinetis Expert Tool •Updates for KDS -> via online update tool •Installation of KSDK -> KEX Tool (smaller download & sizes) •KEX Tool -> pin muxing selection & generation, clock configuration, low power estimation Simplified folder structure KSDK highlights & benefits •Collection of software enablement offered by free •KSDK is fully supported in these IDE: − Atollic® TrueSTUDIO® − GNU toolchain for ARM® Cortex® -M with CMake build system − IAR Embedded Workbench − Keil™ MDK-ARM − Kinetis Design Studio IDE •KSDK supports most of Kinetis MCUs •Created examples for drivers, USB, RTOS, demo applications •Start with development without device register knowledge Support & download Official support of KSDK: Kinetis Software Development Kit Create new SR according to: How to submit a new question for NXP Support More about KSDK... KSDK Official Website www.nxp.com/ksdk Introducing Kinetis SDK v2 https://community.freescale.com/docs/DOC-329783 Kinetis SDK 2.0 Transition Guide Kinetis SDK 2.0 Transition Guide KSDK Community https://community.freescale.com/community/kinetis/kinetis-software-development-kit Let´s continue in reading! See Let´s start with FreeMASTER!​
查看全文
Hello everyone, I have attached the audio recordings of the seminar. Each of them fits the presentations uploaded in the previous post.
查看全文
分享自China-FAE team同事,在此谢过! 有客户需要bootloader功能,于是从网上下到最新版本的AN2295,发现里面添加了很多的内容,包括支持了很多新的器件,比如KM系列,但是真正把它在板子上跑起来,却花了2天时间,为了减少大家工作量,不在重蹈覆辙,我在这里share给大家,目前该代码在FRDM_KL25以及TWR-K60D100M上跑起来了。遇到的问题主要有如下几点: 问题1: 在工程中使用除法命令: a =a /100; 会报错: Error[Li005]: no definition for "__aeabi_uidiv" [referenced from D:\Customer\XinRuiYang\an2295sw_Kl25\src\Kinetis\IAR_6_4\Kinetis L Debug\Obj\bootloader.o] 原因是: 这里Lib选择的是None,说明没有使用任何库,所以不能使用除法。 打开库后,可能会占用比较大的空间,所以不推荐使用。 问题2: FRDM_KL25使用默认代码频率,波特率有问题,发送data = 0但是实际发送值为0x80,通过更改主频为48M,然后分频解决。附件有参考代码。TWR-K60100DM没有此问题。 问题3: FRDM_KL25板子,如果不使能BOOTLOADER_AUTO_TRIMMING这个宏,即不调用SlaveFrequencyCalibration();函数时, 代码上电不能直接运行,而使能该函数后,会一直进行校准频率,上位机无法通讯,查找代码发现: 上版代码为         #if BOOTLOADER_AUTO_TRIMMING == 1                       if(UART_GetChar() != BOOT_CMD_ACK)              {                SlaveFrequencyCalibration();              }                                        #endif 本版代码为:         #if BOOTLOADER_AUTO_TRIMMING == 1                         SlaveFrequencyCalibration();                     #endif 修改为上版代码,可以正常运行并跑起来。 但是不使能BOOTLOADER_AUTO_TRIMMING这个宏,代码依旧跑不起来,现象就是仿真时没有问题,可以正常跑起来,但是如果是上电直接运行,就不能正常通讯: 这个问题出在了USB插拔瞬间,KL25会收到一个数据,该数据并不是上位机下发的FC码,如果不使能BOOTLOADER_AUTO_TRIMMING这个宏,代码会误认为自己进入 等待上位机下发数据的状态机,导致通讯错误。在SlaveFrequencyCalibration(); 函数中,有软件复位功能,会让插拔稳定后KL25不在接收到异常数据,以此保证状态机的正确。 问题4: 仿真时全速跑起来时,指针经常回到__main,说明波特率有问题,代码进入SlaveFrequencyCalibration中,复位了。 AN2295引导MQX Keil工程 AN2295的文档已经说明如何修改CW IAR的工程以便让Bootlaoder引导,但是没有Keil工程的说明,这个就只能自己动手啦。 首先肯定会想到修改scf文件: #define USERFLASH_BASE_ADDR    0x00060000 #define INTFLASH_BASE_ADDR     0x00000000 #define INTFLASH_SIZE          (USERFLASH_BASE_ADDR - INTFLASH_BASE_ADDR) #define MY_ALIGN(address, alignment) ((address + (alignment-1)) AND ~(alignment-1)) LOAD_REGION_INTFLASH INTFLASH_BASE_ADDR INTFLASH_SIZE {     VECTORS INTFLASH_BASE_ADDR     {         vectors.o (.vectors_rom,+FIRST)         vectors.o (.cfmconfig)     }     CODE +0     {         * (InRoot$$Sections)      ; All library sections for example, __main.o,                                   ; __scatter*.o, __dc*.o, and * Region$$Table         * (KERNEL)         * (TEXT)         * (+RO)     }     RAM_VECTORS 0x1FFF0000 ; For ram vector table. Used when  MQX_ROM_VECTORS is set to zero.     {         vectors.o (.vectors_ram)     }     NOUSER +0     {         * (.nouser)     }     ROUSER MY_ALIGN(ImageLimit(NOUSER), 32)     {         * (.rouser)     }     RWUSER MY_ALIGN(ImageLimit(ROUSER), 32)     {         * (.rwuser)     }     DATA MY_ALIGN(ImageLimit(RWUSER), 32)     {         * (+RW)         * (+ZI)     }     USB_BDT MY_ALIGN(ImageLimit(DATA), 512)     {         * (.usb_bdt)     }     KERNEL_DATA_START MY_ALIGN(ImageLimit(USB_BDT), 0x10)     {         * (KERNEL_DATA_START)     ; start of kernel data     }     KERNEL_DATA_END 0x2000FFF0      ; RAM_END     {         * (KERNEL_DATA_END)     ; end of kernel data     }     ; mem_init writes a storeblock_struct at the end of kernel data,     ; max size 32 bytes, so use 0x100 offset     BOOT_STACK_ADDR 0x2000FEF0     {         * (BOOT_STACK)     } } 都是按偏移算的,应该只改INTFLASH_BASE_ADDR     0x00004000就O了,找了个最简单的工程:mqx\examples\hello,编译生成S19文件,通过bootloader下载进片子, 按reset后看屏幕,始终木有出现hello world,没办法,只能上debug了。 打开AN2295工程,加载调试环境,然后在JumpToUserApplication函数上下断点,中断后,单步执行到在__asm("mov pc, r1"); 函数,继续在汇编窗口点单步执行,之后就完全跟crack有点类似,一直点,直到芯片复位,说明之前点那一下是key point,然后对照map文件,于是找到了复位点: init_hardware->_bsp_initialize_hardware->_bsp_watchdog_disable();执行后会复位 不管啦,直接把它屏蔽掉,反正之前就已经关闭看门狗了。 重新编译,继续上。 还是没看到期待已久的hello world,肿么办? 重复上面的方法,发现又一个key point: _sched_start_internal 查看代码发现,这是一个系统call,应该是从vector 11调用的,查看下寄存器: SCB_VTOR 肿么变成0了,bootloader中已经改成0x4000了,什么时候变成0了....... 代码太多了,不知道从哪儿看起,内存断点是个好东西哈,IAR中没找见在哪儿下,算了,换Keil吧。 用Keil打开AN2295工程,加载调试,然后在0xE000ED08(SCB_VTOR )下写断点,直接run,等待中断吧: _time_set_timer_vector函数修改了SCB_VTOR, 大概路径是_bsp_enable_card->BSP_INTERRUPT_VECTOR_TABLE->BSP_TIMER_INTERRUPT_VECTOR 哈哈,找代码看看: __VECTOR_TABLE_ROM_START 是这个宏搞的鬼。 仔细对比代码,发现__VECTOR_TABLE_ROM_START 这个宏是通过条件编译区分开的,IAR是通过icf文件定义的 而Keil是通过#define 来实现的。好了,修改对应的值为0x4000,重新编译,下载,搞定,可以看到hello world喽。 总结一下,使用AN2295引导MQX Keil工程需要做以下3点修改: 1.scf文件INTFLASH_BASE_ADDR     0x00000000改为0x00004000 2.屏蔽_bsp_watchdog_disable()该函数 3.修改__VECTOR_TABLE_ROM_START为0x00004000.
查看全文
  Hello Freedom community users Few weeks before, I produced for the Element14 community a full video review of the FRDM-KL46Z including all the steps to program and debug your first project example. Video has a length of less than 13 min so your evaluation of the Kinetis KL46 should be really quick and easy http://www.element14.com/community/community/designcenter/kinetis_kl2_freedom_board/blog/2014/06/17/frdm-kl46z-full-review-and-getting-started-in-video Enjoy Greg
查看全文
As general introduction on thread https://community.freescale.com/docs/DOC-328302 , I did a smart LED application with GoKit and FRDM-KL02. In this design, FRDM-KL02 will communicate with GoKit by WIFI, and control LED flash. Code Structure Code Basic Introduction In this project structure, you need to do following items on code. ü Add your functions, such as UART, LED, motor driver code. ü Add function running functions in protocol.c ü Add functions order in main loop. You can find my main.c and protocol.c as attachment. In this document, I would like to detail introduce function MessageHandle(), void MessageHandle(void) {                 pro_headPart    tmp_headPart; //Common command package                 memset(&tmp_headPart, 0, sizeof(pro_headPart));                 if(get_one_package)                 {                                                                              get_one_package = 0;                                 memcpy(&tmp_headPart, uart_buf, sizeof(pro_headPart));                                                                 //CRC error, send back error command                                 if(CheckSum(uart_buf, uart_Count) != uart_buf[uart_Count-1])                                 {                                                 SendErrorCmd(ERROR_CHECKSUM, tmp_headPart.sn);                                                 return ;                                 }                                 So, you can see that only get_one_package=1, we can receive frame completely.                                 switch(tmp_headPart.cmd)                                 {                                                              case       CMD_GET_MCU_INFO:                                                                 CmdGetMcuInfo(tmp_headPart.sn);                                                                                                                                     break;                                                                   case CMD_SEND_HEARTBEAT:                                                                 SendCommonCmd(CMD_SEND_HEARTBEAT_ACK, tmp_headPart.sn);                                                                                 break;                                                 case CMD_REBOOT_MCU:                                                                 SendCommonCmd(CMD_REBOOT_MCU_ACK, tmp_headPart.sn);                                                 case       CMD_SEND_MCU_P0:                                                                 CmdSendMcuP0(uart_buf);                                                                 break;                                                 case       CMD_REPORT_MODULE_STATUS:                                                                 CmdReportModuleStatus(uart_buf);                                                                 break;                                                 default:                                                                 SendErrorCmd(ERROR_CMD, tmp_headPart.sn);                                                                 break;                                 }                              } } After that, you can do operations mentioned in thread https://community.freescale.com/docs/DOC-328302. You can see smart LED device and been found.
查看全文
This file was uploaded by the AN4652 author, and is changed from the original release. As far as I can see this file is not in the current zip for the appnote as of apr 25 2013
查看全文
系统框图如下图示: 硬件设计支持如下扩展功能: (1)      USB、SD卡(SDHC接口) (2)      SWD调试+串口Printf。 (3)      SPI外设接口,支持NRF24L01、W5100、WIFI等。 (4)      两路差分ADC输入、一路DAC输出。 (5)      50M有源晶振,供MCU以及以太网PHY工作。 (6)      32.768K RTC时钟晶振。 (7)      SPI Flash、EEPROM(IIC接口) (8)      CAN接口。以太网应用。 (9)      TSI电容触摸按键。 (10)  GPIO:按键输入以及LED输出指示。 (11)  PWM输出。 (12)  FlexBus总线扩展: 扩展应用一:4.3寸LCD。 扩展应用二:FPGA扩展高速ADC采集。(设计进行中) 基于K60+SSD1963驱动4.3寸屏并移植ucGUI的测试实例,移植后的视频效果见如下链接: http://v.youku.com/v_show/id_XNzAwMTE5OTA0.html?firsttime=15 Pixels/sec: 16397220。
查看全文
Our debug firmware is generally downloaded from the official website of nxp. nxp.com/opensda. But sometimes we want to modify the source code of bootloader and firmware according to our own requirements. So we introduce the open source project daplink. Arm Mbed DAPLink is an open source software project that can program and debug application software running on the Arm Cortex CPU. DAPLink is usually called interface firmware, and it runs on the auxiliary MCU connected to the SWD or JTAG port of the application MCU. It provides k20 bootloader and interface firmware and k26 bootloader and interface firmware. Many frdm boards use k20 as a debugger, and a few boards use k26 as a debugger. board:FRDM-K64 OS:WIN10   steps: 1.Install git, python2.7.11 or above, add these two software to the computer system environment variables (required), it is best to add the scripts folder under python to the environment variables, and install keil.  DAPlink currently only supports IDE keil. 2.Use python to install pip, you can search for tutorials online 3.Install virtualenv, use powershell (hold down shift and click the right mouse button), Input ‘pip install virtualenv’ 4.After that, the commands are all completed under powershell. Get the source code. Input ‘git clone https://github.com/mbedmicro/DAPLink’ Note: You must use git to download the code, or you will fail at compiling the code. It Will generate a DAPLink folder in your current directory 5.Enter the directory. Input ‘cd DAPLink’, The docs/DEVELOPERS-GUIDE.md under this folder is more detailed how to use this DAPLink 6.Create a virtual environment,Input ’virtualenv venv’ 7.Input ‘venv/Scripts/activate.bat’ to active the virtual environment 8.Install necessary tools,’pip install -r requirements.txt’ 9.Generate keil project, input ‘progen generate -t uvision’ It will generate projectfiles/uvision, enter the folder and you will find various bootloader and firmware. The name with ‘bl’ is the bootloader, and the name with ‘if’ is the interface firmware, which is to be dragged into the mcu. Open the first project about k20. After compilation, a bin file will be generated. The bin file with crc is what we want to burn or drag. For the name ‘if’ is the same. The git command will be called during compilation. If you do not add this command to the environment variable, the compilation will fail. This is the bootloader source code Bin file This is interface firmware. The generated bin file with ‘0x’ is firmware address. Generally, the default firmware address of the DAPLink bootloader is 0x8000. As you can see from the above figure, this macro defines DAPLINK_ROM_IF_START, so the file we want to drag is the file with the name ‘0x8000’. If the firmware start address is modified in the bootloader, the interface firmware should also be modified accordingly Burn the bootloader into k20, then drag the interface firmware into k20 to see this result.  
查看全文
Here you can find both the code and project files for the Serial communication project, in this example the serial port (UART) is configured to establish communication between the computer using a serial terminal and the evaluation board. The default baud rate for the serial port is 9600 bauds. The code also implements an echo function, any key pressed in the computer's keyboard will be captured and displayed in the serial terminal. If your computer does not have a serial terminal you can download Tera Term from the following link: Tera Term Open Source Project The communication is established through the USB cable attached to the OpenSDA USB port. Code: #include "mbed.h" //Digital output declaration DigitalOut Blue(LED3); //Serial port (UART) configuration Serial pc(USBTX,USBRX); int main() {     Blue=1;     pc.printf("Serial code example\r\n");        while(1)     {         Blue=0;         pc.putc(pc.getc());     }    }
查看全文
Hello. I am trying to use a PIT interrupt. I had never used Kinetis so there are certain things which with I am not familiarized yet. once i have created de PE code, cleaned and then I build the proyect, the following error pops up 'undefined reference to int_disp'. What it is about? Where should I write my ISR fuction? Does the ISR pit function has to have an specific name so as to be recognised by PIT.c?
查看全文
El proyecto está basado en Kinetis KL25Z, consiste en utilizar un tapete de 9 “Botones” y un nunchuck para rehabilitación en piernas y o entrenar sus capacidades sicomotrices llevarlo a cabo atravez de programas especiales en PC, bien esto se lleva acabo utilizando la función de HID de Processor Expert, en el caso del nunchuck funciona como mouse y el tapete como teclado, el joystick del nunchuck actúan como el desplazamiento del mouse y los dos botones con los que cuenta actúan como clic derecho e izquierdo y el tapete actúa como las teclas W, A, S, D, (están son configurables) más 5 teclas adicionales, el tapete está formado por sensores de presión que al pisarlos simulan las teclas correspondientes.     BodyPCcontrol Kinetis Challenge México 2013 - YouTube Original Attachment has been moved to: HID-KEYRUG-KL25Z.rar
查看全文
The board used: FRDM-KE02 SWD: The ARM Serial Wire Debug interface uses a single bidirectional data connection(SWDIO) and a separate clock (SWDCLK) to transfer data synchronously. An operation on the wire consists of two or three phases: Packet request       The external host debugger issues a request to the DP. The DP is the target of the request. Acknowledge response   The target sends an acknowledge response to the host. Data transfer phase First enter into SWD mode: Send at least 50 SWCLKTCK cycles with SWDIOTMS HIGH and 0xE79E. This ensures that the current interface is in its reset state and enable the SWD mode. uint8_t SWJ_JTAG2SWD(void) {     uint32_t i;     SWDIO_SET();     for(i = 0; i < 56; i++)     {         SW_CLOCK_CYCLE();     }     SWJ_SendData(0xE79E);//SWJ_SendData(0xB76D);以后遇到再加     for(i = 0; i < 56; i++)     {         SW_CLOCK_CYCLE();     }     SWDIO_CLR();     for(i = 0; i < 16; i++)     {         SW_CLOCK_CYCLE();     }     return 0; } Then write DP/AP register. A successful write operation is as below: DP Register: Address     Read              Write 0x00        IDCODE           ABORT 0x04        CTRL/STAT      CTRL/STAT 0x08        RESEND           SELECT 0x0C        RDBUFF           N/A Address     Read              Write 0x00         CSW               CSW 0x04         TAR               TAR 0x08         N/A                N/A 0x0C         DRW              DRW 0xFC         IDR                N/A Read IDCODE: uint8_t SWJ_ReadDP(uint8_t adr, uint32_t *val) {     uint32_t tmp_in;     uint8_t ack;     uint8_t err;     tmp_in = SWD_REG_DP | SWD_REG_R | SWD_REG_ADR(adr);     ack = SWD_Transfer(tmp_in, val);     (ack == DAP_TRANSFER_OK) ? (err = 0) : (err = 1);     return err; } uint8_t SWJ_ReadAP(uint32_t adr, uint32_t *val) {     uint8_t tmp_in, ack, err;     uint32_t apsel = adr & APSEL;     uint32_t bank_sel = adr & APBANKSEL;     if(SWJ_WriteDP(DP_SELECT, apsel | bank_sel))     {         return 1;     } tmp_in = SWD_REG_AP | SWD_REG_R | SWD_REG_ADR(adr);     /* first dummy read */     ack = SWD_Transfer(tmp_in, val);     ack = SWD_Transfer(tmp_in, val);     (ack == DAP_TRANSFER_OK) ? (err = 0) : (err = 1);     return err; }
查看全文