KDS porting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,568件の閲覧回数
vigneshbalaji
Senior Contributor I

I want to port this example project in CodeWarrior which I have attached here to KDS 3.2. ? Please check it on your side and provide me a working KDS project of the same explaining the changes that you have done.

Original Attachment has been moved to: kds_porting.zip

ラベル(1)
タグ(3)
1 解決策
2,380件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi VIGNESH,

Sure , i create one new KDS project ,then copy your file ,

then add the "Includes paths" :

pastedImage_0.png


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,380件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

I have configure it , please check the attachment .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,380件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Alice,

            Thanks a lot.I am able to build and compile with the project and add things easily.

1)Can you please tell me what changes you have done compared to project which I gave you?

0 件の賞賛
返信
2,381件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi VIGNESH,

Sure , i create one new KDS project ,then copy your file ,

then add the "Includes paths" :

pastedImage_0.png


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,380件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Alice,

             Instead of the two dots specifying the path.Can I use ${ProjName} Variable? in the linker includes path???

0 件の賞賛
返信