Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?

ソリューションへジャンプ
5,370件の閲覧回数
r_trivedi123
Contributor IV

Hi,
I am worrking on a custom hardware having i.mx8qxp-c0 revision cpu.

I am using LF5.10.35_2.0.0 from here.

As per this guide i have downloaded scfw-kit-1.9.0.

I have used MT53D1024M32D4DT-053 AAT:D LPDDR4 micro.

I have been through the link provided.

My query is which RPA tool will be aligned with scfw-kit-1.9.0. and LF5.10.35_2.0.0 ?

Also I am not able to find LPDDR's parameters(Density per channel , total DRAM density, total number of CS used etc.) or datasheet from micron technology, so how do i proceed ?

Any help would be appreciated.

--
Thanks
Rutvij

 

 

タグ(4)
0 件の賞賛
返信
1 解決策
5,345件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes for i.MX8QXP LPDDR4 it is v.16.

 

Best regards
igor

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,347件の閲覧回数
r_trivedi123
Contributor IV

Hi Igor,
Thanks for the quick replay.

The suggested link has versions 15,16,21 available(image attached), will version 16 be good to go with?

--
Thanks




0 件の賞賛
返信
5,346件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes for i.MX8QXP LPDDR4 it is v.16.

 

Best regards
igor

 

 

0 件の賞賛
返信
5,351件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rutvij

 

one can use latest version from link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming...

 

Best regards
igor

0 件の賞賛
返信