Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?

跳至解决方案
5,394 次查看
r_trivedi123
Contributor IV

Hi,
I am worrking on a custom hardware having i.mx8qxp-c0 revision cpu.

I am using LF5.10.35_2.0.0 from here.

As per this guide i have downloaded scfw-kit-1.9.0.

I have used MT53D1024M32D4DT-053 AAT:D LPDDR4 micro.

I have been through the link provided.

My query is which RPA tool will be aligned with scfw-kit-1.9.0. and LF5.10.35_2.0.0 ?

Also I am not able to find LPDDR's parameters(Density per channel , total DRAM density, total number of CS used etc.) or datasheet from micron technology, so how do i proceed ?

Any help would be appreciated.

--
Thanks
Rutvij

 

 

标记 (4)
0 项奖励
回复
1 解答
5,369 次查看
igorpadykov
NXP Employee
NXP Employee

yes for i.MX8QXP LPDDR4 it is v.16.

 

Best regards
igor

 

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,371 次查看
r_trivedi123
Contributor IV

Hi Igor,
Thanks for the quick replay.

The suggested link has versions 15,16,21 available(image attached), will version 16 be good to go with?

--
Thanks




0 项奖励
回复
5,370 次查看
igorpadykov
NXP Employee
NXP Employee

yes for i.MX8QXP LPDDR4 it is v.16.

 

Best regards
igor

 

 

0 项奖励
回复
5,375 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rutvij

 

one can use latest version from link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming...

 

Best regards
igor

0 项奖励
回复