ROM bootloader changed to CPU rev 1.3 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ROM bootloader changed to CPU rev 1.3 ?

ソリューションへジャンプ
2,543件の閲覧回数
peterbärtsch
Contributor III

Hi

We use the imx6sx process with raw NAND Flash. Everything works fine with processor rev 1.2.

Now we produced some modules with CPU rev 1.3. And the CPU dosn't boot form NAND it goes directly in USB boot mode. I can download u-boot over USB (mfg tool) and then it is able to boot the Linux. But the ROM bootloader doesn't work.

I was not able to find out what chaned to rev 1.3 ... wtf..

What should I do?

Peter

ラベル(1)
0 件の賞賛
返信
1 解決策
2,388件の閲覧回数
peterbärtsch
Contributor III

Hi

Thx for your response.

I found a patch for kobs-ng.

https://community.nxp.com/docs/DOC-331342 

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,388件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

please check EB832 i.MX6SoloX Application Processor Silicon Revision 1.2 to 1.3 Comparison
http://www.nxp.com/assets/documents/data/en/engineering-bulletins/EB832.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,389件の閲覧回数
peterbärtsch
Contributor III

Hi

Thx for your response.

I found a patch for kobs-ng.

https://community.nxp.com/docs/DOC-331342 

Peter

0 件の賞賛
返信