It is one mandatory patch if you are in the case:
The chip you are using is imx6sx TO1.3 and newer, and use the kobs-ng to flash your image to the Nand memory chip. If you are using MFG, you also need rebuild the kobs-ng, and update the binary into your MFG tool. The patch have been integrated into the default release yocto_4.1.15, but if you are using the older version release before yocto_4.1.15, please make sure you have integrated the modification when you need to use kobs-ng to flash the image to Nand memory chip.
commit 5ecf08703da489a3bd317341f630870a3d07dab9
Author: Han Xu <[email protected]>
Date: Thu Jan 28 14:40:14 2016 -0600
MMT-105: change the i.mx6sx revision check change the i.mx6sx revision check since v1.3 uses v1.2 boot config as well.
Signed-off-by: Han Xu <[email protected]>
(cherry picked from commit 1dac0c14d1e2016c2fa804f6628543d8d238c680)
diff --git a/src/plat_boot_config.c b/src/plat_boot_config.c
index 461675a..e1ef6f3 100644
--- a/src/plat_boot_config.c
+++ b/src/plat_boot_config.c
@@ -1,5 +1,5 @@
/*
-* Copyright (C) 2010-2015 Freescale Semiconductor, Inc. All Rights Reserved.
+* Copyright (C) 2010-2016 Freescale Semiconductor, Inc. All Rights Reserved.
*/
/*
@@ -256,10 +256,12 @@ int discover_boot_rom_version(void)
}
fgets(line_buffer, sizeof(line_buffer), revision);
if (!strncmp(line_buffer, "1.0", strlen("1.0")) ||
- !strncmp(line_buffer, "1.1", strlen("1.1")))
+ !strncmp(line_buffer, "1.1", strlen("1.1"))) {
plat_config_data = &mx6sx_boot_config;
- if (!strncmp(line_buffer, "1.2", strlen("1.2")))
+ /* all other revisions should use the latest boot config */
+ } else {
plat_config_data = &mx6sx_to_1_2_boot_config;
+ }
}
if (!strncmp(line_buffer, plat_imx6ul, strlen(plat_imx6ul)))
How to apply it to older version quickly:
Apply the patch and rebuild the kobs-ng in yocto_3.14_x environment:
Apply the patch and rebuild the kobs-ng in yocto_3.10_53 environment:
As one alternation method, you also can download the whole imx-kobs-5.4 package which yocto_4.1.15 is using to build.