ROM bootloader changed to CPU rev 1.3 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ROM bootloader changed to CPU rev 1.3 ?

跳至解决方案
2,553 次查看
peterbärtsch
Contributor III

Hi

We use the imx6sx process with raw NAND Flash. Everything works fine with processor rev 1.2.

Now we produced some modules with CPU rev 1.3. And the CPU dosn't boot form NAND it goes directly in USB boot mode. I can download u-boot over USB (mfg tool) and then it is able to boot the Linux. But the ROM bootloader doesn't work.

I was not able to find out what chaned to rev 1.3 ... wtf..

What should I do?

Peter

标签 (1)
0 项奖励
回复
1 解答
2,398 次查看
peterbärtsch
Contributor III

Hi

Thx for your response.

I found a patch for kobs-ng.

https://community.nxp.com/docs/DOC-331342 

Peter

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,398 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Peter

please check EB832 i.MX6SoloX Application Processor Silicon Revision 1.2 to 1.3 Comparison
http://www.nxp.com/assets/documents/data/en/engineering-bulletins/EB832.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,399 次查看
peterbärtsch
Contributor III

Hi

Thx for your response.

I found a patch for kobs-ng.

https://community.nxp.com/docs/DOC-331342 

Peter

0 项奖励
回复