ROM bootloader changed to CPU rev 1.3 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ROM bootloader changed to CPU rev 1.3 ?

Jump to solution
2,538 Views
peterbärtsch
Contributor III

Hi

We use the imx6sx process with raw NAND Flash. Everything works fine with processor rev 1.2.

Now we produced some modules with CPU rev 1.3. And the CPU dosn't boot form NAND it goes directly in USB boot mode. I can download u-boot over USB (mfg tool) and then it is able to boot the Linux. But the ROM bootloader doesn't work.

I was not able to find out what chaned to rev 1.3 ... wtf..

What should I do?

Peter

Labels (1)
0 Kudos
Reply
1 Solution
2,383 Views
peterbärtsch
Contributor III

Hi

Thx for your response.

I found a patch for kobs-ng.

https://community.nxp.com/docs/DOC-331342 

Peter

View solution in original post

0 Kudos
Reply
2 Replies
2,383 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

please check EB832 i.MX6SoloX Application Processor Silicon Revision 1.2 to 1.3 Comparison
http://www.nxp.com/assets/documents/data/en/engineering-bulletins/EB832.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,384 Views
peterbärtsch
Contributor III

Hi

Thx for your response.

I found a patch for kobs-ng.

https://community.nxp.com/docs/DOC-331342 

Peter

0 Kudos
Reply