Java ME support in i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Java ME support in i.MX6

ソリューションへジャンプ
4,144件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I want to know a support of Java ME in i.MX6.

My customer want to use i.MX6UL with Linux and end customer also want to use CLDC 1.1 of Java ME.

Connected Limited Device Configuration (CLDC) is as flow.

Connected Limited Device Configuration (CLDC)

Connected Limited Device Configuration - Wikipedia, the free encyclopedia

I searched a i.MX Community and found following thread. But I couldn't figure out. So please let me know.

All Boards Java

NXP ARM-based processor with Java SE support

Can i.MX6UL support CLDC 1.1 ?

Ko-hey

ラベル(4)
0 件の賞賛
返信
1 解決策
3,224件の閲覧回数
SergioSolis
NXP Employee
NXP Employee
0 件の賞賛
返信
3 返答(返信)
3,225件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Yes, you can use Java ME 8 for the i.MX6, please take a look at the following document:

http://www.oracle.com/technetwork/java/embedded/javame/embed-me/documentation/me-e-otn-faq-1852008.p...

0 件の賞賛
返信
3,224件の閲覧回数
janekschumann
Contributor II

This seems to be the only source I could find regarding i.MX6 and Java ME 8.

Can you please clarify your answer:

is Java ME 8 (Embedded) supported on the Cortex-A9 cores out-of-the-box? (like i.MX6 DualLite)

The linked documentation only talks about Cortex-M4 (which would be i.MX6 SoloX) as well as ARM9. As far as I know, ARM9 is not the same as the ARM Cortex-A9 used in the i.MX6, or is it?

Do you have any supporting documentation on how to get Java ME 8 up and running on an (Cortex-A9) i.MX6?

Your help is much appreciated.

Janek

0 件の賞賛
返信
3,224件の閲覧回数
ko-hey
Senior Contributor II

Hi SergioSolis

Thanks!!

0 件の賞賛
返信