Java ME support in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Java ME support in i.MX6

Jump to solution
4,243 Views
ko-hey
Senior Contributor II

Hi all

I want to know a support of Java ME in i.MX6.

My customer want to use i.MX6UL with Linux and end customer also want to use CLDC 1.1 of Java ME.

Connected Limited Device Configuration (CLDC) is as flow.

Connected Limited Device Configuration (CLDC)

Connected Limited Device Configuration - Wikipedia, the free encyclopedia

I searched a i.MX Community and found following thread. But I couldn't figure out. So please let me know.

All Boards Java

NXP ARM-based processor with Java SE support

Can i.MX6UL support CLDC 1.1 ?

Ko-hey

Labels (4)
0 Kudos
Reply
1 Solution
3,323 Views
SergioSolis
NXP Employee
NXP Employee

Yes, you can use Java ME 8 for the i.MX6, please take a look at the following document:

http://www.oracle.com/technetwork/java/embedded/javame/embed-me/documentation/me-e-otn-faq-1852008.p...

View solution in original post

0 Kudos
Reply
3 Replies
3,324 Views
SergioSolis
NXP Employee
NXP Employee

Yes, you can use Java ME 8 for the i.MX6, please take a look at the following document:

http://www.oracle.com/technetwork/java/embedded/javame/embed-me/documentation/me-e-otn-faq-1852008.p...

0 Kudos
Reply
3,323 Views
janekschumann
Contributor II

This seems to be the only source I could find regarding i.MX6 and Java ME 8.

Can you please clarify your answer:

is Java ME 8 (Embedded) supported on the Cortex-A9 cores out-of-the-box? (like i.MX6 DualLite)

The linked documentation only talks about Cortex-M4 (which would be i.MX6 SoloX) as well as ARM9. As far as I know, ARM9 is not the same as the ARM Cortex-A9 used in the i.MX6, or is it?

Do you have any supporting documentation on how to get Java ME 8 up and running on an (Cortex-A9) i.MX6?

Your help is much appreciated.

Janek

0 Kudos
Reply
3,323 Views
ko-hey
Senior Contributor II

Hi SergioSolis

Thanks!!

0 Kudos
Reply