H.264 encode bit rate.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

H.264 encode bit rate.

Jump to solution
3,552 Views
takashitakahash
Contributor III

Hi community.

Our customer has two questions.

1, By IMX6SDLRM.PDF description to encode in H.264 CBP Bitrat comes to 14 Mbit/s 1080 p ,

Please tell me the compression rate and Bitrate of the case of 720p.

2,Would it be possible to change dynamically  encode H.264 CBP in the Bitrate?

This is because i want to dynamically change depending on network conditions.

Labels (1)
0 Kudos
Reply
1 Solution
3,278 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. bitrate for 720p case is the same as shown on presentation slide 5

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

compression rate depends on content as discussed on

http://stackoverflow.com/questions/5024114/suggested-compression-ratio-with-h-264

2. yes bitrate can be changed, this is described in attached VPU API

Manual sect.4.2.5 Dynamic Configuration Commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,279 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. bitrate for 720p case is the same as shown on presentation slide 5

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

compression rate depends on content as discussed on

http://stackoverflow.com/questions/5024114/suggested-compression-ratio-with-h-264

2. yes bitrate can be changed, this is described in attached VPU API

Manual sect.4.2.5 Dynamic Configuration Commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply