H.264 encode bit rate.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

H.264 encode bit rate.

ソリューションへジャンプ
3,529件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has two questions.

1, By IMX6SDLRM.PDF description to encode in H.264 CBP Bitrat comes to 14 Mbit/s 1080 p ,

Please tell me the compression rate and Bitrate of the case of 720p.

2,Would it be possible to change dynamically  encode H.264 CBP in the Bitrate?

This is because i want to dynamically change depending on network conditions.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,255件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. bitrate for 720p case is the same as shown on presentation slide 5

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

compression rate depends on content as discussed on

http://stackoverflow.com/questions/5024114/suggested-compression-ratio-with-h-264

2. yes bitrate can be changed, this is described in attached VPU API

Manual sect.4.2.5 Dynamic Configuration Commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,256件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. bitrate for 720p case is the same as shown on presentation slide 5

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

compression rate depends on content as discussed on

http://stackoverflow.com/questions/5024114/suggested-compression-ratio-with-h-264

2. yes bitrate can be changed, this is described in attached VPU API

Manual sect.4.2.5 Dynamic Configuration Commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信