H.264 encode bit rate.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

H.264 encode bit rate.

跳至解决方案
3,523 次查看
takashitakahash
Contributor III

Hi community.

Our customer has two questions.

1, By IMX6SDLRM.PDF description to encode in H.264 CBP Bitrat comes to 14 Mbit/s 1080 p ,

Please tell me the compression rate and Bitrate of the case of 720p.

2,Would it be possible to change dynamically  encode H.264 CBP in the Bitrate?

This is because i want to dynamically change depending on network conditions.

标签 (1)
0 项奖励
回复
1 解答
3,249 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. bitrate for 720p case is the same as shown on presentation slide 5

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

compression rate depends on content as discussed on

http://stackoverflow.com/questions/5024114/suggested-compression-ratio-with-h-264

2. yes bitrate can be changed, this is described in attached VPU API

Manual sect.4.2.5 Dynamic Configuration Commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,250 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. bitrate for 720p case is the same as shown on presentation slide 5

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

compression rate depends on content as discussed on

http://stackoverflow.com/questions/5024114/suggested-compression-ratio-with-h-264

2. yes bitrate can be changed, this is described in attached VPU API

Manual sect.4.2.5 Dynamic Configuration Commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复