Dual display not working in imx8mq-evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual display not working in imx8mq-evk

4,860 Views
SJ22
Contributor II

Hi,

I connected imx-mipi-hdmi connecter to imx8mq-evk board for enabling dual display, so during u-boot , i loaded a dts file named imx8mq-evk-dual-display.dtb where I have enabled mipi_dsi node, even after that nothing is coming in display. 

I am getting this issue while booting :adv7511 2-003d: Probe failed. Remote port 'mipi_dsi@30a00000' disabled

But I have enabled these nodes in the dts files. Do you know what might be the issue.

Tags (1)
0 Kudos
Reply
12 Replies

4,731 Views
marktsai1989
Contributor I

Hi @Sanket_Parekh 

Can VPU in IMX8MQ support color space conversion and scaling ?

 

0 Kudos
Reply

4,623 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SJ22 

I hope you are doing well.
 
There are many changes in imx8mq-evk.dts file between 5.4 and the latest kernel version.
 
It is not recommended to make changes to the latest device tree in the 5.4 kernel.
 
Please make sure that you have followed the below steps in u-boot.
 
=> setenv fdt_file imx8mq-evk-dual-display.dts
=> saveenv
 
Please try using kernel provided by nxp.
 
Please refer to the below article when the dual display is realized in imx8mq
Please share the part number of both displays connected to the board.
 
Thanks & Regards,
Sanket Parekh

0 Kudos
Reply

4,585 Views
SJ22
Contributor II

Hi @Sanket_Parekh 

I have connected Dell displays (D1918H) 18.5 inch.

0 Kudos
Reply

4,570 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SJ22 ,

 
I hope you are doing well.

 

One can compare the current kernel configuration file with the prebuilt image's(5.4.) configuration file.
 
To obtain a prebuilt image's configuration file on board, use the below command.
 zcat /proc/config.gz > filename.config 
 
Please provide me with the kernel configuration file.
 
Please use linux-imx instead of linux-fslc-imx.

 

 
Thanks & Regards,

Sanket Parekh

0 Kudos
Reply

4,834 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @SJ22 ,

I hope you are doing well.

This issue could be due to the wrong slave address for adv_bridge.

Please share the output of the below command.

# i2cdetect -y 30a40000.i2c

Please mention the BSP version used.

Have you tried using prebuilt images?

Please make sure the below-mentioned options are enabled in the kernel.
CONFIG_DRM_I2C_ADV7511=y
CONIFG_FB_MXC_ADV7535=y


Please refer to AN12188 Quick Start Guide for IMX-MIPI-HDMI for i.MX 8M Evaluation Kit.

Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

4,797 Views
SJ22
Contributor II

Hello Sanket,

The output for i2detect is :

imx8mqevk:~# i2cdetect -y 30a40000.i2c
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- -- -- -- -- -- --
10: UU UU UU UU -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- UU -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- -- 

I am using  linux-fslc-imx kernel whose version is 5.4.114+gitAUTOINC+f9a9b58ef7 ; I am using AGL image for imx8mq-evk board.

I have checked the prebuild image, in that, dual display was working and I compared the dts files , only difference is the use of mipi_dsi_bridge node in the prebuilt image: https://coral.googlesource.com/linux-imx/+/refs/heads/alpha/arch/arm64/boot/dts/freescale/fsl-imx8mq.... The dts file which I am using: https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mq-evk-lcdif-ad...

CONFIG_DRM_I2C_ADV7511 is enabled but CONFIG_FB_MXC_ADV7535 is disabled. I think that is where the issue is coming; I have one general doubt I am not finding this option CONFIG_FB_MXC_ADV7535 in menuconfig. This option is present in Kconfig ,but in the menuconfig path -> Device Drivers -> Graphics support -> Frame buffer Devices, this option is not visible. Do you know what might be the issue?

 

 

 

0 Kudos
Reply

4,778 Views
SJ22
Contributor II

Hi @Sanket_Parekh ,

one more quick update, I enabled CONFIG_FB_MXC_ADV7535 but still nothing is coming in the hdmi .I am getting this issue: adv7535 2-003d: failed to get required video mode. I have attached the screenshot of the log. So the issue narrows down to the dts files right?

Tags (1)
0 Kudos
Reply

4,759 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SJ22 ,

 
I hope you are doing well.
 

 

It is recommended to use BSP provided by NXP for EVK.
 
Please refer to below document.
 
One can use the below options in kernel defconfig.
 
CONFIG_DRM_I2C_ADV7511=y
CONFIG_DRM_I2C_ADV7511_AUDIO=y
CONFIG_DRM_I2C_ADV7511_CEC=y
 
This issue could be due to incorrect device tree configurations or version mismatching.
 
Please refer to below dts file for dual display in nxp linux.
 
 
Above dts supports the below display interface.
1. DCSS + onboard HDMI
2. LCDIF + DSI-HDMI converter: ADV7535

 

 
Thanks & Regards,

Sanket Parekh

0 Kudos
Reply

4,755 Views
SJ22
Contributor II

Hi @Sanket_Parekh ,

These configurations which you mentioned are all enabled.

CONFIG_DRM_I2C_ADV7511=y
CONFIG_DRM_I2C_ADV7511_AUDIO=y
CONFIG_DRM_I2C_ADV7511_CEC=y
 
I am using the same dts file imx8mq-evk-dual-display.dts  which is already present in the bsp layer, also tried loading the corresponding dtb file during u-boot but still no use. 
 
0 Kudos
Reply

4,734 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SJ22 

I hope you are doing well.
 
Base file (imx8mq-evk.dts ) of imx8mq-evk-dual-display.dts has many changes between linux versions.
like below,
 
Please try using the latest linux kernel source provided by nxp.
 
Thanks & Regards,
Sanket Parekh

0 Kudos
Reply

4,702 Views
SJ22
Contributor II

Hi @Sanket_Parekh ,

 

The dts files I am using is same as what is present in the latest kernel source. Also when I checked one of the prebuild images where the dual display is working,the only difference which I noticed in the dts files is that they have used node called mipi_dsi_bridge which is absent in the link which you gave for the latest kernel source. So I added that particular node but still it was failing.

0 Kudos
Reply

4,657 Views
SJ22
Contributor II

Hi @Sanket_Parekh ,

I managed to resolve this particular issue related to adv7511 driver: adv7511 2-003d: Probe failed. Remote port 'mipi_dsi@30a00000' disabled. But still it is not working. I have noticed an absence of this log [ie nwl-mipi-dsi 30a00000.mipi_dsi_bridge: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x215] which is related to mipi-dsi-host-attach function call in mipi dsi host controller driver,nwl-dsi.

Currently I am getting these logs:

mxsfb 30320000.lcdif: Failed to get axi clock: 0

[    3.238761] nwl-dsi 30a00000.mipi_dsi: [drm:imx8mq_dsi_select_input] Using LCDIF as input source

I feel like there is some issue with the mipi-dsi-host controller driver and drm. Do you know why that log is absent

0 Kudos
Reply