Hi @SJ22 ,
I hope you are doing well.
It is recommended to use BSP provided by NXP for EVK.
Please refer to below document.
One can use the below options in kernel defconfig.
CONFIG_DRM_I2C_ADV7511=y
CONFIG_DRM_I2C_ADV7511_AUDIO=y
CONFIG_DRM_I2C_ADV7511_CEC=y
This issue could be due to incorrect device tree configurations or version mismatching.
Please refer to below dts file for dual display in nxp linux.
Above dts supports the below display interface.
1. DCSS + onboard HDMI
2. LCDIF + DSI-HDMI converter: ADV7535
Thanks & Regards,
Sanket Parekh