Hi,
I connected imx-mipi-hdmi connecter to imx8mq-evk board for enabling dual display, so during u-boot , i loaded a dts file named imx8mq-evk-dual-display.dtb where I have enabled mipi_dsi node, even after that nothing is coming in display.
I am getting this issue while booting :adv7511 2-003d: Probe failed. Remote port 'mipi_dsi@30a00000' disabled
But I have enabled these nodes in the dts files. Do you know what might be the issue.
 Sanket_Parekh
		
			Sanket_Parekh
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @SJ22
I have connected Dell displays (D1918H) 18.5 inch.
 Sanket_Parekh
		
			Sanket_Parekh
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @SJ22 ,
 Sanket_Parekh
		
			Sanket_Parekh
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Sanket,
The output for i2detect is :
imx8mqevk:~# i2cdetect -y 30a40000.i2c
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- -- -- -- -- -- --
10: UU UU UU UU -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- UU -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- -- 
I am using linux-fslc-imx kernel whose version is 5.4.114+gitAUTOINC+f9a9b58ef7 ; I am using AGL image for imx8mq-evk board.
I have checked the prebuild image, in that, dual display was working and I compared the dts files , only difference is the use of mipi_dsi_bridge node in the prebuilt image: https://coral.googlesource.com/linux-imx/+/refs/heads/alpha/arch/arm64/boot/dts/freescale/fsl-imx8mq.... The dts file which I am using: https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mq-evk-lcdif-ad...
CONFIG_DRM_I2C_ADV7511 is enabled but CONFIG_FB_MXC_ADV7535 is disabled. I think that is where the issue is coming; I have one general doubt I am not finding this option CONFIG_FB_MXC_ADV7535 in menuconfig. This option is present in Kconfig ,but in the menuconfig path -> Device Drivers -> Graphics support -> Frame buffer Devices, this option is not visible. Do you know what might be the issue?
Hi @Sanket_Parekh ,
one more quick update, I enabled CONFIG_FB_MXC_ADV7535 but still nothing is coming in the hdmi .I am getting this issue: adv7535 2-003d: failed to get required video mode. I have attached the screenshot of the log. So the issue narrows down to the dts files right?
 Sanket_Parekh
		
			Sanket_Parekh
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @SJ22 ,
Sanket Parekh
Hi @Sanket_Parekh ,
These configurations which you mentioned are all enabled.
 Sanket_Parekh
		
			Sanket_Parekh
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @SJ22
Hi @Sanket_Parekh ,
The dts files I am using is same as what is present in the latest kernel source. Also when I checked one of the prebuild images where the dual display is working,the only difference which I noticed in the dts files is that they have used node called mipi_dsi_bridge which is absent in the link which you gave for the latest kernel source. So I added that particular node but still it was failing.
Hi @Sanket_Parekh ,
I managed to resolve this particular issue related to adv7511 driver: adv7511 2-003d: Probe failed. Remote port 'mipi_dsi@30a00000' disabled. But still it is not working. I have noticed an absence of this log [ie nwl-mipi-dsi 30a00000.mipi_dsi_bridge: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x215] which is related to mipi-dsi-host-attach function call in mipi dsi host controller driver,nwl-dsi.
Currently I am getting these logs:
mxsfb 30320000.lcdif: Failed to get axi clock: 0
[ 3.238761] nwl-dsi 30a00000.mipi_dsi: [drm:imx8mq_dsi_select_input] Using LCDIF as input source
I feel like there is some issue with the mipi-dsi-host controller driver and drm. Do you know why that log is absent