Does miracast function have relationship with LCD resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does miracast function have relationship with LCD resolution

Jump to solution
2,436 Views
xiaoqianlin
NXP Employee
NXP Employee

Hi,

One customer used MX6DL with 480X800 LCD RGB interface(JB4.2.2) and reported  error  when connecting two devices using miracast, I attached the log, can you help to check?

Regards,

Linda

Linda Lin
0 Kudos
Reply
1 Solution
2,260 Views
Ivan_liu
NXP Employee
NXP Employee

Hi Linda,

Does the customer use the wifi display sink apk developed by themselves.

The display size doesn't impact the miracast function.

BRs,

Ivan

View solution in original post

0 Kudos
Reply
3 Replies
2,261 Views
Ivan_liu
NXP Employee
NXP Employee

Hi Linda,

Does the customer use the wifi display sink apk developed by themselves.

The display size doesn't impact the miracast function.

BRs,

Ivan

0 Kudos
Reply
2,260 Views
xiaoqianlin
NXP Employee
NXP Employee

Thanks. Checked with customer, they downloaded the source code and compile it.

Linda Lin
0 Kudos
Reply
2,260 Views
YixingKong
Senior Contributor IV

Ivan.liu, could you hep the customer's issue?

Thanks,

Yixing

0 Kudos
Reply