Does miracast function have relationship with LCD resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does miracast function have relationship with LCD resolution

跳至解决方案
3,272 次查看
xiaoqianlin
NXP Employee
NXP Employee

Hi,

One customer used MX6DL with 480X800 LCD RGB interface(JB4.2.2) and reported  error  when connecting two devices using miracast, I attached the log, can you help to check?

Regards,

Linda

Linda Lin
0 项奖励
回复
1 解答
3,096 次查看
Ivan_liu
NXP Employee
NXP Employee

Hi Linda,

Does the customer use the wifi display sink apk developed by themselves.

The display size doesn't impact the miracast function.

BRs,

Ivan

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,097 次查看
Ivan_liu
NXP Employee
NXP Employee

Hi Linda,

Does the customer use the wifi display sink apk developed by themselves.

The display size doesn't impact the miracast function.

BRs,

Ivan

0 项奖励
回复
3,096 次查看
xiaoqianlin
NXP Employee
NXP Employee

Thanks. Checked with customer, they downloaded the source code and compile it.

Linda Lin
0 项奖励
回复
3,096 次查看
YixingKong
Senior Contributor IV

Ivan.liu, could you hep the customer's issue?

Thanks,

Yixing

0 项奖励
回复