Can IMX8M-Mini output 3 displays?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can IMX8M-Mini output 3 displays?

跳至解决方案
2,000 次查看
Takashi_Kashiwagi
Senior Contributor I

Hi all

I am considering a system using the IMX 8 M Mini.

Therefore, I want to know whether IMX 8M Mini can output to 3 displays Physically with MIPI - DSI + bridge IC.

Does anyone know about it?

For now, it seems that Dual Display can be done with TI's SN65 DSIXX bridge IC. However, I can not find a bridge IC that can be used for triple display.

Best Regards

T.Kashiwagi

标签 (1)
标记 (1)
1 解答
1,701 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

seems not as Mini has not DCSS and HDMI compared with i.MX8M.

One can consider custom fpga bridge or other interfaces with LCD like spi

https://community.nxp.com/thread/451152 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,701 次查看
Takashi_Kashiwagi
Senior Contributor I

Hi Igor

Thank you fo responding!

One can consider custom fpga bridge or other interfaces with LCD like spi

OK. I'll consider in the configuration of MIPI - DSI + custom FPGA as follows.

[IMX8M Mini] <-- MIPI-DSI -->[Custom FPGA/PLD]<--LVDS/RGB-->[Display * 3]

Three of the 800 x 480 displays may look like 2400 x 480 from the CPU, but I think that I can do that.

Best Regards,

T.Kashiwagi

0 项奖励
回复
1,702 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

seems not as Mini has not DCSS and HDMI compared with i.MX8M.

One can consider custom fpga bridge or other interfaces with LCD like spi

https://community.nxp.com/thread/451152 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------