Can IMX8M-Mini output 3 displays?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can IMX8M-Mini output 3 displays?

Jump to solution
1,955 Views
Takashi_Kashiwagi
Senior Contributor I

Hi all

I am considering a system using the IMX 8 M Mini.

Therefore, I want to know whether IMX 8M Mini can output to 3 displays Physically with MIPI - DSI + bridge IC.

Does anyone know about it?

For now, it seems that Dual Display can be done with TI's SN65 DSIXX bridge IC. However, I can not find a bridge IC that can be used for triple display.

Best Regards

T.Kashiwagi

Labels (1)
Tags (1)
1 Solution
1,656 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

seems not as Mini has not DCSS and HDMI compared with i.MX8M.

One can consider custom fpga bridge or other interfaces with LCD like spi

https://community.nxp.com/thread/451152 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,656 Views
Takashi_Kashiwagi
Senior Contributor I

Hi Igor

Thank you fo responding!

One can consider custom fpga bridge or other interfaces with LCD like spi

OK. I'll consider in the configuration of MIPI - DSI + custom FPGA as follows.

[IMX8M Mini] <-- MIPI-DSI -->[Custom FPGA/PLD]<--LVDS/RGB-->[Display * 3]

Three of the 800 x 480 displays may look like 2400 x 480 from the CPU, but I think that I can do that.

Best Regards,

T.Kashiwagi

0 Kudos
Reply
1,657 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

seems not as Mini has not DCSS and HDMI compared with i.MX8M.

One can consider custom fpga bridge or other interfaces with LCD like spi

https://community.nxp.com/thread/451152 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------