UUU is an evolution of MFGTools. The introduction of UUU detail you can see the uuu.pdf file.. Please download uuu.exe and follow the UUU introduction. Here are some running examples. If you are not familiar with uuu, you can refer to them firstly. Under Windows (should be as admin): • For SD card: Linux: .\uuu -b sd_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard • For EMMC: Linux: .\uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard or .\uuu.exe uuu.auto Android: .\uuu_imx_android_flash.bat -f imx8mm -u trusty Under Linux: • For EMMC Linux: sudo .\uuu uuu.auto If you download BSP release from nxp.com, you could find a file uuu.auto in the package. This is a preset script that can be executed directly (default for EMMC). You could change the script based on your requirement. Copy the uuu.exe under the release package, then execute the instructions. For UUU tool the prebuilt image and document are here: • https://github.com/NXPmicro/mfgtools/releases • UUU.pdf is snapshot of wiki
Environment
PC: Window 10 64bit
Board: i.MX8MMLPDDR4 EVK
BSP: Q10.0.0_2.0.0 Demo images
Screen: MX8-DSI-OLED1
Downloading android images to i.MX 8M Mini EVK LPDDR4 via UUU Tool
1\Hardware Preparations
(1) Make the board enter serial download mode.
For Rev. B boards, change the first two bits of board's sw1101 to 10 (from 1-2 bit) to enter serial download mode.
For Rev. C boards, change the first four bits of board's sw1101 to 1010 (from 1-4 bit) to enter serial download mode.
(2) Connecting J901to PC USB by a USB OTG cable.
(3) Connecting J301(usb type c) to PC USB.
(4) Plugging adapter into Power Jack (J302)
(5) Power on i.MX 8M Mini EVK LPDDR4 board via SW101 Switch
When first connect the board to PC, windows 10 64bit can’t automatically install FT2232D
driver from official website of manufacture, you need to Install the usb to uart driver manually:
https://www.ftdichip.com/Drivers/D2XX.htm Download the setup executable and then install it.
When installed success you can see the usb serial port can be used.
2\Downloading UUU Tool
For the UUU binary file, download it from github: uuu release page on github.
For the Q10.0.0_2.0.0 version use the UUU 1.3.124 version.
For Linux OS, download the file named "uuu".
For Windows OS, download the file named "uuu.exe".
Here I use win10 system, so I download the uuu.exe file.
3\Download the Q10.0.0_2.0.0 Demo images for i.MX8MM
Now all the android os for i.MX products are here: Android OS for i.MX Applications Processors.
Decompress release_package/android-10.0.0_2.0.0_image_8mmevk.tar.gz for LPDDR4 board.
The package contains the image files and uuu_imx_android_flash tool.
Copy uuu.exe to the directory of Q10.0.0_2.0.0 Demo images.
4\ Execute the uuu_imx_android_flash to flash image
Power on the board.
Open the serial port terminal and setting as following:
Open a command line window.
For the use and the Options for uuu_imx_android_flash tool details can see the Table 2 in the Android_Quick_Start_Guide.
Here I use the OLED screen, to test MIPI panel output, need execute the tool with "-d mipi-panel".
So here I use the .\uuu_imx_android_flash.bat -f imx8mm -e -d mipi-panel .
When I use the download I meet the follow question:
C:\Work\Products\Android BSP\New folder\Q10.0.0_2.0.0 Demo images\android-10.0.0_2.0.0_image_8mmevk>.\uuu_imx_android_flash.bat -f imx8mm -e -d mipi-panel
This script is validated with uuu 1.3.124 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic partition is supported
You do not have sufficient privilege to perform this operation.
So here can change to use the Windows PowerShell, it works well and finished download.
Power off the board.
5\Boot up the board from emmc
Set boot mode
For Rev. C boards:
Change sw1101 to 0110110010 and change sw1102 to 0001101000 if you want to boot from SD card.
Change sw1101 to 0110110001 and change sw1102 to 0001010100 if you want to boot from eMMC.
Set the U-Boot environment variables for the MIPI panel display
U-Boot > setenv bootargs console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init
androidboot.console=ttymxc1 androidboot.hardware=freescale cma=800M@0x400M-0xb80M
androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware
transparent_hugepage=never androidboot.wificountrycode=CN androidboot.lcd_density=240
U-Boot > saveenv
Then use the boot to boot up and then display on OLED screen.
Hope this can do help for some users.
Best Regards
Rita
查看全文