i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This is a How-To documentation for OpenCL on i.MX6 using LTIB, there are all necessary steps and sample code to create,  build and run a HelloWorld application.
View full article
Q: When trying to mount his SDIO WiFi module (an Azurewave module containing a Marvel 88W8790)  in 4 bit mode, and got error wifi module on iMX6 Smart SD dev board using the alpha kernel (3.5.7+3285970). mwifiex_sdio mmc0:0001:1: WLAN FW is active mwifiex_sdio mmc0:0001:1: mwifiex_cmd_timeout_func: Timeout cmd id (2004.239824) = 0xa9, act = 0x0 mwifiex_sdio mmc0:0001:1: num_data_h2c_failure = 0 mwifiex_sdio mmc0:0001:1: num_cmd_h2c_failure = 0 mwifiex_sdio mmc0:0001:1: num_cmd_timeout = 1 mwifiex_sdio mmc0:0001:1: num_tx_timeout = 0 mwifiex_sdio mmc0:0001:1: last_cmd_index = 1 mwifiex_sdio mmc0:0001:1: last_cmd_resp_index = 0 mwifiex_sdio mmc0:0001:1: last_event_index = 0 mwifiex_sdio mmc0:0001:1: data_sent=1 cmd_sent=1 mwifiex_sdio mmc0:0001:1: ps_mode=1 ps_state=0 +++++++++++++++++++++++ There are only two known issues with the SDHC driver as noted in the release notes and these don't seem to match.  The Linux Reference Manual states the operation of the SDIO was veriifed usign the AR6003.  My assumption is that this is the Silex module we have standardized on.  Was 4 bit mode verified using this module? Does anyone have any idea what could be happening here? A: L3.5.7 is an alpha release, and WiFi function is not stable. The test report shows that open WiFi issue exists. Wifi module sometime can't work on mx6q_smd. After insmod ath, ath6kl_core and ath6kl_sdio. Insert the wifi card, sometime(50%) will display -------------------------- ath6kl: unable to read RX_LOOKAHEAD_VALID                                      ath6kl: Unable to recv target info: -84                                        ath6kl: Failed to init ath6kl core                                             ath6kl_sdio: probe of mmc0:0001:1 failed with error -84    -------------------------- reinsert the wifi card may solve the problem. when execute "udhcpc -i wlan0", sometime (30%) will cause program exception. Sometime can't get the wlan0 ip(program hang). Environment(OS,Platform,Driver, etc): HW: MX6Q_SMD Num014 and Num017 MX6Q_ARD don't have this problem SW: Kernel 3.5.7-1.0.0 GNU/Linux Case ID: TGE-LV-WIFI-0043 Reproduce Steps: #modprobe ath #modprobe ath6kl_core #modprobe ath6kl_sdio insert the wifi card # iwconfig wlan0 mode managed # iwlist wlan0 scanning | grep MAD-wifi #iwconfig wlan0 key 00112233445566778899123456 #iwconfig wlan0 essid MAD-wifi #udhcpc -i wlan0 Attached MX6 ARD WiFi issue also. [Kernel3.5.7_MX6QARD]Wifi:wifi card can't work during suspend and resume. 100% -- Bug detailed description: With wifi card inserted in the board. doing system suspend and resume test. wifi card can't work well after the system suspend and resume. Always report : ath6kl: Unable to decrement the command credit count register: -84             ath6kl: Unable to write to the device: -84                                     ath6kl: bmi_write_memory for uart debug failed                                 ath6kl: Failed to boot hw in resume: -5          Environment(OS,Platform,Driver, etc): HW: MX6QARD -023 Only tried on this platform SW: root@imx6qsabreauto:~# uname -a                                                Linux imx6qsabreauto 3.5.7-1.0.0+3285970 #1 SMP PREEMPT Sat Jun 29 10:20:45 CDT 2013 armv7l GNU/Linux Case ID:  TGE-LV-WIFI-1060 and TGE-LV-WIFI-1062 Reproduce Steps: 1. boot the kernel with wif card inserted 2. doing wifi stress test 3. doing suspend and resume
View full article
This doc show how to use i.MX8QXP Display Controller GammaCor unit to tune gamma. HW: i.MX8QXP MEK board, HDMI monitor SW: i.MX Linux 4.14.98_2.2.0 BSP release, patch in this doc 1.Introduce gamma The gamma, gamma correction, gamma encoding, gamma compression , these words all related one kind operation , see wiki page of it: The device used for image capture/print/display follow this power-law. For example the camera captured image , to view this image on display device as good as original captured image : gamma encoding when camera saved sensor data to image file,  and  gamma decoding when that image file display on your PC LCD monitor. That is : 2. i.MX8QXP Display Controller Gamma Correction Unit The Gamma Correction unit position is located between Frame Gen unit and TCon unit.   More detail see below contents from i.MX8QXP RM: So GammaCor unit could be used as adjust display gamma , or brightness or contrast. To used it, need follow the steps at RM 15.9.2.4.4.8.3.   Something need to note: You need program 33 sample point value into the register, these sample point value range is from 0 to 1023. Note, first write is start sample point value , then the other is delta value: current sample point minus previous sample point value. You can use GammaCor unit on any channel of R/G/B. If you use normalized function f(x), the following formula should be used to clut[i = 0..32] = round( f(i * 32 / 1023) * 1023) 3. i.MX8QXP Linux device driver patch and test code Apply attached  patch 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on Linux kernel. In the kernel patch, function dpu_gammacor_update, I choose not calculate delta value between each sample pint , let user space application calculate delta value and passed to kernel. Apply 8qxp-dpu-gammacor-modetst.diff on libdrm-imx, to get test application which is based on modetest.  Test app will read one greyscale image file 720P.rgb, put it under same folder of test application , calculate sample point value by pow function  , and calling drmModeCrtcSetGamma to pass related value to kernel,  next loop will change sample point value, and will see that greyscale image will changed on HDMI monitor. After system boot up, run below cmd to check result of test application systemctl stop weston ./gamma_show_rgba.out -P 29@32:1280x720@AB24 Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.2.0_MX8QXP&appType=license c> https://source.codeaurora.org/external/imx/libdrm-imx/ d> https://en.wikipedia.org/wiki/Gamma_correction
View full article
The following document contains a list of document, questions and discussions that are relevant in the community based on amount of views. If you are having a problem, doubt or getting started in i.MX processors, you should check the following links to see if your doubt is in there. Yocto Project Freescale Yocto Project main page‌ Yocto Training - HOME‌ i.MX Yocto Project: Frequently Asked Questions‌ Useful bitbake commands‌ Yocto Project Package Management - smart  How to add a new layer and a new recipe in Yocto  Setting up the Eclipse IDE for Yocto Application Development Guide to the .sdcard format  Yocto NFS & TFTP boot  YOCTO project clean  Yocto with a package manager (ex: apt-get)  Yocto Setting the Default Ethernet address and disable DHCP on boot.  i.MX x Building QT for i.MX6  i.MX6/7 DDR Stress Test Tool V3.00  i.MX6DQSDL DDR3 Script Aid  Installing Ubuntu Rootfs on NXP i.MX6 boards  iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP i.MX Design&Tool Lists  Simple GPIO Example - quandry  i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines  Streaming USB Webcam over Network  Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53  Linux / Kernel Copying Files Between Windows and Linux using PuTTY  Building Linux Kernel  Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)  load kernel from SD card in U-boot  Changing the Kernel configuration for i.MX6 SABRE  Android  The Android Booting process  What is inside the init.rc and what is it used for.  Others How to use qtmultimedia(QML) with Gstreamer 1.0
View full article
This patch implements (or exposes) routines to poll the imx uarts. The KGDB drivers need these methods to be implemented or the ttymxc driver is not sufficient. The synthetic CONFIG_CONSOLE_POLL value activates these routines (or CONFIG_SERIAL_MXC_CONSOLE for the polled write). There is still no poll routines in -855-ge067785, which is the September 2010 Linux release from Freescale. Also not in Linux 2.6.36 drivers/serial/imx.c either. $ git diff drivers/serial/mxc_uart.c diff --git a/drivers/serial/mxc_uart.c b/drivers/serial/mxc_uart.c index ae6d2e1..728b607 100644 --- a/drivers/serial/mxc_uart.c +++ b/drivers/serial/mxc_uart.c @@ -1551,6 +1551,28 @@ mxcuart_pm(struct uart_port *port, unsigned int state, unsigned int oldstate)                             clk_enable(umxc->clk);    }  +#ifdef CONFIG_CONSOLE_POLL +/* + * Read a character from the UART. + */ +static inline int mxcuart_console_read_char(struct uart_port *port) +{ +       volatile unsigned int status; +    int ch; + +       do { +               status = readl(port->membase + MXC_UARTUSR2); +       } while ((status & MXC_UARTUSR2_RDR) == 0); +       ch = readl(port->membase + MXC_UARTURXD); +/* Ignore parity errors, etc. */ +/*  status = ch | UART_CREAD_BIT; */ +    ch &= 0xff; + +    return ch; +} +static void mxcuart_console_write_char(struct uart_port *port, char ch); +#endif +    /*!     * This structure contains the pointers to the control functions that are     * invoked by the core serial driver to access the UART hardware. The @@ -1575,14 +1597,18 @@ static struct uart_ops mxc_ops = {                 .config_port = mxcuart_config_port,                 .verify_port = mxcuart_verify_port,                 .send_xchar = mxcuart_send_xchar, +#ifdef CONFIG_CONSOLE_POLL +              .poll_put_char = mxcuart_console_write_char, +              .poll_get_char = mxcuart_console_read_char, +#endif };  -#ifdef CONFIG_SERIAL_MXC_CONSOLE +#if defined(CONFIG_SERIAL_MXC_CONSOLE) || defined (CONFIG_CONSOLE_POLL)     /*     * Write out a character once the UART is ready     */ -static inline void mxcuart_console_write_char(struct uart_port *port, char ch) +static void mxcuart_console_write_char(struct uart_port *port, char ch)    {            volatile unsigned int status;  @@ -1592,6 +1618,10 @@ static inline void mxcuart_console_write_char(struct uart_port *port, char ch)                writel(ch, port->membase + MXC_UARTUTXD);     }  +#endif + +#ifdef CONFIG_SERIAL_MXC_CONSOLE +    /*!     * This function is called to write the console messages through the UART port.     *
View full article
The PICO-PI-IMX7 is a TechNexion board defined here. It is now supported in mainline U-Boot, mainline Kernel, FSL Community BSP and Buildroot. In mainline U-Boot it is supported since v2017.07. In mainline Linux Kernel it is supported since 4.13. To generate an image for PICO-PI-IMX7 using FSL Community BSP, please see: The imx7d-pico board is now supported in FSL Community BSP - i.MXDev Blog. To generate an image for PICO-PI-IMX7 using Buildroot, please see: The imx7d-pico board is now supported in Buildroot - i.MXDev Blog.
View full article
Attached is a chunk of the filesystem for the Linux Image https://community.freescale.com/docs/DOC-93887
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343273 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343518 
View full article
Pre-Sales: i.MX8/8X applications in automotive(Chinese Version) https://community.nxp.com/docs/DOC-345825 i.MX8X website design resource guide: (Chinese Version) https://community.nxp.com/docs/DOC-345676 After-Sales: i.MX8X memory configuration&test application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345803 i.MX8X hardware design guide: (Chinese Version) https://community.nxp.com/docs/DOC-346582 i.MX8X_4.19.35_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345713 i.MX8X_4.19.35_kernal customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345714 i.MX8X_4.14.98_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-342448 i.MX8X_4.14.98_kernal customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-344217 i.MX8X_5.4.24_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-347131
View full article
This is a generic script which flashes a Linux System (U-boot, uImage and root filesystem) into a SD card. Steps:     1. Download the script into a Linux system     2. Make the script executable (chmod +x mk_mx_sd)     3. Run it with '-H' to know its usage.     4. Run the script with real parameters, specifying the paths for U-boot, uImage and the root filesystem as seen above     5. Plug the SD into your target, boot the board and change the corresponding U-boot variables $ IMAGE=/data/BSP/L2.6.35_11.09.01_ER/L2.6.35_11.09.01_ER_images_MX5X $ ./mk_mx_sd  -d /dev/sdc \                       -u $IMAGE/u-boot-mx53-loco.bin \                       -k $IMAGE/uImage \                       -r $IMAGE/rootfs     6. In case you only want to flash a single binary (like U-boot), just specify the U-boot parameter (-u)
View full article
Platform: Ubuntu 12.04 Board: Freescale MCIMX6Q-SDP  and  MCIMX-LVDS1 Screen BSP: L3.0.35_4.1.0_ER_SOURCE_BSP Other device: PC , One Router, 3 Network Cable and 2 usb-otg lines The  platform is as follow: Boot form NFS is very convenient in porting and debugging, and will value us much time. If the customers have modified the kernel and rebuild the kernel to generate the uImage running on board, he can directly download the uImage to the board by TFTP network. It is fast and can avoid the normal operation ,  first customers need to copy the images to the mfgtool specified directory and download the u-boot, uImage and file sytem again to the flash device in board, and then change to boot up mode to boot up the board. If customers are doing debug this operation will waste lot of time. So use the NFS is vey convenient. Beyond this, in the target board customers can also read the files and content in host machine. In a word, use NFS it will help save much time and also convenient. So the follows is introduce and show how to set NFS and then boot up the board. 1 Preparation (1)Build the BSP Build up the L3.0.35_4.1.0_ER_SOURCE_BSP use LTIB on the Ubuntu12.04, you can refer to our user guide document here no details. The u-boot, uImage and file system are all under the directory of litb. Boot up from NFS, so when build uImage some items are needed, here you can see the build details in the section of  Setting Target Linux Image to use NFS in this articel. (2)Download the u-boot to the target board Use the mfgtool Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER to download the u-boot to the SD card of MCIMX6Q-SDP board or use dd command to write the u-boot to SD card.( By the way, writing to the EMMC is also OK) 2 Setting the NFS Environment Set host machine 1 - Install NFS Service on host typing:     $sudo apt-get install nfs-kernel-server       2 - Create symbolic link to ltib/rootfs     $sudo ln -s <ltib instalation folder>/rootfs /tftpboot/rootfs       3 - Setup exports typing:     $sudo gedit /etc/exports       and add the following line:     /tftpboot/rootfs/ *(rw,no_root_squash,no_subtree_check,async) 4 - Restart the NFS server:     $sudo /etc/init.d/nfs-kernel-server restart       Now the host is ready to use NFS Setting Target Linux Image to use NFS       1. Run LTIB configuration by typing: $cd <ltib instalation folder>       $./ltib -c       2. On first page menu, go to "Target Image Generation -> Options"       3. Select the option NFS only and exit LTIB configuration to compile with the new configuration. 4. LTIB should start new compiling and create a new Linux image on /<ltib instalation folder>/rootfs/boot/uImage      5. Copy the created image on /<ltib instalation folder>/rootfs/boot/uImage to /tftpboot/uImage 6. The system is ready to run with NFS. The root file system on target will be located on host on /<ltib instalation folder>/rootfs/ 3 Setting the u-boot command line (1)Download the u-boot to the target board fist according to the section 1 (2) Download the u-boot to the target board. Then give the power to the board, boot up board, u-boot boot up. (2)Configuration the Network Configure the Network and IP , to make the target board and the host machine IP are in the local area network of Router. (3)Set the u-boot command line As follow is my setting for you to refer to : 4 Boot up the board Running the “run bootcmd” after setting the u-boot parameters then boot up the kernel and file system. We can see that the board download the uImage by the TFTP from host machine, then boot up the kernel and finally mount the NFS in the kernel. As follows is the details: Downloading the uImage success and boot up kernel: Input root and access the system. Test: Create a new file in the host machine directory, you can see in the next picture: Then open the target board, in the terminal go to the same directory  in the unit_test we can see the same name. So as we can see in the above operation we can see it is very convenient and fast use the NFS. It will help save time and speed the development time.
View full article
Platform: i.mx8qm/qxp OS: imx-yocto-L4.14.98_2.0.0_ga Camera: max9286 deserializer <=> max96705 serializer  + ar0144 or: max9286 deserializer <=> max96705 serializer + ov9284 Note that currently only one camera is support and the serializer should be connected to the IN0 of max9286. Data format: ar0144: mono raw 12bit. ov9284: mono raw 10bit. On imx8qm/qxp the data will be recieved as raw 16bit and the valid data bit start from bit[13] to LSB. for mono raw 12bit the valid data bit is 0bxxdd_dddd_dddd_ddxx for mono raw 10bit the valid data bit is 0bxxdd_dddd_dddd_xxxx max9286 and max96705 configuration: dbl bws PXL_CRC/edc hven hibw lccen him should be the same on both sides, this can be achieved by pin or register configurations. The crossbar function of max96705 can be used to fix the reversed data bit. for example, reversed 12bit with dbl to 1. 0x20 0xb 0x21 0xa 0x22 0x9 ....... 0x2b 0x0 0x30 0xb 0x31 0xa .... 0x3b 0x0 0x20 to 0x2b and 0x30 to 0x3b are the registers of max96705. Patch apply: 1. push the kernel-patch to the kernel source and apply it. 2. reconfig the kernel setting, make sure there is only CONFIG_MAX9286_AR0144 or        CONFIG_MAX9286_WISSEN(ov9284) enabled, all other max9286 related are disabled. You can run menuconfig to achieve this. 3. For testing copy the vulkan-v4l2.tar to the board, and run vulkan-v4l2.     the source code is at https://github.com/sheeaza/vulkan-v4l2 branch ar0144 for ar0144, branch ov9284 for ov9284. =========== updated patch for data format.
View full article
Most i.MX8QXP/QM customers already work on L4.14.98 GA for their Auto product, like C-V2X TBOX, Car infortainment system. Some customers also want to adopt OP-TEE in their security design, but OP-TEE on i.MX8QXP/QM platform don't support HW cryptography accelerating which base on CAAM module. So I worked on the issue last week and fixed it. The package meta-optee-add-on_4.14.98_2.0.0_ga.tgz is Yocto layer which includes all patches for fixing the issue. Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga HW platform:  i.MX8QM/QXP MEK. How to build: 1, decompress meta-optee-add-on_4.14.98_2.0.0_ga.tgz and copy meta-optee-add-on to folder (Yocto 4.14.98_2.0.0_ga dir)/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-optee and add BBLAYERS += " ${BSPDIR}/sources/meta-optee-add-on " into (Yocto 4.14.98_2.0.0_ga dir)/build-optee/conf/bblayers.conf  3, Run bitbake fsl-image-validation-imx. 4, You can run xtest or xtest -l 1 4007 on your MEK board to test optee crypto feature after completing build image. You can find it only take about one second comparing no CAAM accelerating when test "regression_4007.11 Generate RSA-2048 key".
View full article
This document provide an overall guide how to get started with i.MX6 development. There are several chapters: 1. how to get necessary docs from freescale website; 2. how to setup environment and build your own images;3. Hardware design consideration;4. How to get help. I hope the doc will bring you in i.MX world more easily, and hope you all have a fun in it.
View full article
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source. tar.gz $ ./L3.0.35_4.1.0_130816_source/install      After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/m4/m4.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/m4-1.4.16-1383761043.patch    pkgs/m4-1.4.16-1383761043.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 m4 compilation issue: 1. https://github.com/hashdist/hashstack/commit/f6be2a58de62327d05e052d89c9aa931d4c926b3 2. https://github.com/hashdist/hashstack/issues/81 rpm-fs package failed to build issue: https://community.freescale.com/message/355771#355771 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343715 
View full article