1. To setup the Yocto environment, from the BASE folder run
fsl-community-bsp $ . setup-environment build
2. Build the toolchain
build $ bitbake meta-toolchain
# Other toolchains:
# Qt Embedded toolchain build: bitbake meta-toolchain-qte
# Qt X11 toolchain build: bitbake meta-toolchain-qt
3. Install it on your PC
build $ sudo sh \
tmp/deploy/sdk/poky-eglibc-x86_64-arm-toolchain-<version>.sh
4. Setup the toolchain environment
build $ source \
/opt/poky/<version>/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi
5. Get the Linux Kernel's source code.
$ git clone git://git.freescale.com/imx/linux-2.6-imx.git linux-imx
$ cd linux-imx
6. Create a local branch
linux-imx $ BRANCH=imx_3.0.35_4.0.0 # Change to any branch you want,
# Use 'git branch -a' to list all
linux-imx $ git checkout -b ${BRANCH} origin/${BRANCH}
7. Export ARCH and CROSS_COMPILE
linux-imx $ export ARCH=arm
linux-imx $ export CROSS_COMPILE=arm-poky-linux-gnueabi-
linux-imx $ unset LDFLAGS
8. Choose configuration and compile
linux-imx $ make imx6_defconfig
linux-imx $ make uImage
9. To Test your changes, copy the `uImage` into your SD Card
linux-imx $ sudo cp arch/arm/boot/uImage /media/boot
10. If case you want your changes to be reflected on your Yocto Framework, create the patches following the document i.MX Yocto Project: How can I patch the kernel?
Hi,
For 3.10.17 Kernel above steps remains same?
make imx6_defconfig gives error
Can't find default configuration "arch/arm/configs/imx6_defconfig"!
You are right saurabh206, the defconfig is indeed different. It is imx_v7_defconfig. You can check all possibles configs either on the folder you mentioned or with 'make help':
$ make help | grep imx
imx6_ssd_lite_defconfig - Build for imx6_ssd_lite
imx6_ssd_net_lite_defconfig - Build for imx6_ssd_net_lite
imx_v4_v5_defconfig - Build for imx_v4_v5
imx_v6_v7_defconfig - Build for imx_v6_v7
imx_v7_defconfig - Build for imx_v7
imx_v7_mfg_defconfig - Build for imx_v7_mfg
Hi, I have imx6q sabresd board, compile & run imx yocto(bitbake fsl-image-gui) without any problem. Now i tried kernel branch imx_3.0.35_4.1.0 as shown above step 5 onwards, compile no issue, however, when run, I can't see any gui on the lcd, I already enable devtmpfs.
Please don't base new products in 3.0.35 kernel as the Freescale GA is now the 3.10.17-1.0.1 one. Regarding building the kernel, my advice goes to use the toolchain generated for this so your development process is highly boosted.
You may want to also look at: Embedded Linux Development with Yocto Project book released | Freescale Community
I follow the steps above and compile kernel 3.10.17-1.0.1, and got this error:
| CC | drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.o | 
drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.c:29:27: fatal error: mach/hardware.h: No such file or directory
#include <mach/hardware.h>
| ^ | 
compilation terminated.
make[3]: *** [drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.o] Error 1
I ran also into this problem. Please follow Eric's comment
http://boundarydevices.com/mx6-linux-kernel-3-10-17-beta/#comment-124454
Hi Otavio,
I want to link to the link you mentioned as below for learning how to do kernel related tasks. But it can't be access. May you redirect me?
Embedded Linux Development with Yocto Project book released | Freescale Community
Sure, you can link to our blog post about it:
Hi Leo,
Which one is suit for i.mx53 I tried with imx_v7_defconfig but kernel panic on my i.mx53 quick start board.
Thanks!
Wenming
The kernel panic may have several causes; without further information it is hard to guess.
In any case you should open a new topic specific for this as this is not related to the original topic context.