i.MX Yocto Project: How can I patch the kernel?

Document created by Leonardo Sandoval Gonzalez Employee on Jul 30, 2013Last modified by Leonardo Sandoval Gonzalez Employee on Jun 4, 2014
Version 2Show Document
  • View in full screen mode

The Linux Kernel is just another recipe for Yocto, so learning to patch it you learn to patch any other package. In the other hand, Yocto **should not** be used for package development, but in those rare cases follow the below steps. It is assumed that you have already build the package you want to patch.

 

1. Create the patch or patches. In this example we are patching the Linux kernel for [wandboard-dual](http://www.wandboard.org/) machine; in other words, the value of MACHINE on the `build/conf/local.conf` is `MACHINE ??= 'wandboard-dual'`. In case you already have the patches, make sure these can be nicely applied with the commands `git apply --check <PATCH_NAME>`, and jump this step

 

 

build $ cd tmp/work/wandboard_dual-poky-linux-gnueabi/linux-wandboard/3.0.35-r0/git

build $ # Edit any files you want to change

build $ git add <modified file 1> <modified file 2> .. # Select the files you want to commit

build $ git commit -s -m '<your commit's title>' # Create the commit

build $ git format-patch -1 # Create the patch

 

2. Create a new layer (see document i.MX Yocto Proyect: How can I create a new Layer?)

 

3. On the new layer (e.g `meta-fsl-custom`) , create the corresponding subfolders and the `.bbfile`

 

sources $ mkdir -p meta-fsl-custom/recipes-kernel/linux/linux-wandboard-3.0.35/

sources $ cat > meta-fsl-custom/recipes-kernel/linux/linux-wandboard_3.0.35.bbappend

FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}-${PV}:"

SRC_URI += "file://0001-calibrate-Add-printk-example.patch"

PRINC := "${@int(PRINC) + 1}" # SEE NOTE BELLOW

^d

 

(The PRINC variable is not needed starting at Yocto 1.6 ([RFC] base.bbclass: Deprecate the PRINC logic - Patchwork))

 

4. Move the patch to the new layer

 

sources $ cp \

../build/tmp/work/wandboard_dual-poky-linux-gnueabi/linux-wandboard/3.0.35-r0/git/0001-calibrate-Add-printk-example.patch \

meta-fsl-custom/recipes-kernel/linux/linux-wandboard-3.0.35

 

5. Setup the enviroment and clean previous package's build data (sstate)

 

fsl-community-bsp $ . setup-environment build

build $ bitbake -c cleansstate linux-wandboard

 

6. Compile and Deploy

 

build $ bitbake -f -c compile linux-wandboard

build $ bitbake -c deploy linux-wandboard

 

7. Insert the SD into your Host and copy the `uImage` into the first partition. Do not forget to unmount the partition before removing the card!

 

 

build $ sudo cp tmp/deploy/images/uImage /media/Boot\ wandbo/

 

8. Insert the SD into your board and test your change.

7 people found this helpful

Attachments

    Outcomes