Add i.MX8MPlus pci driver in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add i.MX8MPlus pci driver in uboot

Add i.MX8MPlus pci driver in uboot

 

Platform & BSP : i.MX8MPlus EVK , L6.12.3, uboot lf_v2024.04

 

The attachments enable the i.MX8MPlus pci function in uboot.

lspci in Linux

root@imx8mpevk:~# lspci -nn
00:00.0 PCI bridge [0604]: Synopsys, Inc. DWC_usb3 / PCIe bridge [16c3:abcd] (rev 01)
01:00.0 Ethernet controller [0200]: Marvell Technology Group Ltd. Device [1b4b:2b42] (rev 11)

pci test results in uboot: 

u-boot=> pci
BusDevFun  VendorId   DeviceId   Device Class       Sub-Class
_____________________________________________________________
00.00.00   0x16c3     0xabcd     Bridge device           0x04
01.00.00   0x1b4b     0x2b42     Network controller      0x00

u-boot=> pci bar 00.00.00
ID   Base                Size                Width  Type
----------------------------------------------------------
 0   0x0000000018000000  0x0000000000100000  32     MEM

u-boot=> pci regions 00
Buses 00-01
#   Bus start          Phys start         Size                Flags
0   0x0000000000000000 0x000000001ff80000 0x0000000000010000  io
1   0x0000000018000000 0x0000000018000000 0x0000000007f00000  mem
2   0x0000000040000000 0x0000000040000000 0x0000000016000000  mem sysmem
3   0x0000000058000000 0x0000000058000000 0x00000000a8000000  mem sysmem
4   0x0000000100000000 0x0000000100000000 0x00000000c0000000  mem sysmem

u-boot=> pci header 00.00.00
  vendor ID =                   0x16c3
  device ID =                   0xabcd
  command register ID =         0x0007
  status register =             0x0010
  revision ID =                 0x01
  class code =                  0x06 (Bridge device)
  sub class code =              0x04
  programming interface =       0x00
  cache line =                  0x08
  latency time =                0x00
  header type =                 0x01
  BIST =                        0x00
  base address 0 =              0x18000000
  base address 1 =              0x00000000
  primary bus number =          0x00
  secondary bus number =        0x01
  subordinate bus number =      0x01
  secondary latency timer =     0x00
  IO base =                     0x10
  IO limit =                    0x00
  secondary status =            0x0000
  memory base =                 0x1820
  memory limit =                0x1810
  prefetch memory base =        0xfff0
  prefetch memory limit =       0x0000
  prefetch memory base upper =  0x00000000
  prefetch memory limit upper = 0x00000000
  IO base upper 16 bits =       0x0000
  IO limit upper 16 bits =      0x0000
  expansion ROM base address =  0x18100000
  interrupt line =              0xff
  interrupt pin =               0x01
  bridge control =              0x0000

u-boot=> pci header 01.00.00
  vendor ID =                   0x1b4b
  device ID =                   0x2b42
  command register ID =         0x0006
  status register =             0x0010
  revision ID =                 0x11
  class code =                  0x02 (Network controller)
  sub class code =              0x00
  programming interface =       0x00
  cache line =                  0x08
  latency time =                0x00
  header type =                 0x00
  BIST =                        0x00
  base address 0 =              0x1810000c
  base address 1 =              0x00000000
  base address 2 =              0x1820000c
  base address 3 =              0x00000000
  base address 4 =              0x00000000
  base address 5 =              0x00000000
  cardBus CIS pointer =         0x00000000
  sub system vendor ID =        0x0000
  sub system ID =               0x0000
  expansion ROM base address =  0x00000000
  interrupt line =              0xff
  interrupt pin =               0x01
  min Grant =                   0x00
  max Latency =                 0x00

Attachments
Comments

Hi I have an imx8qm, does that need the U-Boot patch in order to enable the PCI/PCIe function in U-Boot?

Hi @xnsmx 

No, default uboot support imx8qm.

Hi Zhiming :

Currently, we can correctly scan the host through the patch, but when we use PCI enumeration, it seems we cannot scan other devices. How should we modify this part?

Hi.

I'm using i.mx8mp. Currently I can't use PCI related commands in bootloader.

If I apply this patch, will I be able to use PCI commands in bootloader?

Could you also tell me how to apply the patch?

 

제목 없음.png

100% helpful (1/1)
Version history
Last update:
‎05-27-2025 08:01 PM
Updated by: