无线连接知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wireless Connectivity Knowledge Base

讨论

排序依据:
By default, FRDM-KW36 board includes a 32MHz XTAL (YI) as shown in Figure 1 but there are cases where a 26MHz XTAL is needed instead of 32MHz XTAL for FRDM-KW36 or a custom KW36 board.   Figure 1. 32MHz XTAL from FRDM-KW36 schematics Wireless connectivity demos from FRDM-KW36 Sofware Development Kit are configured to run with a 32MHz XTAL by default, but it's very easy to modify the software to operate with a 26MHz XTAL. Follow next steps to configure a FRDM-KW36 wireless connectivity demo to operate with a 26MHz XTAL: 1. In clock_config.h file, change BOARD_XTAL0_CLK_HZ define from 32000000U to 26000000U as shown in Figure 2.   Figure 2. BOARD_XTAL0_CLK_HZ define in clock_config.h 2. Add RF_OSC_26MHZ=1 line in preprocessor: If using IAR IDE: Right click on your project, then click options (Figure 3). Figure 3. IAR project options Go to C/C++ Compiler tab, then Preprocessor, and add RF_OSC_26MHZ=1 line in defined symbols window (Figure 4). Figure 4. IAR Preprocessor If using MCUXpresso IDE: Right click on your project, select Properties, go to Settings under C/C++ Build, then Preprocessor under MCU C Compiler (Figure 5). Figure 5. MCUXpresso Preprocessor Click on add button from Defined symbols, write RF_OSC_26MHZ=1 and click OK to finish (Figure 6). Figure 6. MCUXpresso Defined symbols To finish, re-compile your project and it will be ready to operate with a 26MHz XTAL. FRDM-KW36 SDK can be downloaded from the MCUXpresso webpage.
查看全文
Introduction This document is a quick start guide to load a new software image in a KW36 device through FSCI (Freescale Serial Communication Interface) bootloader software. Also, it contains all the steps needed to install the software required in a Windows host to handle the FSCI communication protocol. Software Requirements IAR Embedded Workbench IDE or MCUXpresso IDE. FRDM-KW36 SDK. Hardware Requirements FRDM-KW36 board. Downloading the SDK When downloading the SDK, select your specific IDE or simply choose all toolchains as shown below. In the option "Add software component", ensure to select all middleware components as depicted below. Installing FSCI Host in Windows OS The host software for the Windows OS was designed to work in a Python environment. The following steps are to download and install the software needed to use FSCI in a Windows OS. Visit the Python web site and download the latest Python 2.7.x MSI installer package for Windows OS. Open the MSI installer package. When customizing the installation options, check "Add python.exe to Path" as shown below Complete the rest of the steps for the Python installation process. Unzip the FRDM-KW36 SDK. Depending on your Python environment architecture, copy the HSDK.dll from <SDK_root>\tools\wireless\host_sdk\sdk-python\lib\<x86_or_x64> to <Python_directory>\DLLs (default in C:\Python27\DLLs). Download and install Visual C++ Redistributable Packages for Microsoft Visual Studio 2013 depending on the Windows architecture (vcredist_x86.exe or vcredist_x64.exe) from the Microsoft web site. Download and install the Microsoft Visual C++ Compiler for Python 2.7 from the following web site. To run Python scripts from the Command Prompt of Windows, we must create a system variable named PYTHONPATH. Search “System” in the Windows browser. Go to Advanced system settings -> Environment Variables… -> System variables. Click on the “New…” button and create the PYTHONPATH variable with the following value: <SDK_root>\tools\wireless\host_sdk\hsdk-python\src. Programming the FSCI bootloader on FRDM-KW36 board Attach the FRDM-KW36 board to your PC. Drag and drop the “bootloader_fsci_frdmkw36.bin” from the previously unzipped SDK file, you can find this file in: <SDK_root>\tools\wireless\binaries to your board. Like a common USB device. Creating a binary image to reprogram the device   IAR Embedded Workbench Open the connectivity project that you want to program through the FSCI bootloader from your SDK. This example will make use of the heart rate sensor project, located at the following path: <SDK_root>\boards\frdmkw36\wireless_examples\bluetooth\hrs\freertos\iar\hrs_freertos.eww. Open the project options window (Alt+F7). In Linker -> Config window, edit the “Configuration file symbol definitions” add the “gUseBootloaderLink_d=1” linker flag as shown below. Go to the “Output Converter” window and ensure that the output file is in binary format (.bin), otherwise, deselect the “Override default” checkbox, expand the “Output format” combo box and select “Raw binary. Click the OK button. Rebuild the project. The binary will be saved at: <SDK_root>\boards\frdmkw36\wireless_examples\bluetooth\hrs\freertos\iar\debug   MCUXpresso IDE Import your FRDM-KW36 SDK to MCUXpresso. Drag and drop your SDK on the "installed SDK's" toolbar. (In this step, it is not necessary to unzip the package). Open any connectivity project that you want to program through the FSCI bootloader from your SDK. This example will make use of the heart rate sensor project. Go to Project -> Properties, a new window will appear. Then, open the C/C++ Build -> Settings -> Linker -> Miscellaneous. Press the icon below, a new window will be deployed. Add “--defsym=gUseBootloaderLink_d=1”. Click on “Apply and Close”. Build the project. Deploy the “Binaries” icon in the workspace. Click the right mouse button on the “.axf” file. Select “Binary Utilities -> Create binary” option. The binary file will be saved at “Debug” folder in the workspace with “.bin” extension. Reprogramming an FRDM-KW36 board using the FSCI bootloader The following steps are to test the FSCI bootloader in a Windows OS. Search "Command Prompt" in the Windows browser. Run the "fsci_bootloader.py" Python script. Type the “python.exe” path in the console (default C:\Python27\python.exe). Drag and drop the “fsci_bootloader.py” from: <SDK_root>\tools\wireless\host_sdk\hsdk-python\src\com\nxp\wireless_connectivity\test\bootloader on the command prompt screen. Search the COM Port of your FRDM-KW36 board and type in the console. You can find it typing ‘Device manager’ from windows home and then search it in Ports (COM & LPT) toolbar. As you can see in this example the port may change depending on each case. Search the binary image file (created in the last section). Drag and drop on the screen. Press “Enter” to start the firmware update trough FSCI bootloader. Automatically the KW36 device will trigger to run the new software. To see all your process running, you can download the ‘IoT Toolbox’ from the app store to your smartphone and connect your device with the board to verify the random data that the heart rate sensor example generates.
查看全文
Introduction This document provides guidance to load a new software image in a KW35 device through OTAP (Over The Air Programming) bootloader for KW35. This article also provides the steps needed to download and install the SDK used in the tutorial. Software Requirements IAR Embedded Workbench IDE or MCUXpresso IDE. SDK MKW36A512xxx4 RC4 or further. Hardware Requirements MKW35A512xxx4 device. KW35 Flash Memory Used for the OTAP Software Deployment The KW35 Flash is partitioned into: 2x256 KB Program Flash (P-Flash) array divided into 2 KB sectors with a flash address range from 0x0000_0000 to 0x0007_FFFF.     The statements to comprehend how the OTAP Client software and his features works are: The OTAP Client software is split into two parts, the OTAP bootloader and the OTAP client service. The OTAP bootloader verifies if there is a new image already available to reprogram the device. The OTAP client service software provides the Bluetooth LE custom services needed to communicate with the server that contains the new image file. Therefore, before to start the test, the device has been programmed twice, first with the OTAP bootloader then with the OTAP client service project. The mechanism used to have two different software in the same device is to store each one in different memory regions and this is implemented by the linker file. In the KW35 device, the bootloader application has reserved a 16KB slot of memory starting from the 0x0 address (0x0 to 0x3FFF) thus, the left memory of the first P-Flash memory bank is reserved, among other things, by the OTAP client service application.   To create a new image file for the client device, the developer needs to specify to the linker file that the code will be stored with an offset of 16KB since the first addresses are reserved for the bootloader. At connection event, the server sends all the chunks of code to the client via Bluetooth LE. The client stores the code at the second P-Flash memory bank but is not able to run yet.   When the broadcast has finished, and all chunks were sent, the OTAP bootloader detects this situation and triggers a command to reprogram the device with the new application. Due the new application was built with an offset of 16KB, the OTAP bootloader program the device starting from the 0x3FFF address and the OTAP client service application is overwritten by the new image. Then the OTAP bootloader triggers the new application, starting the execution of the code.   Software Development Kit download and install   Go to MCUXpresso web page. Log in with your registered account. Search for “MKW36A” device. Then click on the suggested processor and click on “Build MCUXpresso SDK” The next page is displayed. Select “All toolchains” in the “Toolchain / IDE” combo box and provide the name to identify the package. Click on “Add software component”, then deploy the combo box and click on “Select All” option. Save the changes. Click on “Download SDK” button and accept the license agreement. If MCUXpresso IDE is used, drag and drop the SDK zip folder in “Installed SDK’s” perspective to install the package.     Preparing the software to test the OTAP for KW35 device using IAR Embedded Workbench   This section provides the steps needed to test the OTAP software on the KW35. Program the OTAP bootloader on the KW35. 1.1 Open the OTAP_bootloader project located at the following path: <SDK_download_root>\boards\virtual-board-kw35\wireless_examples\framework\bootloader_otap\bm\iar\bootloader_otap_bm.eww     1.2 Flash the project (Ctrl + D). Stop the debug session (Ctrl + Shift + D). Program the OTAP client application on the KW35.         2.1 Open the OTAP client project located in the path below.          <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\otac_att\freertos\iar\otac_att_freertos.eww          2.2 Follow the steps 2 to 12 described in the “4.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from               MKW36Z512xxx4 to MKW35Z512xxx4” application note.            2.3 Open the app_preinclude.h file under the source directory in the workspace. Find the “gEepromType_d” definition and update the value to                                 “gEepromDevice_InternalFlash_c” as shown below.   #define gEepromType_d gEepromDevice_InternalFlash_c‍‍‍‍‍            2.4 Save the MKW35Z512xxx4_connectivity.icf file located at:                <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\iar                               Into the folder of the OTAP Client ATT project:                <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\otac_att\freertos\iar            2.5 Open the project options window (Alt+F7). In Linker/Config window click the icon next to linker path and select the linker configuration file “MKW35Z512xxx4_connectivity.icf”. Set the "gUseInternalStorageLink_d” flag to 1.              2.6 Click the OK button in the project options window to save the new configuration.          2.7 Flash the project (Ctrl + D). Stop the debug session (Ctrl + Shift + D).    Preparing the software to test the OTAP for KW35 device using MCUXpresso IDE   This section provides the steps needed to test the OTAP software on the KW35. Program the OTAP bootloader on the KW35.          1.1 Open MCUXpresso IDE. Click on “Import SDK example(s)” option in the “Quickstart Panel” view.                        1.2 Click on virtual-board-kw35 SDK icon.          1.3 Deploy the wireless_examples\framework\bootloader_otap folders and select bm project. Click Finish button.                                                                           1.4 Select “Debug” option in the Quickstart Panel. Once the project is already loaded on the device, stop the debug session.      2. Program the OTAP client application on the KW35.          2.1 Open MCUXpresso IDE. Click on “Import SDK example(s)” option in the “Quickstart Panel” view.                          2.2 Click twice on the frdmkw36 icon.                                                                            2.3 Type “otac_att” in the examples textbox and select the freertos project at wireless_examples\bluetooth\otac_att\freertos. Finally, click on Finish button.              2.4 Follow the steps 5 to 17 described in the “5.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from MKW36Z512xxx4 to MKW35Z512xxx4” application note.            2.5. Open the app_preinclude.h file under the source directory in the workspace. Find the “gEepromType_d” definition and update the value to                “gEepromDevice_InternalFlash_c” as shown below. #define gEepromType_d gEepromDevice_InternalFlash_c‍‍‍‍‍            2.6 Save the MKW35Z512xxx4_connectivity.ld file located at:                <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\gcc                Into the source folder in the workspace.              2.7 Open the Project/Properties window. Next, go to the MCU Linker/Managed Linker Script perspective and edit the Linker Script name to “MKW35Z512xxx4_connectivity.ld”.              2.8 Go to MCU Linker/Miscellaneous view. Press the icon below, a new window will be deployed. Add the following definition in the “Other options” box: --defsym=gUseInternalStorageLink_d=1.              2.9 Click the “Apply and Close” button in the project options window to save the new configuration.          2.10 Select “Debug” option in the Quickstart Panel. Once the project is already loaded on the device, stop the debug session.   Running OTAP demo with the IoT Toolbox App Save the S-Record file created with the steps in Appendix A or Appendix B in your smartphone at a known location. Open the IoT Toolbox App and select OTAP demo. Press “SCAN” to start scanning for a suitable advertiser. Perform a falling edge on the PTB18 in the KW35 to start advertising. Create a connection with the founded device. Press “Open” and search the S-Record file. Press “Upload” to start the transfer. Once the transfer is complete, wait a few seconds until the bootloader has finished programming the new image. The new application will start automatically.    Appendix A. Creating an S-Record image file for KW35 client using IAR Embedded Workbench Open the connectivity project that you want to program using the OTAP bootloader from your SDK. This example will make use of the glucose sensor project. <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\glucose_s\freertos\iar\glucose_s_freertos.eww Follow the steps 2 to 12 described in the “4.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from              MKW36Z512xxx4 to MKW35Z512xxx4” application note. Save the MKW35Z512xxx4_connectivity.icf file located at: <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\iar                In the containing folder of your project. <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\glucose_s\freertos\iar Open the project options window (Alt+F7). In Linker/Config window click the icon next to linker path and select the linker configuration file MKW35Z512xxx4_connectivity.icf. Then, enable “gUseBootloaderLink_d” macro in the “Configuration file symbol definitions” textbox. Go to the “Output Converter” window. Deselect the “Override default" checkbox, expand the “Output format” combo box and select Motorola S-records format. Click OK button.                                                                                                                                           Rebuild the project. Search the S-Record file in the following path: <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\glucose_s\freertos\iar\debug   Appendix B. Creating an S-Record image file for KW35 client using MCUXpresso IDE Open the connectivity project that you want to program using the OTAP bootloader from MCUXpresso IDE This example will make use of the glucose sensor project Follow the steps 5 to 17 described in the “5.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from MKW36Z512xxx4 to MKW35Z512xxx4” application note. Save the MKW35Z512xxx4_connectivity.ld file located at: <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\gcc Into the source folder in the workspace.                                                                                                                  Open the Project/Properties window. Next, go to the MCU Linker/Managed Linker Script perspective and edit the Linker Script name to “MKW35Z512xxx4_connectivity.ld”.                                                                                  Go to MCU Linker/Miscellaneous view. Press the icon below, a new window will be deployed. Add the following definition in the “Other options” box: --defsym=gUseBootloaderLink_d=1. Click the “Apply and Close” button.                              Build the project. Deploy the “Binaries” icon in the workspace. Click the right mouse button on the “.axf” file. Select “Binary Utilities/Create S-Record” option. The S-Record file will be saved at “Debug” folder in the workspace with “.s19” extension.  
查看全文
The attached PDF file contains two A3 format "posters". The first one summarize the contents of the SMP Pairing Request and SMP Pairing Response packets (BLE 4.2). It shows how are the sub-fields of these packets set and what do they represent. The second one contains a diagram which summarizes how the pairing method and it's properties are determined during the SMP Pairing procedure for both BLE Legacy Pairing (BLE4.0 and BLE 4.1) and BLE Secure Connections Pairing with ECDH (BLE 4.2). Some of the tables in the diagram are taken from the BLE Specification. If you find any errors or have any suggestions of improvement please leave a comment or send me a message. Preview:
查看全文
Hello everyone, Over The Air Programming (OTAP) NXP's custom Bluetooth LE service provides the developer a solution to upgrade the software that the MCU contains. It removes the need for cables and a physical link between the OTAP client (the device that is reprogrammed) and the OTAP server (the device that contains the software update). This post explains how to run the OTAP Client Software that comes within the FRDM-KW36 package: Reprogramming a KW36 device using the OTAP Client Software. As it is mentioned in the last post, the OTAP Client can reprogram the KW36 while it is running, with new software using Bluetooth LE. However, this implementation for most of the applications is not enough since once you have reprogrammed the new image, the KW36 can not be reprogramed a second time using this method. For these applications that require to be updated many times using Bluetooth LE during run-time, we have created the following application note, that comes with a functional example of how to implement the OTAP Client software, taking advantage of this service. You can download the software clicking on the link in blue and the documentation is in the link in green. Please visit the following link: DOCUMENTS and Application Notes for KW36 In the "DOCUMENTS" section, you can found more information of the KW36. In the "Application Note" section, you can found more software and documentation of interesting topics like this.        Best Regards.
查看全文
Introduction This document describes the hardware considerations for the schematic and layout of the MKW36A512VFT4 device. This MCU is packaged into a 48-pin HVQFN - 7x7 mm, dissimilar to MKW36Z512VHT4 which comes packaged into a 48-pin LQFN - 7x7 mm (the last one takes part of FRDM-KW36).   Pin Layout  The MKW36A512VFT4 MCU is pin to pin compatible with the MKW36Z512VHT4 (FRDM-KW36) MCU, except for the DCDC pins. The following figure shows the distribution of the pins in the MKW36A512VFT4 MCU (left), compared with the MKW36Z512VHT4 (FRDM-KW36 MCU, right). Surely, this is the most important consideration for MKW36A512VFT4, since you can not simply move the FRDM-KW36 layout on your design. Minimum BOM The following figures show the minimum BOM necessary for each DCDC mode in KW36. For more information about DCDC modes and hardware guidelines, please visit: MKW4xZ/3xZ/3xA/2xZ DC-DC Power Management Bypass Mode   Buck Auto-Start Mode   Buck Manual-Start Mode     Layout Recommendations The footprint and layout are critical for RF performance, hence if the recommended design is followed exactly in the RF region of the PCB, sensitivity, output power, harmonic and spurious radiation, and range, you will succeed. For more information of layout recommendations, please visit Hardware Design Considerations for MKW35A/36A/35Z/36Z Bluetooth Low Energy Devices. The footprint recommended for the MKW36A512VFT4 is shown in the figure below. NXP prefers to use a top layer thickness of no less than 8-10 mils. The use of a correct substrate like the FR4 with a dielectric constant of 4.3 will assist you in achieving a good RF design. Other recommendations during EMC certification stages are: - Specific attention must be taken on 4 pins PTC1, 2, 3 & 4 if they are used on the application. - 4 decoupling capacitors of 3pF are mandatory on those pins and be positioned as close as possible. - Wires from those 4 pins must be underlayer. - NXP recommends putting the vias under the package in case the customer HW design rules allow it. Some recommendations for a good Vdd_RF supply layout are: - Vdd_RF1 and Vdd_RF2 lines must have the same length as possible, linked to pointA (‘Y’ connection). - 12pF decoupling capacitor from Vdd_RF wire must be connected to the Ground Antenna. The purpose is to get the path as short as possible from Vdd_RF1/Vdd_RF2 to the ground antenna. - 12pF decoupling capacitor from the Vdd_RF3 pin must be as close as possible. Return to ground must be as short as possible. So vias (2 in this below picture) must be placed near to the decoupling capacitor to get close connection to the ground layer. The recommended RF stage is shown in the following figure. The MKW36A512VFT4 has a single-ended RF output with a 2 components matching network composed of a shunt capacitor and a series inductor. Both elements transform the device impedance to 50 ohms. The value of these components may vary depending on your board layout. Avoid routing traces near or parallel to RF transmission lines or crystal signals. Maintain a continuous ground under an RF trace is critical to keep unaltered the characteristic impedance of the transmission line. Avoid routing on the ground layer that will result in disrupting the ground under RF traces. For more information about RF considerations please visit: Freescale IEEE 802.15.4 / ZigBee Package and Hardware Layout Considerations.
查看全文
This document describes how to sniff ZigBee packets to identify messages and layers from the ZigBee stack using the MC1322x USB dongle and Wireshark protocol analyzer. --------------------------------------------------------------------------------------------------------- Pre-Requisites If not done yet, download & Install Wireshark protocol analyzer http://www.wireshark.org/download.html Download the Wireshark ZigBee Utility Zip file from Sourceforge http://sourceforge.net/projects/wiresharkzigbee/ Unzip the file in a known location -------------------------------------------------------------------------------------------------------- 1. Install MC1322x dongle Plug-in MC1322xUSB dongle and wait for Windows to install the driver. If the driver was not found, steer Windows manually to the directory         C:\Program Files\Freescale\Drivers If BeeKit is not installed, be aware of the following: The 1322x USB Dongle uses the FTDI serial to USB converter, Virtual COM Port (VCP) driver for Windows, available at www.ftdichip.com/ftdrivers.htm. The FTDI web site offers drivers for other platforms including Windows® (98 through Vista x64 and CE), MAC OS (8 through X) and Linux. Download the appropriate driver and follow the instructions to complete driver installation. 2. Check COM port Once installed, the MC1322xUSB dongle should be listed in the available COM ports in Widows device manager. Verify the board’s drivers were successfully installed and take note of the COM port assigned      3. Run the ZigBee Utility Open a command console and navigate to the directory where Wireshark Zigbee utility files were unzipped. c:\<path> Then start the .exe utility and set the serial port and ZigBee channel to monitor, for instance:     4. Setting Wireshark Start Wireshark and open Capture>Options Dialog Click on “Manage Interfaces” and add a new pipe with ‘\\.\pipe\wireshark’. Save it and start capture. 5. Start sniffing
查看全文
Introduction In some applications, is it necessary to keep updated the software running in many MCU's that take part in the system, fortunately, Over The Air Programming, it's a custom Bluetooth LE service developed to send "over the air" software updates for the KW MCU series. FRDM-KW36 SDK already provides the "otap_client" software, that can be used together with the "otap_bootloader" such as it is described in the following community post: Reprogramming a KW36 device using the OTAP Client Software to reprogram the KW36. This example can be modified to store code for another MCU and later send the software update to this device as depicted in the figure below. This post guides you on modifying the OTAP client software to support software updates for other MCU's. Preparing the OTAP client software The starting point of the following modifications is supposing that there is no need to perform over the air updates for the KW36 MCU, so the use of the "otap_bootloader" is obsolete and will be removed in this example. In other words, KW36 will be programmed only with the "otap_client" code. Open the MCUXpresso settings window (Project->Properties->"C/C++ Build->MCU settings") and configure the following fields. Save the changes. For external storage: For internal storage: Locate the "app_preinclude.h" file, and set the storage method, as follows: For external storage: #define gEepromType_d       gEepromDevice_AT45DB041E_c For internal storage: #define gEepromType_d        gEepromDevice_InternalFlash_c Locate the "main_text_section.ldt" linker script into the "linkscripts" folder, and delete it from the project.  Search in the project for "OTA_SetNewImageFlag();" and "ResetMCU();" functions in the "otap_client.c" file (source->common->otap_client->otap_client.c) and delete or comment. (For reference, there are 4 in total). Locate the following code in "OtaSupport.h" (framework->OtaSupport->Interface) and delete or comment. extern uint16_t gBootFlagsSectorBitNo;‍‍‍‍‍‍ void OTA_SetNewImageFlag(void);‍‍‍‍‍‍‍ Locate the following code in "OtaSupport.c" (framework->OtaSupport->Source) and delete or comment. extern uint32_t __BootFlags_Start__[]; #define gBootImageFlagsAddress_c ((uint32_t)__BootFlags_Start__)‍‍‍‍‍‍‍‍‍‍‍‍ #if !gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d) /*! Variables used by the Bootloader */ #if defined(__IAR_SYSTEMS_ICC__) #pragma location = "BootloaderFlags" const bootInfo_t gBootFlags = #elif defined(__GNUC__) const bootInfo_t gBootFlags __attribute__ ((section(".BootloaderFlags"))) = #elif defined(__CC_ARM) volatile const bootInfo_t gBootFlags __attribute__ ((section(".BootloaderFlags"))) = #else #error "Compiler unknown!" #endif { {gBootFlagUnprogrammed_c}, {gBootValueForTRUE_c}, {0x00, 0x02}, {gBootFlagUnprogrammed_c}, #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) {PLACEHOLDER_SBKEK}, {BOOT_MAGIC_WORD} #endif }; #endif /* !gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d) */‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ uint16_t gBootFlagsSectorBitNo; gBootFlagsSectorBitNo = gBootImageFlagsAddress_c/(uint32_t)((uint8_t*)FSL_FEATURE_FLASH_PFLASH_BLOCK_SECTOR_SIZE);‍‍‍‍ gBootFlagsSectorBitNo = gBootImageFlagsAddress_c/(uint32_t)((uint8_t*)FSL_FEATURE_FLASH_PAGE_SIZE_BYTES);‍‍‍‍ void OTA_SetNewImageFlag(void) { #if (gEepromType_d != gEepromDevice_None_c) && (!gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d)) /* OTA image successfully written into the non-volatile storage. Set the boot flag to trigger the Bootloader at the next CPU Reset. */ union{ uint32_t value; uint8_t aValue[FSL_FEATURE_FLASH_PFLASH_BLOCK_WRITE_UNIT_SIZE]; }bootFlag; #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) uint8_t defaultSBKEK[SBKEK_SIZE] = {DEFAULT_DEMO_SBKEK}; #endif uint32_t status; if( mNewImageReady ) { NV_Init(); bootFlag.value = gBootValueForTRUE_c; status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.newBootImageAvailable, sizeof(bootFlag), bootFlag.aValue); if( (status == kStatus_FLASH_Success) && FLib_MemCmpToVal(gBootFlags.internalStorageAddr, 0xFF, sizeof(gBootFlags.internalStorageAddr)) ) { bootFlag.value = gEepromParams_StartOffset_c + gBootData_ImageLength_Offset_c; status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.internalStorageAddr, sizeof(bootFlag), bootFlag.aValue); } #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) if( status == kStatus_FLASH_Success ) { /* Write the default SBKEK for secured OTA */ status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.sbkek, SBKEK_SIZE, defaultSBKEK); } #endif if( status == kStatus_FLASH_Success ) { mNewImageReady = FALSE; } } #endif }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   At this point, the FRDM-KW36 can receive and store any image for any MCU and can request a further software update from the OTAP server device.    Adding API's to reprogram the "MCU X" on OTAP client software Once the software update has been downloaded from the OTAP Server into the OTAP Client, the developer should request the software update from the OTAP Client to the "MCU X" through a serial protocol such as UART, SPI, CAN, etc. You should develop the API's and the protocol according to the requirements for your system to send the software update to the "MCU X" (as well as the bootloader for the MCU X). The handling your protocol can be integrated into the OTAP client code replacing "ResetMCU()" (The same code removed in step 4) in the code by "APISendSoftwareUpdateToMCUX()" for instance, since at this point the image was successfully sent over the air and stored in the memory of the KW36. 
查看全文
The image below shows the different types of devices in a Thread Network. Router Routers provide routing services to network devices. Routers also provide joining and security services for devices trying to join the network. Routers are not designed to sleep. Routers can downgrade their functionality and become REEDs (Router-eligible End Devices). A Router can become a Leader and start a Thread network. Border Router A Border Router is a type of Router that provides connectivity from the 802.15.4 network to adjacent networks on other physical layers (for example, Wi-Fi and Ethernet). Border Routers provide services for devices within the 802.15.4 network, including routing services for off-network operations. There may be one or more Border Routers in a Thread Network. The Border Router also serves as an interface point for the Commissioner when the Commissioner is on a non-Thread Network; it requires a Thread interface and may be combined in any device with other Thread roles except the Joiner. Leader A Router or Border Router can assume a Leader role for certain functions in the Thread Network. This Leader is required to make decisions within the network. For example, the Leader assigns Router addresses and allows new Router requests. The Leader role is elected and if the Leader fails, another Router or Border Router assumes the Leader role. It is this autonomous operation that ensures there is no single point of failure. Router-eligible End Device REEDs have the capability to become Routers but due to the network topology or conditions these devices are not acting as Routers. These devices do not generally forward messages or provide joining or security services for other devices in the Thread Network. The Thread Network manages REEDs becoming Routers if necessary without user interaction. Sleepy End Device Sleepy end devices are host devices. They communicate only through their Parent Router and cannot forward messages for other devices References: Thread Whitepapers available at http://threadgroup.org 
查看全文
Introduction The FRDM-KW36 includes an RSIM (Radio System Integration Module) module with an external 32 MHz crystal oscillator. This clock source reference is mainly intended to supply the Bluetooth LE Radio peripheral, but it can be used as the main clock source of the MCU as well. This oscillator includes a set of programmable capacitors to support crystals with different load capacitance needs. Changing the value of these capacitors can modify the frequency the oscillator provides, that way, the central frequency can be tuned to meet the wireless protocol standards. This configurable capacitance range is from C1: 5.7pF - C2: 7.1pF to C1: 22.6pF - C2: 28.2pF and it is configured through the BB_XTAL_TRIM field at the ANA_TRIM. The KW36 comes preprogrammed with a default load capacitance value. However, since there is variance in devices due to tolerances and parasite effects, the correct load capacitance should be checked by verifying that the optimal central frequency is attained.  You will need a spectrum analyzer to measure the central frequency. To find the most accurate value for the load capacitance, it is recommended to use the Connectivity Test demo application. Adjusting Frequency Example Program the KW36 Connectivity Test software on the device. This example can be found in wireless_examples -> genfsk -> conn_test folder from your SDK package. Baremetal and FreeRTOS versions are available. In case that FRDM-KW36 board is being used to perform the test, you should move the 10pF capacitor populated in C55 to C57, to direct the RF signal on the SMA connector. Connect the board to a serial terminal software. When you start the application, you will be greeted by the NXP logo screen:  Press the enter key to start the test. Then press "1" to select "Continuous tests": Finally, select "6" to start a continuous unmodulated RF test. At this point, you should be able to measure the signal in the spectrum analyzer. You can change the RF channel from 0 to 127 ("q" Ch+ and "w" Ch- keys), which represents the bandwidth from 2.360GHz to 2.487GHz, stepping of 1MHz between two consecutive channels. To demonstrate the trimming procedure, this document will make use of channel 42 (2.402GHz) which corresponds to the Bluetooth LE channel 37. In this case, with the default capacitance value, our oscillator is not exactly placed at the center of the 2.402GHz, instead, it is slightly deflected to 2.40200155 GHz, as depicted in the following figure: The capacitance can be adjusted with the "d" XtalTrim+ and "f" XtalTrim- keys. Increasing the capacitance bank means a lower frequency. In our case, we need to increase the capacitance to decrease the frequency. The nearest frequency of 2.402 GHz was 2.40199940 GHz  Once the appropriate XTAL trim value has been found, it can be programmed as default in any Bluetooth LE example, changing the mXtalTrimDefault constant located in the board.c file: static const uint8_t mXtalTrimDefault‍ = 0x36;‍‍‍
查看全文
Regarding to the "Reprogramming a KW36 device using the OTAP Client Software" and "Reprogramming a KW35 device using the OTAP Client Software" documents, there are some additional steps to debug the OTAP client software in the specific case when you use MCUXpresso together with a P&E micro debug probe. Just before to program the OTAP client project (the second software), the user must do the following: Open the "Debug Configurations" view clicking on the green bug as depicted below. Go to the "Debugger" perspective and search the "Advanced Options" button. Enable the "Preserve this range (Memory Range 0)" checkbox, and edit the textbox "From: 0" To: 1fff" for the KW36 device or "From: 0 To: 3fff" for the KW35 device. After to flash the device, disconnect and connect again. If everything it's OK, the RGB LED must blink (If you are using an FRDM board). Then, test the demo as described in the document.
查看全文
This patch fixes some minor issues with the Connectivity Software v1.0.2 when working with the Kinetis BLE Toolbox application for smartphones. Following issues are fixed. BLE OTAP Application: Fixes application failing to download the new image when the previous image upload has been interrupted due a disconnection. BLE Wireless UART: Fixes MTU exchange issue causing some characters not bein shown in the smartphone application in iOS and Android. Hybrid BLE + Thread console: Fixes MTU exchange issue causing some characters not bein shown in the smartphone application console in iOS and Android. Make sure the Connectivity Software version 1.0.2 is installed in your computer before proceeding to install this application.
查看全文
This guide will show a way to set up and enable an I2C Serial Interface to send a string of data instances using one of the Wireless Bluetooth SDK examples and the Serial Manager API.
查看全文
Introduction The MTU (Maximum Transmission Unit) in Bluetooth LE, is an informational parameter that indicates to the remote device, the maximum number of bytes that the local can handle in such channel, for example, the ATT_MTU for KW36 is fixed in 247 bytes. A few applications require to have long characteristics defined in the GATT database, and sometimes the length of the characteristic exceeds the MTU negotiated by the client and server Bluetooth LE devices. For this scenario, the Bluetooth LE specification defines a procedure to write and read the characteristic of interest. In summary, it consists in perform multiple writes and reads on the same characteristic value, using specific commands. For the "write long characteristic value" procedure, these commands are ATT_PREPARE_WRITE_REQ and ATT_EXECUTE_WRITE_REQ. For the "read long characteristic value" procedure, these commands are ATT_READ_REQ and ATT_READ_BLOB_REQ. This document provides an example of how to write and read long characteristic values, from the perspective of Client and Server devices.   APIs to Write and Read Characteristic Values Write Characteristic Values The GattClient_WriteCharacteristicValue API is used to perform any write operation. It is implemented by the GATT Client device. The following table describes the input parameters. Input Parameters Description deviceId_t deviceId Device ID of the peer device. gattCharacteristic_t * pCharacteristic Pointer to a gattCharacteristic struct type. This struct must contain a valid handle of the characteristic value in the "value.handle" field. The handle of the characteristic value that you want to write is commonly obtained after the service discovery procedure.  uint16_t valueLength This value indicates the length of the array pointed by aValue. const uint8_t * aValue Pointer to an array containing the value that will be written to the GATT database. bool_t withoutResponse If true, it means that the application wishes to perform a "Write Without Response", in other words, when the command will be ATT_WRITE_CMD or ATT_SIGNED_WRITE_CMD. bool_t signedWrite If withoutResponse and signedWrite are both true, the command will be ATT_SIGNED_WRITE_CMD. If withoutResponse is false, this parameter is ignored. bool_t doReliableLongCharWrites This field must be set to true if the application needs to write a long characteristic value. const uint8_t * aCsrk If withoutResponse and signedWrite are both true, this pointer must contain the CSRK to sign the data. Otherwise, this parameter is ignored.   Read Characteristic Values The GattClient_ReadCharacteristicValue API is used to perform read operations. It is implemented by the GATT Client device. The following table describes the input parameters. Input Parameters Description deviceId_t deviceId Device ID of the peer device. gattCharacteristic_t * pIoCharacteristic Pointer to a gattCharacteristic struct type. This struct must contain a valid handle of the characteristic value in the "value.handle" field. The handle of the characteristic value that you want to write is commonly obtained after the service discovery procedure. As well, the "value.paValue" field of this struct, must point to an array which will contain the characteristic value read from the peer. unit16_t maxReadBytes The length of the characteristic value that should be read. This API takes care of the long characteristics, so there is no need to worry about a special parameter or configuration. The following sections provide a functional example of how to write and read long characteristics. This example was based on the temperature collector and temperature sensor SDK examples. The example also shows how to create a custom service at the GATT database and how to discover its characteristics.   Bluetooth LE Server (Temperature Sensor) Modifications in gatt_uuid128.h Define the 128 bit UUID of the "custom service" which will be used for this example. Add the following code: /* Custom service */ UUID128(uuid_service_custom, 0xE0, 0x1C, 0x4B, 0x5E, 0x1E, 0xEB, 0xA1, 0x5C, 0xEE, 0xF4, 0x5E, 0xBA, 0x00, 0x01, 0xFF, 0x01) UUID128(uuid_char_custom, 0xE0, 0x1C, 0x4B, 0x5E, 0x1E, 0xEB, 0xA1, 0x5C, 0xEE, 0xF4, 0x5E, 0xBA, 0x01, 0x01, 0xFF, 0x01)‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Modifications in gatt_db.h Define the characteristics of the "custom service", for this example, our service will have just one characteristic, it can be written or read, and it has a variable-length limited to 400 bytes (remember that the ATT_MTU of KW36 is 247 byte, so with this length, we ensure long writes and reads). Add the following code: PRIMARY_SERVICE_UUID128(service_custom, uuid_service_custom) CHARACTERISTIC_UUID128(char_custom, uuid_char_custom, (gGattCharPropWrite_c | gGattCharPropRead_c)) VALUE_UUID128_VARLEN(value_custom, uuid_char_custom, (gPermissionFlagWritable_c | gPermissionFlagReadable_c), 400, 1)‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Modifications in app_preinclude.h One of the most important considerations to write and read long characteristics is the memory allocation needed for this. You must increment the current "AppPoolsDetails_c" configuration, the "_block_size_" and "_number_of_blocks_". Please ensure that "_block_size_" is aligned with 4 bytes. Once you have found the configuration that works in your application, please follow the steps in Memory Pool Optimizer on MKW3xA/KW3xZ Application Note, to found the best configuration without waste memory resources. For this example, configure "AppPoolsDetails_c" as follows: /* Defines pools by block size and number of blocks. Must be aligned to 4 bytes.*/ #define AppPoolsDetails_c \ _block_size_ 264 _number_of_blocks_ 8 _eol_‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Bluetooth LE Client (Temperature Collector) Modifications in gatt_uuid128.h Define the 128 bit UUID of the "custom service" which will be used for this example. Add the following code: /* Custom service */ UUID128(uuid_service_custom, 0xE0, 0x1C, 0x4B, 0x5E, 0x1E, 0xEB, 0xA1, 0x5C, 0xEE, 0xF4, 0x5E, 0xBA, 0x00, 0x01, 0xFF, 0x01) UUID128(uuid_char_custom, 0xE0, 0x1C, 0x4B, 0x5E, 0x1E, 0xEB, 0xA1, 0x5C, 0xEE, 0xF4, 0x5E, 0xBA, 0x01, 0x01, 0xFF, 0x01)‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Modifications in temperature_collector.c 1. Define the following variables at the "Private type definitions" section: typedef struct customServiceConfig_tag { uint16_t hService; uint16_t hCharacteristic; } customServiceConfig_t; typedef struct appCustomInfo_tag { tmcConfig_t tempClientConfig; customServiceConfig_t customServiceClientConfig; }appCustomInfo_t; typedef enum { mCustomServiceWrite = 0, mCustomServiceRead }customServiceState_t;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 2. Add two arrays of 400 bytes, one to send and the other to receive the data from the server in "Private memory declarations" section: /* Dummy array for custom service */ uint8_t mWriteDummyArray[400]; uint8_t mReadDummyArray[400];‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 3. Define a new function in "Private functions prototypes" section, to write and read the characteristic value: static void BleApp_SendReceiveCustomService (customServiceState_t state);‍‍‍‍ 4. Locate the "BleApp_Config" function, add the following code here to fill the "mWriteDummyArray" with a known pattern before to write our custom characteristic. static void BleApp_Config(void) { uint16_t fill_pattern; /* Fill pattern to write long characteristic */ for (fill_pattern = 0; fill_pattern<400; fill_pattern++) { mWriteDummyArray[fill_pattern] = (uint8_t)fill_pattern; } /* Configure as GAP Central */ BleConnManager_GapCommonConfig(); ... ... }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 5. Locate the "BleApp_StoreServiceHandles" function. Modify this function to include our custom service in the service discovery procedure. This is to save the handle of the custom characteristic since it is used by GattClient_WriteCharacteristicValue and GattClient_ReadCharacteristicValue APIs. static void BleApp_StoreServiceHandles ( gattService_t *pService ) { uint8_t i,j; if ((pService->uuidType == gBleUuidType128_c) && FLib_MemCmp(pService->uuid.uuid128, uuid_service_temperature, 16)) { /* Found Temperature Service */ mPeerInformation.customInfo.tempClientConfig.hService = pService->startHandle; for (i = 0; i < pService->cNumCharacteristics; i++) { if ((pService->aCharacteristics[i].value.uuidType == gBleUuidType16_c) && (pService->aCharacteristics[i].value.uuid.uuid16 == gBleSig_Temperature_d)) { /* Found Temperature Char */ mPeerInformation.customInfo.tempClientConfig.hTemperature = pService->aCharacteristics[i].value.handle; for (j = 0; j < pService->aCharacteristics[i].cNumDescriptors; j++) { if (pService->aCharacteristics[i].aDescriptors[j].uuidType == gBleUuidType16_c) { switch (pService->aCharacteristics[i].aDescriptors[j].uuid.uuid16) { /* Found Temperature Char Presentation Format Descriptor */ case gBleSig_CharPresFormatDescriptor_d: { mPeerInformation.customInfo.tempClientConfig.hTempDesc = pService->aCharacteristics[i].aDescriptors[j].handle; break; } /* Found Temperature Char CCCD */ case gBleSig_CCCD_d: { mPeerInformation.customInfo.tempClientConfig.hTempCccd = pService->aCharacteristics[i].aDescriptors[j].handle; break; } default: ; /* No action required */ break; } } } } } } else if ((pService->uuidType == gBleUuidType128_c) && FLib_MemCmp(pService->uuid.uuid128, uuid_service_custom, 16)) { /* Found Custom Service */ mPeerInformation.customInfo.customServiceClientConfig.hService = pService->startHandle; if (pService->cNumCharacteristics > 0U && pService->aCharacteristics != NULL) { /* Found Custom Characteristic */ mPeerInformation.customInfo.customServiceClientConfig.hCharacteristic = pService->aCharacteristics[0].value.handle; } } else { ; } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 6. Develop the "BleApp_SendReceiveCustomService" as shown below. This function is used to write and read the custom characteristic values using long operations. Focus your attention in this function, here is the example of how to use GattClient_WriteCharacteristicValue and GattClient_ReadCharacteristicValue APIs to write and read long characteristic values. Note that the "characteristic" struct was filled before to use the last APIs, with the handle of our custom characteristic and a destination address to receive the value read from the peer. Note that the "doReliableLongCharWrites" field must be TRUE to allow long writes using GattClient_WriteCharacteristicValue.  static void BleApp_SendReceiveCustomService (customServiceState_t state) { bleResult_t bleResult; gattCharacteristic_t characteristic; /* Verify if there is a valid peer */ if (gInvalidDeviceId_c != mPeerInformation.deviceId) { /* Fill the characteristic struct with a read destiny and the custom service handle */ characteristic.value.handle = mPeerInformation.customInfo.customServiceClientConfig.hCharacteristic; characteristic.value.paValue = &mReadDummyArray[0]; /* Try to write the custom characteristic value */ if(mCustomServiceWrite == state) { bleResult = GattClient_WriteCharacteristicValue(mPeerInformation.deviceId, &characteristic, (uint16_t)400, &mWriteDummyArray[0], FALSE, FALSE, TRUE, NULL); /* An error occurred while trying to write the custom characteristic value, disconnect */ if(gBleSuccess_c != bleResult) { (void)Gap_Disconnect(mPeerInformation.deviceId); } } /* Try to read the custom characteristic value */ else { bleResult = GattClient_ReadCharacteristicValue(mPeerInformation.deviceId, &characteristic, (uint16_t)400); /* An error occurred while trying to read the custom characteristic value, disconnect */ if(gBleSuccess_c != bleResult) { (void)Gap_Disconnect(mPeerInformation.deviceId); } } } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 7. Modify the "BleApp_GattClientCallback" as shown below. In this function, we implement the "BleApp_SendReceiveCustomService" which writes or reads the characteristic depending on the input parameter "state". The expected behavior of this example is, first, write the 400-byte pattern contained in the mWriteDummyArray to our custom characteristic value, just after to write the characteristic descriptor of the temperature service (which is indicated by this callback in the gGattProcWriteCharacteristicDescriptor_c event). When the write has been executed successfully, it is indicated in this callback, by the "gGattProcWriteCharacteristicValue_c" event, therefore, here we can execute our function to read the characteristic value. Then "gGattProcReadCharacteristicValue_c" event is triggered if the read has been completed, here, we compare the value written with the value read from the GATT server and, if both are the same, the green RGB led should turn on indicating that our long characteristic has been written and read successfully, otherwise, the GATT client disconnects from the GATT server.   static void BleApp_GattClientCallback( deviceId_t serverDeviceId, gattProcedureType_t procedureType, gattProcedureResult_t procedureResult, bleResult_t error ) { if (procedureResult == gGattProcError_c) { attErrorCode_t attError = (attErrorCode_t)(uint8_t)(error); if (attError == gAttErrCodeInsufficientEncryption_c || attError == gAttErrCodeInsufficientAuthorization_c || attError == gAttErrCodeInsufficientAuthentication_c) { /* Start Pairing Procedure */ (void)Gap_Pair(serverDeviceId, &gPairingParameters); } BleApp_StateMachineHandler(serverDeviceId, mAppEvt_GattProcError_c); } else { if (procedureResult == gGattProcSuccess_c) { switch(procedureType) { case gGattProcReadCharacteristicDescriptor_c: { if (mpCharProcBuffer != NULL) { /* Store the value of the descriptor */ BleApp_StoreDescValues(mpCharProcBuffer); } break; } case gGattProcWriteCharacteristicDescriptor_c: { /* Try to write to the custom service */ BleApp_SendReceiveCustomService(mCustomServiceWrite); } break; case gGattProcWriteCharacteristicValue_c: { /* If write to the custom service was completed, try to read the custom service */ BleApp_SendReceiveCustomService(mCustomServiceRead); } break; case gGattProcReadCharacteristicValue_c: { /* If read to the custom service was completed, compare write and read buffers */ if(FLib_MemCmp(&mWriteDummyArray[0], &mReadDummyArray[0], 400)) { Led3On(); } else { (void)Gap_Disconnect(mPeerInformation.deviceId); } } break; default: { ; /* No action required */ break; } } BleApp_StateMachineHandler(serverDeviceId, mAppEvt_GattProcComplete_c); } } /* Signal Service Discovery Module */ BleServDisc_SignalGattClientEvent(serverDeviceId, procedureType, procedureResult, error); }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Modifications in app_preinclude.h One of the most important considerations to write and read long characteristics is the memory allocation needed for this. You must increment the current "AppPoolsDetails_c" configuration, the "_block_size_" and "_number_of_blocks_". Please ensure that "_block_size_" is aligned with 4 bytes. You can know when the current configuration of pools do not satisfy the application requirements if the return value of either "GattClient_WriteCharacteristicValue" or "GattClient_ReadCharacteristicValue " is "gBleOutOfMemory_c" instead of "gBleSuccess_c" (If it is the case, the device will disconnect to the peer according to the code in step 6 in "Modifications in temperature_collector.c"). Once you have found the configuration that works in your application, please follow the steps in Memory Pool Optimizer on MKW3xA/KW3xZ Application Note, to found the best configuration without waste memory resources. For this example, configure "AppPoolsDetails_c" as follows: /* Defines pools by block size and number of blocks. Must be aligned to 4 bytes.*/ #define AppPoolsDetails_c \ _block_size_ 112 _number_of_blocks_ 6 _eol_ \ _block_size_ 256 _number_of_blocks_ 3 _eol_ \ _block_size_ 280 _number_of_blocks_ 2 _eol_ \ _block_size_ 432 _number_of_blocks_ 1 _eol_‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Please let us know any question regarding this topic.
查看全文
With the release of the Bluetooth LE core erratum 10734, two new Host test cases (SM/SLA/KDU/BI-01-C and SM/MAS/KDU/BI-01-C) were added to the Test Case Reference List (TCRL) and are active since 24-Jan-19. This has an impact on new product qualifications based on Component (Tested) QDIDs that used an older TCRL when the test cases for this erratum were not required. Products that rely on NXP HOST QDIDs have 2 options for covering the erratum 10734 in order to complete the qualification: NXP provides a new qualification/QDID that includes these 2 tests. This is scheduled for later this year for QN908x, KW35/36 and KW41/31 products. NXP provides the test evidence/logs for these 2 tests and the test house reviews them before completing the product qualification. Right now, option 2 can be followed using the test evidence/logs provided by NXP. Later in the year, option 1 can be followed with an updated QDID. To obtain the test evidence/logs, please submit a support request.
查看全文
This document describes the implementation of the Connected Home Gateway for the Internet of Things (IoT) and its controller implemented in a Smart device (tablet) running Android OS. The gateway is intended to serve as a communication bridge between WiFi/Ethernet and ZigBee Protocol, making every ZigBee-enabled device accessible and controllable from any smart device with Wi-Fi capabilities such as a smart phone or tablet. This will remove the need of having a ZigBee transceiver in every mobile device attempting to control the house appliances. In general, users will be able to: Remote control of Home Appliances using ZigBee protocol Any WiFi-enabled device could control the appliances without a ZigBee transceiver Achieve bi-directional communication between users and appliances Real system implementation would require a powerful MCU to manage all WiFi/Ethernet communication and a second MCU to manage all ZigBee communications. The Kinetis K60 and KW24 were selected among the different options available.
查看全文
This video shows how to load the Open SDA software from PE micro to the TWR-KW2x in order to debug applications using USB port and without needing external JTAG debuggers. Required downloads: TWR-KW2x Board Support Package:Kinetis KW2x Tower System Modules|Freescale PE Micro - Open SDA: P&E Microcomputer Systems
查看全文
QTool is a PC software tool that works with QN9080 USB dongle to assist in the development of BLE projects with the QN9080. You control the dongle via the QTool software, which issues and receives FSCI (Framework Serial Communication Interface) formatted commands over a virtual COM port. The dongle can then act either as a master or a slave to a QN9080DK board over BLE.  Before using the BLE dongle with QTool though, the firmware on the QN9080 Dongle must be updated. The updated firmware can be found inside the QTool installation directory, and you will need to put the dongle into bootloader mode to drag-and-drop new firmware on it. Updating the Firmware on the QN9080 Dongle. 1. Install QTool: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup   2. Plug the QN9080 Dongle into a USB port on your computer 3. Using a wire, connect TP5 to ground. You can use either TP4 or the USB shield for GND. 4. While that wire is connected, press the reset button on the dongle. This will now put the dongle into bootloader mode. 5. A drive will enumerate on your computer named “CRP_DISABLD”     6. You can now remove the wire 7. Delete the firmware.bin file found in that drive 8. Drag-and-drop the firmware.bin file found in C:\NXP\Connectivity QTool\bin files into that enumerated drive. 9. Once done copying, unplug and replug in the USB Dongle, and the new firmware will now be running.  Installing the QN9080 Dongle Driver The dongle will enumerate as a USB CDC COM device. If the CDC driver is not automatically detected, you will need to manually install the driver. 1. Right-click Computer and choose Properties, the System Management window appears. 2. Click Device Manager and navigate to MCU VIRTUAL COM DEMO      3. Right-click the device MCU VIRTUAL COM DEMO and choose Update Driver Software 4. Click the  Browse my computer for driver software option in the window. 5. Click Browse button to go to the folder  C:\NXP\Connectivity QTool\drivers 6. Click the Next button at the bottom to install the driver.  7. After the driver is installed you will see the Virtual Com Port device under the Ports category    Using QTool: Now that the QN9080 dongle has the updated firmware and has the correct driver installed, you can follow the instructions in the QTool documentation found at C:\NXP\Connectivity QTool\UM11085.pdf Related documentation: QN908x Quick Start Guide QN908x DK User's Guide
查看全文
FRDM-KW36 Software Development Kit (SDK) includes drivers and examples of FlexCAN module for KW36 which can be easily configured for a custom communication. For example, if user want to change the default baud rate from FlexCAN driver demo examples then the only needed change is the default value on "config->baudRate" and "config->baudRateFD" from "FLEXCAN_GetDefaultConfig" function (See Figure 1). Segments within a bit time will be automatically configured to obtain the desired baud rate. By default, demos are configured to work with CAN FD communication. Figure 1. FRDM-KW36's default baudrate from flexcan_interrupt_transfer driver example Even so, there are cases where segments within a bit time are not well configured and it's necessary that user configure segments manually. An example occurs by setting the maximum FD baud rate "3.2MHz" using the 32MHz xtal or "2.6MHz" using a 26MHz xtal where demo reports an error. See Figure 2. Figure 2. Error by setting maximum baud rate When this error occurs, the fix is on setting the timing config parameters correctly by including the definition of SET_CAN_QUANTUM on application source file (see Figure 3) and then declare and initialize the timing config parameters shown in Figure 4. Figure 3. SET_CAN_QUANTUM define Figure 4. Custom timing config parameters For this example we are going to show how to calculate timing config parameters in an scenario where a CAN FD communication is used with baud rate of 500kHz on nominal phase and 3.2MHz on FD phase. See Figure 5.  To do it, we need to calculate Time Quanta and value of segments within the bit time.    Figure 5. Custom CAN FD baudrate KW36 Reference Manual in chapter "37.4.8.7 Protocol timing" shows the segments within a bit time for CAN nominal phase configured in "CAN_CTRL1" register (see Figure 6), and segments for FD phase configured in CAN_FDCBT register (see Figure 7). Figure 6. Segment within a bit time for CAN nominal phase Figure 7. Segment within a bit time for CAN FD phase Before calculating the value of segments, first we need to calculate the Time Quanta which is the atomic number of time handled by the CAN engine. The formula to calculate Time Quanta is shown in Figure 8 taken from KW36 Reference Manual. Figure 8. Time Quanta Formula CANCLK can be selected by CLKSRC bits on CAN_CTRL1 register as shown in Figure 9, where the options are Peripheral clock=20MHz or Oscillator clock (16MHz if using 32MHz xtal or 13MHz if using 26MHz xtal). The recomiendation is to use the Oscillator clock due to peripheral clock can have jitter that affect communication.  Figure 9. CAN clocks To select the Oscillator clock, search for flexcanConfig.clkSrc definition and set it to kFLEXCAN_ClkSrcOsc as shown in Figure 10. Figure 10. CANCLK selection Next step is selecting the PRESDIV value for nominal phase and FPRESDIV for FD phase. You have to select the right value to achieve the TQ needed to obtain the configured baudrate. For this example, let's set FPRESDIV value to 0 and PRESDIV value to 3. TQ calculation for nominal phase: TQ = (PRESDIV + 1) / CANCLK = (3 + 1) / 16000000 = 0.00000025 TQ calculation for FD phase: TQ = (FPRESDIV + 1) / CANCLK = (0 + 1) / 16000000 = 0.0000000625 The bit rate, which defines the rate of CAN message is given by formula shown in Figure 11 taken from KW36 Reference Manual. Figure 11. CAN Bit Time and Bit Rate Formulas With this info and with our TQ calculated, we can deduce that we need: For Nominal phase: 8 = Number of Time Quanta in 1 bit time For FD phase: 5 = Number of Time Quanta in 1 bit time Now, let's define the value of segments. For nominal phase: Bit Time =  (number of Tq in 1 bit time) x Tq CAN Bit Time = (1 + (PROPSEG + PSEG1 + 2) + (PSEG2 + 1) ) x Tq CAN Bit Time = (1 + (1 + 2  + 2) + (1 + 1) ) x Tq = 8 x 0.00000025 =  Baud rate = 1/ CAN Bit Time = 500KHz For FD phase: CAN Bit Time = (number of Tq in 1 bit time) x Tq CAN Bit Time = (1 + (FPROPSEG + FPSEG1 + 1) + (FPSEG2 + 1) ) x Tq CAN Bit Time = (1 + (0 + 1 + 1) + (1 + 1) ) x Tq = 5 x Tq =  0.0000003125 Bit Rate = 1/CAN Bit Time = 1 / 0.0000003125 =  3.2MHz To finish, just update the calculated values on your firmware on flexcanConfig.timingConfig structure.  Notes: FRDM-KW36 Software Development Kit (SDK) can be downloaded from MCUXpresso webpage. FlexCAN driver examples are located in path: "SDK_2.2.0_FRDM-KW36\boards\frdmkw36\driver_examples" from your downloaded FRDM-KW36 SDK. Take in consideration that not all the baud rates are achievables and will depend on the flexcan clock and segment values used.
查看全文