Based on i.MX8MN-EVK And Linux 5.4.70_2.3.0 BSP 
 As an example of NXP Bluetooth Bluetooth application, this article describes how to use  Bluetooth to realize file transfer between windows PC and i.MX8MN-EVK (linux), and between  Android mobile phone and i.MX8MN-EVK.  The test architecture used in this example is as follows: 
   
 The following steps are for the application example: 
 Step 1 Preparation  
  --Downloading DEMO Image For i.MX8MN-EVK   --Downloading uuu tool   --Compiling L5.4.70_2.3.0 BSP for i.MX8MN-EVK   --Copying rootfs to the DEMO Image directory   --Modifying example_kernel_emmc.uuu as uuu programming script   --Programming images to i.MX8MN-EVK board   Booting i.MX8MN-EVK board 
 Step 2 Loading WIFI/BT driver and Enable Bluetooth  Step 3 File Transter between Windows 10 PC and i.MX8MN-EVK board  Step 4 File Transter between Android Mobile and i.MX8MN-EVK board  [Summary] 
 More detailed information, see attachment, please! 
 
        
        查看全文