Vybrid Linux BSP Support for eMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid Linux BSP Support for eMMC

跳至解决方案
4,369 次查看
almagest
Contributor III

Hello.

We wish to use eMMC with the Vybrid.Does the linux BSP(s) from Timesys Support support eMMC memory technologies currently?

From different forum posts, it seems a bit unclear if this support is in place or not.

Please clarify.

MQX does not support this in their BSP;

Vybrid, eMMC, MQX

TimeSys has commented a similar request at an earlier stage

How to use both sdhc0 and sdhc1?

I.Mx Sabre Board with Linux seems to support this

Booting Linux from eMMC

Thanks!

Regards

Andreas Eknes Lie

标签 (3)
1 解答
4,105 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,106 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
4,107 次查看
timesyssupport
Senior Contributor II

Hi Andreas,

While there is support for some eMMC devices in the 3.13 Linux kernel in the Timesys BSP, this support is not specifically enabled for the Vybrid platform. At a minimum, supporting this would require modifying the kernel configuration and device tree source.

Thanks,

Timesys Support