Vybrid Linux BSP Support for eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid Linux BSP Support for eMMC

ソリューションへジャンプ
4,332件の閲覧回数
almagest
Contributor III

Hello.

We wish to use eMMC with the Vybrid.Does the linux BSP(s) from Timesys Support support eMMC memory technologies currently?

From different forum posts, it seems a bit unclear if this support is in place or not.

Please clarify.

MQX does not support this in their BSP;

Vybrid, eMMC, MQX

TimeSys has commented a similar request at an earlier stage

How to use both sdhc0 and sdhc1?

I.Mx Sabre Board with Linux seems to support this

Booting Linux from eMMC

Thanks!

Regards

Andreas Eknes Lie

ラベル(3)
1 解決策
4,068件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,069件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
4,070件の閲覧回数
timesyssupport
Senior Contributor II

Hi Andreas,

While there is support for some eMMC devices in the 3.13 Linux kernel in the Timesys BSP, this support is not specifically enabled for the Vybrid platform. At a minimum, supporting this would require modifying the kernel configuration and device tree source.

Thanks,

Timesys Support