Vybrid Linux BSP Support for eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid Linux BSP Support for eMMC

Jump to solution
4,367 Views
almagest
Contributor III

Hello.

We wish to use eMMC with the Vybrid.Does the linux BSP(s) from Timesys Support support eMMC memory technologies currently?

From different forum posts, it seems a bit unclear if this support is in place or not.

Please clarify.

MQX does not support this in their BSP;

Vybrid, eMMC, MQX

TimeSys has commented a similar request at an earlier stage

How to use both sdhc0 and sdhc1?

I.Mx Sabre Board with Linux seems to support this

Booting Linux from eMMC

Thanks!

Regards

Andreas Eknes Lie

Labels (3)
1 Solution
4,103 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
4,104 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
4,105 Views
timesyssupport
Senior Contributor II

Hi Andreas,

While there is support for some eMMC devices in the 3.13 Linux kernel in the Timesys BSP, this support is not specifically enabled for the Vybrid platform. At a minimum, supporting this would require modifying the kernel configuration and device tree source.

Thanks,

Timesys Support