MVF51NN151CMK50/Current consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MVF51NN151CMK50/Current consumption

ソリューションへジャンプ
1,464件の閲覧回数
soichiyamamoto
Contributor V

Hi

I want to use MVF61NN151CMK50 by a substitute of MVF51NN151CMK50.


Please give me DataSheet/Current consumption of MVF51NN151CMK50.


Is the Current consumption of MVF51NN151CMK50 same as MVF61NN151CMK50 ?


Best Reagrds,

soichi yamamoto


ラベル(1)
0 件の賞賛
返信
1 解決策
1,312件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

Formally speaking, power consumption depends on the number of blocks involved in the application.

If these 2 chips are used in the same application (i.e. with the same blocks enabled), their power consumption figures do not differ.

Regards, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,313件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

Formally speaking, power consumption depends on the number of blocks involved in the application.

If these 2 chips are used in the same application (i.e. with the same blocks enabled), their power consumption figures do not differ.

Regards, Naoum Gitnik.

0 件の賞賛
返信