MVF51NN151CMK50/Current consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MVF51NN151CMK50/Current consumption

Jump to solution
1,482 Views
soichiyamamoto
Contributor V

Hi

I want to use MVF61NN151CMK50 by a substitute of MVF51NN151CMK50.


Please give me DataSheet/Current consumption of MVF51NN151CMK50.


Is the Current consumption of MVF51NN151CMK50 same as MVF61NN151CMK50 ?


Best Reagrds,

soichi yamamoto


Labels (1)
0 Kudos
Reply
1 Solution
1,330 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

Formally speaking, power consumption depends on the number of blocks involved in the application.

If these 2 chips are used in the same application (i.e. with the same blocks enabled), their power consumption figures do not differ.

Regards, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
1 Reply
1,331 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

Formally speaking, power consumption depends on the number of blocks involved in the application.

If these 2 chips are used in the same application (i.e. with the same blocks enabled), their power consumption figures do not differ.

Regards, Naoum Gitnik.

0 Kudos
Reply