MVF51NN151CMK50/Current consumption

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MVF51NN151CMK50/Current consumption

跳至解决方案
1,467 次查看
soichiyamamoto
Contributor V

Hi

I want to use MVF61NN151CMK50 by a substitute of MVF51NN151CMK50.


Please give me DataSheet/Current consumption of MVF51NN151CMK50.


Is the Current consumption of MVF51NN151CMK50 same as MVF61NN151CMK50 ?


Best Reagrds,

soichi yamamoto


标签 (1)
0 项奖励
回复
1 解答
1,315 次查看
naoumgitnik
Senior Contributor V

Dear Soichi,

Formally speaking, power consumption depends on the number of blocks involved in the application.

If these 2 chips are used in the same application (i.e. with the same blocks enabled), their power consumption figures do not differ.

Regards, Naoum Gitnik.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,316 次查看
naoumgitnik
Senior Contributor V

Dear Soichi,

Formally speaking, power consumption depends on the number of blocks involved in the application.

If these 2 chips are used in the same application (i.e. with the same blocks enabled), their power consumption figures do not differ.

Regards, Naoum Gitnik.

0 项奖励
回复