1. Overview
This article is the umbrella entry point for a series of automotive embedded workshops built on the FRDM-A-S32K3xx microcontroller family. It groups together five hands-on modules — Lights, Brakes, Steering, Comfort, and Transmission — each demonstrating a different real-world automotive function that a modern Body Control Module (BCM), Chassis ECU, or Powertrain ECU would implement in production vehicles.
All five modules share the same educational philosophy: they take a simple, low-risk hardware setup (FRDM board + FRDM-K64 Click Shield + a few MikroE Click modules) and use it to teach the core embedded concepts that underlie automotive software: analog and digital signal acquisition, real-time processing, actuator control, and safety-aware system design. Together they cover the most common peripherals of the S32K3 family — ADC, GPIO, PWM, FlexIO, LPI2C, eMIOS — and expose students to the same tool-chain used by NXP customers: S32 Design Studio 3.6.5, the S32K3 Real-Time Drivers (RTD), the Application Code Hub (ACH), and the underlying Automotive Software Package.
Learning philosophy — Eat-Sleep-Code-Repeat
The whole workshop series is designed around the Eat-Sleep-Code-Repeat initiative — a learn-by-doing culture where students continuously iterate on real hardware, break things, fix them, refactor, and re-flash until the concepts stick. Every module is small enough to be completed in one lab session, yet rich enough to leave room for extensions (state machines, filtering, CAN networking, closed-loop control, safety fall-backs).
Concepts covered across the series
Analog sensing: potentiometers, force sensors, resistor-ladder buttons → ADC conversion, scaling, debouncing.
Digital I/O: GPIO input handling (buttons, switches), GPIO output sequencing (stepper coils).
Actuation: PWM-based motor speed control (DC motors, fans), PWM-based servo positioning, WS2812 LED driving through FlexIO.
Communication: I²C configuration of external PWM drivers (Servo Click / PCA9685).
Control patterns: continuous mapping, threshold-based decisions, state machines, safety interlocks.
Automotive concepts: Body Control Module (BCM) behavior, functional safety (ISO 26262), fail-safe defaults, redundancy considerations.
What this article gives you
Each of the next five sections provides a short summary of one module — what it demonstrates, which hardware it uses, which peripherals are involved, and a direct link to the full detailed workshop article. Students should read this page first to understand where each module fits in the bigger picture, then dive into the individual articles for step-by-step instructions.
2. Vehicle Lighting Control
The Lights module implements a simplified automotive lighting system that mirrors the behavior of a real vehicle Body Control Module. Six buttons on the Analog Key Click command different lighting functions — low beam, high beam, left/right turn signals, brake lights, and hazard lights — all displayed in real time on a 16-LED 4x4 RGB Click matrix.
Key learning points
Multi-button decoding on a single ADC channel (resistor-ladder input).
Software debouncing and command decoding.
Driving WS2812 LEDs through FlexIO (precise sub-microsecond timing without CPU load).
BCM safety interlocks: high beam requires low beam ON; hazards synchronize left + right turn signals; high beam state preserved between blink cycles.
Peripherals used: ADC0, FlexIO, GPIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference project:Automotive Lighting Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community
Vehicle Lighting Control demo on FRDM-A-S32K344
Demo: Vehicle Lighting Control on FRDM-A-S32K344
Automotive relevance: lighting is one of the most safety-critical driver-visibility functions in modern vehicles — this module teaches how a real BCM manages dependencies, blinking patterns, and fail-safe defaults.
3. Brake Status Monitoring
The Brakes module implements a simplified brake status monitoring system where a Force Click sensor simulates the driver's brake-pedal pressure. As pressure increases, the ADC value grows and the application progressively lights up the 4x4 RGB Click LEDs in green → yellow → orange → red, providing immediate visual feedback of the current braking level.
Key learning points
Continuous analog sensor acquisition through ADC.
Threshold-based decision logic: converting a raw ADC value into discrete alert levels.
Driving the RGB LED matrix through FlexIO to reflect the current system state.
Introduction to real-time monitoring and safety-oriented visual feedback.
Peripherals used: ADC0, FlexIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference project: Automotive Brake Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community
Brake Status Monitoring demo on FRDM-A-S32K344
Demo: Brake Status Monitoring on FRDM-A-S32K344
Automotive relevance: brake status is a core input for many downstream ECUs (ABS, ESC, hill-hold, brake lights). This module teaches the fundamental pattern of sensor → threshold → visual/electrical output that appears everywhere in automotive software.
4. Assisted Steering Control
The Steering module demonstrates a simplified Electric Power Steering (EPS) / steer-by-wire concept. A POT Click potentiometer simulates the steering-wheel angle; the MCU reads it through ADC, scales it linearly, and generates a PWM command through the Servo Click (configured over I²C) that positions a Micro Servo SG 180° in real time.
Key learning points
Analog input scaling and linear mapping (ADC range → servo angle range).
Using an external PWM controller configured over I²C (LPI2C1) — a common embedded pattern that offloads timing-critical work.
Working with the Output Enable (OE) pin for safe-stop behavior.
Understanding the actuation chain sensor → MCU → PWM → actuator.
Peripherals used: ADC0, LPI2C1, GPIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference projects: Automotive Steering Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community
PWM-Based Steering Control demo on FRDM-A-S32K344
Demo: PWM-Based Steering Control on FRDM-A-S32K344
Automotive relevance: steering is a strictly safety-relevant function (ISO 26262 typically classifies it as ASIL C or D). This module introduces the concepts behind EPS and steer-by-wire and lays the foundation for future work with redundant sensors and fault detection.
5. Vehicle Comfort Control
The Comfort module implements two independent comfort functions typical of vehicle body electronics: cabin cooling (a 5 V fan driven through a DC Motor 2 Click using PWM) and electric window control (a NEMA17 stepper motor driven through an H-Bridge Click using full-step GPIO sequencing). On-board push-buttons act as the driver's HVAC and window switches.
Key learning points
PWM motor speed control (fan simulation).
Stepper motor full-step sequencing (A → B → C → D and reverse) through four GPIO outputs.
Handling multiple independent actuators from a single MCU without blocking.
Introduction to window anti-pinch and other real BCM safety concepts.
Peripherals used: GPIO, eMIOS (PWM). Boards: FRDM-A-S32K344 (only). Reference project: Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers - NXP Community
Vehicle Comfort Control demo on FRDM-A-S32K344
Demo: Vehicle Comfort Control on FRDM-A-S32K344
Automotive relevance: comfort systems (HVAC, windows, mirrors, seats) form a huge share of modern body electronics. This module shows how one ECU can coordinate multiple actuators of different types (rotational-speed and positional) using the same S32K3 platform.
6. Transmission Control
The Transmission module demonstrates a continuous, proportional transmission control concept. A POT Click potentiometer represents the driver's acceleration command; the MCU samples it, applies linear scaling, and simultaneously drives two actuators: a Servo Click + Micro Servo that simulates the transmission selector position, and a DC Motor 2 Click + DC motor whose speed reflects the powertrain response.
Key learning points
Dual-actuator control from a single analog input (one MCU commands both servo angle and DC motor speed in parallel).
Linear signal mapping to two different PWM ranges simultaneously.
Combining I²C-configured PWM (Servo Click) and eMIOS-generated PWM (DC Motor 2 Click) in the same application.
Understanding continuous vs. discrete control and how continuous mapping better mirrors real automotive behavior.
Peripherals used: ADC0, LPI2C1, eMIOS. Boards: FRDM-A-S32K344 (only). Reference project: Automotive Transmission Control Using FRDM-A-S32K344 Microcontrollers - NXP Community
Transmission Control demo on FRDM-A-S32K344
Demo: Transmission Control on FRDM-A-S32K344
Automotive relevance: transmission control is part of the powertrain domain and requires deterministic response and safety-aware design. This module introduces the concepts and prepares students for more advanced topics such as closed-loop control, transmission-mode logic (P/R/N/D), and CAN networking with the engine ECU.
7. Conclusion
Together, these five modules give students a complete tour of what a modern Body Control Module, Chassis ECU, and Powertrain ECU actually do in a vehicle — from reading sensors and buttons, through processing and safety interlocks, to driving lights, motors, and actuators. Each module can be studied independently, but the real value emerges when they are viewed as pieces of one coherent picture: the same MCU family (S32K3), the same tool-chain (S32 Design Studio + Application Code Hub), the same hardware base (FRDM-A-S32Kxxx + FRDM-K64 Click Shield + MikroE Click modules), applied to five different automotive domains.
The series is intentionally aligned with the Eat-Sleep-Code-Repeat philosophy: start with a working example, then experiment — add filtering, replace polling with interrupts, introduce a state machine, add CAN communication, or refactor for functional safety. Every extension is a step closer to the way production automotive software is actually written.
Recommended learning path:
Lights — simplest, teaches ADC, FlexIO and BCM logic.
Brakes — introduces continuous sensor thresholds.
Steering — adds I²C-controlled PWM and actuator positioning.
Comfort — multi-actuator, dual-technology control (PWM + stepper).
Transmission — combines everything into a proportional, dual-actuator system.
If you have questions, suggestions for improvement, or ideas for new modules that could extend this series, please leave a comment below — feedback from students and instructors is what keeps the workshops relevant and up to date.
View full article