ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
Video on YouTube done by the University of Applied Sciences of Munich about the Freescale Cup event held on March 18th Freescale Cup 2014 an der Hochschule München - YouTube
記事全体を表示
Most embedded systems must operate continuously without any user input, even if something goes wrong. Most of us have experienced having our desktop or laptop computer locking up and requiring a reboot of the system to get it working again. We simply cannot afford to do this in an embedded system. Ideally, we would write our software so that it never crashes or fails. This, as you can guess, is really hard to do and so our microcontroller manufacturer has included a hardware feature called the Computer Operating Properly, or COP, reset generator. If this hardware feature does not receive a confirmation signal that our program is running properly, it will generate a reset to restart our program from the beginning or from a restart place that we can choose. The COP is also called a watchdog timer.  The COP reset circuitry guards against our program not working properly by expecting the program to execute a particular sequence of instructions at some interval. If the COP does not receive this sequence before it times out, it generates a reset by pulling the RESET_L signal low. This can reset all peripherals connected to the reset line. The CPU then fetches a COP reset vector to restart the program again. Thus the COP is treated like other interrupts except that it cannot be masked once the COP timer has been started. Often you would like to restart at the beginning of your program but in some situations you may choose to enter some diagnostic routine, such as updating a counter that counts the number of COP restarts that have occurred or lighting an LED, before restarting the program. You may also wish to leave some debugging breadcrumbs to help you understand why the COP is resetting the program.
記事全体を表示
Connection Diagram for TRK-MPC5604B to Rev. 1 Motor Control "Shield" Board Connection Diagram for TRK-MPC5604B to Rev. 0 Motor Control Board For the TRK-MPC5604, connect the flat ribbon cable to PortB as seen in the picture below. Make the cable connections as shown below for dual motor with independent drive connection Make the cable connections as shown below for dual motor with series drive connection Make the cable connections as shown below for Single motor connection Protect your electronics 1. Try not to stop the wheels while in motion.  This can cause current spikes. 2. Don’t disconnect or connect any cable when board is powered [ON]. 3. Don’t discharge the battery below 5.5V 4. Don’t hit stationary objects
記事全体を表示
How does a DC Motor work? The DC motor is a machine that transforms electric energy into mechanical energy in form of rotation. Its movement is produced by the physical behavior of electromagnetism. DC motors have inductors inside, which produce the magnetic field used to generate movement. But how does this magnetic field changes if DC current is being used? An electromagnet, which is a piece of iron wrapped with a wire coil that has voltage applied in its terminals. If two fixed magnets are added in both sides of this electromagnet, the repulsive and attractive forces will produce a torque. Then, there are two problems to solve: feeding the current to the rotating electromagnet without the wires getting twisted, and changing the direction of the current at the appropriate time. Both of these problems are solved using two devices: a split-ring commutator, and a pair of brushes. As it can be seen, the commutator has two segments which are connected to each terminal of the electromagnet, besides the two arrows are the brushes which apply electric current to the rotary electromagnet. In real DC motors it can be found three slots instead of two and two brushes. This way, as the electromagnet is moving its polarity is changing and the shaft may keep rotating. Even if it is simple and sounds that it will work great there are some issues which make these motors energy inefficient and mechanically unstable, the principal problem is due to the timing between each polarity inversion. Since polarity in the electromagnet is changed mechanically, at some velocities polarity is changing too soon, which result in reverse impulses and sometimes in changing too late, generating instantaneous “stops” in rotation. Whatever the case, these issues produce current peaks and mechanical instability. How a DC motor can be controlled? DC motors have only two terminals. If you apply a voltage to these terminals the motor will run, if you invert the terminals position the motor will change its direction. If the motor is running and you suddenly disconnect both terminals the motor will keep rotating but slowing down until stopping. Finally if the motor is running and you suddenly short-circuit both terminals the motor will stop. So there is not a third wire to control a DC motor, but knowing the previous behaviors it can be designed a way to control it, and the solution is an H-bridge. Look at the last evolution of the DC Motor above, you can observe that there are four gates and a motor connected between them. This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below. Things to Consider When Using Motors With the Motor and Line scan Camera hooked up to the same board there is a significant problem with noise. The higher you turn the PWM on your drive motors the noise produced and the worse the data will appear from the camera. TO significantly reduce this noise you can simply solder an inductor directly across the 2 drive motors. This will allow you to increase the speed of the car without significantly affecting the data you receive back from the camera.
記事全体を表示
Kinetis Header Part 1 of 2
記事全体を表示
Overview This document has links to videos to give tutorials on how to getting started *from scratch* with the freedom board.    In these tutorials we build projects with bare metal code to see how things work!   It includes the basics on how to get clocks running,  lights blinking and interrupts firing *from scratch*. For more code/peripheral examples that use a "bare metal" approach,  check out the page on the FRDM-TFC board. ERRATA!!!   While working with a large number of Freedom boards in a course,  it was observed that the InitClockRoutines would *sometimes* not work.    *Some* of the crystals on the freedom boards do NOT like "HIGH_GAIN" mode.   The new code is uploaded to this page but you could also change the code yourself:   pll_init(8000000, HIGH_GAIN, CRYSTAL, 4, 24, MCGOUT); to   pll_init(8000000, LOW_POWER, CRYSTAL, 4, 24, MCGOUT); Projects From Scratch for the Freedom Board with Codewarrior 10.3 Projects From Scratch - Part 2 - Importing other projects Using the Freescale Header Files and Blinking the LED Source code for video (Codewarrior 10.3) is in the attached files at the bottom of this document. Clock Distribution Source Code for the Clock Distribution video is in the attached files at the bottom of this document. Interrupts Part 1 - Background Interrupts Part 2 - ARM Systick Timer Source Code for the ARM Systick Timer video is in the attached files at the bottom of this document. Interrupts Part 3 - TPM (Timer Pulse Width Modulator) Overflow Source Code for the TPM Overflow Interrupts video is in the attached files at the bottom of this document
記事全体を表示
Overview An H-Bridge circuit has a control circuit, usually PWM, which then determines the switching of high-voltage supply to drive a current. Typical embedded H-Bridges can drive about 5A of current. In the case, of the Freescale Cup car the motors can sustain much more current resulting in more toque and faster speeds. Performance Tuning Tips 1. You can place H-Bridges in parallel to balance the current load. For example, if you place two 5A (peak) H-Bridge outputs in parallel, the system can support up to 10A current. 2. Keep it Cool. H-Bridge's dissipate A LOT of heat. Heat = increases inefficiency of a semiconductor, so the better job you do keeping it cool, the better (and longer) it will work for you. Operation Theory This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below. H-Bridge States
記事全体を表示
The Kwikstik board is a great board for use in a Freescale Cup car! This page has some videos and example code to get you up and running quickly. For novice embedded developers it is recommended you use the FRDM-KL25Z for your Freescale Cup car. Board Tips The General Purpose TWRPI socket on the Kwikstik K40 board provides access to I2C, SPI, IRQs, GPIOs, timers, analog conversion signals, TWRPI ID signals, reset, and voltage supplies. The pinout for the TWRPI Socket is defined in Kwikstik User's Manual, but the user manual does not describe how to order a connector. Soldering and directly connecting to the pins on the socket itself is very risky and not recommended. When browsing for connectors that interface with the TWRPI sockets you have two main options. 1. The first is a surface mount chip, that is a female connector to connect with the male pins on the board. There are surface mount lead on the top of the chip which will be easier to solder to. The part number is: SFC-110-T2-L-D-A 2. The second option is a female connector which mates with the male connection on the board and is then terminated with a wire for each pin. This option can greatly simplify your wiring challenges on your car as any additional lengths or wires can easily be trimmed off. The part number is: SFSD-10-28-G-12.00-S Image of the SFSD-10-28-G-12.00-S with corresponding Kwikstik TWRPI socket. Connectors can be ordered from Samtec as samples at this website: [http://www.samtec.com/suddenservice/samples/samples.aspx] Useful Videos:   Creating a new baremetal project for a Freescale KwikStik http://www.youtube.com/watch?v=P8X079Qs7cg&feature=g-upl&context=G2f166b6AUAAAAAAADAA   Debugging a bare metal project on the Freescale Kwikstik. http://www.youtube.com/watch?v=nQhhfNJZL_o&feature=g-upl&context=G2dcfcd5AUAAAAAAAEAA   Importing projects and merging code. http://www.youtube.com/watch?v=A_h9W-QRHp8&feature=g-upl&context=G2354416AUAAAAAAACAA   A discussion of the header files (and how to use them!) for Kinetis Devices in Codewarrior V10. This is the first of 2 videos. I had to split them up as I cannot upload videos greater than 15 minutes in length. http://www.youtube.com/watch?v=EP2FydCX9tY&feature=g-upl&context=G2fdf3fcAUAAAAAAABAA   Second part of the Kinetis Header file discussion http://www.youtube.com/watch?v=ygjx-OkJuS4&feature=g-upl&context=G2792e97AUAAAAAAAAAA   Discussion on getting the Clock setup on the Kwikstik http://www.youtube.com/watch?v=_FQzXhLDP2w&feature=youtu.be   How to setup GPIO on the Kinetis. Includes discussion on enabled clocks to peripherals and setting up the pin control registers. http://www.youtube.com/watch?v=GXjRpsGJJt4&feature=youtu.be   How to use the SysTick peripheral in the Cortex core with interrupts http://youtu.be/8SRqlDkJwGU   Discussion of how to setup interrupts on the NVIC. The Flex timer is used as an example http://www.youtube.com/watch?v=_mClHzxm0Wk&feature=youtu.be   Example Programs: All of the programs are bare metal examples for CodeWarrior 10.1 that can be used on the Kwikstik board. Make sure to read all of the comments in the C files! How to Load Programs In CodeWarrior: Copy only the source files and header files into a new folder. Import that new folder into CodeWarrior to avoid debug problems.   ClockSetup - Systick This example will demonstrates how to enable the 4MHz Crystal on the Kwikstik. Early versions of the Kinetis silicon had bug in which the device could crash if the clock dividers are changed while executing from FLASH (errata e2448). This code places clock initialization code in RAM. The clock code is based upon routines from Kinetis Peripheral Module Quick Reference (Freescale document KQRUG.pdf). It also shows how to enable the SysTick module in the Cortex Core. The SysTick is used to provide a delay Function. ClockSetup - SysTick.zip     FlexTimer_NVIC_IRQ This code shows how to use the NVIC in the Cortex Core. The Flex Timer module is used to generate a periodic interrupt (similar to the SysTick example). FlexTimer_NVIC_IRQ.zip   LCD_Example This code will turn on segments on the LCD on the Kwikstik. The LCD driver code is derived from the MQX based example on the Kwikstik page. LCD_Example.zip   PWM_Test This code shows how to setup the flex timers to generate different styles of PWM. Note: One of the examples sets up the flex timer for pseudo-complementary PWM. It DOES NOT use the hardware based complementary mode. It writes 2 individual registers in a software routine. One should use this a starting point to enable full hardware based complementary mode. PWM_Test.zip   CameraTest This example is a basic example on how to interface to the Freescale Linescan Camera. It will display a rough approximation of the output on the LCD. CameraTest.zip Note: The code does not run with the camera by default. This is because the AOUT is set to the pin with the pull up resistor (J15 pin 4). Once changed it will work smoothly.
記事全体を表示
CW_NEW_PROJECT.wmv
記事全体を表示
Official rules of the USA Regional Freescale Cup! New in 2014 - Roll-out of leagues: Depending on region there will now be three leagues.  To advance to the Global race you must use stock league vehicles. Stock League - Race using approved components, less customization allowed Custom League - Race with less restrictions and custom hardware Innovation League - More than just racing.  Complete an objective or task to score points and win. (Scheduled 2015 for USA) Notes You can view this document in PDF format using the Action Menu bar. The Worldwide challenge is only open to the stock (unmodified) challengers at this time.  A team may run in both leagues, but the car must comply accordingly. If you have ANY questions about these rules, post them in the comments section below.  If you have questions about regional rules, ask in your regional group. Section 1: Team Requirements Four person maximum team size. A team may have only one graduate student. Cars will be designed and constructed by students ONLY. Participants, advisers, and audience are expected to exhibit good sportsmanship. Any inappropriate behavior or cheating may result in disqualification. Section 2: Event Registration One person from the team must register the entire team for the worldwide challenge no later than January 31st. Section 3a: STOCK LEAGUE - Equipment Requirements Each team shall use the same basic kit of parts as described below.  The following requirements are in place to keep the playing field level.  You must use one of the approved controller and motor driver boards.  If any standard component of the car model is damaged, then the same replacement component should be used. Mechanical The original and unaltered equipment must be used in the entry. Outer tire treads and rim Drive - DC motors Transmission Ratio of Drive Motor Servo Motor Allowed modifications and restrictions: You may not change the wheel base (distance between wheels) No part of the car shall exceed dimensions of 250mm/9.85in (W) x 400mm/15.75in (L)x 305mm/12in.(H) You may drill holes and mount auxiliary pieces on the chassis assuming it is contained within the above dimensions. You may change the orientation of the servo motor and related linkages. You may add a "skin" to the car but it must be removable during inspection. You may adjust or remove springs, linkages, and other non-essential pieces. You may adhere the tread to the rim.   Electrical Battery (purchase separately) 7.2V, <=3000mAh, rechargeable NiCd or NiMH Only one (1) battery at a time may be used to power the vehicle and any attached hardware You must use one of the approved boards below to control your car. Control System FRDM- series of boards The FRDM-KL25Z is included but not mandatory to use. TRK- series Kinetis based TWR- series High Voltage Motor Control and Interface TFC-SHIELD The TFC-SHIELD is included but not mandatory to use. The Dual Motor Control Board from Landzo technologies. Allowed modifications and restrictions: One processor - No auxiliary processor or other programmable device is allowed. The car must use a optical sensor to navigate DC-DC boost circuit may not exceed battery voltage. Total capacity of all capacitors should not exceed 2000 uF. Sensor Limits You may use additional cameras. Maximum of sixteen (16) sensors Examples of sensor count: IR Transmitter/Receiver pair is 1 sensor A CCD sensor is 1 sensor The provided Line Scan Camera is 1 sensor A hall effect sensor on two rear wheels is 2 sensors An encoder mounted on one wheel is 1 sensor A display (is allowed) does not count as a sensor Section 3b: CUSTOM LEAGUE - Equipment Requirements The custom league allows for greater customization of the vehicle.  There is still a set of standard components that must be used.  If any of the standard component of the car model is damaged, then the same replacement component should be used. Mechanical The original and unaltered equipment must be used in the entry. Outer tire treads and rim Drive - DC motors Transmission Ratio of Drive Motor Servo Motor Allowed modifications and restrictions: You may not change the wheel base (distance between wheels) No part of the car shall exceed dimensions of 250mm/9.85in (W) x 400mm/15.75in (L)x 305mm/12in.(H) You may drill holes and mount auxiliary pieces on the chassis assuming it is contained within the above dimensions. You may change the orientation of the servo motor and related linkages. You may add a "skin" to the car but it must be removable during inspection. You may adjust or remove springs, linkages, and other non-essential pieces. You may adhere the tread to the rim.   Electrical Battery (purchase separately) 7.2V, <=3000mAh, rechargeable NiCd or NiMH Only one (1) battery at a time may be used to power the vehicle and any attached hardware Allowed modifications and restrictions: One Freescale processor to control everything- No auxiliary processor or other programmable device is allowed. You may build your own controller board and/or high-voltage (motor) driver board. The car must use a optical sensor to navigate DC-DC boost circuit may not exceed 12V. Total capacity of all capacitors should not exceed 2000 uF. Sensor Limits You may use additional cameras. Maximum of sixteen (16) sensors Examples of sensor count: IR Transmitter/Receiver pair is 1 sensor A CCD sensor is 1 sensor The provided Line Scan Camera is 1 sensor A hall effect sensor on two rear wheels is 2 sensors An encoder mounted on one wheel is 1 sensor A display (is allowed) does not count as a sensor Section 4: Vehicle Inspection Before the race, the judges will perform a technical inspection of all entries. This includes vehicle specifications, dimensions, and equipment requirements listed in Section 3. All cars must be placed in the Inspection area on or before the designated time. Once in the Inspection Area, you may not touch car until you are called to race! In the event of any violations, the organizing committee may disqualify the corresponding team. Section 5: Timed Race Procedure Race order will be determined by a random drawing. When your team is called you may remove your car  from inspection area.  You will have two (2) minutes to prepare the car. Approved Adjustments - You may: Configure parameters via on-board interfaces. (Switches, Knobs, etc.) Alter the angle of your camera Change batteries Disallowed Adjustments -You may not: Reprogram your processor Configure parameters via wired or wireless communications. There shall be only one team member on the track at any given time. (excludes testing times) Before the 2 minute expires you must signal “Ready” to the referee before starting car. After the referee confirms “Ready”, the vehicle should leave the starting area within 30 seconds. Teams have THREE attempts to complete ONE lap.  The FIRST (not the best) completed time will be recorded. Example: Attempt 1 – Vehicle goes to fast around a curve and goes off track.  Time is not recorded. Attempt 2 – Vehicle makes it around track successfully.  Time is recorded. Attempt 3 – Is forfeit because FIRST time (Attempt 2) has been recorded. After each attempt you have two minutes to make approved (see above) adjustments to vehicle. After the attempts, the team shall return the vehicle to inspection area. Event displays will post the times after each team races. Section 6: Race Day Schedule Practice Time - Prior to final race, a test track will be available. Final calibration may be made at this time.  This will be organized with team slots and/or “free-time”.   2. Reconfigure practice track to final track. Vehicle Inspection (see section 4) Timed Race Awards Ceremony Section 7: Event Personnel Organizing committee – A committee of senior judges and Freescale event organizers.  Will coordinate event day activities and mediate and resolve any disputes. Referees -  Responsible for on-track activities. This includes race track management such as starting and stopping vehicles, as well as timing and scorekeeping. Comprise up of of faculty, student, and/or Freescale and industry employees. Judges  - Interpret and enforce rule compliance.  This will be comprised of Freescale employees and members of contributing industry sponsors. Event Personnel shall not aid any one specific team. Communication shall be open to all teams and shall not disclose any information that might compromise the fairness of the competition. Section 8: Fouls, Failure and Disqualifications The rules will be interpreted by Freescale and the organizing committee of the event.            Foul, is a minor infraction, which results in time penalties. Failure, results in the current attempt time not being recorded. Subsequent attempts are allowed. Disqualification is a major infraction which results all times not being recorded. Referee will determine whether the racing car ran out of the race track and assign time penalties. Any of the following conditions will be considered a foul and will result in time penalty added: The race car fails to leave the starting area within 30 seconds after beginning of the race [+1 second]. The race car fails to stop 2 meters/6 feet or leaves the track after crossing the finish line [+1 second]. Any of the following conditions will be considered a failure and no time will be given: Three or more wheels leave the race surface. The racing team fails to get prepared for the attempt within the two (2) minutes allotment. The player touches the race car after the technical inspection without consent of the referee. The race car fails to finish within 120 seconds after leaving the starting area. Touching the car at any time between start and finish. "Start" - Once the vehicle crosses the starting line. "Finish" - Once the vehicle crosses the finish line. Any of the following conditions will be considered a disqualification:   Any off track equipment or behavior that may influence or impede cars.   Doing a Disallowed Modification anytime after Inspection. More than one team member in the playing field. Any cheating during the competition. Failure to pass the technical inspection. Equality and fairness will be ensured as much as possible on the condition of actual feasibility.  Disputes will be resolved by a vote of Freescale, members of the organizing committee, and judges. Section 9: Timing/Scoring Time will be captured using an electronic gate and/or handheld timer. Time starts and ends when the first part of the racing car breaks the start/finish line. Fouls will result in the time addition to the car’s lap time. Disqualifications and Failures will result in no score. Section 10: Parameters of the Racing Track A test track made from the same material as the final track will be made available on the day prior to the final race for calibration and design modifications. The actual layout of the final racing track will be unknown to competitors until competition day. Width of the racing track shall not be less than 600mm/24in. Material and dimensional specifications can be found on the community. Surface of the racing track is matte white, with a continuous black line (25mm/1in wide) in the center of the track. The racing track can intersect with a crossing angle of 90°. The racing track can have inclines, declines,  and tunnels. The rules and conditions are subject to change by Freescale if necessary. Freescale reserves the right in their sole discretion to cancel, suspend and/or modify The Freescale Cup race at any time. These official rules are drawn up in the English language. If these official rules are provided in any other language and there is a conflict in the text, the English language text shall prevail. Freescale and the Freescale logo are trademarks or registered trademarks of Freescale Semiconductor, Inc. in the U.S. and other countries. All other product or service names are the property of their respective owners. © Freescale Semiconductor, Inc. 2014
記事全体を表示
freescale cup India 2011 trials line follower
記事全体を表示
This tutorial covers the details of Driving a motor on the on the Kinetis K40 using the TWR-K40x256-KIT evaluation board. Overview In this exercise students will utilize the sample project to turn a motor on and off using the TWR-K40x256-KIT evaluation board. Students will: Put together the car chassis Create a Sample Project Build the code Download and run the code on a Kinetis TWR-K40x256 board. Learn how the code works   To successfully complete this exercise students will need the following board and development environment. Kinetis TWR-K40x256 board Motor Driver Board Freescale Cup Chassis with the Motors connected 7.2v Nicad Battery CodeWarrior for Microcontrollers Recommend completing the the Blink LED Tutorial before undertaking this Tutorial Put together the Car Chassis:   There are several steps in this process: Build the Freescale Cup Car Chassis Hardware Design Step Review the Driving A DC Motor Article If needed, obtain background information on motors, timer modules, PWM signals and counters by navigating to the driving a DC motor article. Design and Implement The Hardware 1. You will need to connect the Tower K40 to the Motor Board via the TWR-PROTO or some other mechanism. 2. You will need to connect the Motor Board to the DC motors and Battery This link shows a video of the motors spinning. They start from Off and slowly pick up speed http://www.youtube.com/watch?v=kY2bRiICzwc&feature=relmfu Motor Controller Board This board takes the low-voltage, low-power "control" signals from the MCU and through an H-Bridge takes ahigh-voltage, high-power power supply (the battery) to drive the motors. Motor Board page. 1. Be careful with the wires connected to the motor. Constant flexing of the solder connection can result in joint failure. If this happens, just re-solder it. 2. The wires which protrude from the motors of The Freescale Cup Chassis are in the format of Insulated Crimp On Bullet Connectors. These can be found at Radio Shack if they are missing from the kit. Build the Code If you have more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. Learning Step: Motor Code Description Functions Variables The edge-aligned mode is selected when (QUADEN = 0), (DECAPEN = 0), (COMBINE 0), (CPWMS = 0), and (MSnB = 1). The EPWM period is determined by (MOD − CNTIN + 0x0001) and the pulse width (duty cycle) is determined by (CnV − CNTIN). The CHnF bit is set and the channel (n) interrupt is generated (if CHnIE = 1) at the channel (n) match (FTM counter = CnV), that is, at the end of the pulse width. This type of PWM signal is called edge-aligned because the leading edges of all PWM signals are aligned with the beginning of the period, which is the same for all channels within an FTM. Initialize the Motor void InitMotorPWM()  {     //Enable the Clock to the FTM1 Module     SIM_SCGC6 |= SIM_SCGC6_FTM1_MASK;     // PORTC_PCR4 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;   //Enable GPIO on on the pin -     //route the output of that channel 0 to the pin... (pick a different multiplexer value for routing the timer)     //ch 11.4.1 of the k40 reference manual is the pin control register     //For port c pin 1..   bits 10-8  Pin Mux Control...     PORTA_PCR8  = PORT_PCR_MUX(3)  | PORT_PCR_DSE_MASK;     PORTA_PCR9  = PORT_PCR_MUX(3)  | PORT_PCR_DSE_MASK;     // Choose EDGE-Aligned PWM:  selected when QUADEN=0, DECAPEN=0, COMBINE=0, CPWMS=0, and MSnB=1  (page 964)     // Properly set up Flex Timer Module     //FTM0_MODE[WPDIS] = 1; //Disable Write Protection - enables changes to QUADEN, DECAPEN, etc.      FTM1_MODE |= FTM_MODE_WPDIS_MASK;     //FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0     FTM1_MODE &= ~1;      //Set Edge Aligned PWM     FTM1_QDCTRL &=~FTM_QDCTRL_QUADEN_MASK;      //QUADEN is Bit 1, Set Quadrature Decoder Mode (QUADEN) Enable to 0,   (disabled)     //FTM0_SC = 0x16; //Center Aligned PWM Select = 0, sets FTM Counter to operate in up counting mode,     //it is field 5 of FTMx_SC (status control) - also setting the pre-scale bits here   //   Also need to setup the FTM0C0SC channel control register  - Page 897   section 37.3.6   FTM1_CNT = 0x0; //FTM Counter Value - (initialize the CNT before writing to MOD)  (16 bit available - bits 0-15 are count)   FTM1_MOD = FTM1_MOD_VALUE; //Set the Modulo resister (16 bit available - bits 0-15), Mod is set to 24000   FTM1_CNTIN = 0; //Set the Counter Initial Value to 0   (pg 915)   //change MSnB = 1   FTM1_C0SC |= FTM_CnSC_ELSB_MASK;   FTM1_C0SC &= ~FTM_CnSC_ELSA_MASK;   FTM1_C0SC |= FTM_CnSC_MSB_MASK;   FTM1_C0V = FTM1_MOD_VALUE/2; //Set the Channel n Value to  (16 bit available - bits 0-15)   //Set the complimentary pinout   FTM1_C1SC |= FTM_CnSC_ELSB_MASK;   FTM1_C1SC &= ~FTM_CnSC_ELSA_MASK;   FTM1_C1SC |= FTM_CnSC_MSB_MASK;   FTM1_C1V = FTM1_MOD_VALUE/2;   FTM1_SC = FTM_SC_PS(0) | FTM_SC_CLKS(1);    // Interrupts   FTM1_SC |= FTM_SC_TOIE_MASK; //enable the interrupt mask   enable_irq(63);  // (79-16) Set NVIC location, but you still have to change/check NVIC file sysinit.c under Project Settings Folder } Set the PWM of the Motor void SetMotorPWM(float DutyCycle) {    //float compDuty = (float)100.0-DutyCycle;    FTM1_C0V =(int)((DutyCycle*.01)* (float)FTM1_MOD_VALUE);    FTM1_C1V =(int)((1.0-DutyCycle*.01)* (float)FTM1_MOD_VALUE); } Create Interrupt when motor functions are complete void MotorTick() { if (MotorTickVar < 0xff)//if motor tick less than 255 count up...    MotorTickVar++; //Clear the overflow mask if set    if(FTM1_SC & FTM_SC_TOF_MASK)    FTM1_SC &= ~FTM_SC_TOF_MASK;    //LED_E2_TOGGLE; // ends up being ___ Hz (correct) } Calling the Motor function The function SetMotorPWM(MotorPwm) turns the motor at the "MotorPwm" rate from 0-49 (backwards), 50 (stall) and 100 (forwards).
記事全体を表示
All information can be found in this document
記事全体を表示
TFC2015 UCDavis Team Young Tortoise Final Report Thanks for sharing Lance Halsted​
記事全体を表示
Project Summary Skills Developed: Materials: Step 0: Prerequisite Videos Step 1: Get a FRDM-JAM Step 2: Put it Together Step 3: Download Step 4: Hack and Slash! Sound Samples Utilities, etc: Project Summary MonkeyJam will use the FRDM-K20D50 board (which has a Cortex M4 core with DSP instructions) along with the FRDM-JAM shield so you can  make your very own guitar /bass  stomp box.  The end result will be a functional DSP system that will allow you to do high quality amplifier simulation and effects. The FRDM-JAM does not limit you to DSP on musical instruments!  There are 3.5mm stereo jacks to DSP filtering any type of audio signal.    You could even use the USB interface to create a USB-MIDI Synthesizer!  Lastly,  no need to bring the house down.....  a headphone amplifier circuit is provided so you can jam out without bothering the neighbors. MBED Support coming *very soon* Skills Developed: Real Time Processing DSP Algorithms Fixed Point Mathematics 24-bit I2S Data Converter Interfacing Soldering SOIC8 and 1206 Surface mount devices Cortex CMSIS DSP Library Materials: FRDM-K20D50 FRDM-JAM Development Tools Install Codewarrior 10.5 for Microcontrollers (Eclipse) Special Edition to your  machine Example Code Get the latest copy from Github Step 0: Prerequisite Videos The videos are organized into a nice YouTube playlist: H.I.T 1: Monkey Jam - YouTube https://www.youtube.com/playlist?list=PLWM8NW5LEukgM-D5eRMtKZ8R2WfXnqKGp MonkeyJam Watch Me 1st FRDM-JAM Hardware Overview MonkeyJam Software Overview Introduction to Fixed Point Math for Embedded Systems - Part 1 of 3 Introduction to Fixed Point Math for Embedded Systems - Part 2 of 3 Introduction to Fixed Point Math for Embedded Systems - Part 3 of 3 Real Time Signal Processing Part 1 of 3 Real Time Signal Processing Part 2 of 3 Real Time Signal Processing Part 3 of 3 q31_t (Q0.31) Number Format for the CMSIS DSP Libraries and the MonkeyJam Software Guitar physics in a nutshell Ideas for hacking the MonkeyJam Step 1: Get a FRDM-JAM MonkeyJam Build Package on the FRDM-JAM site.    Please let us know if you are interested in a pre-assembled version.  If there is enough demand we will get some preassembled for purchase, I will get a Kickstarter going!   Don't be afraid to build it yourself,  Soldering is fun!  There is plenty of good stuff on the web on how to do SMT soldering.  All of the parts on the board are fairly simply once you get the hang of it and everything can be hand soldered  The key is having some decent tools. Step 2: Put it Together Attach the FRDM-JAM to the FRDM-K20D50.  The FRDM-K20D50 comes with female headers that you can solder on so the boards can be easily separated.  Note that as of Rev Gamma (current version),   it is possible to connect to a K64F.    The software isn't quite there but it hardware connections are available.   If you are unsure,  stick with the FRDM-K20D50 Step 3: Download Download the Example Software from Github.  The video "Loading and Configuring the MonkeyJam Example Software" will step you though downloading the program and doing some basic configuration. Step 4: Hack and Slash! Plug In and jam! Sound Samples Each sound sample was my Carvin Ultra-V guitar plugged direct into the MonkeyJam Board.  The output was fed to a Zoom Handy Recorder H4n (Thanks to Brandin Claar of Remodulate LLC for the recorder).  The H4N recorded the signal at 44.1KHz Sample rate @16-bit.  The sound files were converted to mono format via Goldwave.  No processing (other than a  volume boost on the files) was performed.   I listen to the recording in real-time via a line out on the H4N.  File (See Attachments) Patch Notes STE-003-Neck-a12b12g12-mlike.wav PATCH_TUBEY_CLEAN Neck Pickup Alpha Pot - 12 O'Cock Beta Pot - 12 O'Cock Gamma Pot - 12 O'Cock Pattern Similar to Metallica Sanitarium STE-005-Neck-a7b5g5-mlike.wav PATCH_TUBEY_CLEAN Neck Pickup Alpha Pot - 7 O'Cock Beta Pot - 5 O'Cock Gamma Pot - 5 O'Cock Pattern Similar to Metallica Sanitarium STE-006-Neck-a12b7g5-mlike.wav PATCH_TUBEY_CLEAN Neck Pickup Alpha Pot - 12 O'Cock Beta Pot - 7 O'Cock Gamma Pot - 5 O'Cock Pattern Similar to Metallica Sanitarium STE-007-Neck-VariousSettings-d-g-em_strum.wav PATCH_TUBEY_CLEAN Neck Pickup The pots were moved around throughout the file Strummed D-Major, G-Major and E-Minor STE-008-Neck+Bridge-VariousSettings-d-g-em_strum.wav PATCH_TUBEY_CLEAN Neck + Bridge Pickup The pots were moved around throughout the file Strummed D-Major, G-Major and E-Minor STE-009-Bridge-VariousSettings-d-g-em_strum.wav PATCH_TUBEY_CLEAN Bridge + Bridge Pickup The pots were moved around throughout the file Strummed D-Major, G-Major and E-Minor STE-010-Neck-VariousSettings-Jammy.wav PATCH_TUBEY_CLEAN Neck + Bridge Pickup The pots were moved around throughout the file B-Minor Type Jam STE-011- Bridge - Various Settings - On-Off Demo-RandomDroppedD.wav PATCH_OVERDRIVE Bridge Pickup Alpha Pot - 5 O'Cock Beta Pot - 12 O'Cock Gamma Pot - 12 O'Cock Random Dropped D twiddling STE-012- Neck - Various Settings - On-Off Demo-Jammy.wav PATCH_OVERDRIVE Neck Pickup Alpha Pot - 5 O'Cock Beta Pot - 7 O'Cock Gamma Pot - 7 O'Cock Random B-Minor twiddles (bluesy) PATCH_OVERDRIVE             +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                               |                  |      |                          |      |                     |                    Signal In  |    IIR BiQuad    |      |      Hard Overdrive      |      |      IIR BiQuad     |  Signal Out       +–––––––––+>|                  +––––+>|                          +––––+>|                     +–––––––––––––+>                |   [Peaking EQ]   |      | [atan24pi Look Up Table] |      |  [Low Pass Filter]  |                               |                  |      |                          |      |                     |                               +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                                                                                                                                                     0.1 < Q < 1.5    [Pot Alpha]                                     Q = 0                                                                                                                                                              50 < Fs < 750    [Pot Gamma]                                   Fs = 2000                                                                                                                                                          -20 < dbGain < 20  [Pot Beta]                                                                                                                                                                                        PATCH_TUBEY_CLEAN              +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                               |                  |      |                          |      |                     |                    Signal In  |    IIR BiQuad    |      |      Soft Overdrive      |      |      IIR BiQuad     |  Signal Out       +–––––––––+>|                  +––––+>|                          +––––+>|                     +–––––––––––––+>                |     [LowShelf]   |      | [atan4pi Look Up Table]  |      |  [Low Pass Filter]  |                               |                  |      |                          |      |                     |                               +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                                                                                                                                                     0.05 < Q < 2.58   [Pot Alpha]                                     Q = 2.0                                                                                                                                                             1000 < Fs < 4000    [Pot Beta]                                   Fs = 2500                                                                                                                                                      -15 < dbGain < 15  [Pot Gamma]                                                                                                                                                                                    Utilities, etc: Biquad Filter View - A IIR Biquad Filter Design &amp; Visualization Tool
記事全体を表示
A Livecast has been set up for you to enjoy The Freescale Cup EMEA Finals on 28-29 April that are hosted at the Politecnico of Torino. Connect on Freescale Cup 2015 live streaming - SeLM - Politecnico di Torino
記事全体を表示
Summary   This page contains the technical information for the FRDM-OLED shield.    This includes the schematics, bill of materials (BOM),  gerber files and raw design files.   Main features: Newhaven NHD-2.7-12864UCY3 128x64 pixel graphic OLED Display Electret microphone interface with gain control RS-485 Interface for doing cool things like driving a DMX lighting system. General purpose I/O (I/O is shared with A/D pins so you could make your own scope!)       Example software, video tutorials tutorials, cool demos, etc are location on the page for MonkeyListen project page located here.     Notes:   You can order PCBs through OSHPark or your favorite board house.   There is a special .zip file with files ready to go for OSHPark  (using their preferred naming convention). There is a complete design package which has the raw design files (Altium Designer Format) as well as gerbers,  a bill of materials,  assembly plots etc.  Look in the "BUILD_PACKAGE" folder for the stuff needed to make the board. A PDF Schematic is also provided for easy reference.   If you are interested in a low cost pre-fabbed board or a fully assembled version,  please leave a comment.  A kickstarter project may follow to get a bunch built!
記事全体を表示