Car Body

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,334件の閲覧回数
thibaultferrant
Contributor I

Hello,

We want to participate this year in the Freescale Cup, and we were thinking about asking design students to make our Car Body , is it possible?

Freescale Cup Rules by Region

Section 2: Team Rules and Requirements

1. A team can either consist of all undergraduate students (minimum of 2;

maximum of 4) or can include 1 graduate student but must contain at least 2

undergraduate students on the team.

2. Cars will be designed and constructed by students ONLY.

Thanks

タグ(1)
0 件の賞賛
1 解決策
1,766件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

hi Thibault,

yes, you can ask design students to create a car body as long as you do not modify the footprint of the chassis, change the wheels or the spacing between the wheels. Just keep in mind that the body must be removed for the technical inspection and that the team has limited time during the race to access the systems or replace the battery

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,767件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

hi Thibault,

yes, you can ask design students to create a car body as long as you do not modify the footprint of the chassis, change the wheels or the spacing between the wheels. Just keep in mind that the body must be removed for the technical inspection and that the team has limited time during the race to access the systems or replace the battery

0 件の賞賛
1,766件の閲覧回数
thibaultferrant
Contributor I

Thanks for the answer, it will be easy to removed.

0 件の賞賛