Technology Days - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

Discussions

Sort by:
With over half a billion parts shipped to date, i.MX applications processors transform interactions in ways you never imagined. Learn about the i.MX portfolio and enablement that offer multicore solutions for multimedia and display applications with high-performance and low-power capabilities that are scalable, safe, and secure. 
View full article
The presenter explains the key principles for localizing objects and gives a description of the silicon IP that is included in the KW devices and supports localization. Algorithms such as RSSI, Time-of-Flight and AoA/AoD are clearly described and examples of implementation are provided through the delivery of test results obtained on devices such as the KW35 and KW36. Partnership with external companies is also mentioned so that support can be obtained companies having a long experience in his technical domain.
View full article
EUF-MHW-T1748 - This session will give an overview of the wearables for the IoT.
View full article
Built with a high-level integration to support graphics, video, image processing, vision, audio and voice functions, the i.MX 8 series is ideal for Automotive applications. Join this session to learn about the i.MX 8/8X families that are comprised of common subsystems establishing an unmatched range of cost-performance scaling with pin-compatible options and the highest level of software reuse.
View full article
A key challenge to the deployment of Edge compute IoT is management and security of 1000s to millions of Edge compute nodes and the software that is running on them. NXP’s EdgeScale technology simplifies this by providing a cloud-based management framework leveraging the hardware security features of NXP Layerscape and i.MX processors. This instructor-led session will demonstrate how to install AWS Greengrass and Azure IoT Edge software on NXP processors using the NXP EdgeScale cloud deployment service, integrate hardware based security and deploy a simple application that collects data, processes it locally and sends updates to the cloud. This session will provide greater understanding of edge computing and cloud computing concepts and technologies.
View full article
This session will provide an overview of the NXP wireless charging solutions portfolio and the reason of why NXP adopts Qi technology. Attendees will have a clear understanding about transmitter and receiver reference designs available for the automotive applications as well as the extension to consumer and infrastructure markets.
View full article
Acceptance of wireless charging is growing exponentially among consumers because of convenience and durability and automotive installation. This session will provide the in-depth technical detail and guidance of the design of in-vehicle wireless charging. Also a review of NFC/RFID cards protection that cover both low-power and medium-power applications.
View full article
Hands-on getting started with S32K. Participants will work with bare metal application code, working with an S32K144 development kit and S32 Design Studio. Short presentations followed by hands-on labs. Learn coding secrets for S32K and Arm® Cortex-M!
View full article
The i.MX 8M was designed with consumer and industrial customers in mind. The i.MX 8M series of processors are the first in a completely new paradigm of processors designed targeting market leading performance for audio, video and voice. The i.MX 8M starts with a system solution in mind and drives optimized solutions (best in class performance, optimized system cost, built with Google/Amazon/Msft ecosystems in mind) for many different customers from HMI, audio, video, voice, IOT, digital signage, printers, machine vision, etc. Best in class 4K video with HDR, best in class audio interfaces, low-power and optimized for lower cost. Come see what this new family of processors is all about and learn where we are headed.
View full article
Automotive and Industrial Battery Management Systems solutions from low to high voltage applications covering key components such as safety battery cell controller, power management, and MCUs.
View full article
Join this session to get a glimpse of where you will see i.MX 8/8X in the near future and why graphics, ML, AI, video, image processing, vision, connectivity, audio and voice functions make the i.MX 8 series ideal for Automotive and Industrial applications. Learn about the i.MX 8/8X families that are comprised of common subsystems establishing an unmatched range of performance scaling with pin-compatible options and the highest level of software reuse. In addition, learn more about the upcoming i.MX 8DualMax product line to help customers meet additional cost performance scaling across the i.MX 8 family.
View full article
Artificial intelligence and machine learning (AI/ML) are revolutionizing the industrial world. For maximal impact, AI/ML must be done close to where data is generated and the output of analysis used. It's an ideal workload for edge computing and complements NXP’s EdgeScale cloud-based device-management platform. Layerscape processors are well suited to hosting AI/ML workloads. Software from NXP and third parties helps enable developers to create industrial applications using AI/ML technology. These applications can be distributed, Layerscape-based edge nodes with endpoints performing multiple tasks including: addressing condition monitoring or first-level classification; running popular edge frameworks to deliver cloud-like services on premises, aggregating data from multiple endpoints or performing additional analysis; running cloud-based software analyzing data for long-term trends.
View full article
As memory interface data rates increase, so does the need for ensuring proper margins have been designed into the system’s usage of that interface. One way Micron has studied the system’s usage of the memory interface is through Timing & Signal Analysis (TSA). A TSA attaches physical hardware to the memory device to observe a subset of the memory interface as operated by the system. Another approach to memory interface is Virtual TSA (vTSA). This method uses the memory controller’s training algorithms to provide margin information without the use of physical test hardware. This method allows characterization of the entire memory interface. This session will compare and contrast the two different methods, and will ultimately demonstrate the value of integrating vTSA tools on the system platform. We intend to reference actual results from the latest i.MX 8 QXP board.
View full article
Join this session to learn how to leverage and get started with NXP’s power optimized LPC546xx MCU family, which now scales up in performance to 220 MHz. With rich peripheral integration, which includes 21 communication interfaces, including HS USB, dual CAN FD, graphics controller, to package option scalability, these microcontrollers address the various needs of today’s embedded IoT applications. Leave the session with the knowledge and skills to get up and running with the LPC546xx MCU family, which includes our comprehensive ecosystem of software and tools.
View full article
Getting started with MCUXpresso SDK, IDE, and Config tools.
View full article
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks.
View full article
NXP continues to expand the i.MX 8M Family with the  addition of the i.MX 8M Mini and i.MX 8M Nano products. Learn the features, performance and benefits of these products and which target applications they are most suited to. Attendees will leave the class with a deep understanding of the i.MX 8M family line-up and how to pick the right product for their application.
View full article
This session shows how to optimize FreeRTOS™ applications using the MCUXpresso SDK and IDE, including tools as Segger SystemView and Percepio Tracealizer. The  session covers optimizing the RTOS with configuration settings, inspecting stack and run-time using NXP Kernel Awareness, streaming real time data using Segger RTT and SystemView and up to analyzing and optimizing system performance with RTOS and application trace.
View full article
Machine learning can performed on a wide range of device categories - from MCUs with Arm® Cortex®-M4 and M7 cores to complex SoCs with high-end A-class cores, GPUs, DSPs, and dedicated machine learning accelerators. The first step is learning how to utilize proper training techniques for model development, but beyond that how to generate optimized inference engines that can be used to perform classifications, anomaly detection, predictions, and other types of decisions. This presentation highlights some basic training techniques, such as data augmentation, but the primary focus will be on various ways to deploy neural network frameworks and classical machine learning algorithms, and most importantly, utilizing a variety of open source tools and techniques. We will show how these techniques fit in with some real use cases such as object recognition and anomaly detection.
View full article
Learn the basics of DDR4, supported features, configuration of the DDR4 controller for QorIQ devices and related tools that assist with DDR bring up and optimization.
View full article