テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Getting started with MCUXpresso SDK, IDE, and Config tools.
記事全体を表示
In automotive applications, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems and the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators, and GPIO expanders are often used to bridge between the interconnects on the board. Also, LED Controllers, LCD Drivers and Real Time Clocks are used for interfacing between the system and user. In this session, we will explore the application of these analog and interface devices from NXP and discuss their applications in automotive applications.
記事全体を表示
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
記事全体を表示
QorIQ platforms provide a rich set of features for embedding security and trust into networking, storage and industrial systems. Learn how you can leverage these features via several tools, APIs and drivers provided by NXP. Additionally, learn about our complete turn-key solutions for IoT and security appliances, and get to know our software services team, which can customize a solution for your specific use-case.
記事全体を表示
Future networks will still use CAN to a huge extend - but the variety of trends is also significantly increasing. This session shows key values, technical background and differentiators of the different CAN trends and the NXP implementation.
記事全体を表示
Evolving IoT Needs of Brands Protect and Enhance Product Experiences through Advances in NFC Technology
記事全体を表示
In this session you will get familiar with i.MX RT (Cortex-M7 @ over 500MHz) tool set, IDE, SDK, RTOS and graphical libraries. This will allow you to design with the higher performance Cortex-M in your next project.
記事全体を表示
Low-power is a system level challenge. Unfortunately, there is not just one feature that resolves the challenge. With LPC, we will focus on delivering low-power capabilities across a broad range of products: Low-power boot, intelligent clocking, ultra-efficient processing, flexible low-power modes and autonomous, low-power peripherals. In this session, we focus on each one of these capabilities, how they address the challenges of designing low-power applications and highlight differentiators LPC MCUs offer the low-power market. What's the most efficient way to communicate with peripherals, how to optimize data transfers, the effects different power modes and clock gating functions have on energy. This session discusses these topics plus explains how one can leverage the unique modes and features available on LPC MCUs to improve energy efficiency of IoT applications and other embedded systems. 
記事全体を表示
Provide an overview of the protocol and implementation of CAN FD in system architectures, including the use of partial networking in relation to the deployment of CAN FD.
記事全体を表示
Learn how NXP's CodeWarrior Development Tools for ARMv8 architecture can boost your productivity and speed your time to market. The vast array of ARM development tool options can make it a challenge to assemble a tool chain and use it productively. NXP offers a complete integrated development environment based on open source tools and advanced capabilities made possible with NXP specific extensions. CodeWarrior combines the power and versatility of open source GNU tools like gcc and gdb with the GUI usability improvements provided by the development tools based on Eclipse. When basics are completed, CodeWarrior further extends the features portfolio with bare-metal debugging capabilities and a simplified user experience with Linux kernel and u-boot awareness capabilities.
記事全体を表示
Learn how to go from an IoT idea to a proof-of-concept as easy as 1-2-3 for a connected, secure, small-form factor IoT end node. The Rapid IoT kit integrates 30+ active components (11 NXP parts) with drivers, middleware, example applications and features an innovative web IDE with GUI-based programming, as well as mobile App and IoT cloud services.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone® technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.
記事全体を表示
This session shows how to optimize FreeRTOS applications using the MCUXpresso SDK and IDE.
記事全体を表示
Get immersed in enriched user interfaces with audio, video, voice and vision. Sense how the i.MX 8M portfolio delivers performance, versatility and connectivity to applications as media streaming, voice assistance, edge computing, machine learning/vision and Industrial IoT.
記事全体を表示
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
記事全体を表示
Car electrification require scalable power computing and functional safety platforms. To address such platform requirements NXP is building backbone solutions based on MCU, SBC and SW. Deep dive attach strategy with S32 to support diversity of car electrification market will be presented, introducing the latest generation of functional safety Power Management solutions (FSBCs).
記事全体を表示
Outline current wireless charging market situation and the trend.
記事全体を表示
Learn how to create an IoT proof-of-concept in real time without writing any C code. Skeptical? Rapid IoT combines processing, connectivity, sensing and security with an easy to use web IDE. The presentation and live demo walks you through creating a simple IoT solution including embedded, mobile and cloud applications. The demo lab will focus on use cases such as anomaly detection and vertical applications.
記事全体を表示