VR5510-FMEDA-external circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510-FMEDA-external circuit

Jump to solution
783 Views
zeyu_yan
Contributor III

Hello, when I analyse the external circuit of VR5510 and calculate the FMEDA of the system,how can I integrate the FMEDA of VR5510 into my system FMEDA?

for example the function block:High voltage buck,Vpre, the MOS Q1 and Q2 has the failure mode and fit

PRE-Regulator has the failure mode and fit.

Accourding to failure mode (regulaterd output  in OV UV drift ...)descripted in sheet<FMEDA_PM>,it seems the sub block <PRE-REGULATOR> includes the external MOSFET of Q1 and Q2.image.pngimage.png

 

 

 

Tags (2)
0 Kudos
1 Solution
776 Views
r40959
NXP Employee
NXP Employee
Hello the HV buck in the FMEDA (VR5510) is not including the external FET. We stop our quantitative analyis to to pinout and we don't consider the ext components. The suggestion is that you use the FMEDA VR5510 in addition to your bill of materials (Q1, Q2 and i guess others you might have). In case you have a doubt of the effect and safety mechanism that will be efficient, please let us know, we can support. Hoping it helps, thank you best regards Valerie

View solution in original post

0 Kudos
1 Reply
777 Views
r40959
NXP Employee
NXP Employee
Hello the HV buck in the FMEDA (VR5510) is not including the external FET. We stop our quantitative analyis to to pinout and we don't consider the ext components. The suggestion is that you use the FMEDA VR5510 in addition to your bill of materials (Q1, Q2 and i guess others you might have). In case you have a doubt of the effect and safety mechanism that will be efficient, please let us know, we can support. Hoping it helps, thank you best regards Valerie
0 Kudos