NXP S32 Design Studio for ARM 2.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP S32 Design Studio for ARM 2.2

ソリューションへジャンプ
1,513件の閲覧回数
Embedded_novice
Contributor III

I want to see how long a certain piece of code is running in the S32DS IDE and how I should do that.

0 件の賞賛
返信
1 解決策
1,494件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer: Measure the running time of one function on S32K
The unit of measurements of the variabile ARM_CM_DWT_CYCCNT is CORE_CLK cycles.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,495件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer: Measure the running time of one function on S32K
The unit of measurements of the variabile ARM_CM_DWT_CYCCNT is CORE_CLK cycles.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,486件の閲覧回数
Embedded_novice
Contributor III

Thank you for your advice.

0 件の賞賛
返信