NXP S32 Design Studio for ARM 2.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP S32 Design Studio for ARM 2.2

Jump to solution
1,482 Views
Embedded_novice
Contributor III

I want to see how long a certain piece of code is running in the S32DS IDE and how I should do that.

0 Kudos
Reply
1 Solution
1,463 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer: Measure the running time of one function on S32K
The unit of measurements of the variabile ARM_CM_DWT_CYCCNT is CORE_CLK cycles.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,464 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer: Measure the running time of one function on S32K
The unit of measurements of the variabile ARM_CM_DWT_CYCCNT is CORE_CLK cycles.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,455 Views
Embedded_novice
Contributor III

Thank you for your advice.

0 Kudos
Reply