If I don't use FIRC, should FIRCREGOFF be set to 1? Will it reduce power consumption?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If I don't use FIRC, should FIRCREGOFF be set to 1? Will it reduce power consumption?

546 Views
PYGC
Contributor II

PYGC_0-1677132161087.png

 

0 Kudos
Reply
1 Reply

537 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

The FIRCREGOFF bit is used to control an internal regulator used by the FIRC internal circuit. In order to guarantee the operation frequency of the FIRC at voltage levels higher than 3V, the application must be sure to set this bit. Otherwise, FIRC operational frequency may get out of spec.

If you don't use FIRC, I think you can set FIRCREGOFF=1 for power saving purposes.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply