S32K ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Knowledge Base

ラベル

ディスカッション

ソート順:
Attached is hands-on presentation Real-Time Control, Sensing, and Visualization with FRDM-A-S32K344 used during Electronica 2026 edge lab LIVE! event The presentation is designed for ​FRDM-A-S32K344 board, but might be reused also for different MCUs/boards with consideration board and pins specification. Brief Content: FRDM-A-S32K344 Board Overview​ Hands-On Application Code Hub (ACH) project Add Timer, GPIO and ADC pins Clock Configuration tips Push buttons Periodic Interrupt FreeMASTER Data Recording FreeMASTER Recorder Tips and Tricks​ As Initial example code we used Real-Time ADC Monitoring and LED Dimming Using FreeMASTER example from Application Code Hub. The content is Public: Free to use, modify, extend and share. We would be happy if you share with us significant improvements, modifications or porting to other boards/derivatives.   S32K3 , #FRDM-A-S32K344, S32DS-S32PLATFORM , FREEMASTER 
記事全体を表示
S32K1xx   S32K144 Example S32K144 CMP Round-robin S32DS2.0  Example S32K144 Verify Backdoor Access Key S32DS1.3  Example S32K144 FlexCAN0 RXFIFO DMA nonSDK S32DS13  Example S32K144 PDB ADC trigger DMA ISR S32DS  Example S32K144 Flash RW simple S32DS  Example S32K144 DMA memory copy test S32DS  Example S32K144 EEEPROM usage Example S32K144 EEEPROM usage - No SDK  Example S32K144 RTC VLPS  Example S32K144 WDOG RCM interrupt  Example S32K144 SRAM ECC Injection  Example S32K144 RAM Retention S32DS.R1 Example S32K144 I2C Master MPL3115A2 S32DSR1_v3  Example S32K144 FlexCAN RXFIFO DMA S32DS.ARM.2018.R1  Example S32K144_printf_implementation - S32DS_1.0  Example S32k144 UART printf/scanf under FreeRTOS - S32DS Example S32K144 SDK Function call on configurable period using LPIT timer.  Example S32K144 .noinit section usage Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1   Example S32K144 RAM selftest simple S32DS 2018.R1  Example S32K144 Position Independent Code  Example S32K144 FlexCAN Pretended Networking STOP mode test S32DS.ARM.2.2  Example S32K144 LPIT DMA LPSPI  Example S32K144 FlexCAN TX/RX/Error ISR test S32DS2.2  Example S32K144 FlexIO Idle Detection S32DS2.2   S32K142 Example_S32K142_LMEN_Cache_v1_0_S32DS3.6_RTD300  Lauterbach_Script_For_MDM_AP_Mass_erase_S32K142    S32K146 Example S32K146 Set_whole_FlexRAM-as_RAM S32DS.ARM.2.2   S32K148 Example S32K148 PDB0-PDB1 ring S32DS3.4 RTM4.0.3  Example S32K148 PDB0-PDB1 ring DMA S32DS3.4 RTM4.0.3  Example S32K148 GPIO Interrupt     S32K116 Example S32K116 WDOG Fast Test  Example S32K116 LPUART LIN Slave TXRX ISR S32DS.ARM.2.2  Example S32K116 FlexCAN PN STOP S32DS.ARM.2.2 Example S32K116 FlexCAN VLPR test S32DS.ARM.2.2   S32K118 Example S32K118-SRAM-keep_data_over_SW_reset v0_1 S32DS.ARM.2.2   S32K3xx   S32K312 Example S32K312 ADC_IP Continuous Scan DMA S32DS36 RTD600    S32K344 Example S32K344 PIT BTCU ADC DMA DS3.4 RTD100   Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200     Example_C40_Ip_ECC_Fault_Skip_S32K312_DS34_RTD2211_v1     Example Siul2_Port_Ip_Example_S32K344_ITCM_DTCM S32DS3.4 RTD300   Example S32K344 LPUART RX/TX ISR FreeRTOS S32DS36 RTD600    Example_S32K344_MCAL_MCU_ClockMonitor_v1_0_S32DS36_RTD600    Example_S32K314_DTCM1_Backdoor_RTD201_DS34_v3    Example_Reg_Prot_Flash_Controller_S32K344   Example_S32K344_EIM_ERM_DTCM_SRAM_Baremetal_v3_0_S32DS36    Example S32K344 PIT SWtrig ADC ANAMUX S32DS 3.6.0 RTD 6.0.0   Example S32K344 EMAC lwIP FreeRTOS miniEVB S32DS 3.6.1 RTD 6.0.0   Example S32K344 EMAC lwIP FreeRTOS MRCANHUB S32DS 3.6.1 RTD600   Example_S32K344_BIST_eMCEM_SPD106_v2_0_S32DS365_RTD700  Example S32K344EVB_T172 UART_ETH_Gateway HLD S32DS368 RTD701   Example_S32K344_CMU_FM_POR_WDG_v1_0_S32DS369_RTD701    Example_S32K344_FLS_Integrity_Margin_Check_v1_0_S32DS36_RTD701    Example S32K344 LPSPI LCD-PAR-S035 FRDM S32DS 3.6.6 RTD 7.0.1   Example FRDM-A-S32K344 FlexCAN TX_RX FreeRTOS S32DS36 RTD600    Example_S32K344_INFLS_ECC_EDC_eMCEM_SPD106_v1_0_S32DS365_RTD700    Example S32K344 EMAC lwIP FreeRTOS S32K3-T-BOX S32DS 3.6.6 RTD7.0.1   Demo EthernetAnalyzer FRDM-A-S32K344 RTD 7.0.1   Example FRDM-A-S32K344 PIT ADC BTCU_ControlMode FIFO DMA HLD S32DS35 RTD300    Example S32K344EVB_T172 LPUART_EMAC_Gateway IP S32DS368 RTD701    S32K358   S32K358 Multicore Start CM7_2 from CM7_0    Example S32K358 FlexCAN TXRX ISR S32DS35 RTD400/500   Example S32K358 GMAC 100M lwIP FreeRTOS S32DS 3.6.1 RTD600   Example S32K358 GMAC 1G lwIP FreeRTOS S32DS 3.6.1 RTD600   Example S32K358 GMAC lwIP FreeRTOS RDBESS S32DS 3.6.1 RTD600   Example_S32K358_XRDC_SEMA42_Multicore_v1_0_S32DS369_RTD701    S32K388 Example S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600   S32K389 Example S32K389 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD 6.0.0   Example S32K389 GMAC1 SABRE lwIP FreeRTOS S32DS 3.6.1 RTD600  
記事全体を表示
* ============================================================================ * Detailed Description: * * The purpose of this demo application is to demonstrate the usage of the * ADC High-Level Driver (HLD) on the S32K312 MCU. * * The example uses PIT timers to periodically trigger BCTU conversion lists * through the TRGMUX. Each conversion list consists of five ADC channels. * Conversion results are stored in BCTU FIFOs and automatically transferred * by eDMA into result arrays. * * Trigger paths: * PIT0_CH0 -> TRGMUX -> BCTU Trigger 23 -> ADC0 (5 channels) * -> BCTU FIFO1 -> eDMA (ch0) * * PIT1_CH1 -> TRGMUX -> BCTU Trigger 47 -> ADC1 (5 channels) * -> BCTU FIFO2 -> eDMA (ch11) * * Converted results from the BCTU FIFOs are moved by eDMA into dedicated * ADC result buffers. * * ADC1 channel S10 is connected to the on-board potentiometer. The converted * value is used to adjust the brightness of the BLUE LED * * ============================================================================ * Test HW: S32K312-T172 * MCU: S32K312 * Compiler: S32DS 3.5.x * RTD release: S32K3_RTD_3_0_0 P07 * Debugger: On-Board Debugger * Target: Internal_FLASH * ============================================================================   I used these channels on --> S32K312-T172 eval board   ADC results :--   ALso  be sure you enable freeze for both PITs :--    
記事全体を表示
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K312 MEM_InFls  DS3.5 RTD300 :-- Example MCAL S32K312 MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE DS3.5 RTD300 :-- Example MCAL S32K312 FEE DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 PWM ICU using Custom IRQ EMIOS DS3.5 RTD300 :-- Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community  Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community Example MCAL S32K312 PIT ADC BTCU DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-MCAL-S32K312-PIT-ADC-BTCU-DS3-5-RTD300/ta-p/2424542
記事全体を表示
**************************************************************************************************** * Detailed Description: * * UART ↔ Ethernet gateway implemented using RTD IP (LLD) drivers. * * Demonstrates bidirectional forwarding of UART data over Automotive Ethernet on S32K344. * UART messages are encapsulated into raw Ethernet frames and transmitted through the GMAC * peripheral; received Ethernet frames are decapsulated and forwarded to UART. * * Key Functionality: * - UART TX/RX interrupt driven communication. * - GMAC TX confirmation and RX indication interrupt processing. * - Four-deep message queue for UART/Ethernet decoupling. * - Runtime MAC address configuration. * - TJA1103 loopback, MASTER and SLAVE operation. * - Raw Ethernet frame transport (EtherType 0x88B5). * - RTD IP implementation. * * Runtime status information including node configuration, * MAC addresses and link status is displayed on the UART terminal. * * Test Configurations: * * Single board: * GATEWAY_MODE_NODE_1_LOOPBACK * * Two-board setup: * Board 1 : GATEWAY_MODE_NODE_1_MASTER * Board 2 : GATEWAY_MODE_NODE_2_SLAVE * * Boards are connected using a 100BASE-T1 cable. * * Notes: * - On the PC terminal, enable local echo * * ------------------------------------------------------------------------------------------------ * Test HW: S32K3x4EVB-T172 Rev B * MCU: S32K344_172HDQFP * PHY: TJA1103 * IDE: S32DS 3.6.8 * RTD release: S32K3_RTD_7_0_1_D2602_ASR_REL_4_9_REV_0000_20260206 * Debugger: Lauterbach, P&E Micro * Target: Internal_FLASH * Serial: 115200, 8N1 ****************************************************************************************************   Terminal prints between two S32K344EVB-T172 boards In case of single board in PHY loopback  
記事全体を表示
This article presents BareMetal and FreeRTOS variants of an embedded Ethernet Analyzer demo for the S32K344 MCU. The application captures RX and TX Ethernet frames and displays them directly on an LCD-PAR-S035 touchscreen, including basic decoding of VLAN and IEEE 802.1CB R-TAG information and hexadecimal inspection of individual frames. The graphical interface uses LVGL 9.4.0 and was created with NXP GUI Guider 2.0.1.
記事全体を表示
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K344 to enable pinging the lwIP stack * from the command window * *ping 192.168.0.210 * *Pinging 192.168.0.210 with 32 bytes of data: *Reply from 192.168.0.210: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.210: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.210: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.210: bytes=32 time=2ms TTL=255 * *Ping statistics for 192.168.0.210: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * Installed packages for S32 Design Studio 3.6.6: * * SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip * SW32K3_FreeRTOS_11.1.0_7.0.0_CD1_HF1_D2511_DesignStudio_updatesite.zip * SW32K3_TCPIP_STACK_5.0.0_CD01_D2605_DesignStudio_updatesite.zip * * * EVB: * - All jumpers in default positions * * Configuration: * - Updated pin configuration * - Updated clock configuration * - IP address set to 192.168.0.210 * - Added DIO * * Excluded from build: * - RTD/src/EthIf.c * - tcpip/lwip/src/apps/http/fsdata * * main.c * - Updated only the header * device.c * - Added required delay before clock init * test.c * - Removed the code that shuts down the TCP/IP stack after * its predefined timeout * - Added LED task * * ----------------------------------------------------------------------------- * Test HW: S32K3-T-BOX * MCU: S32K344 * Debugger: Lauterbach TRACE32 * Target: internal_FLASH * EVB connection: EMAC <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
記事全体を表示
***************************************************************************** *Detailed Description: *This is a basic communication example for LIN transceiver module of FS23 SBC with SPI interface. *The FS23 SBC on the S32K31XEVB-Q100 board integrated a LIN transceiver. To test LIN communication, another board or a LIN analyzer must be used. *In this example, the S32K311 configures and controls the FS23 via LPSPI0. *The FS23 LinTrcv driver is initialized by calling LinTrcv_43_fs23_Init(), while LinTrcv_43_fs23_SetOpMode() is used to change the operating mode of the integrated LIN transceiver. *After initialization is complete, the S32K3 transmits a LIN frame with ID 0x1A. *At this stage, the LIN frame should be received by the LIN analyzer connected to the J9 LIN bus interface on the S32K31XEVB-Q100 board. *LED Indications: Blue LED ON: LIN frame transmission in progress Blue LED OFF: LIN frame transmission completed Red LED flashes: LIN frame transmission timed out *---------------------------------------------------------------------------- *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A1 P32K311HVS 0P98C * PCAN-USB Pro * PCAN-USB Pro | S32K31XEVB-Q100 ------------------------|-------------------- LIN LIN2.4 | J9.1 VBAT LIN2.9 | J9.2 GND LIN2.5 | J9.4 - S32K31XEVB-Q100 Jumper Configuration: J25 1-2 https://www.nxp.com/document/guide/getting-started-with-the-s32k31xevb-q100-evaluation-board-for-general-purpose:GS-S32K31XEVB-Q100?section=plug-it-in_plug-it-in-1 Test SW: *PLIN-View Pro *SDK: * S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.1 (SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip) * 2.0.0 SBC FS23 R23-11 2.0.0 (SBC_FS23_R23-11_2.0.0_D2604_DesignStudio_updatesite.zip) *Debugger: S32DS 3.6.11, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference Documentation: * AN14041 FS23 quick start guide (Rev. 2.0 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.6.11_S32K3_RTD701\S32DS\software\common\SBC_FS23\Sbc_fs23_TS_T40DXXM20I0R0\doc * RTD_LINTRCV_43_FS23_UM.pdf C:\NXP\S32DS.3.6.11_S32K3_RTD701\S32DS\software\common\SBC_FS23\LinTrcv_43_fs23_TS_T40DXXM20I0R0\doc * AUTOSAR_CP_SWS_LINDriver.pdf https://www.autosar.org/fileadmin/standards/R23-11/CP/AUTOSAR_CP_SWS_LINDriver.pdf * This example is migrated from LinTrcv_fs23_Example_S32K312. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 ***************************************************************************** * Revision History: * Ver Date Author Description of Changes * 0.0 10-14-2026 Robin Shen Initial version *****************************************************************************
記事全体を表示
**************************************************************************** * Detailed Description: * * CAN <-> Ethernet gateway demo for FRDM-A-S32K344. * * CAN FD frames are encapsulated into raw Ethernet frames and * transmitted over the 100BASE-TX link. Received Ethernet frames * are decapsulated and forwarded to the CAN FD bus. * * Key Functionality: * - Interrupt-driven CAN FD reception via CanIf_RxIndication callback. * - Interrupt-driven Ethernet reception via EthIf_RxIndication callback * (EthCtrlEnableIngressQueueInterrupt, GMAC0_CH_RX_IRQHandler). * - GMAC TX confirmation interrupt processing (GMAC0_CH_TX_IRQHandler). * - Custom gateway format for CAN ID, DLC, flags and * payload (up to 64 bytes CAN FD) in a fixed 72-byte Ethernet payload. * - PHY CAN transceiver initialization. * - Ethernet PHY auto-detection and MDIO configuration via EthPhy driver. * - PHY initialization selectable at compile time: * PHY_INIT_BY_PIN_STRAPPING (default) * PHY_INIT_BY_SOFTWARE (MDIO register write) * * Main Loop Flow: * - CAN -> ETH : CanIf_bRxFlag set by ISR -> App_EthTransmit() * - ETH -> CAN : ethReceiveFlag set by ISR -> App_CanTransmit() * * Notes: * - Red LED set if Gateway_Init returns E_NOT_OK. * - Green LED toggles upon CAN reception. * - Blue LED toggles upon ETH reception. * - EthIf.c contains the custom EthIf_RxIndication gateway implementation. * - During S32 Configuration Tool code generation select "Keep Existing" * for EthIf.c to avoid overwriting the custom callback. * - Eth_43_GMAC_ReleaseRxBuffer() must be called unconditionally inside * EthIf_RxIndication. * * ------------------------------------------------------------------------- * Test HW : FRDM-A-S32K344 Rev A * MCU : S32K344_257BGA * IDE : S32DS 3.6.10 * RTD : S32K3_RTD_7_0_1_D2602_ASR_REL_4_9_REV_0000_20260206 * AUTOSAR : 4.9.0 * Debugger : P&E Micro * Target : Internal_FLASH * CAN : CAN FD, 500 Kbps nominal / 2 Mbps data, TJA1043 transceiver * Ethernet : RMII 100BASE-TX, DP83848 PHY **************************************************************************** ETH Reception with Wireshark: CAN Reception with PCAN-USB. Note 1: Inside project you can comment NODE_1 and define NODE_2 as 1 to enable simple routine which sends out a CAN frame if SW3 is pressed, and an ETH frame if SW2 is pressed. Note 2: For a real gateway application, use a queue or ring buffer instead of one global frame; otherwise, a second CAN frame can overwrite the first before Ethernet transmission completes. This example is for demostration purposes only.
記事全体を表示
***************************************************************************** *Detailed Description: *This is a basic communication example for CAN transceiver module of FS23 SBC with SPI interface. *The FS23 SBC on the S32K31XEVB-Q100 board integrated a CAN transceiver. To test CAN communication, another board or a CAN analyzer must be used. *In this example, the S32K311 configures and controls the FS23 via LPSPI0. *The FS23 CanTrcv driver is initialized by calling CanTrcv_43_fs23_Init(), while CanTrcv_43_fs23_SetOpMode() is used to change the operating mode of the integrated CAN transceiver. *After initialization is complete, the S32K3 first transmits a standard CAN data frame with ID 0x123. *At this stage, the CAN frame should be received by the CAN analyzer connected to the J8 CAN bus interface on the S32K31XEVB-Q100 board. *In the main application loop, a standard CAN frame with ID 0x100 is transmitted each time a CAN frame is received. *LED Indications: Blue LED ON: CAN frame transmission in progress Blue LED OFF: CAN frame transmission completed Red LED flashes: CAN frame transmission timed out Green LED ON: CAN frame received *---------------------------------------------------------------------------- *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A1 P32K311HVS 0P98C * PCAN-USB Pro * PCAN-USB Pro | S32K31XEVB-Q100 ------------------|-------------------- CANH CAN1.7 | J8.1 (FS23_CANH) CANL CAN1.2 | J8.2 (FS23_CANL) GND CAN1.3 | J8.3 (GND) - S32K31XEVB-Q100 Jumper Configuration: https://www.nxp.com/document/guide/getting-started-with-the-s32k31xevb-q100-evaluation-board-for-general-purpose:GS-S32K31XEVB-Q100?section=plug-it-in_plug-it-in-1 *SDK: * S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.1 (SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip) * 2.0.0 SBC FS23 R23-11 2.0.0 (SBC_FS23_R23-11_2.0.0_D2604_DesignStudio_updatesite.zip) *Debugger: S32DS 3.6.11, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference Documentation: * AN14041 FS23 quick start guide (Rev. 2.0 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.6.11_S32K3_RTD701\S32DS\software\common\SBC_FS23\Sbc_fs23_TS_T40DXXM20I0R0\doc * RTD_CANTRCV_43_FS23_UM.pdf C:\NXP\S32DS.3.6.11_S32K3_RTD701\S32DS\software\common\SBC_FS23\Cantrcv_43_fs23_TS_T40DXXM20I0R0\doc * This example is migrated from CanTrcv_fs23_Example_S32K312. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 * In addition, the implementation was referenced from the Application Code Hub example "Dual-Board Serial Communication with AUTOSAR CAN Driver" for the FRDM-A-S32K118 board. https://mcuxpresso.nxp.com/appcodehub?search=dm-can-p2p-s32k118 * FlexCAN bitrate is calculated with: https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-LPCxxxx-CAN-CAN-FD-bit-timing-calculation/ta-p/1119319 CAN classic (non-FD) 30MHz clock 500Kbps 80.0% Sample Point ***************************************************************************** * Revision History: * Ver Date Author Description of Changes * 0.0 10-13-2026 Robin Shen Initial version *****************************************************************************
記事全体を表示
* ============================================================================ * Detailed Description: * * The purpose of this demo application is to demonstrate the usage of the * ADC High-Level Driver (HLD) on the S32K344 MCU. * * The example uses PIT timers to periodically trigger BCTU conversion lists * through the TRGMUX. Each conversion list consists of five ADC channels. * Conversion results are stored in BCTU FIFOs and automatically transferred * by eDMA into result arrays. * * Trigger paths: * PIT0_CH0 -> TRGMUX -> BCTU Trigger 23 -> ADC0 (5 channels) * -> BCTU FIFO1 -> eDMA (ch0) * * PIT1_CH1 -> TRGMUX -> BCTU Trigger 47 -> ADC1 (5 channels) * -> BCTU FIFO2 -> eDMA (ch16) * * Converted results from the BCTU FIFOs are moved by eDMA into dedicated * ADC result buffers. * * ADC0 channel P7 is connected to the on-board potentiometer. The converted * value is used to adjust the brightness of the BLUE LED * * ============================================================================ * Test HW: FRDM-A-S32K344 (SCH-94921 / SPF-94921 Rev. C) * MCU: S32K344 * Compiler: S32DS 3.5.x * RTD release: S32K3_RTD_3_0_0_P01_D2303_ASR_REL_4_7_REV_0000_20230331 * Debugger: On-Board Debugger * Target: Internal_FLASH * ============================================================================
記事全体を表示
********************************************************************************************** * Detailed Description: * This example uses RTD 7.0.0 and SPD 1.0.6. It initializes the internal * flash and executes the selected C40 UTEST diagnostic through the * Mem_43_INFLS driver. * The available tests are * ECC Logic Check (ECC_LOGIC_CHECK), * EDC-after-ECC Logic Check (EDC_AFTER_ECC_LOGIC_CHECK), * and Address Encode Logic Check (ADDRESS_ENCODE_LOGIC_CHECK). * The test-selection macros enable or disable each diagnostic, and more than one * test may be enabled at the same time. * * ProgramBlock3() is optional and is not required for the UTESTs. * It erases * and programs one data-flash sector only to provide a known, readable test * address. The UTESTs can also run without it, provided that AddressCheck is * a valid, aligned flash address. The ECC and EDC tests use synthetic * data/check-bit values, while the address is used to select the flash block * and trigger the hardware check. * * EMCEM_MODULE_ENABLED enables eMCEM support. WAIT_MAIN pauses execution * before eMcem initialization, while WAIT_AFTER_EMCEM_INIT pauses execution * after eMcem initialization to allow debugger attachment at the required * execution point. eMcem_Init() requires a reset without an attached debugger. * * Mem driver job results and handled eMCEM alarms are stored in g_MemTestResults. * The user alarm handler clears the configured FCCU/eMCEM * faults and records the corresponding alarm result. If a UTEST causes a * HardFault, the handler resumes interrupts and disables C40 UTEST mode * before returning so that pending FCCU alarm interrupts can be serviced. * ------------------------------------------------------------------------------------- * MCU: S32K3x4EVB-Q257 * Fsys: 160 MHz PLL with 16 MHz crystal reference * Debugger: Lauterbach Trace32, S32DS IDE 3.6.5 * Target: internal_FLASH **********************************************************************************************
記事全体を表示
Pad Keeping As explained in the S32K3xx Low Power Management Application Note (AN), the S32K3 family is capable of retaining the output value of some selected pads when device is power-gated in Standby mode. All pins will retain their last set states in run mode during standby mode, and all pins will be placed to its default states after reset event by default. Which means that during the time between wakeup and Port reinitialization, the pins are uncontrollable and driven by default reset values. When pad keeping is enabled, HW ensures that the pin can retain its states from wakeup until the user unlocks it. The S32K3 family provides two pin groups: Run domain & Standby domain, however, the differences between them are not explicitly mentioned in the low power management application. Run domain pins are active only while the MCU is running, while Standby domain pins can also remain functional during Standby Referring to Chapter 41.12 Pad Keeping from S32K3XXRM (Rev. 12), all of the active pins in Standby are: Pin Function in Standby GPIO_4 CMP0_OUT GPIO_5 RESET_b GPIO_9 CMP2_OUT GPIO_11 CMP0_RRT GPIO_12 CLKOUT_STANDBY; CMP1_OUT GPIO_69 CMP2_RRT GPIO_110 CMP0_RRT GPIO_131 CMP0_OUT GPIO_138 CLKOUT_STANDBY GPIO_143 CMP1_RRT GPIO_158 CMP1_OUT GPIO_159 CMP1_RRT GPIO_174 CMP0_OUT GPIO_175 CMP0_RRT GPIO_196 CMP2_OUT GPIO_197 CMP2_RRT (As specified in the RM, see the IOMUX attached to it for details on different derivatives.) Configuration for Pad Keeping for both groups require the same global configuration, but standby domain pins require an additional step.  You could consider DCM.DCMRWF1[STANDBY_IO_CONFIG] field as a global enable for all pad keeping purposes during Standby mode. Additionally, for Standby domain pins, the corresponding MSCRn[PKE] field in SIUL2 must be set. Note: MSCRn[PKE] only needs to be set for Standby domain pins, and does not have effect on Run domain pins. Run domain pins Before entering standby: Configure SIUL2 output for desired pad (HIGH/LOW). Write 0 to DCM.DCMRWF1[STANDBY_IO_CONFIG] (enable global pad keeping). Complete Standby Entry Sequence described in RM. Standby domain pins Before entering standby: Configure SIUL2 output for desired pad (HIGH/LOW). Write 1 to SIUL2.MSCRn[PKE] (enable individual pad keeping). Write 0 to DCM.DCMRWF1[STANDBY_IO_CONFIG] (enable global pad keeping). Complete Standby Entry Sequence described in RM. For both Run and Standby domain pins After standby exit (wake-up event): Write 1 to DCM.DCMRWF1[STANDBY_IO_CONFIG] field on Standby mode exit to disable pad keeping. Note: After enabling Pad Keeping, user must write 1 to DCM.DCMRWF1[STANDBY_IO_CONFIG] to disable it before calling Port_Init() / Siul2_Port_Ip_Init(), otherwise pin initialization may fail. Example routine - Pad keeping    /* ------------------------------------------------------------------------- * Test HW : FRDM-A-S32K344 * MCU : S32K344_172HDQFP * IDE : S32DS 3.6.10 * RTD : S32K3_RTD_7_0_1_D2602_ASR_REL_4_9_REV_0000_20260206 * Debugger : P&E Micro * Target : Internal_FLASH * -------------------------------------------------------------------------*/ The attached example configures PTD13 (GPIO109) & PTD14 (GPIO110). PTD13 is a run domain pin, while PTD14 is a standby domain pin.  The macro PKE_CONFIG can be enabled to configure both SIUL2.MSCRn[PKE] & DCM.DCMRWF1[STANDBY_IO_CONFIG] directly through registers. Otherwise, configuration can be done through Siul2_Ip_Port and Power_Ip drivers: Enable SIUL2.MSCRn[PKE]:   Enable DCM.DCMRWF1[STANDBY_IO_CONFIG]:   After configuring Pad Keeping, the routine waits for USR_SW0 to be pressed, then sets both PTD13 & PTD14 HIGH and enters Standby. MCU can be waken up with USR_SW1. Green LED reflects MCU status (RUN = HIGH, STANDBY = LOW). Note: A small delay is added at to visualize time between standby exit (wake-up) and port initialization. Measurements   Using the attached routine, the following measurements were done: 1. Pad Keeping enabled for both PTD13 & PTD14. 2. Pad Keeping enabled for PTD13 and disabled for PTD14. 3. Pad Keeping disabled for both PTD13 & PTD14.   This example is provided as is with no guarantees and no support.
記事全体を表示
1. Abstract/Introduction Boundary scan is a method for testing interconnects (wire lines) on printed circuit boards or sub-blocks inside an integrated circuit (IC). Boundary scan is also widely used as a debugging method to watch integrated circuit pin states, measure voltage, or analyze sub-blocks inside an integrated circuit. The Joint Test Action Group (JTAG) developed a specification for boundary scan testing that was standardized in 1990 as the IEEE Std. 1149.1-1990. In 1994, a supplement that contains a description of the boundary scan description language (BSDL) was added which describes the boundary-scan logic content of IEEE Std 1149.1 compliant devices. Since then, this standard has been adopted by electronic device companies all over the world. Boundary scan is now mostly synonymous with JTAG. This test is based on existing application notes for LPC55(S)xx, i.MX RT and MCXA (See references). The procedure follows how to do both a BYPASS, IDCODE and SAMPLE test, as well as an EXTEST. Following boundary scan instructions are defined in the IEEE standard: BYPASS (mandatory): TDI is connected to TDO via a single shift register. IDCODE (optional): Reads the device identification register. SAMPLE (mandatory): Takes a snapshot of the normal operation of the IC. EXTEST (mandatory): Apply preloaded data of the boundary scan register to the ports. 2. Hardware platform Lauterbach: LA-3505 POWER-DEBUG-PRO S32K3: S32K3X8EVB-Q289 There are no hardware modifications needed for connecting JTAG interface, as the S32K3 family includes the standard Arm debug port, supporting both the JTAG and SWD interfaces. S32K3XX derivatives can directly use the JTAG interface. Ensure S32K3X8EVB-Q289's jumpers are set as in the Quick Start Guide for S32K3X8EVB Board: Default Jumper settings. Ensure a valid connection between the EVB's JTAG ARM 20-pin Standard Port (On board: J365), and the Debug Cable for Lauterbach interface. 3. Software platform This test uses Lauterbach's TRACE32 Software Package. Download the TRACE32_202509.7z to the computer and install it: Because the installation package is relatively large, you can install software components according to the target processor to save hard disk space. You can find installed driver at C:\T32\bin\windows64\drivers. 4. BSDL file validation using Lauterbach JTAG debugger. Confirm that Lauterbach probe is detected in 'Device Manager': Device Manager Trace32 device enumeration.   Note: Lauterbach debugger used is LA-3500, with Probe LA-3000 + LA-7844A Debug License. Related information can be found on the Lauterbach's page. Open TRACE32 Arm interface: Type in the following commands: SYStem.Down BSDL.RESet BSDL.ParkState Select-DR-Scan BSDL.state    BSDL.state window should now appear. Select 'FILE' and load BSDL from S32K3 HW Design Package. S32K3X8EVB-Q289 should use S32K358_bga289_customer_1995E01D.bsdl. BSDL.state window.  After loading the file, type the following command: BSDL.SOFTRESET​ Switch to the Check tab of the BSDL.state window. Click BYPASSall and IDCODEall button to see if both results pass. Both should change from 'No result' to 'Test PASS': BYPASS and IDCODE check. BYPASS: PASS means the bypass scan completed correctly for all configured devices. This indicates that the JTAG chain connectivity, chain order/length, and basic BSDL configuration are probably correct. IDCODE: PASS means the received device ID matches the expected BSDL description. This is evidence that the correct device and BSDL file are being used, but it still does not validate the boundary-register pin definitions. Next, click the SAMPLEall button, 'No result' should become Test done. Double-click the entity name, and the BSDL.SET window will pop-up: BYPASS and IDCODE check, BSDL.SET window appears. SAMPLE: PASS indicates that the pin can be observed through the boundary-scan cell, the BSDL input/observe mapping is likely correct, and that the captured value corresponds to the actual pad level. In the BSDL.SET window, uncheck Intern option to filter out the internal registers. The remaining contents are the sampled value on each signal pins. Use a multimeter to measure voltage of at least three signal pins and see if the logic state matches the sampled value. BSDL.SET window, SAMPLE check.   Next, in the Instructions field, click EXTEST and in the DR mode field, choose Set Write. Then switch to the BSDL.state window and check SetAndRun and TwoStepDR. BSDL.SET & BSDL.STATE windows EXTEST set up.   Switch back to BSDL.SET window, click 'ENABLE' in Init BSR to enable output of corresponding signal pins, and click the buttons in “Reg.” column to toggle their output logic state 0 or 1. Use a multimeter to measure if the logic state really toggles on those signal pins. At least three signal pins need to be verified. BSDL.SET window enable and toggle signal level Note: PTG29/30/31 (User LED indicators Red/Green/Blue) for simplicity reasons, however, as a diagnostic recommendation, use an unloaded or lightly loaded pad if possible. 5. Conclusion This procedure provides a practical method for validating the S32K3X8EVB JTAG boundary-scan chain using TRACE32 and the appropriate S32K358 BSDL file. BYPASSall and IDCODEall verify JTAG-chain connectivity and device identification, SAMPLEall confirms pin-state observation, and EXTEST verifies pin control through the boundary-scan register. While these checks confirm basic boundary-scan operation, additional pin-level testing is recommended to validate board connectivity and application-specific signals. Any reset observed during EXTEST should be investigated before concluding a BSDL-related issue. The final report should capture the BSDL file used, JTAG-chain results, validated pins, measured logic levels, and any reset behavior observed during EXTEST. 6. References How to Perform Boundary Scan for LPC55(S)xx based on μTrace AN12919: Introduction to Boundary Scan of i.MX RT Series – Application Note How To Perform Boundary Scan On MCXA Series Using μTrace And Trace32 Boundary Scan User's Guide S32K3 Auto General-Purpose MCUs | NXP Semiconductors Software Download | Lauterbach TRACE32
記事全体を表示
* ================================================================================================= * Detailed Description: * * This example demonstrates Classical CAN and CAN FD reception and transmission using * interrupt-driven Message Buffers and FreeRTOS. * * FlexCAN0 is configured in Normal mode. MB0 receives standard-ID frames and MB1 receives * extended-ID frames. The FlexCAN callback copies every received frame into a FreeRTOS queue * and immediately rearms the corresponding RX Message Buffer. * * A dedicated FreeRTOS task waits for frames in the queue and echoes them through CAN TX MB2. * The transmitted frame preserves the received identifier type, identifier, payload length, * payload, CAN FD EDL state, and BRS state. The user LED is toggled after a transmit request * is accepted by the driver. * * Note: * FreeRTOS API functions such as xQueueSendFromISR() are used from the FlexCAN callback. * Therefore, the FlexCAN interrupt priority must comply with the FreeRTOS interrupt-priority * requirements defined by configMAX_SYSCALL_INTERRUPT_PRIORITY. * * ================================================================================================= * Test HW: FRDM-A-S32K344 (SCH-94921 / SPF-94921 Rev. C) * MCU: S32K344 * Compiler: S32DS 3.6.x * RTD release: S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_20250610 * Debugger: On-Board Debugger * Target: Internal_FLASH * Communication: Classical CAN / CAN FD, STD and EXT ID, optional BRS * =================================================================================================    
記事全体を表示
* Detailed Description: * * This project provides a minimal bring-up and reference example for the LCD-PAR-S035 * display and GT911 capacitive touchscreen on the S32K344. It includes standalone LCD * and touchscreen diagnostic modes, together with an LVGL demonstration mode. * * The display is controlled through the LPSPI interface using the ST7796S * display controller driver. The touchscreen is controlled through the LPI2C * interface and uses GPIO signals for interrupt and reset control. * * The original LCD, DBI and touchscreen drivers were obtained from an NXP * App Code Hub MCUXpresso SDK example and adapted to the S32K3 RTD * environment. The project also integrates LVGL 9.4 as the graphical user * interface library. * * The application mode is selected at compile time using the APP_MODE macro * defined in this file. It allows the user to select a standalone display * test, a standalone touchscreen test or the complete LVGL demonstration. * Only one application mode shall be selected for each build. * * A graphical application can be designed using NXP GUI Guider 2.0.1. * GUI Guider is configured for LVGL 9.4.0. The contents of the GUI Guider * "generated" and "custom" output directories can be copied directly into * the corresponding gui_guider directories in this project. After replacing * the generated output, the project shall be rebuilt to include the updated * screens, widgets, events and custom callbacks. * * Installed packages for S32 Design Studio 3.6.6: * * SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip * * Software Sources: * * NXP App Code Hub demo: * https://github.com/nxp-appcodehub/dm-https-lcd-led-demo * * LVGL release/v9.4: * https://github.com/lvgl/lvgl/tree/release/v9.4 * * NXP GUI Guider 2.0.1: * https://www.nxp.com/webapp/Download?colCode=GUI-GUIDER-INSTALLER-2.0.1-WIN&appType=license * * Hardware: * * FRDM-A-S32K344: * Remove jumper JP11 when using an external debugger. * * LCD-PAR-S035: * Set SW1 to 111. * * Board Connections: * * +------------------+----------------------+-----------------+-------------------+------------------------------+ * | FRDM-A-S32K344 | MCU Signal | LCD-PAR-S035 | LCD-PAR-S035 | Function | * | Connector | | Signal | Connector | | * +------------------+----------------------+-----------------+-------------------+------------------------------+ * | J2-20 | PTC27 / GPIO | TP_INT | J5-12 | Touch interrupt, active low | * | J2-19 | PTC7 / LPI2C1_SCL | TP_SCL | J5-8 | Touchscreen I2C clock | * | J2-17 | PTC6 / LPI2C1_SDA | TP_SDA | J5-6 | Touchscreen I2C data | * | J2-13 | GND | GND | J5-4 | Signal ground | * | J2-11 | PTB14 / LPSPI1_SCK | LCD_WR | J5-5 | LCD SPI clock | * | J2-9 | PTB15 / LPSPI1_SIN | LCD_RD | Not connected | SPI data from LCD | * | J2-7 | PTB16 / LPSPI1_SOUT | LCD_MOSI | J5-9 | SPI data to LCD | * | J2-5 | PTB17 / GPIO | LCD_CS | J5-11 | LCD chip select, active low | * | J2-3 | PTC10 / GPIO | LCD_D_C | J5-7 | Command low, data high | * | J2-1 | PTC11 / GPIO | LCD_RST | J5-10 | LCD reset, active low | * | JA3-3 | VDD_HV_A | VCC | J5-1 or J5-2 | 3.3 V supply | * | JA3-13 or JA3-15 | GND | GND | J5-3 | Power ground | * +------------------+----------------------+-----------------+-------------------+------------------------------+ * * Project Files: * * Format: * File or directory - Description - Source - License * * | lvgl_app.c/.h * | LVGL application layer * | Created for this project * | NXP proprietary license * | * | lv_conf.h * | Project-specific LVGL configuration * | Derived from the LVGL v9.4.0 configuration template * | MIT License * | * | lv_port.c/.h * | LVGL initialization and S32K3 port layer * | Created for this project * | NXP proprietary license * | * | main.c * | Application entry point and compile-time mode selection * | Created for this project * | NXP proprietary license * | * +---gui_guider * | +---custom * | | User callbacks and custom GUI logic * | | GUI Guider 2.0.1 output * | | NXP proprietary license * | | * | \---generated * | Generated screens, widgets and events * | GUI Guider 2.0.1 output * | NXP proprietary license * | * +---lcdc * | fsl_st7796s.c/.h * | ST7796S LCD controller driver * | NXP App Code Hub demo * | BSD-3-Clause License * | * +---lcd_par_s035 * | lcd_par_s035.c/.h * | LCD-PAR-S035 board and display integration * | Created for this project * | NXP proprietary license * | * | lcd_par_s035_config.h * | LCD-PAR-S035 project configuration * | Created for this project * | NXP proprietary license * | * +---lvgl * | \---src * | LVGL 9.4 graphics library * | LVGL release/v9.4 * | MIT License * | * +---platform * | display_compat.h * | MCUXpresso SDK and S32K3 RTD compatibility definitions * | Created for this project * | NXP proprietary license * | * | fsl_dbi.c/.h * | Generic display bus interface implementation * | NXP App Code Hub demo * | BSD-3-Clause License * | * | lcd_dbi_s32k3.c/.h * | S32K3 DBI transport implementation using LPSPI * | Created for this project * | NXP proprietary license * | * | lcd_platform.c/.h * | S32K344 board and platform abstraction * | Created for this project * | NXP proprietary license * | * \---touchpanel * fsl_gt911.c/.h * GT911 touchscreen controller driver * NXP App Code Hub demo * BSD-3-Clause License * * gt911_s32k3.c/.h * S32K3 adaptation using LPI2C and GPIO * Created for this project * NXP proprietary license * * ---------------------------------------------------------------------------- * Test Hardware: FRDM-A-S32K344, schematic revision B * MCU: S32K344 * Display: LCD-PAR-S035 with ST7796S controller * Touchscreen: GT911 capacitive touchscreen controller * Debugger: Lauterbach TRACE32 * Build Target: internal_FLASH
記事全体を表示
********************************************************************************* * Detailed Description: * * ADC hardware trigger demonstration using BCTU Trigger Mode on S32K358. * * An eMIOS1 Channel 23 reload event is used as a trigger source for the BCTU). * The BCTU initiates a hardware-triggered conversion of an ADC1 group containing * three channels. * * The result of the third ADC channel, connected to the on-board potentiometer * (ADCPOT0), is used to dynamically update the duty cycle of an * eMIOS Channel 5 PWM output. * * The PWM output drives the on-board LED, allowing the potentiometer position * to control LED brightness. * * Key Functionality: * - eMIOS-triggered BCTU operation. * - BCTU Trigger Mode configuration. * - ADC1 hardware-triggered group conversion. * - ADC notification callback processing. * - PWM duty-cycle update based on ADC result. * - LED brightness control using the potentiometer. * * ------------------------------------------------------------------------------ * Test HW: S32K3x8EVB-Q289 * MCU: S32K358 * IDE: EB Tresos 29.0.0 * RTD Release: S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_20250610 * Debugger: Lauterbach * Target: Internal_FLASH ******************************************************************************** * Revision History: * Ver Date Author Description of Changes * 1.0 02-10-2026 Petr Stancik Initial version ********************************************************************************
記事全体を表示
If your FRDM-A-S32K144 or FRDM-A-S32K144N is not detected during its first USB-C connection, this article explains the cause, how to verify OpenSDA/K20 status, and the steps to quickly enable normal operation.
記事全体を表示
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** For S32K312, please use this correct clock HSE to AIPS clock should be ½. Please make these changes in the below all example code clock setting. HSE clock to 60 MHZ.   S32K312 PIT BTCU ADC-1 BCTU_ADC_DATA_REG DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-ADC-1-BCTU-ADC-DATA-REG-DMA-DS3-5/ta-p/1787778 Example S32K312 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1789908 S32K312 UART Transmit & Receive Using DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1787799 S32K312 EIRQ Interrupt :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-EIRQ-Interrupt-DS3-5-RTD300/ta-p/1787860 S32K312 SPI Transmit & Receive Using DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SPI-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1787856 Example S32K31 SPI multiple packet Transmit & Receive : solution for DMA Cache issue :- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K31-SPI-multiple-packet-Transmit-amp-Receive-solution/ta-p/2130091 Example S32K312 SPI Transmit & Receive Using Polling DS3.5 RTD300 :-- Example S32K312 SPI Transmit & Receive Using Polling DS3.5 RTD300 - NXP Community Example S32K312 SPI Transmit & Receive Using Interrupt DS3.5 RTD300 :-- Example S32K312 SPI Transmit & Receive Using Interrupt DS3.5 RTD300 - NXP Community S32K312 CAN Transmit & Receive Using Polling mode :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-Polling-mode-DS3/ta-p/1789191 S32K312 CAN Transmit & Receive Using MB & FIFO DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-amp-FIFO-DMA/ta-p/1789196 S32K312 ADC :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-ADC-DS3-5-RTD300/ta-p/1789282 S32K312 Switch Debouncing :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Switch-Debouncing-DS3-5-RTD300/ta-p/1789290 S32K312 UART Freemaster :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Freemaster-DS3-5-RTD300/ta-p/1789306 S32K312 PIT BTCU parallel ADC FIFO DMA  :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1789908 S32K312 placing variables in DTCM & code in ITCM  :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-placing-variables-in-DCTM-amp-code-in-ICTM-DS3-5/ta-p/1790101 Example S32K312 Standby mode & Standby RAM and PAD keeping DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Standby-mode-amp-Standby-RAM-and-PAD-keeping-DS3/ta-p/1797713 Example S32K312 SWT DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SWT-DS3-5-RTD300/ta-p/1800559 Example S32K312 Printf Semihosting DS3.5 RTD300 :--- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Printf-Semihosting-DS3-5-RTD300/ta-p/1801354 Example S32K312 I2C Transmit & Receive Using DMA DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-I2C-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1801357 Example S32K312 HARDFAULT Handling Interrupt DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-RTD300/ta-p/1806259 Example S32K312 Bootloader to Application Jump DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Bootloader-to-Application-Jump-DS3-5-RTD300/ta-p/1809810 Example S32K312 PIT timer Toggle LED DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-timer-Toggle-LED-DS3-5-RTD300/ta-p/1809932 Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Interrupt-Handling-using-a-script-DS3/ta-p/1818507 Example S32K312 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Interrupt-DS3-5/ta-p/1818775 Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-Interrupt-DS3/ta-p/1818790 Example S32K312 STANDBY wake up using CAN-0-RX and GPIO Switch DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-CAN-0-RX-and-GPIO-Switch/ta-p/1891411 Example S32K312 STANDBY wake up using RTC DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-RTC-DS3-5-RTD300/ta-p/1930115 S32K312 : ADC Clock selection :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-ADC-Clock-selection/ta-p/1997759 Example IP S32K312 PWM ICU using EMIOS Custom IRQ DS3.5 RTD300 :-- Example IP S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community Example IP S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :-- Example IP S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community Example IP S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :-- Example IP S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community Example S32K312 Continuous SPI Transmit & Receive Using DMA DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Continuous-SPI-Transmit-amp-Receive-Using-DMA/ta-p/2024597 S32K312 : HSE Demo project :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-HSE-Demo-project/ta-p/2112562 S32K312 : FS26 Watchdog trigger using the SBC_FS26 CDD :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-FS26-Watchdog-trigger-using-the-SBC-FS26-CDD/ta-p/2161357
記事全体を表示
********************************************************************************************** * Detailed Description: * This example demonstrates the S32K344 internal flash UTest (User Test) sequence using the * Mem_43_INFLS AUTOSAR driver. It covers Array Integrity Check (MISR-based) and User Margin * Read Check, exercised over the full configured Block 3 address range (starting at * 0x00700000), as defined in the Mem_43_INFLS instance configuration. * * Setup: * ProgramBlock3() erases one sector (8 KB) at 0x00700000 and programs the first 512 bytes * with a sequential byte pattern (0x00..0xFF repeating). The remainder of the block * contains erased cells (0xFF). The UTest operations in Steps 1–3 are performed over the * entire Block 3 — not only the 512 programmed bytes. * * Step 1 — Array Integrity Check, Golden MISR Capture: * Runs the Array Integrity Check at NORMAL read margin using sequential addressing over * the full block. UM0–UM9 are seeded with 0xA5A5A5A5. MisrExpectedValues is intentionally * set to 0x0, so JOB_FAILED is the expected outcome. A custom wait function polls the AID * bit directly (without calling Mem_43_INFLS_MainFunction) so that the UM registers are * read before the driver clears them on job completion. The captured MISR becomes the * golden reference (goldenMisr) for Steps 2 and 3. * GETSTATEUTEST_JOB is called afterward to confirm no real hardware fault occurred * (ECC error, breakpoint, or suspension) during the capture run. * * Step 2 — Array Integrity Check, Verification Run: * Re-runs the identical Array Integrity Check over the full block (same seed, same * sequential addressing) with MisrExpectedValues = goldenMisr captured in Step 1. * JOB_OK confirms flash content is unchanged; JOB_FAILED indicates corruption. * GETSTATEUTEST_JOB is called to verify clean hardware completion. * * Step 3 — User Margin Read Check, Cell Margin Verification: * Re-reads the full block at a tighter read margin (C40_IP_MARGIN_LEVEL_PROGRAM). * Same seed and goldenMisr are used. If all cells retain sufficient voltage margin at * the tighter threshold, the MISR matches and JOB_OK is returned. A JOB_FAILED result * indicates one or more cells are degrading before they produce a detectable ECC error * under normal read conditions. * Note: both Array Integrity Check and User Margin Read Check must use sequential * addressing (C40_IP_SEQUENTIAL) to produce a comparable MISR signature. * * Results are accumulated in the utestResults structure (Utest_TestResultType), recording * both the MISR job outcome (Utest_JobResultType) and the hardware UTest state * (Utest_HwStateType) for each step independently. * * NOTE: This example must be executed from SRAM. The Mem_43_INFLS UTest operations * (Array Integrity Check, User Margin Read Check) place the internal flash controller * in UTest mode, during which the flash array is not available for normal read access. * ------------------------------------------------------------------------------------- * MCU: S32K344 * FX_OSC: 16MHz * RTD: S32K3_RTD_7_0_1_D2602_ASR_REL_4_9_REV_0000_20260206 * Debugger: Lauterbach Trace32 * Target: Internal_FLASH **********************************************************************************************
記事全体を表示