This example project will show user how to use and configure the basic functionalities of WKPU + SIUL2.
------------------------------------------------------------------------------ * Test HW: S32K312EVB-Q172 (SCH-50892 REV B) * MCU: S32K312 * IDE: S32DS v3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH ------------------------------------------------------------------------------
This example routine configures the WKPU unit for a GPIO interrupt wake-up and defines a section in linker file for 32KB of Standby RAM.
How to use Standby RAM?
Modify the linker file to separatethe 32KBstandby RAM(0x2040 0000 ~0x2040 8000) from int_sram memory region, and place standby .bss and .data or .text sections into the new region as well as adjust the link address symbols for customized initialization during startup.
Initialize the standby RAM only if it’s Power-On Reset.
Use key word attribute to define the variable/function in relevant memory section.
Counter variable is placed in standby ram section:
__attribute__ ((section (".sram_standby_bss"))) volatile int RunStandbyCounter0 = 0;
Linker file (.ld) must be modified accordingly. Standby sections and link address symbols must be placed:
MEMORY
{
int_pflash : ORIGIN = 0x00400000, LENGTH = 0x001D4000 /* 2048KB - 176KB (sBAF + HSE)*/
int_dflash : ORIGIN = 0x10000000, LENGTH = 0x00020000 /* 128KB */
int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00008000 /* 32KB */
int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x0000F000 /* 60KB */
int_stack_dtcm : ORIGIN = 0x2000F000, LENGTH = 0x00001000 /* 4KB */
int_standbysram : ORIGIN = 0x20400000, LENGTH = 0X00000100 /* standby ram 256B*/
int_sram : ORIGIN = 0x20400100, LENGTH = 0x00007E00 /* 32KB - 0x100, needs to include int_sram_fls_rsv*/
int_sram_fls_rsv : ORIGIN = 0x20407F00, LENGTH = 0x00000100
int_sram_no_cacheable : ORIGIN = 0x20408000, LENGTH = 0x00007F00 /* 32KB , needs to include int_sram_results */
int_sram_results : ORIGIN = 0x2040FF00, LENGTH = 0x00000100
int_sram_shareable : ORIGIN = 0x20410000, LENGTH = 0x00008000 /* 32KB */
ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */
}
...
.sram_standby (NOLOAD):
{
. += ALIGN(4);
*(.sram_standby_bss)
} > int_standbysram
...
__STANDBY_SRAM_START = ORIGIN(int_standbysram);
__STANDBY_SRAM_SIZE = LENGTH(int_standbysram);
Note 1: RAM ECC must be initialized only if it’s Power-on Reset.
Note 2: CM7 CPU D-Cache MUST be disabled to use the Standby RAM area. Or set the standby RAM(0x2040 0000 ~0x2040 8000) as non-cacheable in MPU configuration.
The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which:
Disables D-Cache.
Initializes RAM ECC (if reset was Power-on Reset).
Adds +1 to the standby counter placed in Standby RAM.
Switches core clock to FIRC.
Initializes the WKPU instance.
Configures WKPU42 (PTB19).
Enters standby.
If SW6 is pressed, MCU will perform a software reset through the Power_Ip_PerformReset() API. After wake-up, MCU resets and polls for SW5 to be pressed again.
In this application, LPUART6 (connected to USB OpenSDA interface) is enabled and will show previous reset reason (external reset, power-on reset, wakeup, functional reset), as well as printing standby counter between resets/standby cycles.
Connect a USB cable to J40, and open a Serial terminal on PC for the serial device with these settings:
9600 baud rate
No parity
One stop bit
No flow control
After either a SW reset, or a wake-up cycle, the standby counter will increase. If a destructive reset or Power-on Reset is asserted, the counter is reset.
Snag_147e19f.png
This example is provided as is with no guarantees and no support.
查看全文